Difference between revisions of "I2C i2c-tools"

[quality revision] [quality revision]
m
 
m
 

Template:ArticleMainWriter Template:ArticleApprovedVersion

1 Article purpose[edit]

This article aims to give some first information useful to start with the LinuxTemplate:Sup ® tool : I2C tools.

2 Introduction[edit]

i2c-tools is a complete user-space package that comes on top of I2C subsystem. It offers:

  • tools: a set of I2C programs that make it easy to debug I2C peripherals without having to write any code
  • libi2c: library to develop applications.

3 Tools list[edit]

4 Installation on your target[edit]

i2c-tools is embedded by default in OpenSTLinux distribution.

I2C tools are already bundled within OpenEmbedded. No installation is thus required.

Warning.png With OpenEmbedded Rocko (2.4.1), I2C tools revision is v3.1.2 and doesn't embed i2ctransfer.

i2ctransfer only comes starting v4.0 included into OpenEmbedded Thud (2.6.x)

5 Getting started[edit]

5.1 Devices detection[edit]

It can be very helpful to see which peripherals are connected to a specific I2C bus.
Check all instantiated I2C adapters:

Board $> i2cdetect -l

If I2C adapters are instantiated, the following return will be print :

i2c-0   i2c             ST I2C(0xAAAAAAA)                       I2C adapter
i2c-1   i2c             ST I2C(0xBBBBBBB)                       I2C adapter
i2c-2   i2c             ST I2C(0xCCCCCCC)                       I2C adapter
i2c-3   i2c             ST I2C(0xDDDDDDD)                       I2C adapter
i2c-4   i2c             ST I2C(0xEEEEEEE)                       I2C adapter
i2c-5   i2c             ST I2C(0xFFFFFFF)                       I2C adapter

Get the list of detected peripherals on the specific I2C bus:

Board $> i2cdetect -y <i2cbus number>

Board $> i2cdetect -y 3
     0  1  2  3  4  5  6  7  8  9  a  b  c  d  e  f
00:          -- -- -- -- -- -- -- -- -- -- -- -- -- 
10: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- 
20: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- 
30: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- 
40: -- -- -- -- -- -- -- -- -- -- UU -- -- -- -- -- 
50: UU -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- 
60: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- 
70: -- -- -- -- -- -- -- -- 

UU -> Probing was skipped, because this address is currently in use by a driver. This strongly suggests that there is a device at this address probed with a driver.

More information about i2cdectect i2cdetect[1]

5.2 Read register[edit]

Read all the registers from a peripheral:

Board $> i2cdump -f -y <i2cbus number> <peripheral address>

Board $> i2cdump -f -y 0 0x5f
No size specified (using byte-data access)
     0  1  2  3  4  5  6  7  8  9  a  b  c  d  e  f    0123456789abcdef
00: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 bc    ...............?
10: 3f 00 87 33 96 be ec a1 9e b2 fe 00 e8 01 80 82    ?.?3???????.????
20: 00 00 00 00 00 00 00 00 51 f2 ae 00 10 f3 c6 00    ........Q??.???.
30: 41 92 a0 0e 00 c4 ee ff 32 03 bf d3 ff ff d0 02    A???.??.2???..??
40: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................
50: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................
60: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................
70: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................
80: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 bc    ...............?
90: 3f 00 87 33 96 be ec a1 9e b2 fe 00 e8 01 80 82    ?.?3???????.????
a0: 00 00 00 00 00 00 00 00 51 f2 ae 00 10 f3 c6 00    ........Q??.???.
b0: 41 92 a0 0e 00 c4 ee ff 32 03 bf d3 ff ff d0 02    A???.??.2???..??
c0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................
d0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................
e0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................
f0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................

More information about i2cdump[2].

To read directly one register, use i2cget[3]:

Board $> i2cget -f -y <i2cbus number> <peripheral address>

Example: read register 0x0f of the peripheral at address 0x5f on bus 0:

Board $> i2cget -f -y 0 0x5f 0x0f
0xbc

5.3 Write register[edit]

To write directly a register, use i2cset[4]:

Board $> i2cset -f -y <i2cbus number> <peripheral address> <value>

Example: write 0xac in register 0x0f of the peripheral at address 0x5f on the bus 0:

Board $> i2cset -f -y 0 0x5f 0x0f 0xac

Info.png A write can fail if the register is in read only mode.

5.4 Auto-increment devices[edit]

Even if not part of the I2C standard, it is common to find an automatic incrementation feature on I2C devices, in particular those dealing with large set of registers (typically I2C RAM or EEPROM).

Such devices automatically increment an internal address pointer at each read or write operation, so when several read commands are issued at the same address, the value returned at each read may be different each time.

Example Here are some examples with WM8994 audio device, reading codec device on STM32MP157x-EV1 Evaluation board:

Warning.png First start an audio playback to power-up audio codec device (refer to How to play audio)

Read WM8994 software reset register at address "0x1a000x0000":

Board $> i2cget -y 0 0x1a0x1b 0x00 w
0x9489

0x9489 reads read as a word, understand 0x89 0x94 which is the device id (WM8994) and is indeed the content of the software reset register.

If the same command is repeated again:

Board $> i2cget -y 0 0x1a0x1b 0x00 w
0x0000
Board $> i2cget -y 0 0x1a0x1b 0x00 w
0x0060

different values are returned, that do not correspond to the software reset register anymore "0x1a000x0000", but correspond successively to registers "0x1a010x0001" and "0x1a020x0002".

To reset the internal address counter, just write a value at the targeted register address:

Board $> i2cset -y 0 0x1a0x1b 0x00 0x00

Then subsequent read will restart at this address:

Board $> i2cget -y 0 0x1a0x1b 0x00 w
0x9489

Please note that the auto-increment mode may usually be disabled by writing into a device specific configuration register (refer to the device datasheet for details).

5.5 I2C transfer[edit]

Warning.png With OpenEmbedded Rocko (2.4.1), I2C tools revision is v3.1.2 and doesn't embed i2ctransfer.

i2ctransfer becomes available starting with I2C tools revision v4.0 included into OpenEmbedded Thud (2.6.x)

This is a user-space program used to send concatenated I2C messages.

Most devices require a write access to a register before being able to read. i2ctransfer[5] offers a way to combine write and read procedures. It also handles multiple bytes write/read in a single command with an additional suffix.

To read a set of bytes:

Board $> i2ctransfer -f -y <i2cbus number> r<number of bytes>@<peripheral address>

To write a set of bytes:

Board $> i2ctransfer -f -y <i2cbus number> w<number of bytes>@<peripheral address> <byte value 1> <byte value 2> ... <byte value n>

To write a set of bytes then read a set of bytes:

Board $> i2ctransfer -f -y <i2cbus number> w<number of bytes to write>@<peripheral address> <byte value 1> <byte value 2> ... <byte value n> r<number of bytes to read>


Example (bus 0, read 8 bytes at offset 0x64 from EEPROM at 0x50)

Board $> i2ctransfer 0 w1@0x50 0x64 r8

"w1" for "write 1 byte" (the 0x64 offset), "r8" for "read 8 bytes"

Example (same EEPROM, at offset 0x42 write 0xff 0xfe ... 0xf0)

Board $> i2ctransfer 0 w17@0x50 0x42 0xff-

"w17" for "write 17 bytes", first 0x42 byte for the offset, and 0xff- for the 16 subsequent bytes ("-" for auto value decrease starting from 0xff).

See following chapter for 16 bits addressing devices handling.

5.6 16 bits devices handling[edit]

The I2C standard protocol supports natively 7 bits of address (or 10 bits of address in extended mode) followed by 8 bits of data.

However some I2C devices embed 16-bit data registers with internal 16-bit address space. Here is how the i2c-tool allows to drive such devices.

  • To read a 16 bits value, add "w" for "word" at the end of command:
Board $> i2cget -f -y <i2cbus number> <peripheral address> <address> w

Please note that <address> is 8-bit wide, while the returned data is 16-bit wide. The interpretation of <address> is device dependent (One possible interpretation is that <address> drives the 8 MSB bits of the 16-bit address while the 8 LSB bits are set to 0).

  • To write a 16 bits value specifying the 16 bits address, send both the address and the data as a set of bytes in a single "I2C block write" by adding "i" at the end of i2cset[4] command:
Board $> i2cset -f -y <i2cbus number> <peripheral address> <MSB address> <LSB address> <MSB value> <LSB value> i


Here are some examples with WM8994 audio codec device on STM32MP157x-EV1 Evaluation board:

Warning.png First start an audio playback to power-up audio codec device (refer to How to play audio)
  • Read the device id from register "Software Reset" at address 0x0000:
Board $> i2cget -y 0 0x1a0x1b 0x0 w
0x9489

"w" stands for "word" access. Since the word is read in little endian and the device is big endian, we have to reverse the endianness.

The returned word 0x9489 should be interpreted as 0x89 0x94 which is the indeed the (WM8994) device ID.


  • Update value of register "AIF1 Control" at address 0x0300:
Board $> i2cget -y 0 0x1a0x1b 0x3 w
0x5040

Current value is 0x4050.

Let's assume the AIF1ADC_TDM pin needs to be put in tristate, this is done by settings bit 13, hence by writing 0x6050:

Board $> i2cset -y 0 0x1a0x1b 0x03 0x00 0x60 0x50 i
Board $> i2cget -y 0 0x1a0x1b 0x3 w
0x5060

The "AIF1 Control" register value has been updated to 0x6050 as expected.

5.6 I2C transfer[edit]

Warning.png With OpenEmbedded Rocko (2.4.1), I2C tools revision is v3.1.2 and doesn't embed i2ctransfer.

i2ctransfer becomes available starting with I2C tools revision v4.0 included into OpenEmbedded Thud (2.6.x)

This is a user-space program used to send concatenated I2C messages.

Most devices require a write access to a register before being able to read. i2ctransfer[5] offers a way to combine read and write procedures. It also handles multiple bytes read/write in a single command with an additional suffix.

Example (bus 0, read 8 byte at offset 0x64 from EEPROM at 0x50)


Doing the same with I2C transfer is far more simple:

Board $> i2ctransfer -f -y 0 w1@0x50w4@0x1b 0x640x03 r8

Example (same EEPROM, at offset 0x42 write 0xff 0xfe ... 0xf0)

Board $> i2ctransfer 0 w17@0x50 0x42 0xff-

0x00 0x60 0x50 -r2
Board $> 0x60 0x50

"w4" for "write 4 bytes": the first 2 bytes for address (0x0300), the next 2 bytes for register address (0x6050)

"r2" for "read 2 bytes": the word register value

6 References[edit]

All these tools (i2cset, i2cget, i2cdump, i2cdectect and i2ctransfer) are available in this GIT:

git clone git://git.kernel.org/pub/scm/utils/i2c-tools/i2c-tools.git or 
git clone https://git.kernel.org/pub/scm/utils/i2c-tools/i2c-tools.git

Source code browsing I2C Tools Code



<noinclude>

{{ArticleMainWriter | Pierre-YvesM}}
{{ ArticleApprovedVersion|Pierre-YvesM| FabriceG(8 Oct'18), HuguesF(4 Oct'2018) |No previous approved version| BrunoB - 19Oct'18 - 8859 |  26 Oct'2018 }}
[[Category:I2C|Category:Tools]]</noinclude>

== Article purpose==
This article aims to give some first information useful to start with the Linux{{<sup>|&reg;}}</sup> tool : I2C tools.

==Introduction==
[[I2C overview#i2c-tools_package | i2c-tools]] is a complete user-space package that comes on top of [[I2C overview | I2C subsystem]]. It offers:
* tools: a set of I2C programs that make it easy to debug I2C peripherals without having to write any code
* libi2c: library to develop applications.

== Tools list==
* i2cdetect<ref name="i2cdectecti2cdetect">https://www.mankier.com/8/i2cdetect</ref>

* i2cdump<ref name="i2cdump">https://www.mankier.com/8/i2cdump</ref>

* i2cget<ref name="i2cget">https://www.mankier.com/8/i2cget</ref>

* i2cset<ref name="i2cset">https://www.mankier.com/8/i2cset</ref>

* i2ctransfer<ref name="i2ctransfer">https://www.mankier.com/8/i2ctransfer</ref>


==Installation on your target==
''i2c-tools'' is embedded by default in [[OpenSTLinux distribution]].

[[I2C_i2c-tools | I2C tools]] are already bundled within [[OpenSTLinux distribution | OpenEmbedded]]. No installation is thus required.

{{Warning| '''With''' OpenEmbedded Rocko (2.4.1)''', I2C tools revision is v3.1.2 and doesn't embed '''i2ctransfer.<br>

'''i2ctransfer''' only comes starting v4.0 included into '''OpenEmbedded  Thud (2.6.x)'''}}

==Getting started ==
=== Devices detection ===
It can be very helpful to see which peripherals are connected to a specific I2C bus.<br />

Check all instantiated I2C adapters:
 {{Board$}} i2cdetect -l
If I2C adapters are instantiated, the following return will be print :<pre>

i2c-0   i2c             ST I2C(0xAAAAAAA)                       I2C adapter
i2c-1   i2c             ST I2C(0xBBBBBBB)                       I2C adapter
i2c-2   i2c             ST I2C(0xCCCCCCC)                       I2C adapter
i2c-3   i2c             ST I2C(0xDDDDDDD)                       I2C adapter
i2c-4   i2c             ST I2C(0xEEEEEEE)                       I2C adapter
i2c-5   i2c             ST I2C(0xFFFFFFF)                       I2C adapter</pre>

Get the list of detected peripherals on the specific I2C bus:
 {{Board$}} i2cdetect -y {{highlight|'''<i2cbus number>'''}}

 {{Board$}} i2cdetect -y 3
      0  1  2  3  4  5  6  7  8  9  a  b  c  d  e  f
 00:          -- -- -- -- -- -- -- -- -- -- -- -- -- 
 10: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- 
 20: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- 
 30: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- 
 40: -- -- -- -- -- -- -- -- -- -- '''UU''' -- -- -- -- -- 
 50: '''UU''' -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- 
 60: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- 
 70: -- -- -- -- -- -- -- -- 
'''UU''' -> Probing was skipped, because this address is currently in use by a driver. This strongly suggests that there is a device at this address probed with a driver.

More information about '''i2cdectecti2cdetect'''<ref name="i2cdectecti2cdetect">https://www.mankier.com/8/i2cdetect</ref>


=== Read register ===
Read all the registers from a peripheral:
 {{Board$}} i2cdump -f -y {{highlight|'''<i2cbus number> <peripheral address>'''}}

 {{Board$}} i2cdump -f -y 0 0x5f
 No size specified (using byte-data access)
      0  1  2  3  4  5  6  7  8  9  a  b  c  d  e  f    0123456789abcdef
 00: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 bc    ...............?
 10: 3f 00 87 33 96 be ec a1 9e b2 fe 00 e8 01 80 82    ?.?3???????.????
 20: 00 00 00 00 00 00 00 00 51 f2 ae 00 10 f3 c6 00    ........Q??.???.
 30: 41 92 a0 0e 00 c4 ee ff 32 03 bf d3 ff ff d0 02    A???.??.2???..??
 40: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................
 50: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................
 60: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................
 70: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................
 80: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 bc    ...............?
 90: 3f 00 87 33 96 be ec a1 9e b2 fe 00 e8 01 80 82    ?.?3???????.????
 a0: 00 00 00 00 00 00 00 00 51 f2 ae 00 10 f3 c6 00    ........Q??.???.
 b0: 41 92 a0 0e 00 c4 ee ff 32 03 bf d3 ff ff d0 02    A???.??.2???..??
 c0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................
 d0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................
 e0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................
 f0: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00    ................
More information about '''i2cdump'''<ref name="i2cdump">https://www.mankier.com/8/i2cdump</ref>.

To read directly one register, use '''i2cget'''<ref name="i2cget">https://www.mankier.com/8/i2cget</ref>:
 {{Board$}} i2cget -f -y {{highlight|'''<i2cbus number> <peripheral address>'''}}

Example: read register 0x0f of the peripheral at address 0x5f on bus 0:
 {{Board$}} i2cget -f -y 0 0x5f 0x0f
 0xbc

=== Write register ===
To write directly a register, use '''i2cset'''<ref name="i2cset">https://www.mankier.com/8/i2cset</ref>:
 {{Board$}} i2cset -f -y {{highlight|'''<i2cbus number> <peripheral address> <value>'''}}

Example: write 0xac in register 0x0f of the peripheral at address 0x5f on the bus 0:
 {{Board$}} i2cset -f -y 0 0x5f 0x0f 0xac
 {{Info|A write can fail if the register is in read only mode.}}

=== Auto-increment devices ===
Even if not part of the I2C standard, it is common to find an automatic incrementation feature on I2C devices, in particular those dealing with large set of registers (typically I2C RAM or EEPROM).

Such devices automatically increment an internal address pointer at each read or write operation, so when several read commands are issued '''at the same address''', the value returned at each read may be different each time.
Example Here are some examples with WM8994 audio codec device, reading  on [[STM32MP157x-EV1 - hardware description|STM32MP157x-EV1 Evaluation board]]:
{{Warning|First start an audio playback to power-up audio codec device (refer to [[How_to_play_audio|How to play audio]])}}

Read WM8994 software reset register at address "0x1a000x0000":
 {{Board$}} i2cget -y 0 0x1a0x1b 0x00 w
 0x9489
0x9489 readsread as a word, understand 0x89 0x94 which is the device id (WM8994) and is indeed the content of the software reset register.

If the same command is repeated again:
 {{Board$}} i2cget -y 0 0x1a0x1b 0x00 w
 0x0000
 {{Board$}} i2cget -y 0 0x1a0x1b 0x00 w
 0x0060
different values are returned, that do not correspond to the software reset register anymore "0x1a000x0000", but correspond successively to registers "0x1a010x0001" and "0x1a020x0002".

To reset the internal address counter, just write a value at the targeted register address:
 {{Board$}} i2cset -y 0 0x1a0x1b 0x00 0x00
Then subsequent read will restart at this address:
 {{Board$}} i2cget -y 0 0x1a0x1b 0x00 w
 0x9489

Please note that the auto-increment mode may usually be disabled by writing into a device specific configuration register (refer to the device datasheet for details).

=== 16 bits devices handling ===I2C transfer ===
{{Warning| '''With''' OpenEmbedded Rocko (2.4.1)''', I2C tools revision is v3.1.2 and doesn't embed '''i2ctransfer.<br>

'''i2ctransfer''' becomes available starting with I2C tools revision v4.0 included into '''OpenEmbedded  Thud (2.6.x)'''}}

This is a user-space program used to send concatenated I2C messages.

Most devices require a write access to a register before being able to read. '''i2ctransfer'''<ref name="i2ctransfer">https://www.mankier.com/8/i2ctransfer</ref> offers a way to combine write and read procedures. It also handles multiple bytes write/read in a single command with an additional suffix.

To read a set of bytes:
 {{Board$}} i2ctransfer -f -y {{highlight|'''<i2cbus number> r<number of bytes>@<peripheral address>'''}}

To write a set of bytes:
 {{Board$}} i2ctransfer -f -y {{highlight|'''<i2cbus number> w<number of bytes>@<peripheral address> <byte value 1> <byte value 2> ... <byte value n>'''}}

To write a set of bytes then read a set of bytes:
 {{Board$}} i2ctransfer -f -y {{highlight|'''<i2cbus number> w<number of bytes to write>@<peripheral address> <byte value 1> <byte value 2> ... <byte value n> r<number of bytes to read>'''}}

Example (bus 0, read 8 bytes at offset 0x64 from EEPROM at 0x50)
 {{Board$}} i2ctransfer 0 w1@0x50 0x64 r8
"w1" for "write 1 byte" (the 0x64 offset), "r8" for "read 8 bytes"

Example (same EEPROM, at offset 0x42 write 0xff 0xfe ... 0xf0)
 {{Board$}} i2ctransfer 0 w17@0x50 0x42 0xff-
"w17" for "write 17 bytes", first 0x42 byte for the offset, and 0xff- for the 16 subsequent bytes ("-" for auto value decrease starting from 0xff).

{{highlight|'''See following chapter for 16 bits addressing devices handling.'''}}

=== 16 bits devices handling ===The I2C standard protocol supports natively 7 bits of address (or 10 bits of address in extended mode) followed by 8 bits of data.

However some I2C devices embed 16-bit data registers with internal 16-bit address space. Here is how the i2c-tool allows to drive such devices.

* To read a 16 bits value, add "w{{highlight|'''w'''}}" for "word" at the end of command:
 {{Board$}} i2cget -f -y <i2cbus number> <peripheral address> <address> {{highlight|'''w'''}}
Please note that <address> is 8-bit wide, while the returned data is 16-bit wide. The '''interpretation of <address> is device dependent''' (One possible interpretation is that <address> drives the 8 MSB bits of the 16-bit address while the 8 LSB bits are set to 0). 

* To write a 16 bits value specifying the 16 bits address, send both the address and the data as a set of bytes in a single "I2C block write" by adding "i{{highlight|'''i'''}}" at the end of '''i2cset'''<ref name="i2cset">https://www.mankier.com/8/i2cset</ref> command:
 {{Board$}} i2cset -f -y <i2cbus number> <peripheral address> <MSB address> <LSB address> <MSB value> <LSB value> {{highlight|'''i'''}}

Here are some examples with WM8994 audio codec device:
 on [[STM32MP157x-EV1 - hardware description|STM32MP157x-EV1 Evaluation board]]:
{{Warning|First start an audio playback to power-up audio codec device (refer to [[How_to_play_audio|How to play audio]])}}
* Read the device id from register "Software Reset" at address 0x0000:
 {{Board$}} i2cget -y 0 0x1a0x1b 0x0 w
 0x9489
"w" stands for "word" access. Since the word is read in '''little endian''' and the device is big endian, we have to reverse the endianness. 

The returned word 0x9489 should be interpreted as 0x89 0x94 which is the indeed the (WM8994) device ID.

* Update value of register "AIF1 Control" at address 0x0300:
 {{Board$}} i2cget -y 0 0x1a0x1b 0x3 w
 0x5040
Current value is 0x4050.

Let's assume the AIF1ADC_TDM pin needs to be put in tristate, this is done by settings bit 13, hence by writing 0x6050:
 {{Board$}} i2cset -y 0 0x1a0x1b 0x03 0x00 0x60 0x50 i
 {{Board$}} i2cget -y 0 0x1a0x1b 0x3 w
 0x5060
The "AIF1 Control" register value has been updated to 0x6050 as expected.
=== I2C transfer ===
{{Warning| '''With''' OpenEmbedded Rocko (2.4.1)''', I2C tools revision is v3.1.2 and doesn't embed '''i2ctransfer.<br>

'''i2ctransfer''' becomes available starting with I2C tools revision v4.0 included into '''OpenEmbedded  Thud (2.6.x)'''}}

This is a user-space program used to send concatenated I2C messages.

Most devices require a write access to a register before being able to read. '''i2ctransfer'''<ref name="i2ctransfer">https://www.mankier.com/8/i2ctransfer</ref> offers a way to combine read and write procedures. It also handles multiple bytes read/write in a single command with an additional suffix.

Example (bus 0, read 8 byte at offset 0x64 from EEPROM at 0x50)
 {{Board$}} i2ctransfer 0 w1@0x50 0x64 r8
Example (same EEPROM, at offset 0x42 write 0xff 0xfe ... 0xf0)
 {{Board$}} i2ctransfer 0 w17@0x50 0x42 0xff-


{{highlight|'''Doing the same with [[#I2C transfer|I2C transfer]] is far more simple:'''}}
 {{Board$}} i2ctransfer -f -y 0 w4@0x1b 0x03 0x00 0x60 0x50 -r2
 {{Board$}} 0x60 0x50
"w4" for "write 4 bytes": the first 2 bytes for address (0x0300), the next 2 bytes for register address (0x6050)

"r2" for "read 2 bytes": the word register value
== References ==

All these tools ({{Highlight|i2cset}}, {{Highlight|i2cget}}, {{Highlight|i2cdump}}, {{Highlight|i2cdectect}} and {{Highlight|i2ctransfer}}) are available in this GIT:
 git clone git://git.kernel.org/pub/scm/utils/i2c-tools/i2c-tools.git or 
 git clone https://git.kernel.org/pub/scm/utils/i2c-tools/i2c-tools.git
Source code browsing [https://git.kernel.org/pub/scm/utils/i2c-tools/i2c-tools.git/tree/  I2C Tools Code]
<references/>

<noinclude>

{{PublicationRequestId | 8859 | 2018-10-19 | BrunoB}}
[[Category:I2C|Category:Tools]]</noinclude>
(17 intermediate revisions by 2 users not shown)
Line 1: Line 1:
<noinclude>
 
{{ArticleMainWriter | Pierre-YvesM}}
 
{{ ArticleApprovedVersion|Pierre-YvesM| FabriceG(8 Oct'18), HuguesF(4 Oct'2018) |No previous approved version| BrunoB - 19Oct'18 - 8859 |  26 Oct'2018 }}
 
[[Category:I2C|Category:Tools]]
 
</noinclude>
 
 
 
== Article purpose==
 
== Article purpose==
This article aims to give some first information useful to start with the Linux{{sup|&reg;}} tool : I2C tools.
+
This article aims to give some first information useful to start with the Linux<sup>&reg;</sup> tool : I2C tools.
   
 
==Introduction==
 
==Introduction==
Line 14: Line 8:
   
 
== Tools list==
 
== Tools list==
* i2cdetect<ref name="i2cdectect">https://www.mankier.com/8/i2cdetect</ref>
+
* i2cdetect<ref name="i2cdetect">https://www.mankier.com/8/i2cdetect</ref>
 
* i2cdump<ref name="i2cdump">https://www.mankier.com/8/i2cdump</ref>
 
* i2cdump<ref name="i2cdump">https://www.mankier.com/8/i2cdump</ref>
 
* i2cget<ref name="i2cget">https://www.mankier.com/8/i2cget</ref>
 
* i2cget<ref name="i2cget">https://www.mankier.com/8/i2cget</ref>
Line 57: Line 51:
 
'''UU''' -> Probing was skipped, because this address is currently in use by a driver. This strongly suggests that there is a device at this address probed with a driver.
 
'''UU''' -> Probing was skipped, because this address is currently in use by a driver. This strongly suggests that there is a device at this address probed with a driver.
   
More information about '''i2cdectect'''<ref name="i2cdectect">https://www.mankier.com/8/i2cdetect</ref>
+
More information about '''i2cdetect'''<ref name="i2cdetect">https://www.mankier.com/8/i2cdetect</ref>
   
 
=== Read register ===
 
=== Read register ===
Line 104: Line 98:
 
Such devices automatically increment an internal address pointer at each read or write operation, so when several read commands are issued '''at the same address''', the value returned at each read may be different each time.
 
Such devices automatically increment an internal address pointer at each read or write operation, so when several read commands are issued '''at the same address''', the value returned at each read may be different each time.
   
Example with WM8994 audio device, reading software reset register at address "0x1a00":
+
Here are some examples with WM8994 audio codec device on [[STM32MP157x-EV1 - hardware description|STM32MP157x-EV1 Evaluation board]]:
  {{Board$}} i2cget -y 0 0x1a 0x00 w
+
{{Warning|First start an audio playback to power-up audio codec device (refer to [[How_to_play_audio|How to play audio]])}}
  +
 
  +
Read WM8994 software reset register at address "0x0000":
  +
  {{Board$}} i2cget -y 0 0x1b 0x00 w
 
  0x9489
 
  0x9489
0x9489 reads as a word, understand 0x89 0x94 which is the device id (WM8994) and is indeed the content of the software reset register.
+
0x9489 read as a word, understand 0x89 0x94 which is the device id (WM8994) and is indeed the content of the software reset register.
   
 
If the same command is repeated again:
 
If the same command is repeated again:
  {{Board$}} i2cget -y 0 0x1a 0x00 w
+
  {{Board$}} i2cget -y 0 0x1b 0x00 w
 
  0x0000
 
  0x0000
  {{Board$}} i2cget -y 0 0x1a 0x00 w
+
  {{Board$}} i2cget -y 0 0x1b 0x00 w
 
  0x0060
 
  0x0060
different values are returned, that do not correspond to the software reset register anymore "0x1a00", but correspond successively to registers "0x1a01" and "0x1a02".
+
different values are returned, that do not correspond to the software reset register anymore "0x0000", but correspond successively to registers "0x0001" and "0x0002".
   
 
To reset the internal address counter, just write a value at the targeted register address:
 
To reset the internal address counter, just write a value at the targeted register address:
  {{Board$}} i2cset -y 0 0x1a 0x00 0x00
+
  {{Board$}} i2cset -y 0 0x1b 0x00 0x00
 
Then subsequent read will restart at this address:
 
Then subsequent read will restart at this address:
  {{Board$}} i2cget -y 0 0x1a 0x00 w
+
  {{Board$}} i2cget -y 0 0x1b 0x00 w
 
  0x9489
 
  0x9489
   
Please note that the auto-increment mode may usually be disabled by writing into a device configuration register (refer to the device datasheet for details).
+
Please note that the auto-increment mode may usually be disabled by writing into a device specific configuration register (refer to the device datasheet for details).
  +
 
  +
=== I2C transfer ===
  +
{{Warning| '''With''' OpenEmbedded Rocko (2.4.1)''', I2C tools revision is v3.1.2 and doesn't embed '''i2ctransfer.<br>
  +
'''i2ctransfer''' becomes available starting with I2C tools revision v4.0 included into '''OpenEmbedded  Thud (2.6.x)'''}}
  +
 
  +
This is a user-space program used to send concatenated I2C messages.
  +
 
  +
Most devices require a write access to a register before being able to read. '''i2ctransfer'''<ref name="i2ctransfer">https://www.mankier.com/8/i2ctransfer</ref> offers a way to combine write and read procedures. It also handles multiple bytes write/read in a single command with an additional suffix.
  +
 
  +
To read a set of bytes:
  +
{{Board$}} i2ctransfer -f -y {{highlight|'''<i2cbus number> r<number of bytes>@<peripheral address>'''}}
  +
 
  +
To write a set of bytes:
  +
{{Board$}} i2ctransfer -f -y {{highlight|'''<i2cbus number> w<number of bytes>@<peripheral address> <byte value 1> <byte value 2> ... <byte value n>'''}}
  +
 
  +
To write a set of bytes then read a set of bytes:
  +
{{Board$}} i2ctransfer -f -y {{highlight|'''<i2cbus number> w<number of bytes to write>@<peripheral address> <byte value 1> <byte value 2> ... <byte value n> r<number of bytes to read>'''}}
  +
 
  +
 
  +
Example (bus 0, read 8 bytes at offset 0x64 from EEPROM at 0x50)
  +
{{Board$}} i2ctransfer 0 w1@0x50 0x64 r8
  +
"w1" for "write 1 byte" (the 0x64 offset), "r8" for "read 8 bytes"
  +
 
  +
Example (same EEPROM, at offset 0x42 write 0xff 0xfe ... 0xf0)
  +
{{Board$}} i2ctransfer 0 w17@0x50 0x42 0xff-
  +
"w17" for "write 17 bytes", first 0x42 byte for the offset, and 0xff- for the 16 subsequent bytes ("-" for auto value decrease starting from 0xff).
  +
 
  +
{{highlight|'''See following chapter for 16 bits addressing devices handling.'''}}
   
 
=== 16 bits devices handling ===
 
=== 16 bits devices handling ===
Line 129: Line 154:
 
However some I2C devices embed 16-bit data registers with internal 16-bit address space. Here is how the i2c-tool allows to drive such devices.
 
However some I2C devices embed 16-bit data registers with internal 16-bit address space. Here is how the i2c-tool allows to drive such devices.
   
* To read a 16 bits value, add "w" for "word" at the end of command:
+
* To read a 16 bits value, add "{{highlight|'''w'''}}" for "word" at the end of command:
  {{Board$}} i2cget -f -y <i2cbus number> <address> {{highlight|'''w'''}}
+
  {{Board$}} i2cget -f -y <i2cbus number> <peripheral address> <address> {{highlight|'''w'''}}
 
Please note that <address> is 8-bit wide, while the returned data is 16-bit wide. The '''interpretation of <address> is device dependent''' (One possible interpretation is that <address> drives the 8 MSB bits of the 16-bit address while the 8 LSB bits are set to 0).  
 
Please note that <address> is 8-bit wide, while the returned data is 16-bit wide. The '''interpretation of <address> is device dependent''' (One possible interpretation is that <address> drives the 8 MSB bits of the 16-bit address while the 8 LSB bits are set to 0).  
   
* To write a 16 bits value specifying the 16 bits address, send both the address and the data as a set of bytes in a single "I2C block write" by adding "i" at the end of '''i2cset'''<ref name="i2cset">https://www.mankier.com/8/i2cset</ref> command:
+
* To write a 16 bits value specifying the 16 bits address, send both the address and the data as a set of bytes in a single "I2C block write" by adding "{{highlight|'''i'''}}" at the end of '''i2cset'''<ref name="i2cset">https://www.mankier.com/8/i2cset</ref> command:
  {{Board$}} i2cset -f -y <i2cbus number> <MSB address> <LSB address> <MSB value> <LSB value> {{highlight|'''i'''}}
+
  {{Board$}} i2cset -f -y <i2cbus number> <peripheral address> <MSB address> <LSB address> <MSB value> <LSB value> {{highlight|'''i'''}}
   
   
Here are some examples with WM8994 audio codec device:
+
Here are some examples with WM8994 audio codec device on [[STM32MP157x-EV1 - hardware description|STM32MP157x-EV1 Evaluation board]]:
  +
{{Warning|First start an audio playback to power-up audio codec device (refer to [[How_to_play_audio|How to play audio]])}}
   
 
* Read the device id from register "Software Reset" at address 0x0000:
 
* Read the device id from register "Software Reset" at address 0x0000:
  {{Board$}} i2cget -y 0 0x1a 0x0 w
+
  {{Board$}} i2cget -y 0 0x1b 0x0 w
 
  0x9489
 
  0x9489
 
"w" stands for "word" access. Since the word is read in '''little endian''' and the device is big endian, we have to reverse the endianness.  
 
"w" stands for "word" access. Since the word is read in '''little endian''' and the device is big endian, we have to reverse the endianness.  
Line 148: Line 174:
   
 
* Update value of register "AIF1 Control" at address 0x0300:
 
* Update value of register "AIF1 Control" at address 0x0300:
  {{Board$}} i2cget -y 0 0x1a 0x3 w
+
  {{Board$}} i2cget -y 0 0x1b 0x3 w
 
  0x5040
 
  0x5040
 
Current value is 0x4050.
 
Current value is 0x4050.
   
 
Let's assume the AIF1ADC_TDM pin needs to be put in tristate, this is done by settings bit 13, hence by writing 0x6050:
 
Let's assume the AIF1ADC_TDM pin needs to be put in tristate, this is done by settings bit 13, hence by writing 0x6050:
  {{Board$}} i2cset -y 0 0x1a 0x03 0x00 0x60 0x50 i
+
  {{Board$}} i2cset -y 0 0x1b 0x03 0x00 0x60 0x50 i
  {{Board$}} i2cget -y 0 0x1a 0x3 w
+
  {{Board$}} i2cget -y 0 0x1b 0x3 w
 
  0x5060
 
  0x5060
 
The "AIF1 Control" register value has been updated to 0x6050 as expected.
 
The "AIF1 Control" register value has been updated to 0x6050 as expected.
   
=== I2C transfer ===
 
{{Warning| '''With''' OpenEmbedded Rocko (2.4.1)''', I2C tools revision is v3.1.2 and doesn't embed '''i2ctransfer.<br>
 
'''i2ctransfer''' becomes available starting with I2C tools revision v4.0 included into '''OpenEmbedded  Thud (2.6.x)'''}}
 
   
This is a user-space program used to send concatenated I2C messages.
+
{{highlight|'''Doing the same with [[#I2C transfer|I2C transfer]] is far more simple:'''}}
  +
{{Board$}} i2ctransfer -f -y 0 w4@0x1b 0x03 0x00 0x60 0x50 -r2
  +
{{Board$}} 0x60 0x50
  +
"w4" for "write 4 bytes": the first 2 bytes for address (0x0300), the next 2 bytes for register address (0x6050)
   
Most devices require a write access to a register before being able to read. '''i2ctransfer'''<ref name="i2ctransfer">https://www.mankier.com/8/i2ctransfer</ref> offers a way to combine read and write procedures. It also handles multiple bytes read/write in a single command with an additional suffix.
+
"r2" for "read 2 bytes": the word register value
 
 
Example (bus 0, read 8 byte at offset 0x64 from EEPROM at 0x50)
 
{{Board$}} i2ctransfer 0 w1@0x50 0x64 r8
 
Example (same EEPROM, at offset 0x42 write 0xff 0xfe ... 0xf0)
 
{{Board$}} i2ctransfer 0 w17@0x50 0x42 0xff-
 
   
 
== References ==
 
== References ==
Line 179: Line 200:
   
 
<references/>
 
<references/>
  +
  +
<noinclude>
  +
{{PublicationRequestId | 8859 | 2018-10-19 | BrunoB}}
  +
[[Category:I2C|Category:Tools]]
  +
</noinclude>