- Last edited one year ago ago
How to use TTY with User Terminal
Template:ArticleMainWriter Template:ArticleApprovedVersion
Contents
- 1 Purpose
- 2 Print the file name of the terminal connected to standard input (with tty tool)
- 3 Change serial port configuration (with stty tool)
- 4 Send / Receive data (with stty, minicom, echo and cat tools)
- 5 Identify processes using a tty serial device (with fuser tool)
- 6 Link a tty serial device with a line discipline (with ldattach tool)
- 7 File transfer over serial console
- 8 References
1 Purpose[edit]
This article describes how to use TTY with a user terminal. The TTY overview is described in Serial TTY overview article.
The use case of the following examples is a data transfer between a STM32 MPU board and PC, over a USB to a RS232 adapter cable.
The setup of this use case is described in details in the How to get Terminal article.
For the following examples:
- uart4 is activated by default (for the Linux console)
- usart3 is enabled by device tree
- The usart3 pins are connected to a RS232 card
- The RS232 card is connected to the PC over the USB to RS232 adapter cable.
Note: Some TTY tools are used in this article. A list of TTY tools is defined a dedicated article [TTY Tools ].
2 Print the file name of the terminal connected to standard input (with tty tool)[edit]
tty /dev/ttySTM0 /* the console is connected to uart4, aka ttySTM0 */
3 Change serial port configuration (with stty tool)[edit]
Many serial port properties can be displayed and changed with the stty tool. The full feature list is available in stty user manual pages [1] .
stty --help
- Display the current configuration:
stty -a -F /dev/ttySTM1 /* display the configuration of uart3 aka ttySTM1*/
speed 115200 baud; rows 45; columns 169; line = 0;
- Display only the current baud rate:
stty -F /dev/ttySTM1 speed
115200 /* uart3 aka ttySTM1 baud rate is set to 115200 bps */
- Change the baud rate:
stty -F /dev/ttySTMx EXPECTED_BAUDRATE
Example: change the baud rate to 19200
stty -F /dev/ttySTM1 19200 /* uart3 aka ttySTM1 baud rate has been changed to 19200 bps */
The stty tool proposes many arguments allowing many operations on a tty terminal, such as:
- special settings (various arguments such as speed, line discipline, minimum number of characters for a completed read, size, timeout, etc...)
- control settings
- input settings
- output settings
- local settings
- combination settings
Note: If you want to go further, an interesting tutorial describes termios and stty [2].
4 Send / Receive data (with stty, minicom, echo and cat tools)[edit]
Sending data can be simply done by opening the device as a file and writing data to it:
- Configure a port on ttySTM1 (usart3)
stty -F /dev/ttySTM1 115200 -echo
- Open a port on ttySTM1 (usart3) to receive data
cat /dev/ttySTM1 &
- On the remote PC, identify the tty terminal associated to RS232 card connected on STM32MPU USART3 pins
ls /dev/ttyUSB* /dev/ttyUSB0
- Open a minicom terminal on the remote device connected on USART3 pins
minicom -D /dev/ttyUSB0
- Send data from remote PC to STM32MPU over USART3
echo "HELLO" > /dev/ttyUSB0
- send data from STM32MPU to remote PC over USART3
echo "HELLO" > /dev/ttySTM1
5 Identify processes using a tty serial device (with fuser tool)[edit]
fuser /dev/ttySTM0
395 691 3872 /* the process numbered 395, 691 and 3872 are using a tty serial device*/
6 Link a tty serial device with a line discipline (with ldattach tool)[edit]
Attach ttySTM1 with line discipline number n :
ldattach n /dev/ttySTM1
7 File transfer over serial console[edit]
Please see the dedicated article How to transfer a file over serial console.