Difference between revisions of "How to start the coprocessor from the bootloader"
[quality revision] | [quality revision] |
m
|
m
|
Applicable for | STM32MP15x lines |
Contents
1 Introduction[edit]
The coprocessor firmware can be loaded and started:
- either by the second stage bootloader, U-Boot (see Boot_chain_overview for details) or
- by the Linux® kernel (see Linux_remoteproc_framework_overview for details)
This article explains how the coprocessor firmware is loaded by U-Boot and started before the Linux kernel.
2 Location of the coprocessor firmware[edit]
With generic DISTRO configuration, U-Boot searches and loads the required binaries in the first GPT bootable partition (generic DISTRO configuration) for block device, which is bootfs in the OpenSTLinux distribution, or the boot UBIFS volume in UBI mtd partition (see STM32MP15_STM32 MPU Flash _ mapping), so the coprocessor firmware must be installed in that bootfs this partition. The
For block device, the simplest way to do it consists in copying the firmware from the rootfs partition to the bootfs partition as follows.
- Boot from an SD card:
mount /dev/mmcblk0p4mmcblk0p6 /boot cp rproc-m4-fw.elf /boot/ sync
- Here with TF-A update support, bootfs is the 6th partition on SD card. To check the partition name, following commands can be used:
ls -l /dev/disk/by-partlabel/
- Boot from with UBI mtd partition "boot":
mount -t ubifs ubi0:boot /mnt cp rproc-m4-fw.elf /mnt/ sync
As an alternative method, you can use the Eclipse IDE, or transfer the firmware over the serial console or over the network. Note:
![]() |
The default name of the firmware used in this WIKI is rproc-m4-fw.elf. |
3 Starting the coprocessor firmware[edit]
U-Boot can boot the coprocessor before the kernel (coprocessor early boot) with remoteproc uclass . Several methods are possible:
- Manual start by using rproc commands
-
Automatic start, at each boot by using
- the bootcmd (needing U-Boot recompilation)
- a generic DISTRO boot script
- the FIT image
3.1 Manual start[edit]
You can load and start the coprocessor firmware by using the rproc
command in the U-Boot console (to access to the U-boot console, press any key during the U-Boot execution).
STM32MP> rproc
rproc - Control operation of remote processors in an SoC
Usage:
rproc [init|list|load|start|stop|reset|is_running|ping]
Where:
[addr] is a memory address
<id> is a numerical identifier for the remote processor
provided by 'list' command.
Note: Remote processors must be initalized prior to usage
Note: Services depend on the driver capability
'list' command shows the capability of each device
Subcommands:
init - Enumerates and initializes the remote processors
list - lists available remote processors
load <id> [addr] [size]- Loads the remote processor with
image stored at address [addr] in memory
start <id> - Starts the remote processor(must be loaded)
stop <id> - Stops the remote processor
reset <id> - Resets the remote processor
is_running <id> - Reports if the remote processor is running
ping <id> - Pings the remote processor for communication
In this example, the firmware is loaded from an SD card into RAM (at ${kernel_addr_r}), and then launched.
STM32MP> ext4loadload mmc 0:40#bootfs ${kernel_addr_r} rproc-m4-fw.elf -> SD card is mmc 0, bootfs is ext4 partition numberSTM32MP> 4) rproc init -> initializes all coprocessors STM32MP> rproc load 0 ${kernel_addr_r} ${filesize} -> loads firmware for coprocessor 0 (code part found in .elf) STM32MP> rproc start 0 -> starts coprocessor 0
You can then resume the normal boot process:
STM32MP> run bootcmd
3.2 Automatic start[edit]
3.2.1 Start from the bootcmd[edit]
You can update the bootcmd which is exectued automatically: modify CONFIG_EXTRA_ENV_SETTINGS in your Configuration file (for example include/configs/stm32mp1stm32mp15_st_common.h for STM32MP15x STMicroelectronics board) and then recompile U-Boot.
For example, to boot a firmware from an SD card, proceed as follows:
#define CONFIG_EXTRA_ENV_SETTINGS \ "stdin=serial\0" \ "stdout=serial\0" \ "stderr=serial\0" \ ... BOOTENV \ "m4fw_name=rproc-m4-fw.elf\0" \ "m4fw_addr=${kernel_addr_r}\0" \ "boot_m4fw=rproc init; rproc load 0 ${m4fw_addr} ${filesize}; rproc start 0\0" \ "boot_m4_mmc0=if ext4loadload mmc 0:40#bootfs ${m4fw_addr} ${m4fw_name} ; then run boot_m4fw; fi;\0" "bootcmd=run boot_m4_mmc0; run bootcmd_mmc0\0"
Note: It is recommended to check STM32MP15_U-Boot for compilation.
3.2.2 Start from a generic DISTRO boot script[edit]
Without U-boot recompilation, you can also use a DISTRO boot script boot.scr.uimg to automatically load and run the firmware.
For example, use the following script boot.scr.cmd to boot from mmc 0 , boot.scr.cmdwith GPT partition bootfs:
env set m4fw_name "rproc-m4-fw.elf" env set m4fw_addr ${kernel_addr_r} #load M4 firmware if ext4loadload mmc 0:40#bootfs ${m4fw_addr} ${m4fw_name} then rproc init rproc load 0 ${m4fw_addr} ${filesize} rproc start 0 fi #load kernel and device tree ext4loadload mmc 0:40#bootfs ${kernel_addr_r} uImage ext4loadload mmc 0:40#bootfs ${fdt_addr_r} ${board_name}.dtb # start kernel env set bootargs root=/dev/mmcblk0p6 rootwait rw console=ttySTM0,115200 bootm ${kernel_addr_r} - ${fdt_addr_r}
or this one to boot from a nand 0 with UBI mtd partition and boot UBI volume mounted as ubi 0:
# M4 Firmware load
env set m4fw_name "rproc-m4-fw.elf"
env set m4fw_addr ${kernel_addr_r}
# mount UBIFS on boot UBI volume is not required: it is already done in DISTRO bootcmd
# ubi part UBI
# ubifsmount ubi0:boot
if load ubi 0 ${m4fw_addr} ${m4fw_name}
then
rproc init
rproc load 0 ${m4fw_addr} ${filesize}
rproc start 0
fi
#load kernel and device tree
load ubi 0 ${kernel_addr_r} uImage
load ubi 0 ${fdt_addr_r} ${board_name}.dtb
# start kernel
env set bootargs ubi.mtd=UBI rootfstype=ubifs root=ubi0:rootfs rootwait rw console=ttySTM0,115200
bootm ${kernel_addr_r} - ${fdt_addr_r}
Then generate the associated image using mkimage U-Boot tool:
mkimage -T script -C none -A arm -d boot.scr.cmd boot.scr.uimg
Lastly, install boot.scr.uimg in the bootfs partition (following the same procedure used for coprocessor firmware)
sudo mount /dev/mmcblk0p6 /boot cp boot.scr.uimg /mediaboot/$USER/bootfs sync. sudo
mount /dev/mmcblk0p6 /boot rm -r / |
boot/ |
extlinux sync |
3.2.3 Start from the FIT image[edit]
The coprocessor firmware can also be included in the new U-Boot image format, Flattened uImage Tree (FIT) . This firmware is then automatically loaded when it is detected by U-Boot.
![]() |
Please note that the upstreaming of this example is in progress, only a part of the files are present in the U-boot sources provided by STMicroelectronics |
Refer to chapter 'Coprocessor firmware' in board/st/stm32mp1/README : it contains an example of '.its' file, <U-Boot directory>/board/st/stm32mp1/fit_copro_kernel_dtb.its, and shows how to generate the FIT with U-Boot mkimage tool:
mkimage -f fit_copro_kernel_dtb.its fit_copro_kernel_dtb.itb
You can load the generated FIT using:
- 'bootm' command (see doc/uImage.FIT/command_syntax_extensions.txt )
- extlinux.conf in bootfs in extlinux directory to automatically load the FIT by generic DISTRO,
for example: < U-Boot directory>/board/st/stm32mp1/extlinux.conf
To go deeper, read:
- doc/README.pxe
- doc/uImage.FIT/howto.txt
- support of firmware in FIT is done in board_stm32copro_image_process() function in board/st/stm32mp1/stm32mp1.c associated to image type IH_TYPE_STM32COPRO.
4 Synchronizing the remote firmware with Linux[edit]
The STM32MPU Embedded Software distribution provides the ability to detect and manage a firmware loaded by U-Boot thanks to the remoteproc Linux framework.
4.1 STM32Cube[edit]
The developer must pay attention to how he/she implements the Arm Cortex-M4 firmware, if the RPMsg is used to communicate with Linux. In this case a synchronization is required. The Arm Cortex-M4 core has to wait until Linux is booted to start RPMsg communications. When Linux is ready, the Linux kernel automatically updates the vdev status in the resource table, and sends a signal to the Arm Cortex-M4 core using the IPCC peripheral.
Two methods can be implemented to wait for the synchronization:
- Blocking method: the firmware is blocked on MX_OPENAMP_Init call (by the rproc_virtio_wait_remote_ready function) until the Linux kernel is ready to communicate (update of the vdev status in the resource table).
- Non-blocking method: when it is ready to communicate, the Linux kernel generates an interrupt towards the Arm Cortex-M4 core using the IPCC peripheral. This interrupt can be used by the Arm Cortex-M4 firmware to initialize the OpenAMP middleware and start the RPMsg protocol.
4.2 Linux kernel[edit]
On Linux kernel boot, The Linux remoteproc framework is able to detect if a firmware is already running on the Cortex-M4. If detected, the remoteproc state is set to "detached".
cat >/sys/class/remoteproc/remoteproc0/state detached
- To manually attach to the Cortex-M4 and start the RPMsg communication, the state has to be updated to "running":
echo start > /sys/class/remoteproc/remoteproc0/state cat /sys/class/remoteproc/remoteproc0/state running
- To automatically attach to the Cortex-M4 on Linux remoteproc framework probe, add the "st,auto-boot" property in the remote proc node of the Linux kernel device tree:
&m4_rproc { st,auto-boot = <1>; };
== <noinclude>{{ApplicableFor |MPUs list=STM32MP15x |MPUs checklist=STM32MP13x, STM32MP15x }}</noinclude> == Introduction == The [[Coprocessor_management_overview|coprocessor]] firmware can be loaded and started: * either by the second stage bootloader, U-Boot (see [[Boot_chain_overview]] for details) or * by the Linux<sup>®</sup> kernel (see [[Linux_remoteproc_framework_overview]] for details) This article explains how the coprocessor firmware is loaded by [[U-Boot_overview|U-Boot]] and started before the Linux kernel. == Location of the coprocessor firmware == With [[U-Boot _overview#Generic_Distro_configuration|generic DISTRO configuration]], U-Boot searches and loads the required binaries in the first GPT bootable partition ([[U-Boot_overview#Generic_Distro_configuration|generic DISTRO configuration]]) which is '''bootfs'''for block device, which is {{Highlight|bootfs}} in the OpenSTLinux distribution (see [[STM32MP15_Flash_, or the {{Highlight|boot}} UBIFS volume in UBI mtd partition (see [[STM32 MPU Flash mapping]]), so the coprocessor firmware must be installed in that bootfs this partition.The For block device, the simplest way to do it consists in copying the firmware from the rootfs partition to the bootfs partition as follows: {{Board$}} mount /dev/mmcblk0p4. * '''Boot from an SD card:''' {{Board$}} mount /dev/mmcblk0p{{Highlight|6}} /boot {{Board$}} cp rproc-m4-fw.elf /boot/ {{Board$}} sync :Here with TF-A update support, bootfs is the {{Highlight|6th}} partition on SD card. To check the partition name, following commands can be used: {{Board$}} ls -l /dev/disk/by-partlabel/ * '''Boot from with UBI mtd partition "boot":''' {{Board$}} mount -t ubifs ubi0:boot /mnt {{Board$}} cp rproc-m4-fw.elf /mnt/ {{Board$}} sync As an alternative method, you can use the Eclipse IDE, or transfer the firmware [[How to transfer a file over serial console|over the serial console]] or [[How to transfer a file over network|over the network]]. ''Note: {{Info|The default name of the firmware used in this WIKI is '''rproc-m4-fw.elf'''''.}} == Starting the coprocessor firmware == U-Boot can boot the coprocessor before the kernel (coprocessor early boot) with remoteproc {{CodeSource|U-Boot|doc/driver-model/remoteproc-framework.rst|uclass}}. Several methods are possible: # [[#Manual start|Manual start]] by using rproc commands # [[#Automatic start|Automatic start]], at each boot by using #* [[#Start from the bootcmd|the bootcmd]] (needing U-Boot recompilation) #* [[#Start from a generic DISTRO boot script|a generic DISTRO boot script]] #* [[#Start from the FIT image|the FIT image]] === Manual start === You can load and start the coprocessor firmware by using the '''<code>rproc'''</code> command in the [[U-Boot_overview#U-Boot_command_line_interface_(CLI)|U-Boot console]] (to access to the U-boot console, press any key during the U-Boot execution). {{Board$U-Boot$}} rproc rproc - Control operation of remote processors in an SoC Usage: rproc [init|list|load|start|stop|reset|is_running|ping] Where: [addr] is a memory address<id> is a numerical identifier for the remote processor provided by 'list' command. Note: Remote processors must be initalized prior to usage Note: Services depend on the driver capability 'list' command shows the capability of each device Subcommands: init - Enumerates and initializes the remote processors list - lists available remote processors load <id> [addr] [size]- Loads the remote processor with image stored at address [addr] in memory start <id> - Starts the remote processor(must be loaded) stop <id> - Stops the remote processor reset <id> - Resets the remote processor is_running <id> - Reports if the remote processor is running ping <id> - Pings the remote processor for communication In this example, the firmware is loaded from an SD card into RAM (at ${kernel_addr_r}), and then launched. {{Board$}} ext4load mmc 0:4U-Boot$}} load mmc 0#bootfs ${kernel_addr_r} rproc-m4-fw.elf {{Highlight|-> SD card is mmc 0, bootfs is ext4 partition number 4)}} {{Board$}} {{U-Boot$}} rproc init {{Highlight|-> initializes all coprocessors}} {{Board$U-Boot$}} rproc load 0 ${kernel_addr_r} ${filesize} {{Highlight|-> loads firmware for coprocessor 0 (code part found in .elf)}} {{Board$U-Boot$}} rproc start 0 {{Highlight|-> starts coprocessor 0}} You can then resume the normal boot process: {{Board$U-Boot$}} run bootcmd === Automatic start === ==== Start from the bootcmd ==== You can update the [[U-Boot_overview#bootcmd|bootcmd]] which is exectued automatically: modify '''CONFIG_EXTRA_ENV_SETTINGS''' in your [[How_to_configure_U-Boot_for_your_board#Configuration_file|Configuration file]] (for example {{CodeSource | U-Boot | include/configs/stm32mp1stm32mp15_st_common.h}} for STM32MP15x STMicroelectronics board) and then [[U-Boot_overview#U-Boot_build|recompile U-Boot]]. For example, to boot a firmware from an SD card, proceed as follows:<pre> #define CONFIG_EXTRA_ENV_SETTINGS \ "stdin=serial\0" \ "stdout=serial\0" \ "stderr=serial\0" \ ... BOOTENV \ "m4fw_name=rproc-m4-fw.elf\0" \ "m4fw_addr=${kernel_addr_r}\0" \ "boot_m4fw=rproc init; rproc load 0 ${m4fw_addr} ${filesize}; rproc start 0\0" \ "boot_m4_mmc0=if ext4loadload mmc 0:40#bootfs ${m4fw_addr} ${m4fw_name} ; then run boot_m4fw; fi;\0" "bootcmd=run boot_m4_mmc0; run bootcmd_mmc0\0"</pre> Note: It is recommended to check [[STM32MP15_U-Boot]] for compilation. ==== Start from a generic DISTRO boot script ==== Without U-boot recompilation, you can also use a DISTRO boot script '''boot.scr.uimg''' to automatically load and run the firmware. For example, use the following script '''boot.scr.cmd''' to boot from mmc 0, '''boot.scr.cmd with GPT partition '''bootfs''': env set m4fw_name "rproc-m4-fw.elf" env set m4fw_addr ${kernel_addr_r} #load M4 firmware if ext4loadload mmc 0:40#bootfs ${m4fw_addr} ${m4fw_name} then rproc init rproc load 0 ${m4fw_addr} ${filesize} rproc start 0 fi #load kernel and device treeext4loadload mmc 0:4 0#bootfs ${kernel_addr_r} uImageext4loadload mmc 0:4 0#bootfs ${fdt_addr_r} ${board_name}.dtb # start kernel env set bootargs root=/dev/mmcblk0p6 rootwait rw console=ttySTM0,115200 bootm ${kernel_addr_r} - ${fdt_addr_r} or this one to boot from a nand 0 with UBI mtd partition and '''boot''' UBI volume mounted as ubi 0: # M4 Firmware load env set m4fw_name "rproc-m4-fw.elf" env set m4fw_addr ${kernel_addr_r} # mount UBIFS on boot UBI volume is not required: it is already done in DISTRO bootcmd # ubi part UBI # ubifsmount ubi0:boot if load ubi 0 ${m4fw_addr} ${m4fw_name} then rproc init rproc load 0 ${m4fw_addr} ${filesize} rproc start 0 fi #load kernel and device tree load ubi 0 ${kernel_addr_r} uImage load ubi 0 ${fdt_addr_r} ${board_name}.dtb # start kernel env set bootargs ubi.mtd=UBI rootfstype=ubifs root=ubi0:rootfs rootwait rw console=ttySTM0,115200 bootm ${kernel_addr_r} - ${fdt_addr_r} Then generate the associated image using mkimage U-Boot tool: {{PC$}} mkimage -T script -C none -A arm -d boot.scr.cmd boot.scr.uimg Lastly, install '''boot.scr.uimg''' in the bootfs partition (following the same procedure used for [[#Location of the coprocessor firmware|coprocessor firmware]]) {{PC$}} sudo Board$}} mount /dev/mmcblk0p{{Highlight|6}} /boot {{Board$}} cp boot.scr.uimg /media/$USER/bootfs {{PC$ /boot/ {{Board$}} sync {{Info|The name of '''boot.scr.uimg''' may be adapted according to your configuration. For example, it may be '''mmc0_boot.scr.uimg'''.'}} <br/>The distro variables can be used in script ${devtype} ${devnum}:${distro_bootpart} to identify the boot device and have more generic script}}. {{Warning|The 'boot.scr.uimg' U-Boot script is executed only if 'extlinux/extlinux.conf' is not found (scan_dev_for_scripts is called after scan_dev_for_extlinux)<br>You should remove pre-existing file in bootfs partition:}} {{PC$}} sudo rm -r /media/$USER/bootfs/extlinux {{PC$}} sync {{Board$}} mount /dev/mmcblk0p{{Highlight|6}} /boot {{Board$}} rm -r /boot/extlinux {{Board$}} sync }} ==== Start from the FIT image ==== The coprocessor firmware can also be included in the new U-Boot image format, {{CodeSource | U-Boot | doc/uImage.FIT/ |Flattened uImage Tree (FIT)}}. This firmware is then automatically loaded when it is detected by U-Boot. {{Info|Please note that the upstreaming of this example is in progress, only a part of the files are present in the U-boot sources provided by STMicroelectronics}} Refer to chapter 'Coprocessor firmware' in {{CodeSource | U-Boot | board/st/stm32mp1/README}}: it contains an example of '.its' file, <U-Boot directory>/board/st/stm32mp1/fit_copro_kernel_dtb.its, and shows how to generate the FIT with U-Boot mkimage tool: {{PC$}} mkimage -f fit_copro_kernel_dtb.its fit_copro_kernel_dtb.itb You can load the generated FIT using: * 'bootm' command (see {{ CodeSource | U-Boot | doc/uImage.FIT/command_syntax_extensions.txt}}) * extlinux.conf in bootfs in extlinux directory to automatically load the FIT by [[U-Boot_overview#Generic_Distro_configuration|generic DISTRO]],<br/>for example: < U-Boot directory>/board/st/stm32mp1/extlinux.conf To go deeper, read: * {{ CodeSource | U-Boot | doc/README.pxe }} * {{ CodeSource | U-Boot | doc/uImage.FIT/howto.txt }} * support of firmware in FIT is done in board_stm32copro_image_process() function in {{CodeSource | U-Boot | board/st/stm32mp1/stm32mp1.c}} associated to image type IH_TYPE_STM32COPRO. == Synchronizing the remote firmware with Linux == The [[STM32MPU Embedded Software distribution]] provides the ability to detect and manage a firmware loaded by U-Boot thanks to the [[Linux_remoteproc_framework_overview#Remote_processor_.27early.27_boot | remoteproc]] Linux framework.<BR> === STM32Cube === The developer must pay attention to how he/she implements the Arm Cortex-M4 firmware, if the RPMsg is used to communicate with Linux. In this case a synchronization is required. The Arm Cortex-M4 core has to wait until Linux is booted to start RPMsg communications. When Linux is ready, the Linux kernel automatically updates the vdev status in the [[Coprocessor_resource_table | resource table]], and sends a signal to the Arm Cortex-M4 core using the [[IPCC_internal_peripheral | IPCC peripheral]].<BR> Two methods can be implemented to wait for the synchronization: * '''Blocking method''': the firmware is blocked on MX_OPENAMP_Init call (by the rproc_virtio_wait_remote_ready function) until the Linux kernel is ready to communicate (update of the vdev status in the resource table). * '''Non-blocking method''': when it is ready to communicate, the Linux kernel generates an interrupt towards the Arm Cortex-M4 core using the [[IPCC_internal_peripheral | IPCC peripheral]]. This interrupt can be used by the Arm Cortex-M4 firmware to initialize the OpenAMP middleware and start the RPMsg protocol. === Linux kernel === On Linux kernel boot, The [[Linux remoteproc framework overview | Linux remoteproc framework]] is able to detect if a firmware is already running on the Cortex-M4. If detected, the remoteproc state is set to '''"detached"'''. {{Board$}} cat >/sys/class/remoteproc/remoteproc0/state detached * To manually attach to the Cortex-M4 and start the RPMsg communication, the state has to be updated to '''"running"''': {{Board$}} echo start > /sys/class/remoteproc/remoteproc0/state {{Board$}} cat /sys/class/remoteproc/remoteproc0/state running * To automatically attach to the Cortex-M4 on [[Linux remoteproc framework overview | Linux remoteproc framework]] probe, add the '''"st,auto-boot"''' property in the remote proc node of the Linux kernel [[Device tree|device tree]]: &m4_rproc { st,auto-boot = <1>; }; <noinclude> [[Category:How to run use cases]] [[Category:Coprocessor management STM32Cube]] [[Category:U-Boot|U-Boot - 9]] {{PublicationRequestId | 16353| 2020-06-09 | (previous version reviewed by AlainF)}}</noinclude>
(20 intermediate revisions by 4 users not shown) | |||
Line 1: | Line 1: | ||
+ | <noinclude>{{ApplicableFor |
||
+ | |MPUs list=STM32MP15x |
||
+ | |MPUs checklist=STM32MP13x, STM32MP15x |
||
+ | }}</noinclude> |
||
== Introduction == |
== Introduction == |
||
The [[Coprocessor_management_overview|coprocessor]] firmware can be loaded and started: |
The [[Coprocessor_management_overview|coprocessor]] firmware can be loaded and started: |
||
Line 8: | Line 12: | ||
== Location of the coprocessor firmware == |
== Location of the coprocessor firmware == |
||
− | U-Boot searches and loads the required binaries in the first bootable partition |
+ |
With [[U-Boot_overview#Generic_Distro_configuration|generic DISTRO configuration]], U-Boot searches and loads the required binaries in the first GPT bootable partition for block device, which is {{Highlight|bootfs}} in the OpenSTLinux distribution, or the {{Highlight|boot}} UBIFS volume in UBI mtd partition (see [[STM32 MPU Flash mapping]]), so the coprocessor firmware must be installed in this partition. |
− | {{Board$}} mount /dev/ |
+ | |
+ |
For block device, the simplest way to do it consists in copying the firmware from the rootfs partition to the bootfs partition as follows.
|
||
+ |
* '''Boot from an SD card:'''
|
||
+ | {{Board$}} mount /dev/mmcblk0p{{Highlight|6}} /boot |
||
{{Board$}} cp rproc-m4-fw.elf /boot/ |
{{Board$}} cp rproc-m4-fw.elf /boot/ |
||
+ | {{Board$}} sync |
||
+ | |||
+ | :Here with TF-A update support, bootfs is the {{Highlight|6th}} partition on SD card. To check the partition name, following commands can be used: |
||
+ | {{Board$}} ls -l /dev/disk/by-partlabel/ |
||
+ | |||
+ | * '''Boot from with UBI mtd partition "boot":''' |
||
+ | {{Board$}} mount -t ubifs ubi0:boot /mnt |
||
+ | {{Board$}} cp rproc-m4-fw.elf /mnt/ |
||
{{Board$}} sync |
{{Board$}} sync |
||
As an alternative method, you can use the Eclipse IDE, or transfer the firmware [[How to transfer a file over serial console|over the serial console]] or [[How to transfer a file over network|over the network]]. |
As an alternative method, you can use the Eclipse IDE, or transfer the firmware [[How to transfer a file over serial console|over the serial console]] or [[How to transfer a file over network|over the network]]. |
||
− | + |
{{Info|The default name of the firmware used in this WIKI is '''rproc-m4-fw.elf'''''.}}
|
|
== Starting the coprocessor firmware == |
== Starting the coprocessor firmware == |
||
Line 28: | Line 43: | ||
=== Manual start === |
=== Manual start === |
||
− | You can load and start the coprocessor firmware by using the |
+ | You can load and start the coprocessor firmware by using the <code>rproc</code> command in the [[U-Boot_overview#U-Boot_command_line_interface_(CLI)|U-Boot console]] (to access to the U-boot console, press any key during the U-Boot execution). |
− | {{ |
+ | {{U-Boot$}} rproc |
rproc - Control operation of remote processors in an SoC |
rproc - Control operation of remote processors in an SoC |
||
Line 56: | Line 71: | ||
In this example, the firmware is loaded from an SD card into RAM (at ${kernel_addr_r}), and then launched. |
In this example, the firmware is loaded from an SD card into RAM (at ${kernel_addr_r}), and then launched. |
||
− | {{ |
+ | {{U-Boot$}} load mmc 0#bootfs ${kernel_addr_r} rproc-m4-fw.elf {{Highlight|-> SD card is mmc 0, bootfs partition}} |
− | {{ |
+ | {{U-Boot$}} rproc init {{Highlight|-> initializes all coprocessors}} |
− | {{ |
+ | {{U-Boot$}} rproc load 0 ${kernel_addr_r} ${filesize} {{Highlight|-> loads firmware for coprocessor 0 (code part found in .elf)}} |
− | {{ |
+ | {{U-Boot$}} rproc start 0 {{Highlight|-> starts coprocessor 0}} |
You can then resume the normal boot process: |
You can then resume the normal boot process: |
||
− | {{ |
+ | {{U-Boot$}} run bootcmd |
=== Automatic start === |
=== Automatic start === |
||
==== Start from the bootcmd ==== |
==== Start from the bootcmd ==== |
||
− | You can update the [[U-Boot_overview#bootcmd|bootcmd]] which is exectued automatically: modify '''CONFIG_EXTRA_ENV_SETTINGS''' in {{CodeSource | U-Boot | include/configs/ |
+ | You can update the [[U-Boot_overview#bootcmd|bootcmd]] which is exectued automatically: modify '''CONFIG_EXTRA_ENV_SETTINGS''' in your [[How_to_configure_U-Boot_for_your_board#Configuration_file|Configuration file]] (for example {{CodeSource | U-Boot | include/configs/stm32mp15_st_common.h}} for STM32MP15x STMicroelectronics board) and then [[U-Boot_overview#U-Boot_build|recompile U-Boot]]. |
For example, to boot a firmware from an SD card, proceed as follows: |
For example, to boot a firmware from an SD card, proceed as follows: |
||
Line 79: | Line 94: | ||
"m4fw_addr=${kernel_addr_r}\0" \ |
"m4fw_addr=${kernel_addr_r}\0" \ |
||
"boot_m4fw=rproc init; rproc load 0 ${m4fw_addr} ${filesize}; rproc start 0\0" \ |
"boot_m4fw=rproc init; rproc load 0 ${m4fw_addr} ${filesize}; rproc start 0\0" \ |
||
− | "boot_m4_mmc0=if |
+ | "boot_m4_mmc0=if load mmc 0#bootfs ${m4fw_addr} ${m4fw_name} ; then run boot_m4fw; fi;\0" |
"bootcmd=run boot_m4_mmc0; run bootcmd_mmc0\0" |
"bootcmd=run boot_m4_mmc0; run bootcmd_mmc0\0" |
||
</pre> |
</pre> |
||
Line 89: | Line 104: | ||
Without U-boot recompilation, you can also use a DISTRO boot script '''boot.scr.uimg''' to automatically load and run the firmware. |
Without U-boot recompilation, you can also use a DISTRO boot script '''boot.scr.uimg''' to automatically load and run the firmware. |
||
− | For example, use the following script to boot from mmc 0 |
+ | For example, use the following script '''boot.scr.cmd''' to boot from mmc 0 with GPT partition '''bootfs''': |
env set m4fw_name "rproc-m4-fw.elf" |
env set m4fw_name "rproc-m4-fw.elf" |
||
Line 95: | Line 110: | ||
#load M4 firmware |
#load M4 firmware |
||
− | if |
+ | if load mmc 0#bootfs ${m4fw_addr} ${m4fw_name} |
then |
then |
||
rproc init |
rproc init |
||
Line 103: | Line 118: | ||
#load kernel and device tree |
#load kernel and device tree |
||
− | + | load mmc 0#bootfs ${kernel_addr_r} uImage |
|
− | + | load mmc 0#bootfs ${fdt_addr_r} ${board_name}.dtb |
|
# start kernel |
# start kernel |
||
env set bootargs root=/dev/mmcblk0p6 rootwait rw console=ttySTM0,115200 |
env set bootargs root=/dev/mmcblk0p6 rootwait rw console=ttySTM0,115200 |
||
bootm ${kernel_addr_r} - ${fdt_addr_r} |
bootm ${kernel_addr_r} - ${fdt_addr_r} |
||
+ | |||
+ | or this one to boot from a nand 0 with UBI mtd partition and '''boot''' UBI volume mounted as ubi 0: |
||
+ | |||
+ | # M4 Firmware load |
||
+ | env set m4fw_name "rproc-m4-fw.elf" |
||
+ | env set m4fw_addr ${kernel_addr_r} |
||
+ | |||
+ | # mount UBIFS on boot UBI volume is not required: it is already done in DISTRO bootcmd |
||
+ | # ubi part UBI |
||
+ | # ubifsmount ubi0:boot |
||
+ | |||
+ | if load ubi 0 ${m4fw_addr} ${m4fw_name} |
||
+ | then |
||
+ | rproc init |
||
+ | rproc load 0 ${m4fw_addr} ${filesize} |
||
+ | rproc start 0 |
||
+ | fi |
||
+ | |||
+ | #load kernel and device tree |
||
+ | load ubi 0 ${kernel_addr_r} uImage |
||
+ | load ubi 0 ${fdt_addr_r} ${board_name}.dtb |
||
+ | |||
+ | # start kernel |
||
+ | env set bootargs ubi.mtd=UBI rootfstype=ubifs root=ubi0:rootfs rootwait rw console=ttySTM0,115200 |
||
+ | bootm ${kernel_addr_r} - ${fdt_addr_r} |
||
Then generate the associated image using mkimage U-Boot tool: |
Then generate the associated image using mkimage U-Boot tool: |
||
Line 116: | Line 156: | ||
Lastly, install '''boot.scr.uimg''' in the bootfs partition (following the same procedure used for [[#Location of the coprocessor firmware|coprocessor firmware]]) |
Lastly, install '''boot.scr.uimg''' in the bootfs partition (following the same procedure used for [[#Location of the coprocessor firmware|coprocessor firmware]]) |
||
− | {{ |
+ | {{Board$}} mount /dev/mmcblk0p{{Highlight|6}} /boot
|
− | {{ |
+ |
{{Board$}} cp boot.scr.uimg /boot/ |
+ | {{Board$}} sync |
||
+ | |||
+ | {{Info|The name of '''boot.scr.uimg''' may be adapted according to your configuration. For example, it may be '''mmc0_boot.scr.uimg'''.'<br/>The distro variables can be used in script ${devtype} ${devnum}:${distro_bootpart} to identify the boot device and have more generic script}}. |
||
− | {{ |
+ | {{Warning|The 'boot.scr.uimg' U-Boot script is executed only if 'extlinux/extlinux.conf' is not found (scan_dev_for_scripts is called after scan_dev_for_extlinux)<br>You should remove pre-existing file in bootfs partition:
|
− | {{ |
+ |
{{Board$}} mount /dev/mmcblk0p{{Highlight|6}} /boot
|
− | {{ |
+ | {{Board$}} rm -r /boot/extlinux |
− | {{ |
+ | {{Board$}} sync |
+ | }} |
||
==== Start from the FIT image ==== |
==== Start from the FIT image ==== |
||
Line 172: | Line 216: | ||
[[Category:How to run use cases]] |
[[Category:How to run use cases]] |
||
[[Category:Coprocessor management STM32Cube]] |
[[Category:Coprocessor management STM32Cube]] |
||
− | [[Category:U-Boot]] |
+ | [[Category:U-Boot|U-Boot - 9]] |
{{PublicationRequestId | 16353| 2020-06-09 | (previous version reviewed by AlainF)}} |
{{PublicationRequestId | 16353| 2020-06-09 | (previous version reviewed by AlainF)}} |
||
</noinclude> |
</noinclude> |