Approved version. Approved on: 08:34, 16 October 2020
You are viewing an old version of this page. Return to the latest version.
[quality revision] | [quality revision] |
m (→Modifying target password)
|
(Merge articles)
|
When debugging the Cortex®-M in "production mode", in case of a typo entering the target password , we need implies to modify the target password registered by the STM32CubeIDE. Indeed, this prevent you from using Debug prevents the user from debugging in "production mode".
This password is managed by MPU SSH connection object managed by RSE perspective. It is possible to clear corresponding password from here.
can be updated with Remote Connections preferences menu: Window > Preferences > Remote Development.
Note that if "MPU SSH" is connectedopened, it has to must be disconnected closed first to enable edit.
==Modifying the target password== When debugging the Cortex<sup>®</sup>-M in "production mode", in case of typo entering target password, we need to modify a typo entering the target password implies to modify the target password registered by the STM32CubeIDE. Indeed, this prevent you from using Debug prevents the user from debugging in "production mode". This password is managed by '''MPU SSH''' connection object managed by [[How_to_use_the_RSE_Perspective_with_STM32CubeIDE|RSE perspective]]. It is possible to clear corresponding password from here. [[File:RSE Clear Pwd.png|center|RSE Password Clear]] can be updated with ''Remote Connections'' preferences menu: ''Window > Preferences > Remote Development''. [[File:MPU Password Setup.png|700px|center|thumb|Linux device password setup]] Note that if "MPU SSH" is connectedopened, it has to must be disconnectedclosed first to enable edit. <noinclude> [[Category:STM32CubeIDE|4]]{{PublicationRequestId | 19684 (LudovicB) |2021-04-20 }}</noinclude>
(One intermediate revision by the same user not shown) | |||
Line 1: | Line 1: | ||
− | ==Modifying target password== |
+ | ==Modifying the target password== |
− | When debugging Cortex-M in "production mode", |
+ | When debugging the Cortex<sup>®</sup>-M in "production mode", a typo entering the target password implies to modify the target password registered by the STM32CubeIDE. Indeed, this prevents the user from debugging in "production mode". |
− | This password |
+ | This password can be updated with ''Remote Connections'' preferences menu: ''Window > Preferences > Remote Development''. |
− | |||
− | [[File: |
+ | [[File:MPU Password Setup.png|700px|center|thumb|Linux device password setup]] |
− | + | Note that if "MPU SSH" is opened, it must be closed first to enable edit. |
|
− | Note that if "MPU SSH" is |
||
<noinclude> |
<noinclude> |
||
[[Category:STM32CubeIDE|4]] |
[[Category:STM32CubeIDE|4]] |
||
+ | {{PublicationRequestId | 19684 (LudovicB) |2021-04-20 }} |
||
</noinclude> |
</noinclude> |