Difference between revisions of "How to set up proxy and P2P Ethernet connection with STM32CubeIDE"

[quality revision] [checked revision]
m
m
 

1 Introduction[edit]

This article explain explains how to set up a Pointpoint-to-Point point connection to the STM32 MPU board, especially in case of if a proxy is also setup on the PC for accessing the Internet.

2 Setting up the network[edit]

To set up the connection

  • go to Windows -> Preferences -> General -> Network Connections
  • select "Manual" in the Active Provider field, and:
    • adjust your proxy setup with Edit... in Proxy entries
    • configure a new Proxy bypass with Add Host... giving the IP address of the STM32 MPUtarget.MPU target


Network Setting in STM32CubeIDE


==Introduction==
This article explainexplains how to set up a Pointpoint-to-Pointpoint connection to the STM32 MPU board, especially  in case of if a proxy is also setup on the PC for accessing the Internet. 

==Setting up the network==
To set up the connection 
*go to ''Windows'' -> ''Preferences'' -> ''General'' -> ''Network Connections''
*select "Manual" in the ''Active Provider'' field, and:
**adjust your proxy setup with ''Edit...'' in ''Proxy entries''
**configure a new ''Proxy bypass'' with ''Add Host...'' giving the IP address of the STM32 MPUtarget.
MPU target
[[File:CubeIDE-Proxy.png|link=|500px|center|Network Setting in STM32CubeIDE]]
<noinclude>

[[Category:STM32CubeIDE|27]]{{PublicationRequestId | 19682 (LudovicB) |2021-04-20 }}</noinclude>
(2 intermediate revisions by 2 users not shown)
Line 1: Line 1:
 
==Introduction==
 
==Introduction==
This article explain how to set up a Point-to-Point connection to the STM32 MPU board, especially in case of a proxy is also setup on the PC for accessing the Internet.  
+
This article explains how to set up a point-to-point connection to the STM32 MPU board, especially if a proxy is also setup on the PC for accessing the Internet.  
   
==Setting up network==
+
==Setting up the network==
 
To set up the connection  
 
To set up the connection  
*go to ''Windows -> Preferences -> General -> Network Connections''
+
*go to ''Windows'' -> ''Preferences'' -> ''General'' -> ''Network Connections''
 
*select "Manual" in the ''Active Provider'' field, and:
 
*select "Manual" in the ''Active Provider'' field, and:
 
**adjust your proxy setup with ''Edit...'' in ''Proxy entries''
 
**adjust your proxy setup with ''Edit...'' in ''Proxy entries''
**configure a new ''Proxy bypass'' with ''Add Host...'' giving the IP address of the STM32 MPUtarget.
+
**configure a new ''Proxy bypass'' with ''Add Host...'' giving the IP address of the STM32 MPU target
   
   
Line 14: Line 14:
 
<noinclude>
 
<noinclude>
 
[[Category:STM32CubeIDE|27]]
 
[[Category:STM32CubeIDE|27]]
  +
{{PublicationRequestId | 19682 (LudovicB) |2021-04-20 }}
 
</noinclude>
 
</noinclude>