Approved version. Approved on: 08:02, 8 April 2022
Difference between revisions of "How to modify the panel backlight"
[unchecked revision] | [quality revision] |
m
|
m
|
[unchecked revision] | [quality revision] |
m
|
m
|
Applicable for | STM32MP13x lines, STM32MP15x lines |
First identify the backlight device linked to your panel, thanks to the sysfs:
ls /sys/class/backlight 5a000000.dsi.0
In the above example, there is a single entry named "5a000000.dsi.0", which is replaced by "*" in the below command.
To adjust the panel backlight, enter the following command:
echo 32 > /sys/class/backlight/*/brightness # set the dsi panel backlight to the value 32
Note: Only values between 0 and max_brightness must be used.
To get the maximum panel backlight value, enter:
cat /sys/class/backlight/*/max_brightness 255
To get the actual panel backlight value, enter:
cat /sys/class/backlight/*/actual_brightness 32
Use one of the following commands to quickly test the panel backlight:
export bl=/sys/class/backlight/5a000000.dsi.0/brightness # switch on/off test (while true; do echo 0 > $bl; sleep 0.5; echo 255 > $bl; sleep 0.5; done) # slow 32-step tests (i=0; while true; do i=$(((i+32)%256)); echo $i > $bl; sleep 0.5; done) # fast 1-step test (i=0; while true; do i=$(((i+1)%256)); echo $i > $bl; done)
![]() |
Be sure the panel is running (power on) before modifying its backlight. |
<noinclude>{{ApplicableFor |MPUs list=STM32MP13x, STM32MP15x |MPUs checklist=STM32MP13x,STM32MP15x }}</noinclude> {{ClonedFrom|stm32mpuv3}} First identify the backlight device linked to your panel, thanks to the sysfs: {{Board$}} ls /sys/class/backlight 5a000000.dsi.0 In the above example, there is a single entry named "5a000000.dsi.0", which is '''replaced by "*"''' in the below command. To adjust the panel backlight, enter the following command: {{Board$}} echo '''32''' > /sys/class/backlight/*/'''brightness''' # set the dsi panel backlight to the value '''32''' Note: Only values between 0 and '''max_brightness''' must be used. To get the maximum panel backlight value, enter: {{Board$}} cat /sys/class/backlight/*/'''max_brightness''' 255 To get the actual panel backlight value, enter: {{Board$}} cat /sys/class/backlight/*/'''actual_brightness''' 32 Use one of the following commands to quickly test the panel backlight: {{Board$}} export bl=/sys/class/backlight/5a000000.dsi.0/brightness {{Board$}} # switch on/off test {{Board$}} (while true; do echo 0 > $bl; sleep 0.5; echo 255 > $bl; sleep 0.5; done) {{Board$}} # slow 32-step tests {{Board$}} (i=0; while true; do i=$(((i+32)%256)); echo $i > $bl; sleep 0.5; done) {{Board$}} # fast 1-step test {{Board$}} (i=0; while true; do i=$(((i+1)%256)); echo $i > $bl; done) {{Info | Be sure the panel is running (power on) before modifying its backlight.}} <noinclude> {{PublicationRequestId | 10715 | 2019-02-18 | AnneJ}} [[Category:How to run use cases]] [[Category:DRM KMS]]</noinclude>
Line 3: | Line 3: | ||
|MPUs checklist=STM32MP13x,STM32MP15x |
|MPUs checklist=STM32MP13x,STM32MP15x |
||
}}</noinclude> |
}}</noinclude> |
||
− | + | ||
First identify the backlight device linked to your panel, thanks to the sysfs: |
First identify the backlight device linked to your panel, thanks to the sysfs: |
||
{{Board$}} ls /sys/class/backlight |
{{Board$}} ls /sys/class/backlight |