Difference between revisions of "How to manually update bootloaders"
[checked revision] | [quality revision] |
m
|
m
|
This page explains how to manually update the bootloaders binary (including U-Boot and TF-A) on an SD card or on the e•MMC.
Contents
1 To update an SD card with the Linux dd command[edit]
When a Linux console has access to the SD card device partitions:
- on a Linux PC
- with a card reader of this PC
- through a USB connection to the target and the
ums
command executed on a U-Boot console
- on target, with Linux console.
The 3 first GPT partitions on the SD card are:
- FSBL1
- FSBL2
- FIP
See Boot_chain_overview for the bootloader definitions.
You can use the Linux dd
command to copy the FSBL and SSBL directly to the correct partition:
dd if=<file> of=/dev/<dev> conv=fdatasync
<dev> is:
- mmcblk<X>p<n>: PC-embedded card reader case or target Linux console
- sd<X><n>: USB-connected SD card reader case
where <X> is the ID of the device, and <n> the ID of the partition.
Note: the dd option conv=fdatasync is used to force synchronous copying.
1.1 U-Boot environment[edit]
The U-Boot environment is saved at the end of the U-Boot partition, named "fip": ID = 3.
To clear this environment, erase the U-Boot partition before any update; for example, by writing 0 to this partition:
dd if=/dev/zero of=/dev/mmcblk<X>p3 conv=fdatasync
dd if=/dev/zero of=sd<X>3 conv=fdatasync
1.2 SD card update example[edit]
The internal card reader is /dev/mmcblk0 or for a target Linux console, GPT partition <n> is /dev/mmcblk0p<n>:
dd if=tf-a-sdcard.stm32 of=/dev/mmcblk0p1 conv=fdatasync dd if=tf-a-sdcard.stm32 of=/dev/mmcblk0p2 conv=fdatasync dd if=/dev/zero of=/dev/mmcblk0p3 conv=fdatasync dd if=fip.bin of=/dev/mmcblk0p3 conv=fdatasync
Alternatively, with U-Boot console, dev = 0 (SD card device on ST Microelectronics board), GPT partition <n> is /dev/sda<n>:
mmc dev 0 ums 0 mmc 0 dd if=tf-a-sdcard.stm32 of=/dev/sda1 conv=fdatasync dd if=tf-a-sdcard.stm32 of=/dev/sda2 conv=fdatasync dd if=/dev/zero of=/dev/sda3 conv=fdatasync dd if=fip.bin of=/dev/sda3 conv=fdatasync
1.3 SD card update example with SPL as FSBL[edit]
The USB card reader is /dev/sdb, GPT partition <n> is /dev/sdb<n>:
dd if=u-boot-spl.stm32 of=/dev/sdb1 conv=fdatasync dd if=u-boot-spl.stm32 of=/dev/sdb2 conv=fdatasync dd if=/dev/zero of=/dev/sdb3 conv=fdatasync dd if=u-boot.img of=/dev/sdb3 conv=fdatasync
2 Update of e•MMC with the Linux dd command[edit]
The same command, dd
, can be used to update e•MMC memory mapping:
- SSBL U-Boot is the first GPT partition in the e•MMC user area
- FSBL = TF-A (or SPL) is saved at the beginning of the e•MMC boot partition
The user needs to select the e•MMC hardware partition to update: user data, boot1, or boot2.
2.1 On a Linux console[edit]
If dev = mmcblk1 for e•MMC device (default on ST Microelectronics board)
The boot partitions are available in /dev/mmcblk1boot0 and /dev/mmcblk1boot1 [1].
The user perhaps needs to allow access, for example with:
echo 0 > /sys/class/block/mmcblk1boot0/force_ro
The mmc tools allow the boot partition to be selected [2].
The STM32MP15x ROM code requires:
- <send_ack> =1
- the eMMC boot configuration is: 1 wire configuration and 25 MHz, it is done with the command:
mmc bootbus set single_backward x1 x1 dev/mmcblk1
To update TF-A in boot1 and select this boot partition:
dd if=tf-a-emmc.stm32 of=/dev/mmcblk1boot0 conv=fdatasync mmc bootpart enable 1 1 /dev/mmcblk1
To update TF-A in boot2 and select this boot partition:
dd if=tf-a-emmc.stm32 of=/dev/mmcblk1boot1 conv=fdatasync mmc bootpart enable 2 1 /dev/mmcblk1
To update U-Boot in the first GPT partition:
dd if=/dev/zero of=/dev/mmcblk1p1 conv=fdatasync dd if=fip.bin of=/dev/mmcblk1p1 conv=fdatasync
See also [3].
2.2 On a U-Boot console[edit]
Before the first boot, select the e•MMC correct boot configuration (1 wire, 25 MHz) with the command:
mmc bootbus 1 0 0 0
2.2.1 mmc partconf[edit]
The targeted e•MMC HW partition is selected in U-Boot by the command mmc partconf
:
help mmc
...
mmc bootbus dev boot_bus_width reset_boot_bus_width boot_mode
- Set the BOOT_BUS_WIDTH field of the specified device
mmc bootpart-resize <dev> <boot part size MB> <RPMB part size MB>
- Change sizes of boot and RPMB partitions of specified device
mmc partconf dev [boot_ack boot_partition partition_access]
- Show or change the bits of the PARTITION_CONFIG field of the specified device
For example:
* dev = 1 (e•MMC device on ST Microelectronics board) * boot_ack=1 (Boot Acknowledge is needed by ROM code) * boot_partition = 1 (Boot partition 1 enabled for boot) * partition_access = 0 (user data partition - default)
The command to select the boot partition used by ROM code on e•MMC at next reboot is:
- for boot1:
mmc partconf 1 1 1 0
- for boot2:
mmc partconf 1 1 2 0
Don't change the last parameter partition_access value if you don't manually access to the boot partition content with mmc read
or mmc write
:
- 0: user data partition (default)
- 1: boot partition 1
- 2: boot partition 2
2.2.2 ums[edit]
The e•MMC update is done with the ums
command, with the U-Boot's partition syntax[4]:
<command> <interface> [devnum][.hwpartnum][:partnum|#partname]
For example, the The exported e•MMC block device is mounted on the Linux PC as a block device named sd<X> and the GPT partitions are exported by sd<X><n> where <X> is the ID of the device starting at a and <n> the ID of the partition.
In the next example we assume <X> = a, so the block device e•MMC available in /dev/sda but this value need to be verified on your PC.
boot partitions
To update FSBL=TF-A in the boot1 HW partition.
ums 0 mmc 1.1 UMS: LUN 0, dev 1, hwpart 1, sector 0x0, count 0x1000
On boot partitions, without GPT partitions, just copy TF-A binary on the block device /dev/sda exported by U-Boot.
dd if=tf-a-emmc.stm32 of=/dev/sda conv=fdatasync
For boot2, change the mmc device to 1.2.
user data partition
To export all the e•MMC in /dev/sda, including all GPT partitions in /dev/sdaN:
ums 0 mmc 1
And copy the FIP binary in the first partition of this block device availalbe in /dev/sda1:
dd if=fip.bin of=/dev/sda1 conv=fdatasync
You can also export only the first GPT partition ("fip" partition index is 1) in /dev/sda:
ums 0 mmc 1:1 dd if=fip.bin of=/dev/sda conv=fdatasync
3 References[edit]
Please refer to the following links for additional information:
This page explains how to manually update the bootloaders binary (including [[U-Boot_overview|U-Boot]] and [[TF-A_overview|TF-A]]) on an SD card or on the ''e''•MMC. == To update an SD card with the Linux dd command == When a Linux console has access to the SD card device partitions: * on a Linux PC ** with a card reader of this PC ** through a USB connection to the target and the [[How to use USB mass storage in U-Boot|<code>ums</code> command]] executed on a U-Boot console * on target, with Linux console. [[STM32MP15_Flash_mapping#SD_card_memory_mapping|The 3 first GPT partitions on the SD card]] are: # FSBL1 # FSBL2 # FIP See [[Boot_chain_overview]] for the bootloader definitions. You can use the Linux <code>dd</code> command to copy the FSBL and SSBL directly to the correct partition: {{PC$}} dd if={{HighlightParam|<file>}} of=/dev/{{HighlightParam|<dev>}} conv={{HighlightParam|fdatasync}} {{HighlightParam|<dev>}} is: * mmcblk{{Highlight|<X>}}p{{Highlight|<n>}}: PC-embedded card reader case or target Linux console * sd{{Highlight|<X>}}{{Highlight|<n>}}: USB-connected SD card reader case where {{Highlight|<X>}} is the ID of the device, and {{Highlight|<n>}} the ID of the partition. Note: the dd option {{HighlightParam|conv}}={{HighlightParam|fdatasync}} is used to force synchronous copying. === U-Boot environment === The U-Boot environment is saved at the end of the U-Boot partition, named "fip": ID = {{HighlightParam|3}}. To clear this environment, erase the U-Boot partition before any update; for example, by writing 0 to this partition: {{PC$}} dd if=/dev/zero of=/dev/mmcblk{{Highlight|<X>}}p{{HighlightParam|3}} conv=fdatasync {{PC$}} dd if=/dev/zero of=sd{{Highlight|<X>}}{{HighlightParam|3}} conv=fdatasync === SD card update example === The internal card reader is /dev/mmcblk0 or for a target Linux console, GPT partition <n> is {{HighlightParam|/dev/mmcblk0}}p<n>: {{PC$}} dd if={{HighlightParam|tf-a-sdcard.stm32}} of={{HighlightParam|/dev/mmcblk0}}p1 conv=fdatasync {{PC$}} dd if={{HighlightParam|tf-a-sdcard.stm32}} of={{HighlightParam|/dev/mmcblk0}}p2 conv=fdatasync {{PC$}} dd if=/dev/zero of={{HighlightParam|/dev/mmcblk0}}p3 conv=fdatasync {{PC$}} dd if={{HighlightParam|fip.bin}} of={{HighlightParam|/dev/mmcblk0}}p3 conv=fdatasync Alternatively, with U-Boot console, dev = {{Highlight|0}} (SD card device on ST Microelectronics board), GPT partition <n> is {{HighlightParam|/dev/sda}}<n>: {{Board$}} mmc dev {{Highlight|0}} {{Board$}} ums 0 mmc {{Highlight|0}} {{PC$}} dd if={{HighlightParam|tf-a-sdcard.stm32}} of={{HighlightParam|/dev/sda}}1 conv=fdatasync {{PC$}} dd if={{HighlightParam|tf-a-sdcard.stm32}} of={{HighlightParam|/dev/sda}}2 conv=fdatasync {{PC$}} dd if=/dev/zero of={{HighlightParam|/dev/sda}}3 conv=fdatasync {{PC$}} dd if={{HighlightParam|fip.bin}} of={{HighlightParam|/dev/sda}}3 conv=fdatasync === SD card update example with SPL as FSBL === The USB card reader is /dev/sdb, GPT partition <n> is {{HighlightParam|/dev/sdb<n>}}: {{PC$}} dd if={{HighlightParam|u-boot-spl.stm32}} of={{HighlightParam|/dev/sdb1}} conv=fdatasync {{PC$}} dd if={{HighlightParam|u-boot-spl.stm32}} of={{HighlightParam|/dev/sdb2}} conv=fdatasync {{PC$}} dd if=/dev/zero of={{HighlightParam|/dev/sdb3}} conv=fdatasync {{PC$}} dd if={{HighlightParam|u-boot.img}} of={{HighlightParam|/dev/sdb3}} conv=fdatasync == Update of ''e''•MMC with the Linux dd command == The same command, <code>dd</code>, can be used to update [[STM32MP15_Flash_mapping#eMMC_memory_mapping|''e''•MMC memory mapping]]: * SSBL U-Boot is the first GPT partition in the ''e''•MMC user area * FSBL = TF-A (or SPL) is saved at the beginning of the ''e''•MMC boot partition The user needs to select the ''e''•MMC hardware partition to update: user data, boot1, or boot2. === On a Linux console === If dev = {{Highlight|mmcblk1}} for ''e''•MMC device (default on ST Microelectronics board) The boot partitions are available in /dev/{{Highlight|mmcblk1}}{{HighlightParam|boot0}} and /dev/{{Highlight|mmcblk1}}{{HighlightParam|boot1}} <ref>https://www.kernel.org/doc/Documentation/mmc/mmc-dev-parts.txt</ref>. The user perhaps needs to allow access, for example with: {{Board$}} echo 0 > /sys/class/block/{{Highlight|mmcblk1}}{{HighlightParam|boot0}}/force_ro The mmc tools allow the boot partition to be selected <ref>https://manpages.debian.org/buster/mmc-utils/mmc.1.en.html</ref>. The STM32MP15x ROM code requires: * <send_ack> =1 * the eMMC boot configuration is: 1 wire configuration and 25 MHz, it is done with the command: {{Board$}} mmc bootbus set single_backward x1 x1 dev/{{Highlight|mmcblk1}} To update TF-A in boot1 and select this boot partition: {{Board$}} dd if={{HighlightParam|tf-a-emmc.stm32}} of=/dev/{{Highlight|mmcblk1}}{{HighlightParam|boot0}} conv=fdatasync {{Board$}} mmc bootpart enable {{HighlightParam|1}} 1 /dev/{{Highlight|mmcblk1}} To update TF-A in boot2 and select this boot partition: {{Board$}} dd if={{HighlightParam|tf-a-emmc.stm32}} of=/dev/{{Highlight|mmcblk1}}{{HighlightParam|boot1}} conv=fdatasync {{Board$}} mmc bootpart enable {{HighlightParam|2}} 1 /dev/{{Highlight|mmcblk1}} To update U-Boot in the first GPT partition: {{Board$}} dd if=/dev/zero of=/dev/{{Highlight|mmcblk1}}{{HighlightParam|p1}} conv=fdatasync {{Board$}} dd if={{HighlightParam|fip.bin}} of=/dev/{{Highlight|mmcblk1}}{{HighlightParam|p1}} conv=fdatasync See also <ref>https://www.emcraft.com/som/stm32mp1/booting-linux-from-emmc</ref>. === On a U-Boot console === Before the first boot, select the ''e''•MMC correct boot configuration (1 wire, 25 MHz) with the command: {{Board$}} mmc bootbus {{HighlightParam|1}} 0 0 0 ==== mmc partconf ==== The targeted ''e''•MMC HW partition is selected in U-Boot by the command <code>mmc partconf</code>: {{Board$}} help mmc ... mmc bootbus dev boot_bus_width reset_boot_bus_width boot_mode - Set the BOOT_BUS_WIDTH field of the specified device mmc bootpart-resize <dev> <boot part size MB> <RPMB part size MB> - Change sizes of boot and RPMB partitions of specified device mmc partconf dev [boot_ack boot_partition {{HighlightParam|partition_access}}] - Show or change the bits of the PARTITION_CONFIG field of the specified device For example: * dev = {{Highlight|1}} (''e''•MMC device on ST Microelectronics board) * boot_ack=1 (Boot Acknowledge is needed by ROM code) * boot_partition = {{HighlightParam|1}} (Boot partition 1 enabled for boot) * partition_access = 0 (user data partition - default) The command to '''select the boot partition used by ROM code''' on ''e''•MMC at next reboot is: * for {{Highlight|boot1}}: {{Board$}} mmc partconf {{Highlight|1}} 1 {{HighlightParam|1}} 0 * for {{Highlight|boot2}}: {{Board$}} mmc partconf {{Highlight|1}} 1 {{HighlightParam|2}} 0 Don't change the last parameter {{HighlightParam|partition_access}} value if you don't manually access to the boot partition content with <code>mmc read</code> or <code>mmc write</code>: * {{HighlightParam|0}}: user data partition (default) * {{HighlightParam|1}}: boot partition 1 * {{HighlightParam|2}}: boot partition 2 ==== ums ==== The ''e''•MMC update is done with the [[How to use USB mass storage in U-Boot|<code>ums</code> command]], with the U-Boot's partition syntax<ref>https://u-boot.readthedocs.io/en/latest/usage/partitions.html</ref>:<command> <interface> [devnum][.hwpartnum][:partnum|#partname] For example, the The exported ''e''•MMC block device is mounted on the Linux PC as {{HighlightParam|/dev/sda}}a block device named sd{{Highlight|<X>}} and the GPT partitions are exported by sd{{Highlight|<X>}}{{Highlight|<n>}} where {{Highlight|<X>}} is the ID of the device starting at '''a''' and {{Highlight|<n>}} the ID of the partition. In the next example we assume {{Highlight|<X>}} = '''a''', so the block device ''e''•MMC available in {{HighlightParam|/dev/sda}} but this value need to be verified on your PC. '''boot partitions''' To update FSBL=TF-A in the {{HighlightParam|boot1}} HW partition. {{Board$}} ums 0 mmc {{Highlight|1}}.{{HighlightParam|1}} UMS: LUN 0, dev {{Highlight|1}}, hwpart {{HighlightParam|1}}, sector 0x0, count 0x1000 On boot partitions, without GPT partitions, just copy TF-A binary on the block device {{HighlightParam|/dev/sda}} exported by U-Boot. {{PC$}} dd if=tf-a-emmc.stm32 of={{HighlightParam|/dev/sda}} conv=fdatasync For {{HighlightParam|boot2}}, change the mmc device to {{Highlight|1}}.{{HighlightParam|2}}. '''user data partition''' To export all the ''e''•MMC in {{HighlightParam|/dev/sda}}, including all GPT partitions in {{HighlightParam|/dev/sda}}N: {{Board$}} ums 0 mmc {{Highlight|1}} And copy the FIP binary in the first partition of this block device availalbe in {{HighlightParam|/dev/sda}}{{Highlight|1}}: {{PC$}} dd if={{HighlightParam|fip.bin}} of={{HighlightParam|/dev/sda}}{{Highlight|1}} conv=fdatasync You can also export only the first GPT partition ("fip" partition index is {{Highlight|1}}) in {{HighlightParam|/dev/sda}}: {{Board$}} ums 0 mmc {{Highlight|1}}:{{Highlight|1}} {{PC$}} dd if={{HighlightParam|fip.bin}} of={{HighlightParam|/dev/sda}} conv=fdatasync ==References== Please refer to the following links for additional information: <references /> <noinclude> [[Category:How to populate boards]] {{PublicationRequestId | 16075 | 2020-05-12}}</noinclude>
Line 134: | Line 134: | ||
<command> <interface> [devnum][.hwpartnum][:partnum|#partname] |
<command> <interface> [devnum][.hwpartnum][:partnum|#partname] |
||
− | + |
The exported ''e''•MMC is mounted on the Linux PC as a block device named sd{{Highlight|<X>}} and the GPT partitions are exported by sd{{Highlight|<X>}}{{Highlight|<n>}} where {{Highlight|<X>}} is the ID of the device starting at '''a''' and {{Highlight|<n>}} the ID of the partition.
|
|
+ | |||
+ |
In the next example we assume {{Highlight|<X>}} = '''a''', so the block device ''e''•MMC available in {{HighlightParam|/dev/sda}} but this value need to be verified on your PC. |
||
'''boot partitions''' |
'''boot partitions''' |
||
Line 152: | Line 154: | ||
{{Board$}} ums 0 mmc {{Highlight|1}} |
{{Board$}} ums 0 mmc {{Highlight|1}} |
||
− | And copy the FIP binary in the first partition of block device |
+ | And copy the FIP binary in the first partition of this block device: |
{{PC$}} dd if={{HighlightParam|fip.bin}} of={{HighlightParam|/dev/sda}}{{Highlight|1}} conv=fdatasync |
{{PC$}} dd if={{HighlightParam|fip.bin}} of={{HighlightParam|/dev/sda}}{{Highlight|1}} conv=fdatasync |
||