Difference between revisions of "How to create your own STM32MPU distribution for Android"

[quality revision] [quality revision]
m (Bootloaders)
m (Bootloaders)
 

This article explains how you can create your own STM32MPU distribution for Android (adapted to your device) starting from an existing one based on STMicroelectronics reference boards.

It is performed in several steps:
1- Create your own device directory, and configure it depending on your device capability
2- Customize the <STM32Series> setup
3- Customize the <STM32Series> associated BSP (TF-A, U-Boot, OP-TEE, Linux)
4- Build your distribution
5- Flash your distribution
6- Debug your distribution

It is also possible to create your own device structure, getting back only the required <STM32Series> associated BSP (TF-A, U-Boot, OP-TEE or/and Linux kernel). For that purpose refer directly to the chapter Customize the BSP.

It is intended for Distribution Package users.

1 Prerequisites[edit]

The environment used must be installed using the right Distribution Package for your selected microprocessor device. See Distribution_Package to allow understanding how to get back the referenced distribution.

The STM32CubeProgrammer must be installed.

2 Create your device[edit]

You need to create your device folder in the Android distribution tree with the name of your device in device/stm/<STM32Series>/<your device name>.

Once created, you must put all necessary configuration files dedicated to your device, like it is done for STMicroelectronics reference <BoardId>.

  • MakeFiles[1]
    • device.mk: declares the files and modules needed for the device
    • aosp_<your device name>.mk: creates a specific product definition makefile
    • AndroidProducts.mk: points to the products makefiles aosp_<your device name>.mk
    • BoardConfig.mk: contains board-specific configurations


  • Overlays: some overlays need to be adapt to match your device configuration especially frameworks/base/core/res/res/values/config.xml.. They must be added in device/stm/<STM32Series>/<your device name>/overlay

3 Customize the distribution setup[edit]

3.1 Adapt the Android distribution[edit]

A mechanism is in place to select required modules version and potentially apply some patches directly to the Android distribution source files.

It is recommended to take a look at the list of modifications performed. All explanations are available in Modify Android distribution chapter.

3.2 Adapt the flash layout[edit]

A configuration file is used to configure the layout. It is recommended to take a look at the current layout configuration and adapt it if needed.

All explanations are available in Layout configuration chapter.

3.3 Execute the setup[edit]

PC $> source ./build/envsetup.sh
PC $> <STM32Series>setup

The <STM32Series>setup (ex: stm32mp1setup for STM32MP1 series) script must be executed only once.

During the distribution setup, the required graphics libraries are loaded.

4 Customize the BSP[edit]

You can change various elements to customize the BSP to match your device.

Info white.png Information
Every scripts used below need to be configured for your device.

You need to change on every build_xxxx (available in device/stm/<STM32Series>-xxxx/source directory) the values of the board name list BOARD_NAME_LIST with your device name and the associated board flavour list BOARD_FLAVOUR_LIST which are used to select the device tree (naming convention: <STM32Series>-<board flavour>)

4.1 Bootloaders[edit]

If you want to use the same bootloaders as on STMicroelectronics reference board (TF-A and U-Boot), you have first to load the source (please refer to Load the bootloader sources chapter).


You can update the TF-A and U-boot with your own device tree (it is possible to use the STM32CubeMX tool to help you creating it):

  • TF-A device trees are available in device/stm/<STM32Series>-bootloader/tf-a-<STM32Series>/fdts/ directory
  • U-Boot device trees are available in device/stm/<STM32Series>-bootloader/u-boot-<STM32Series>/arch/arm/dts/ directory

You can adapt the used U-boot defconfig available in device/stm/<STM32Series>-bootloader/u-boot-<STM32Series>/configs/:

  • <STM32Series>_trusted_defconfig if you do not need any trusted execution environment

You have then to rebuild the bootloaders (please refer to Build the bootloaders chapter).

4.2 TEE[edit]

If you want to use the same trusted execution environment (OP-TEE), you have first to load the source (please refer to Load OP-TEE sources chapter).


You can update OP-TEE OS with your own device tree (it is possible to use the STM32CubeMX tool to help you creating it).

OP-TEE OS device trees are available in device/stm/<STM32Series>-tee/optee_os-<STM32Series>/core/arch/arm/fdts/ directory.

You have then to rebuild the trusted execution environment (please refer to Build OP-TEE OS chapter).

You can also build the list of trusted applications required (please refer to Build Trusted Applications chapter).

4.3 Kernel[edit]

You can update the Linux kernel configuration, please refer to How to customize kernel for Android.

5 Build your distribution[edit]

To be able to build your customized distribution you need to

PC $> lunch aosp_<your device>-<build_type>

Available build_type values:

  • user: to generate an end-user production image;
  • userdebug: similar to an user build but with root access and debug capabilities;
  • eng: development configuration with additional debugging tools.

Then build it

PC $> make -j

For more details please have a look at How to build STM32MPU distribution for Android.

6 Flash your distribution[edit]

From this stage you can flash the generated images on your device (please refer to Flashing the built image).

7 Debug your distribution[edit]

From this stage, there are various ways to debug your device (please refer to STM32MP1 Platform trace and debug environment overview for Android).

8 References[edit]


This article explains how you can create your own STM32MPU distribution for Android (adapted to your device) starting from an existing one based on STMicroelectronics reference boards.

It is performed in several steps:<br>

1- Create your own device directory, and configure it depending on your device capability<br>

2- Customize the {{HighlightParam|<STM32Series>}} setup<br>

3- Customize the {{HighlightParam|<STM32Series>}} associated BSP (TF-A, U-Boot, OP-TEE, Linux)<br>

4- Build your distribution<br>

5- Flash your distribution<br>

6- Debug your distribution<br>


It is also possible to create your own device structure, getting back only the required {{HighlightParam|<STM32Series>}} associated BSP (TF-A, U-Boot, OP-TEE or/and Linux kernel). For that purpose refer directly to the chapter [[#Customize the BSP|Customize the BSP]].

It is intended for Distribution Package users.

== Prerequisites ==

The environment used must be installed using the right Distribution Package for your selected microprocessor device.
See [[Which_STM32MPU_Embedded_Software_Package_for_Android_better_suits_your_needs#Distribution_Package | Distribution_Package]] to allow understanding how to get back the referenced distribution.

The [[STM32CubeProgrammer]] must be installed.

== Create your device ==

You need to create your device folder in the Android distribution tree with the name of your device in <code>device/stm/{{HighlightParam|''<STM32Series>''}}/{{HighlightParam|''<your device name>''}}</code>.

Once created, you must put all necessary configuration files dedicated to your device, like it is done for STMicroelectronics reference <BoardId>.

*MakeFiles<ref>https://source.android.com/setup/develop/new-device</ref>

**<code>device.mk</code>: declares the files and modules needed for the device
**<code>aosp_{{HighlightParam|''<your device name>''}}.mk</code>: creates a specific product definition makefile
**<code>AndroidProducts.mk</code>: points to the products makefiles <code>aosp_{{HighlightParam|''<your device name>''}}.mk</code>

**<code>BoardConfig.mk</code>: contains board-specific configurations

*Overlays: some overlays need to be adapt to match your device configuration especially <code>frameworks/base/core/res/res/values/config.xml.</code>. They must be added in <code>device/stm/{{HighlightParam|''<STM32Series>''}}/{{HighlightParam|''<your device name>''}}/overlay</code>


*Configurations: depending on your device some configurations must be changed like for Bluetooth, WiFi, audio etc... Please have a look at [[How to customize the STM32MPU distribution for Android]].

== Customize the distribution setup ==

=== Adapt the Android distribution ===

A mechanism is in place to select required modules version and potentially apply some patches directly to the Android distribution source files.

It is recommended to take a look at the list of modifications performed.
All explanations are available in [[How to customize the STM32MPU distribution for Android#Modification of the Android distribution|Modify Android distribution]] chapter.

=== Adapt the flash layout ===

A configuration file is used to configure the layout. It is recommended to take a look at the current layout configuration and adapt it if needed.

All explanations are available in [[How to customize the STM32MPU distribution for Android#Layout configuration | Layout configuration]] chapter.

=== Execute the setup ===

 {{PC$}} source ./build/envsetup.sh
 {{PC$}} {{HighlightParam|''<STM32Series>''}}setup

The <code>{{HighlightParam|<STM32Series>}}setup</code> (ex: stm32mp1setup for STM32MP1 series) script must be executed only once.

During the distribution setup, the required graphics libraries are loaded.

== Customize the BSP ==

You can change various elements to customize the BSP to match your device. 

{{Info| Every scripts used below need to be configured for your device. 

You need to change on every <code>build_xxxx</code> (available in <code>device/stm/{{HighlightParam|''<STM32Series>''}}-xxxx/source</code> directory) the values of the board name list <code>BOARD_NAME_LIST</code> with your device name and the associated board flavour list <code>BOARD_FLAVOUR_LIST</code> which are used to select the device tree (naming convention: {{HighlightParam|''<STM32Series>''}}-{{HighlightParam|''<board flavour>''}})}}

=== Bootloaders ===

If you want to use the same bootloaders as on STMicroelectronics reference board (TF-A and U-Boot), you have first to load the source (please refer to [[How to build bootloaders for Android#Load the bootloader sources | Load the bootloader sources]] chapter).

You can update the TF-A and U-boot with your own device tree (it is possible to use the [[STM32CubeMX]] tool to help you creating it):
* TF-A device trees are available in <code>device/stm/{{HighlightParam|''<STM32Series>''}}-bootloader/tf-a-{{HighlightParam|''<STM32Series>''}}/fdts/</code> directory
* U-Boot device trees are available in <code>device/stm/{{HighlightParam|''<STM32Series>''}}-bootloader/u-boot-{{HighlightParam|''<STM32Series>''}}/arch/arm/dts/</code> directory

You can adapt the used U-boot defconfig available in <code>device/stm/{{HighlightParam|''<STM32Series>''}}-bootloader/u-boot-{{HighlightParam|''<STM32Series>''}}/configs/</code>:
* {{HighlightParam|<STM32Series>}}_trusted_defconfig if you do not need any trusted execution environment

You have then to rebuild the bootloaders (please refer to [[How to build bootloaders for Android#Build the bootloaders | Build the bootloaders]] chapter).

=== TEE ===
If you want to use the same trusted execution environment (OP-TEE), you have first to load the source (please refer to [[How to build TEE for Android#Load the TEE sources | Load OP-TEE sources]] chapter).

You can update OP-TEE OS with your own device tree (it is possible to use the [[STM32CubeMX]] tool to help you creating it).

OP-TEE OS device trees are available in <code>device/stm/{{HighlightParam|''<STM32Series>''}}-tee/optee_os-{{HighlightParam|''<STM32Series>''}}/core/arch/arm/fdts/</code> directory.

You have then to rebuild the trusted execution environment (please refer to [[How to build TEE for Android#Build the TEE | Build OP-TEE OS]] chapter).

You can also build the list of trusted applications required (please refer to [[How to build TEE for Android#Build Trusted Applications | Build Trusted Applications]] chapter).

=== Kernel ===

You can update the Linux kernel configuration, please refer to [[How to customize kernel for Android]].

== Build your distribution ==

To be able to build your customized distribution you need to
 {{PC$}} lunch aosp_{{HighlightParam|''<your device>''}}-{{HighlightParam|''<build_type>''}}
Available <code>build_type</code> values:
*<code>user</code>: to generate an end-user production image;
*<code>userdebug</code>: similar to an <code>user</code> build but with root access and debug capabilities;
*<code>eng</code>: development configuration with additional debugging tools.

Then build it
 {{PC$}} make -j

For more details please have a look at [[How to build STM32MPU distribution for Android]].

== Flash your distribution ==

From this stage you can flash the generated images on your device (please refer to [[STM32MP1 Distribution Package for Android#Flashing the built image|Flashing the built image]]).

== Debug your distribution ==

From this stage, there are various ways to debug your device (please refer to [[STM32MP1 Platform trace and debug environment overview for Android]]).

== References ==<references />

<noinclude>

[[Category:How to Android]]
[[Category:Android]]
{{PublicationRequestId |13268 | 2019-09-12}}</noinclude>
(No difference)