Difference between revisions of "How to create an SDK for OpenSTLinux distribution"

[quality revision] [quality revision]
m
 

Template:ArticleMainWriter Template:ReviewersList Template:ArticleApprovedVersion

When an OpenSTLinux distribution has been modified, it is pertinent to build a new software development package that integrates the modifications, and to redistribute this SDK to developers (see SDK development cycle model).

Contents

1 Prerequisites

  • 2 SDK generation
  • 3 To go further: eSDK generation
  • 4 Reference list
  • 1 Prerequisites[edit]

    The Distribution Package relative to your STM32 microprocessor Series is installed: Category:Distribution Package.

    On the installation:

    • some pieces of software might have been modified or integrated
    • the build environment script has been executed
    • the selected image has been rebuilt

    2 SDK generation[edit]

    The OpenEmbedded build system uses BitBake to generate the software development package (SDK) installation script.

    For more information about the SDK, see the SDK for OpenSTLinux distribution article.

    Standard SDK generation
    Source: Yocto Project[1]

    The do_populate_sdk task helps to create the standard SDK and handles two parts: a target part and a host part. The target part is built for the target hardware and includes libraries and headers. The host part is the part of the SDK that runs on the host machine.

    • Check that the build environment script has been executed, and that the current directory is the build directory of the OpenSTLinux distribution (for example, openstlinux-4.1921-thud-mp1-19-10-0911-17/build-openstlinuxweston-stm32mp1')
    • Generate the SDK installation files (including the installation script) for a standard SDK with the following command :
     bitbake -c populate_sdk <image>
    
    Where:
    <image> Image name; example:
    • st-image-weston
    Example:
    bitbake -c populate_sdk st-image-weston
    • The SDK installation files (<image>-<distro>-<machine>-<host machine>-toolchain-<Yocto release>+-snapshot.*) are written to the deploy/sdk directory inside the build directory build-<distro>-<machine> as shown in the figure above
    Where:
    <host machine> Host machine on which the SDK is generated
    • x86_64 (64-bit host machine; this is the only supported value)
    <Yocto release> Release number of the Yocto Project; example:
    • 23.6 1.11 (aka thuddunfell)
    Example
     ls tmp-glibc/deploy/sdk/
    st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-23.6-snapshot.1.11-openstlinux-5.10-dunfell-mp1-21-11-17.host.manifest
    st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-23.6-snapshot.1.11-openstlinux-5.10-dunfell-mp1-21-11-17.license
    st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-3.1.11-openstlinux-5.10-dunfell-mp1-21-11-17.html
    st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-3.1.11-openstlinux-5.10-dunfell-mp1-21-11-17.sh
    st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-23.6-snapshot.1.11-openstlinux-5.10-dunfell-mp1-21-11-17.target.manifest
    st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-23.6-snapshot.1.11-openstlinux-5.10-dunfell-mp1-21-11-17.testdata.json
    

    The main final output is the cross-development toolchain installation script (.sh file), which includes the environment setup script.
    Note that several OpenEmbedded variables exist that help configure these files. The following list shows the variables associated with a standard SDK:

        DEPLOY_DIR: points to the deploy directory.
        SDKMACHINE: specifies the architecture of the machine on which the cross-development tools are run to create packages for the target hardware.
        SDKIMAGE_FEATURES: lists the features to include in the "target" part of the SDK.
        TOOLCHAIN_HOST_TASK: lists packages that make up the host part of the SDK (that is, the part that runs on the SDKMACHINE). This variable allows packages other than the default ones to be added.
        TOOLCHAIN_TARGET_TASK: lists packages that make up the target part of the SDK (that is, the part built for the target hardware).
        SDKPATH: Defines the default SDK installation path offered by the installation script.
    

    3 To go further: eSDK generation[edit]

    The OpenEmbedded build system uses BitBake to generate the extensible software development package (eSDK) installation script. The eSDK is a SDK in which user can execute Yocto commands, such as devtool. For more information about eSDK, please refer to Yocto SDK manual [2].

    The do_populate_sdk_ext task helps to create the eSDK. You can customize a little bit the eSDK, to add or not the toolchain inside and to add or not all build artifacts inside (please note that the eSDK will be big in that case, more than 1GB).

    • Generate the eSDK installation files (including the installation script) for a extensible SDK with the following command :
    bitbake -c populate_sdk_ext <image>
    Where:
    <image> Image name; example:
    • st-image-weston
    Example:
    bitbake -c populate_sdk st-image-weston
    • The eSDK installation files (<image>-<distro>-<machine>-<host machine>-toolchain-ext-<Yocto release>-snapshot.*) are written to the deploy/sdk directory inside the build directory build-<distro>-<machine> as shown in the figure above
    Where:
    <host machine> Host machine on which the eSDK is generated
    • x86_64 (64-bit host machine; this is the only supported value)
    <Yocto release> Release number of the Yocto Project; example:
    • 2.6 (aka thud)
    Example
    ls tmp-glibc/deploy/sdk/ st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-ext-2.6-snapshot.host.manifest st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-ext-2.6-snapshot.sh st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-ext-2.6-snapshot.target.manifest st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-ext-2.6-snapshot.testdata.json

    The main final output is the cross-development toolchain installation script (.sh file), which includes the environment setup script.
    Note that several OpenEmbedded variables exist that help configure these files. Variables used to configure standard SDK also impact eSDK and following are specific to the eSDK:

    
        SDK_EXT_TYPE: Controls whether or not shared state artifacts are copied into the extensible SDK.
        SDK_INCLUDE_TOOLCHAIN : Include or not the toolchain in the extensible SDK.
    
    

    4 Reference list[edit]


    <noinclude>
    
    {{ArticleMainWriter | Jean-ChristopheT}}
    {{ReviewersList | NathalieS, BernardP, RomualdJ, DenisH}}
    {{ArticleApprovedVersion | Jean-ChristopheT | NathalieS(29May'18,Done), BernardP (24 May'18, PASS), RomualdJ (Passed, 1Jun'18), DenisH (Passed, 30May'18) | No previous approved version | PhilipS - 4Jun'18 - 7651 | 20Jun'18}}
    
    [[Category:How to build software]]</noinclude>
    
    When an OpenSTLinux distribution has been modified, it is pertinent to build a new software development package that integrates the modifications, and to redistribute this SDK to developers (see [[SDK for OpenSTLinux distribution#SDK development cycle model|SDK development cycle model]]).
    
    ==Prerequisites==
    The Distribution Package relative to your STM32 microprocessor Series is installed: [[:Category:Distribution Package]].
    
    On the installation:
    * some pieces of software might have been modified or integrated
    * the build environment script has been executed
    * the selected image has been rebuilt
    
    ==SDK generation==
    The OpenEmbedded build system uses BitBake to generate the software development package (SDK) installation script. 
    
    For more information about the SDK, see the [[SDK for OpenSTLinux distribution]] article.
    
    [[File: Standard_SDK_generation.png|thumb|upright=4|center|link=|Standard SDK generation<br>Source: Yocto Project<ref>http://www.yoctoproject.org/documentation</ref>]]
    
    The ''do_populate_sdk'' task helps to create the standard SDK and handles two parts: a target part and a host part. The target part is built for the target hardware and includes libraries and headers. The host part is the part of the SDK that runs on the host machine.
    
    * Check that the build environment script has been executed, and that the current directory is the build directory of the OpenSTLinux distribution (for example, ''openstlinux-4.19-thud-mp1-19-10-0921-11-17/build-openstlinuxweston-stm32mp1')
    
    * Generate the SDK installation files (including the installation script) for a standard SDK with the following command :
     {{PC$}} bitbake -c populate_sdk <image>
    
    : Where:
    :{|
    | <image> || Image name; example:
    * st-image-weston
    |}
    : Example:
    : {{PC$}} bitbake -c populate_sdk st-image-weston
    
    * The SDK installation files (''<image>-<distro>-<machine>-<host machine>-toolchain-<Yocto release>+-snapshot.*'') are written to the ''deploy/sdk'' directory inside the build directory ''build-<distro>-<machine>'' as shown in the figure above
    : Where:
    :{|
    | <host machine> || Host machine on which the SDK is generated
    * x86_64	(64-bit host machine; this is the only supported value)
    |-
    | <Yocto release> || Release number of the Yocto Project; example:
    * 2.63.1.11		(aka thuddunfell)
    |}
    
    : Example
     {{PC$}} ls tmp-glibc/deploy/sdk/
     st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-2.6-snapshot.3.1.11-openstlinux-5.10-dunfell-mp1-21-11-17.host.manifest
     st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-2.6-snapshot.3.1.11-openstlinux-5.10-dunfell-mp1-21-11-17.license
     st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-3.1.11-openstlinux-5.10-dunfell-mp1-21-11-17.html
     st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-3.1.11-openstlinux-5.10-dunfell-mp1-21-11-17.sh
     st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-2.6-snapshot.3.1.11-openstlinux-5.10-dunfell-mp1-21-11-17.target.manifest
     st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-2.6-snapshot.3.1.11-openstlinux-5.10-dunfell-mp1-21-11-17.testdata.json
    
    The main final output is the cross-development toolchain installation script (''.sh'' file), which includes the environment setup script. <br>
    
    Note that several OpenEmbedded variables exist that help configure these files. The following list shows the variables associated with a standard SDK:<pre>
    
        DEPLOY_DIR: points to the deploy directory.
        SDKMACHINE: specifies the architecture of the machine on which the cross-development tools are run to create packages for the target hardware.
        SDKIMAGE_FEATURES: lists the features to include in the "target" part of the SDK.
        TOOLCHAIN_HOST_TASK: lists packages that make up the host part of the SDK (that is, the part that runs on the SDKMACHINE). This variable allows packages other than the default ones to be added.
        TOOLCHAIN_TARGET_TASK: lists packages that make up the target part of the SDK (that is, the part built for the target hardware).
        SDKPATH: Defines the default SDK installation path offered by the installation script.</pre>
    
    
    ==To go further: eSDK generation==
    The OpenEmbedded build system uses BitBake to generate the extensible software development package (eSDK) installation script. The eSDK is a SDK in which user can execute Yocto commands, such as devtool. For more information about eSDK, please refer to Yocto SDK manual <ref>https://www.yoctoproject.org/docs/2.6.3/sdk-manual/sdk-manual.html</ref>.
    
    The ''do_populate_sdk_ext'' task helps to create the eSDK.
    You can customize a little bit the eSDK, to add or not the toolchain inside and to add or not all build artifacts inside (please note that the eSDK will be big in that case, more than 1GB).
    
    * Generate the eSDK installation files (including the installation script) for a extensible SDK with the following command :
     {{PC$}} bitbake -c populate_sdk_ext <image>
    
    : Where:
    :{|
    | <image> || Image name; example:
    * st-image-weston
    |}
    : Example:
    : {{PC$}} bitbake -c populate_sdk st-image-weston
    
    * The eSDK installation files (''<image>-<distro>-<machine>-<host machine>-toolchain-ext-<Yocto release>-snapshot.*'') are written to the ''deploy/sdk'' directory inside the build directory ''build-<distro>-<machine>'' as shown in the figure above
    : Where:
    :{|
    | <host machine> || Host machine on which the eSDK is generated
    * x86_64	(64-bit host machine; this is the only supported value)
    |-
    | <Yocto release> || Release number of the Yocto Project; example:
    * 2.6		(aka thud)
    |}
    
    : Example
     {{PC$}} ls tmp-glibc/deploy/sdk/
     st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-ext-2.6-snapshot.host.manifest
     st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-ext-2.6-snapshot.sh
     st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-ext-2.6-snapshot.target.manifest
     st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-ext-2.6-snapshot.testdata.json
    
    The main final output is the cross-development toolchain installation script (''.sh'' file), which includes the environment setup script. <br>
    
    Note that several OpenEmbedded variables exist that help configure these files. Variables used to configure standard SDK also impact eSDK and following are specific to the eSDK:<pre>
    
        SDK_EXT_TYPE: Controls whether or not shared state artifacts are copied into the extensible SDK.
        SDK_INCLUDE_TOOLCHAIN : Include or not the toolchain in the extensible SDK.</pre>
    
    
    ==Reference list==<references />Reference list==<references />
    
    <noinclude>
    
    [[Category:How to build software]]
    {{PublicationRequestId | 7651 | 2018-06-04 | PhilipS}}</noinclude>
    (10 intermediate revisions by 4 users not shown)
    Line 1: Line 1:
    <noinclude>
     
    {{ArticleMainWriter | Jean-ChristopheT}}
     
    {{ReviewersList | NathalieS, BernardP, RomualdJ, DenisH}}
     
    {{ArticleApprovedVersion | Jean-ChristopheT | NathalieS(29May'18,Done), BernardP (24 May'18, PASS), RomualdJ (Passed, 1Jun'18), DenisH (Passed, 30May'18) | No previous approved version | PhilipS - 4Jun'18 - 7651 | 20Jun'18}}
     
     
    [[Category:How to build software]]
     
    </noinclude>
     
     
     
    When an OpenSTLinux distribution has been modified, it is pertinent to build a new software development package that integrates the modifications, and to redistribute this SDK to developers (see [[SDK for OpenSTLinux distribution#SDK development cycle model|SDK development cycle model]]).
     
    When an OpenSTLinux distribution has been modified, it is pertinent to build a new software development package that integrates the modifications, and to redistribute this SDK to developers (see [[SDK for OpenSTLinux distribution#SDK development cycle model|SDK development cycle model]]).
       
    Line 26: Line 18:
     
    The ''do_populate_sdk'' task helps to create the standard SDK and handles two parts: a target part and a host part. The target part is built for the target hardware and includes libraries and headers. The host part is the part of the SDK that runs on the host machine.
     
    The ''do_populate_sdk'' task helps to create the standard SDK and handles two parts: a target part and a host part. The target part is built for the target hardware and includes libraries and headers. The host part is the part of the SDK that runs on the host machine.
       
    * Check that the build environment script has been executed, and that the current directory is the build directory of the OpenSTLinux distribution (for example, ''openstlinux-4.19-thud-mp1-19-10-09/build-openstlinuxweston-stm32mp1')
    +
    * Check that the build environment script has been executed, and that the current directory is the build directory of the OpenSTLinux distribution (for example, ''openstlinux-21-11-17/build-openstlinuxweston-stm32mp1')
       
     
    * Generate the SDK installation files (including the installation script) for a standard SDK with the following command :
     
    * Generate the SDK installation files (including the installation script) for a standard SDK with the following command :
    Line 38: Line 30:
     
    : {{PC$}} bitbake -c populate_sdk st-image-weston
     
    : {{PC$}} bitbake -c populate_sdk st-image-weston
       
    * The SDK installation files (''<image>-<distro>-<machine>-<host machine>-toolchain-<Yocto release>+snapshot.*'') are written to the ''deploy/sdk'' directory inside the build directory ''build-<distro>-<machine>'' as shown in the figure above
    +
    * The SDK installation files (''<image>-<distro>-<machine>-<host machine>-toolchain-<Yocto release>-snapshot.*'') are written to the ''deploy/sdk'' directory inside the build directory ''build-<distro>-<machine>'' as shown in the figure above
     
    : Where:
     
    : Where:
     
    :{|
     
    :{|
    Line 45: Line 37:
     
    |-
     
    |-
     
    | <Yocto release> || Release number of the Yocto Project; example:
     
    | <Yocto release> || Release number of the Yocto Project; example:
    * 2.6 (aka thud)
    +
    * 3.1.11 (aka dunfell)
     
    |}
     
    |}
       
     
    : Example
     
    : Example
     
      {{PC$}} ls tmp-glibc/deploy/sdk/
     
      {{PC$}} ls tmp-glibc/deploy/sdk/
      st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-2.6-snapshot.host.manifest
    +
      st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-3.1.11-openstlinux-5.10-dunfell-mp1-21-11-17.host.manifest
      st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-2.6-snapshot.sh
    +
      st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-3.1.11-openstlinux-5.10-dunfell-mp1-21-11-17.license
      st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-2.6-snapshot.target.manifest
    +
    st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-3.1.11-openstlinux-5.10-dunfell-mp1-21-11-17.html
      st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-2.6-snapshot.testdata.json
    +
    st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-3.1.11-openstlinux-5.10-dunfell-mp1-21-11-17.sh
      +
      st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-3.1.11-openstlinux-5.10-dunfell-mp1-21-11-17.target.manifest
      +
      st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-3.1.11-openstlinux-5.10-dunfell-mp1-21-11-17.testdata.json
       
     
    The main final output is the cross-development toolchain installation script (''.sh'' file), which includes the environment setup script. <br>
     
    The main final output is the cross-development toolchain installation script (''.sh'' file), which includes the environment setup script. <br>
    Line 64: Line 58:
     
         TOOLCHAIN_TARGET_TASK: lists packages that make up the target part of the SDK (that is, the part built for the target hardware).
     
         TOOLCHAIN_TARGET_TASK: lists packages that make up the target part of the SDK (that is, the part built for the target hardware).
     
         SDKPATH: Defines the default SDK installation path offered by the installation script.
     
         SDKPATH: Defines the default SDK installation path offered by the installation script.
    </pre>
     
     
    ==To go further: eSDK generation==
     
    The OpenEmbedded build system uses BitBake to generate the extensible software development package (eSDK) installation script. The eSDK is a SDK in which user can execute Yocto commands, such as devtool. For more information about eSDK, please refer to Yocto SDK manual <ref>https://www.yoctoproject.org/docs/2.6.3/sdk-manual/sdk-manual.html</ref>.
     
     
    The ''do_populate_sdk_ext'' task helps to create the eSDK.
     
    You can customize a little bit the eSDK, to add or not the toolchain inside and to add or not all build artifacts inside (please note that the eSDK will be big in that case, more than 1GB).
     
     
    * Generate the eSDK installation files (including the installation script) for a extensible SDK with the following command :
     
    {{PC$}} bitbake -c populate_sdk_ext <image>
     
    : Where:
     
    :{|
     
    | <image> || Image name; example:
     
    * st-image-weston
     
    |}
     
    : Example:
     
    : {{PC$}} bitbake -c populate_sdk st-image-weston
     
     
    * The eSDK installation files (''<image>-<distro>-<machine>-<host machine>-toolchain-ext-<Yocto release>-snapshot.*'') are written to the ''deploy/sdk'' directory inside the build directory ''build-<distro>-<machine>'' as shown in the figure above
     
    : Where:
     
    :{|
     
    | <host machine> || Host machine on which the eSDK is generated
     
    * x86_64 (64-bit host machine; this is the only supported value)
     
    |-
     
    | <Yocto release> || Release number of the Yocto Project; example:
     
    * 2.6 (aka thud)
     
    |}
     
     
    : Example
     
    {{PC$}} ls tmp-glibc/deploy/sdk/
     
    st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-ext-2.6-snapshot.host.manifest
     
    st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-ext-2.6-snapshot.sh
     
    st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-ext-2.6-snapshot.target.manifest
     
    st-image-weston-openstlinux-weston-stm32mp1-x86_64-toolchain-ext-2.6-snapshot.testdata.json
     
     
    The main final output is the cross-development toolchain installation script (''.sh'' file), which includes the environment setup script. <br>
     
    Note that several OpenEmbedded variables exist that help configure these files. Variables used to configure standard SDK also impact eSDK and following are specific to the eSDK:
     
    <pre>
     
        SDK_EXT_TYPE: Controls whether or not shared state artifacts are copied into the extensible SDK.
     
        SDK_INCLUDE_TOOLCHAIN : Include or not the toolchain in the extensible SDK.
     
     
    </pre>
     
    </pre>
       
     
    ==Reference list==
     
    ==Reference list==
     
    <references />
     
    <references />
      +
      +
    <noinclude>
      +
    [[Category:How to build software]]
      +
    {{PublicationRequestId | 7651 | 2018-06-04 | PhilipS}}
      +
    </noinclude>