Approved version. Approved on: 09:45, 24 January 2020
- Last edited one year ago ago
How to control a GPIO in kernel space
Contents
1 Purpose[edit]
This article gives an example of a driver that controls GPIOs from kernel space.
Sample source files are provided as examples: kernel module (driver), device tree and Makefile.
This example is available for STM32MP15_Evaluation_boards or STM32MP15_Discovery_kits
2 Code[edit]
2.1 Objective[edit]
Sample gpiolib usage code that makes an LED blink for 20 seconds.
2.2 Device tree[edit]
dummy_device { compatible = "st,dummy"; status = "okay"; greenled-gpios = <&gpioa 14 0>; };
See GPIO_device_tree_configuration for more details of GPIO use in a device tree.
2.3 Kernel module code[edit]
#include <linux/module.h>
#include <linux/of_device.h>
#include <linux/kernel.h>
#include <linux/delay.h>
#include <linux/gpio/consumer.h>
#include <linux/platform_device.h>
struct gpio_desc *red, *green;
static int gpio_init_probe(struct platform_device *pdev)
{
int i = 0;
printk("GPIO example init\n");
/* "greenled" label is matching the device tree declaration. OUT_LOW is the value at init */
green = devm_gpiod_get(&pdev->dev, "greenled", GPIOD_OUT_LOW);
/* blink of the green led */
while (i < 10)
{
ssleep(1);
gpiod_set_value(green, 1);
ssleep(1);
gpiod_set_value(green, 0);
i++;
}
return(0);
}
static int gpio_exit_remove(struct platform_device *pdev)
{
printk("GPIO example exit\n");
return(0);
}
/* this structure does the matching with the device tree */
/* if it does not match the compatible field of DT, nothing happens */
static struct of_device_id dummy_match[] = {
{.compatible = "st,dummy"},
{/* end node */}
};
static struct platform_driver dummy_driver = {
.probe = gpio_init_probe,
.remove = gpio_exit_remove,
.driver = {
.name = "dummy_driver",
.owner = THIS_MODULE,
.of_match_table = dummy_match,
}
};
module_platform_driver(dummy_driver);
MODULE_AUTHOR("Bernard Puel");
MODULE_DESCRIPTION("Gpio example");
MODULE_LICENSE("GPL");
MODULE_ALIAS("platform:dummy_driver");
2.4 Kernel module build[edit]
See Adding_external_out-of-tree_Linux_kernel_modules for further information on module compilation.
2.5 Kernel module use[edit]
scp dummy_driver.ko root@<board ip address>:/lib/modules/
- Update dependency descriptions for loadable kernel modules, and synchronize the data on disk with memory
/sbin/depmod -a sync
- Insert the kernel module example into the Linux kernel
modprobe dummy_driver [18167.821725] dummy_driver: GPIO example init