This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Template:ArticleMainWriter Template:ArticleApprovedVersion
1 Purpose[edit source]
This article describes how to configure the Ethernet interface using the Ifconfig tool.
- Connect an Ethernet cable and enjoy
At startup SSH daemon (sshd) and ifplugd daemon are automatically launched:
- sshd (useful to perform ssh, scp)
- ifplugd detect:
- udhcpc is launched on cable detection to retrieve an IP address,
If a DHCP server is not available, one can set the Ethernet IP adress with :
ifconfig eth0 uuu.xxx.yyy.zzz
- To check if eth0 and the gateway are well configured, one can type:
ifconfig route
- In the console, a log similar to the one below should be displayed:
ifconfig eth0 Link encap:Ethernet HWaddr 00:80:E1:01:39:61 inet addr:10.48.1.172 Bcast:10.48.3.255 Mask:255.255.252.0 UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1 RX packets:18 errors:0 dropped:0 overruns:0 frame:0 TX packets:2 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:1000 RX bytes:3038 (2.9 KiB) TX bytes:684 (684.0 B) Interrupt:103 STM32MP1 # route Kernel IP routing table Destination Gateway Genmask Flags Metric Ref Use Iface default lme-gw-vl802.lm 0.0.0.0 UG 10 0 0 eth0 10.48.0.0 * 255.255.252.0 U 0 0 0 eth0