Difference between revisions of "How to configure U-Boot for your board"
[quality revision] | [quality revision] |
m
|
m (→USB OTG node: Corrected "st,stm32mp1-hsotg" in "st,stm32mp15-hsotg")
|
Applicable for | STM32MP13x lines, STM32MP15x lines |
This page explains how to configure the U-Boot source for your board.
Contents
Many existing ressources [1][2] explain the porting of U-Boot on a new board. This article only provides basic guidelines for STM32MP1 Series.
To summarize, you need to configure U-Boot for your <VENDOR> <BOARD> with the following steps:
- Add your board device tree: arch/arm/dts/<board>.dts and <board>-u-boot.dtsi.
- Create your own board support directory: board/<vendor>/<board>.
- Add TARGET_<VENDOR> _<BOARD> in Kconfig.
- Create your board defconfig: defconfig/<board>_defconfig.
- Add your configuration file : include/configs/<board>.h.
1 Device tree[edit]
Add the board device tree files <board>.dts and <board>-u-boot.dtsi in arch/arm/dts , following the steps below:
- Copy the Linux kernel device tree in the directory arch/arm/dts : <board>.dts.
- Update arch/arm/dts/Makefile to compile your device tree:
dtb-$(CONFIG_STM32MP13x) += \
<STM32MP13 board>.dtb
dtb-$(CONFIG_STM32MP15x) += \
<STM32MP15 board>.dtb
- Add a U-Boot addon device tree for your board in the arch/arm/dts directory: <board>-u-boot.dtsi
This file is automatically included during <board>.dts processing.
It includes the <STM32MP series>-u-boot.dtsi file provided by STMicroelectronics (arch/arm/dts/stm32mp13-u-boot.dtsi or arch/arm/dts/stm32mp15-u-boot.dtsi ) and add all the properties on nodes needed by U-Boot (added nodes, config nodes and u-boot,dm-pre-reloc or u-boot,dm-pre-proper attibutes as described in U-Boot overview, device tree).
At this point you can use the generic STM32 MPU defconfig with the STMicroelectronics board directory, but with your board device tree.
The board-specific features are not correctly managed, but should be sufficient for a simple board derived from STMicroelectronics designs.
You can use the STMicroelectronics code with your device tree as follows:
make stm32mp13_defconfig make DEVICE_TREE=<STM32MP13 board> all
make stm32mp15_defconfig make DEVICE_TREE=<STM32MP15 board> all
The next steps are required if the STMicroelectronics generic board does not comply with all of the expected behavioral aspects for your board (for example MAC address not located in OTP, specific PMIC, specific boot command).
1.1 Console[edit]
The U-Boot console use stdout-path
defined in the chosen
node of the Linux kernel device tree as described in the Linux kernel binding[3].
As the console is used before relocation, you must add the flags u-boot,dm-pre-reloc for each associated nodes (and sub-nodes).
For example in device tree from kernel = <board>.dts:
/ { ... chosen { stdout-path = " serial0:115200n8"; }; aliases { serial0 = &uart4; }; ... }; ... &uart4 { pinctrl-names = "default"; pinctrl-0 = <&uart4_pins_a>; status = "okay"; };
And in the U-Boot add-on file = <board>-u-boot.dtsi:
&uart4 { u-boot,dm-pre-reloc; }; &uart4_pins_a { u-boot,dm-pre-reloc; pins1 { u-boot,dm-pre-reloc; }; pins2 { u-boot,dm-pre-reloc; }; };
The variable baudrate, initialized with CONFIG_BAUDRATE value, is used to configure the desired baud rate; the default value is 115200 bauds.
An early DEBUG trace, before the device tree parsing, can be also activated with CONFIG_DEBUG_UART and board_debug_uart_init() (see U-Boot-How to debug page for details).
1.2 Config node[edit]
Some properties in the 'config' node are also used to dynamically configure the U-Boot behavior in the board device tree as follows:
- Generic U-Boot configuration: doc/device-tree-bindings/config.txt
- u-boot,mmc-env-partition = name of partition used to save U-Boot environment
- u-boot,boot-led = name of boot-progress indicator LED
- u-boot,error-led = name of error indicator LED
- Some STMicroelectronics properties:
- st,adc_usb_pd = ADC channels used to check USB power supply
- st,stm32prog-gpios = GPIO used to force STM32CubeProgrammer mode
- st,fastboot-gpios = GPIO used to force Android Fastboot mode
These parameters are managed in U-Boot generic code or in STMicroelectronics board code (in line with LEDs and buttons on STM32 MPU boards); they can only be used if your board reuses the associated code.
E.g for STM32MP15x lines , in arch/arm/dts/stm32mp157a-dk1-u-boot.dtsi , the properties are:
config { u-boot,boot-led = "heartbeat"; u-boot,error-led = "error"; u-boot,mmc-env-partition = "u-boot-env"; st,adc_usb_pd = <&adc1 18>, <&adc1 19>; st,fastboot-gpios = <&gpioa 13 GPIO_ACTIVE_LOW>; st,stm32prog-gpios = <&gpioa 14 GPIO_ACTIVE_LOW>; };
1.3 USB OTG node[edit]
The U-Boot driver for USB OTG, with the compatible st,stm32mp1stm32mp15-hsotg, does not have a full OTG support, so only the gadget is used in STM32 MPU board with drivers/usb/host/dwc2.c .
Two U-Boot specific properties are added to support the possible USB connection of ID pin and VBUS on the board:
- u-boot,force-b-session-valid: this property forces USB B session (by deactivating the detection with ID pin) and deactivates VBus sensing. It is used when all these features are managed by the board.
- u-boot,force-vbus-detection: this property forces Vbus sensing when u-boot,force-b-session-valid is used (typically when the ID pin is not correctly managed).
Examples of USB configuration in <board>-u-boot.dtsi:
- B session forced as device mode, USB ID pin not used and VBus sensing deactivated:
&usbotg_hs {
u-boot,force-b-session-valid;
dr_mode = "peripheral";
};
- B session and VBus sensing forced (deactived by default with "force-b-session-valid")
&usbotg_hs { u-boot,force-b-session-valid; u-boot,force-vbus-detection; dr_mode = "peripheral"; };
2 Board subdirectory[edit]
Create your own board support subdirectory = board/<vendor>/<board> and add a Makefile file.
You can add any source files needed for your board.
In this Makefile, you can compile the STMicroelectronics files (in board/st/stm32mp1 or in board/st/common) or just copy them as starting point then modify them.
For example board/dhelectronics/dh_stm32mp1/Makefile uses STMicroelectronics board files in ../../st/stm32mp1 directory and local file "board.c"
ifdef CONFIG_SPL_BUILD obj-y += ../../st/stm32mp1/spl.o endif obj-y += ../../st/stm32mp1/board.o board.o
3 Kconfig[edit]
You need to support your board in Kconfig with a new configuration flag: TARGET_<VENDOR>_<BOARD>
3.1 Arch Kconfig: arch/arm/mach-stm32mp/Kconfig [edit]
- Add new CONFIG_TARGET_<VENDOR>_<BOARD>.
- Select the required option; at least, select the options:
- Include your board Kconfig (source "board/<vendor>/<board>/Kconfig") in:
- for STM32MP13x lines
: arch/arm/mach-stm32mp/Kconfig.13x
- for STM32MP15x lines
: arch/arm/mach-stm32mp/Kconfig.15x
- for STM32MP13x lines
E.g for STM32MP15x lines , the file arch/arm/mach-stm32mp/Kconfig.15x is modified:
if STM32MP15x [...] choice prompt "STM32MP15x board select" optional [...] config TARGET_<VENDOR>_<BOARD> bool "<vendor> <board> board" select STM32MP15x help target the <vendor> <board> board with SOC STM32MP15x managed by board/<vendor>/<board> endchoice [...] source "board/st/stm32mp1/Kconfig" source "board/dhelectronics/dh_stm32mp1/Kconfig" source "board/<vendor>/<board>/Kconfig" endif
3.2 Board Kconfig: board/<vendor>/<board>/Kconfig[edit]
The mininimal content of this file is:
if TARGET_<VENDOR>_<BOARD> config SYS_BOARD default "<board>" config SYS_VENDOR default "<vendor>" config SYS_CONFIG_NAME default "<config>" endif
For example see board/dhelectronics/dh_stm32mp1/Kconfig .
SYS_CONFIG_NAME selects the used configuration file: include/configs/SYS_CONFIG_NAME.h.
4 Defconfig[edit]
Add a new defconfig for your board in configs .
- copy the correct defconfig to your "<vendor>_<board>_defconfig" (configs/stm32mp13_defconfig or configs/stm32mp15_defconfig )
- select your new defconfig:
make <vendor>_<board>_defconfig"
- use
make menuconfig
to change your defconfig- remove the STMicroelectronics board config (CONFIG_TARGET_ST_STM32MP13x or CONFIG_TARGET_ST_STM32MP15x)
- add CONFIG_TARGET_<VENDOR>_<BOARD>
- change CONFIG_DEFAULT_DEVICE_TREE to the name of the board device tree: "<board>"
- save the updated defconfig:
make savedefconfig
- verify and copy the file "defconfig" in configs/<vendor>_<board>_defconfig
For example see the file configs/stm32mp15_dhcom_basic_defconfig .
5 Configuration file[edit]
The configuration file is the include file in include/configs directory selected in Makefile.autoconf by CONFIG_SYS_CONFIG_NAME.
This file defines the CONFIG_ flags of the boards that are not defined with Kconfig.
For example, in this configuration file, you can choose the initial U-Boot environment through CONFIG_EXTRA_ENV_SETTINGS, including the boot command.
A generic configuration file is provided for each family:
- STM32MP13x lines
: include/configs/stm32mp13_common.h
- STM32MP15x lines
: include/configs/stm32mp15_common.h
For STMicroelectronics boards in OpenSTLinux, some configuration (bootcmd) are modified with CONFIG_SYS_CONFIG_NAME =
- STM32MP13x lines
: stm32mp13_st_common and the configuration file is include/configs/stm32mp13_st_common.h
- STM32MP15x lines
: stm32mp15_st_common and the configuration file is include/configs/stm32mp15_st_common.h
These STMicroelectronics configuration files can be:
- either used in your project without mofiication (through CONFIG_SYS_CONFIG_NAME="stm32mp13_common.h", "stm32mp13_st_common.h", "stm32mp15_common.h" or " stm32mp15_st_common.h"), or
- included in your board configuration file (e.g. #include "stm32mp13_common.h") before to override them or
- used a starting point for your configuration file (copy and update it).
6 Configuration example[edit]
6.1 MTD partitions[edit]
In U-Boot, all the mtd partitions are managed in mtdparts
and mtdids
U-Boot variables.
U-Boot then dynamically updates the Linux® kernel device tree with these information under CONFIG_OF_BOARD_SETUP in board/st/stm32mp1/stm32mp1.c ::ft_board_setup().
This device tree update enables the alignment of MTD configuration between U-Boot and Linux, and avoids STM32CubeProgrammer support issues as the MTD partition sizes has to be aligned with Flashlayout.
To define the MTD partitions in Linux device tree, deactivate CONFIG_OF_BOARD_SETUP in the customer defconfig. However this might result in misalignments with U-Boot.
To simplify the STMicroelectronics board deployment (same software for boot with and without TEE and for all devices), the mtdparts
and mtdids
variables are dynamically built under CONFIG_SYS_MTDPARTS_RUNTIME with :
- several CONFIG_MTDPARTS_XXX config defined in board/st/common/Kconfig
- some hardcoded treatment in board/st/common/stm32mp_mtdparts.c ::board_mtdparts_default() function.
To check this U-Boot behavior and the generated value of theses variables, execute the mtdparts
command via a U-Boot console.
The default values of CONFIG_MTDPARTS_XXX are used for STMicroelectronics boards (see values provided in board/st/common/Kconfig ).
However the customer can modify them in her/his defconfig if the stm32mp_mtdparts.c file is also used in board configuration file.
For example CONFIG_MTDPARTS_NAND0_BOOT = "1m(u-boot),512k(params)" and the 'UBI' partition is automatically added at the end of the device.
The MTD default configuration can also be directly hardcoded in the customer defconfig (stm32mp_mtdparts.c is not used). To do this:
- Deactivate CONFIG_SYS_MTDPARTS_RUNTIME
- Select your MTDPARTS default configuration with
- CONFIG_MTDPARTS_DEFAULT
- CONFIG_MTDIDS_DEFAULT
For example:
CONFIG_MTDPARTS_DEFAULT="mtdparts=nand0:1m(u-boot),512k(params),-(ubifs)" CONFIG_MTDIDS_DEFAULT="nand0=nand0"
For information, only mtdids_default
and mtdparts_default
are generated in mtdparts_init() / board_mtdparts_default() and these defaults values are used only if mtdpart
/mtdids
variables are empty.
As a result you can also define the MTD configuration directly through these U-Boot variables by setting CONFIG_EXTRA_ENV_SETTINGS in your board configuration file:
- mtdparts="mtdparts=nand0:2m(fsbl),4m(fip1),4m(fip2),-(UBI)"
- mtdids="nand0=nand0"
This corresponds to a generic U-Boot configuration (see U-Boot documentation for additional details).
![]() |
Other U-Boot configurations depend on the offset of MTD partition. |
E.g for STM32MP1 Series, the offset of U-Boot ENV in NOR is defined by
- CONFIG_ENV_SECT_SIZE=0x40000, aligned with the maximum supported erase block for NOR = 256 Kbytes
- CONFIG_ENV_OFFSET=0x900000, offset of ENV partition in NOR
- CONFIG_ENV_OFFSET_REDUND=0x940000, offset of the second 'sector' in the ENV partition
7 References[edit]
- ↑ https://archive.fosdem.org/2018/schedule/event/state_of_the_art_uboot/attachments/slides/2051/export/events/attachments/state_of_the_art_uboot/slides/2051/fosdem_2018_u_boot.pdf
- ↑ https://elinux.org/images/2/2a/Schulz-how-to-support-new-board-u-boot-linux.pdf
- ↑ Documentation/devicetree/bindings/chosen.txt the Linux kernel binding for chosen node
<noinclude>{{ApplicableFor |MPUs list=STM32MP13x, STM32MP15x |MPUs checklist=STM32MP13x,STM32MP15x }}</noinclude> This page explains how to configure the [[U-Boot_overview|U-Boot]] source for your board. __TOC__ Many existing ressources<ref>https://archive.fosdem.org/2018/schedule/event/state_of_the_art_uboot/attachments/slides/2051/export/events/attachments/state_of_the_art_uboot/slides/2051/fosdem_2018_u_boot.pdf</ref> <ref>https://elinux.org/images/2/2a/Schulz-how-to-support-new-board-u-boot-linux.pdf</ref> explain the porting of U-Boot on a new board. This article only provides basic guidelines for STM32MP1 Series. To summarize, you need to [[U-Boot_overview#U-Boot_configuration|configure U-Boot]] for your {{HighlightParam|<VENDOR>}} {{HighlightParam|<BOARD>}} with the following steps: # Add your board [[#Device tree|device tree]]: arch/arm/dts/{{HighlightParam|<board>}}.dts and {{HighlightParam|<board>}}-u-boot.dtsi. # Create your own board support [[#Board subdirectory|directory]]: board/{{HighlightParam|<vendor>}}/{{HighlightParam|<board>}}. # Add TARGET_{{HighlightParam|<VENDOR>}} _{{HighlightParam|<BOARD>}} in [[#Kconfig|Kconfig]]. # Create your board [[#Defconfig|defconfig]]: defconfig/{{HighlightParam|<board>}}_defconfig. # Add your [[#Configuration file|configuration file]] : include/configs/{{HighlightParam|<board>}}.h. == Device tree == Add the board [[U-Boot_overview#Device_tree|device tree]] files {{HighlightParam|<board>}}.dts and {{HighlightParam|<board>}}-u-boot.dtsi in {{CodeSource | U-Boot |arch/arm/dts}}, following the steps below: * Copy the Linux kernel device tree in the directory {{CodeSource | U-Boot |arch/arm/dts}}: {{HighlightParam|<board>}}.dts. * Update {{CodeSource | U-Boot |arch/arm/dts/Makefile}} to compile your device tree: E.g for {{MicroprocessorDevice | device=13}} dtb-$(CONFIG_STM32MP13x) += \ {{HighlightParam|<STM32MP13 board>}}.dtb E.g for {{MicroprocessorDevice | device=15}} dtb-$(CONFIG_STM32MP15x) += \ {{HighlightParam|<STM32MP15 board>}}.dtb * Add a U-Boot addon device tree for your board in the {{CodeSource | U-Boot |arch/arm/dts}} directory: '''{{HighlightParam|<board>}}-u-boot.dtsi'''<br/>This file is automatically included during {{HighlightParam|<board>}}.dts processing.<br/>It includes the <STM32MP series>-u-boot.dtsi file provided by STMicroelectronics ({{CodeSource | U-Boot |arch/arm/dts/stm32mp13-u-boot.dtsi}} or {{CodeSource | U-Boot |arch/arm/dts/stm32mp15-u-boot.dtsi}}) and add all the properties on nodes needed by U-Boot (added nodes, config nodes and '''u-boot,dm-pre-reloc''' or '''u-boot,dm-pre-proper''' attibutes as described in [[U-Boot_overview#Device_tree|U-Boot overview, device tree]]). At this point you can use the generic STM32 MPU defconfig with the STMicroelectronics board directory, but with your board device tree. The board-specific features are not correctly managed, but should be sufficient for a simple board derived from STMicroelectronics designs. You can use the STMicroelectronics code with your device tree as follows: E.g for {{MicroprocessorDevice | device=13}} {{PC$}} make {{HighlightParam|stm32mp13_defconfig}} {{PC$}} make DEVICE_TREE={{HighlightParam|<STM32MP13 board>}} all E.g for {{MicroprocessorDevice | device=15}} {{PC$}} make {{HighlightParam|stm32mp15_defconfig}} {{PC$}} make DEVICE_TREE={{HighlightParam|<STM32MP15 board>}} all The next steps are required if the STMicroelectronics generic board does not comply with all of the expected behavioral aspects for your board (for example MAC address not located in OTP, specific PMIC, specific boot command). === Console === The U-Boot console use <code>stdout-path</code> defined in the <code>chosen</code> node of the Linux kernel device tree as described in the Linux kernel binding<ref>{{CodeSource | Linux kernel | Documentation/devicetree/bindings/chosen.txt | Documentation/devicetree/bindings/chosen.txt}} the Linux kernel binding for chosen node</ref>. As the console is used before relocation, you must add the flags {{HighlightParam|u-boot,dm-pre-reloc}} for each associated nodes (and sub-nodes). For example in device tree from kernel = '''{{Highlight|<board>}}.dts''': / { ... chosen { stdout-path = " {{Highlight|serial0}}:115200n8"; }; aliases { {{Highlight|serial0}} = &{{Highlight|uart4}}; }; ... }; ... {{Highlight|&uart4}} { pinctrl-names = "default"; pinctrl-0 = <{{Highlight|&uart4_pins_a}}>; status = "okay"; }; And in the U-Boot add-on file = '''{{Highlight|<board>}}-u-boot.dtsi''': {{Highlight|&uart4}} { {{HighlightParam|u-boot,dm-pre-reloc;}} }; {{Highlight|&uart4_pins_a}} { {{HighlightParam|u-boot,dm-pre-reloc;}} pins1 { {{HighlightParam|u-boot,dm-pre-reloc;}} }; pins2 { {{HighlightParam|u-boot,dm-pre-reloc;}} }; }; The variable {{HighlightParam|baudrate}}, initialized with {{HighlightParam|CONFIG_BAUDRATE}} value, is used to configure the desired baud rate; the default value is 115200 bauds. An early DEBUG trace, before the device tree parsing, can be also activated with '''CONFIG_DEBUG_UART''' and '''board_debug_uart_init()''' (see [[U-Boot_-_How_to_debug|U-Boot-How to debug]] page for details). === Config node === Some properties in the 'config' node are also used to dynamically configure the U-Boot behavior in the board device tree as follows: * Generic U-Boot configuration: {{CodeSource | U-Boot | doc/device-tree-bindings/config.txt }} ** {{HighlightParam|u-boot,mmc-env-partition}} = name of partition used to save U-Boot environment ** {{Highlight|u-boot,boot-led}} = name of boot-progress indicator LED ** {{Highlight|u-boot,error-led}} = name of error indicator LED * Some STMicroelectronics properties: ** {{Highlight|st,adc_usb_pd}} = ADC channels used to check USB power supply ** {{Highlight|st,stm32prog-gpios}} = GPIO used to force STM32CubeProgrammer mode ** {{Highlight|st,fastboot-gpios}} = GPIO used to force Android Fastboot mode These parameters are managed in {{HighlightParam|U-Boot generic code}} or in {{Highlight|STMicroelectronics board code}} (in line with [[LEDs and buttons on STM32 MPU boards]]); they can only be used if your board reuses the associated code. E.g for {{MicroprocessorDevice | device=15}}, in {{CodeSource | U-Boot |arch/arm/dts/stm32mp157a-dk1-u-boot.dtsi}}, the properties are: config { {{Highlight|u-boot,boot-led}} = "heartbeat"; {{Highlight|u-boot,error-led}} = "error"; {{HighlightParam|u-boot,mmc-env-partition}} = "u-boot-env"; {{Highlight|st,adc_usb_pd}} = <&adc1 18>, <&adc1 19>; {{Highlight|st,fastboot-gpios}} = <&gpioa 13 GPIO_ACTIVE_LOW>; {{Highlight|st,stm32prog-gpios}} = <&gpioa 14 GPIO_ACTIVE_LOW>; }; === USB OTG node === The U-Boot driver for USB OTG, with the compatible {{HighlightParam|st,stm32mp1stm32mp15-hsotg}}, does not have a full OTG support, so only the gadget is used in STM32 MPU board with {{CodeSource | U-Boot |drivers/usb/host/dwc2.c }}. Two U-Boot specific properties are added to support the possible USB connection of ID pin and VBUS on the board: * {{Highlight|u-boot,force-b-session-valid}}: this property forces USB B session (by deactivating the detection with ID pin) and deactivates VBus sensing. It is used when all these features are managed by the board. * {{Highlight|u-boot,force-vbus-detection}}: this property forces Vbus sensing when '''u-boot,force-b-session-valid''' is used (typically when the ID pin is not correctly managed). Examples of USB configuration in '''{{HighlightParam|<board>}}-u-boot.dtsi''': * B session forced as device mode, USB ID pin not used and VBus sensing deactivated: &usbotg_hs { {{Highlight|u-boot,force-b-session-valid}}; dr_mode = "peripheral"; }; * B session and VBus sensing forced (deactived by default with "force-b-session-valid") &usbotg_hs { {{Highlight|u-boot,force-b-session-valid}}; {{Highlight|u-boot,force-vbus-detection}}; dr_mode = "peripheral"; }; == Board subdirectory == Create your own board support subdirectory = board/{{HighlightParam|<vendor>}}/{{HighlightParam|<board>}} and add a Makefile file. You can add any source files needed for your board. In this Makefile, you can compile the STMicroelectronics files (in board/st/stm32mp1 or in board/st/common) or just copy them as starting point then modify them. For example {{CodeSource | U-Boot |board/dhelectronics/dh_stm32mp1/Makefile}} uses STMicroelectronics board files in {{HighlightParam|../../st/stm32mp1}} directory and local file "{{Highlight|board}}.c" ifdef CONFIG_SPL_BUILD obj-y += {{HighlightParam|../../st/stm32mp1}}/spl.o endif obj-y += {{HighlightParam|../../st/stm32mp1}}/board.o {{Highlight|board}}.o == Kconfig == You need to support your board in Kconfig with a new configuration flag: TARGET_{{HighlightParam|<VENDOR>}}_{{HighlightParam|<BOARD>}} === Arch Kconfig: {{CodeSource | U-Boot |arch/arm/mach-stm32mp/Kconfig}} === # Add new CONFIG_TARGET_{{HighlightParam|<VENDOR>}}_{{HighlightParam|<BOARD>}}. # Select the required option; at least, select the options: #* for {{MicroprocessorDevice | device=13}}: {{Highlight|CONFIG_STM32MP13x}}. #* for {{MicroprocessorDevice | device=15}}: {{Highlight|CONFIG_STM32MP15x}}. # Include your board Kconfig (source "board/{{HighlightParam|<vendor>}}/{{HighlightParam|<board>}}/Kconfig") in: #* for {{MicroprocessorDevice | device=13}}: {{CodeSource | U-Boot | arch/arm/mach-stm32mp/Kconfig.13x}} #* for {{MicroprocessorDevice | device=15}}: {{CodeSource | U-Boot | arch/arm/mach-stm32mp/Kconfig.15x}} E.g for {{MicroprocessorDevice | device=15}}, the file {{CodeSource | U-Boot | arch/arm/mach-stm32mp/Kconfig.15x}} is modified: if STM32MP15x [...] choice prompt "STM32MP15x board select" optional [...] config TARGET_{{HighlightParam|<VENDOR>}}_{{HighlightParam|<BOARD>}} bool "{{HighlightParam|<vendor>}} {{HighlightParam|<board>}} board" select {{Highlight|STM32MP15x}} help target the {{HighlightParam|<vendor>}} {{HighlightParam|<board>}} board with SOC {{Highlight|STM32MP15x}} managed by board/{{HighlightParam|<vendor>}}/{{HighlightParam|<board>}} endchoice [...] source "board/st/stm32mp1/Kconfig" source "board/dhelectronics/dh_stm32mp1/Kconfig" source "board/{{HighlightParam|<vendor>}}/{{HighlightParam|<board>}}/Kconfig" endif === Board Kconfig: board/{{HighlightParam|<vendor>}}/{{HighlightParam|<board>}}/Kconfig === The mininimal content of this file is: if TARGET_{{HighlightParam|<VENDOR>}}_{{HighlightParam|<BOARD>}} config SYS_BOARD default "{{HighlightParam|<board>}}" config SYS_VENDOR default "{{HighlightParam|<vendor>}}" config {{Highlight|SYS_CONFIG_NAME}} default "{{Highlight|<config>}}" endif For example see {{CodeSource | U-Boot |board/dhelectronics/dh_stm32mp1/Kconfig}}. {{Highlight|SYS_CONFIG_NAME}} selects the used [[#Configuration file|configuration file]]: include/configs/{{Highlight|SYS_CONFIG_NAME}}.h. == Defconfig == Add a new defconfig for your board in {{CodeSource | U-Boot |configs}}. * copy the correct defconfig to your "{{HighlightParam|<vendor>}}_{{HighlightParam|<board>}}_defconfig" ({{CodeSource | U-Boot |configs/stm32mp13_defconfig}} or {{CodeSource | U-Boot |configs/stm32mp15_defconfig}}) * select your new defconfig: <code>make {{HighlightParam|<vendor>}}_{{HighlightParam|<board>}}_defconfig"</code> * use <code>make menuconfig</code> to change your defconfig ** remove the STMicroelectronics board config (CONFIG_TARGET_ST_STM32MP13x or CONFIG_TARGET_ST_STM32MP15x) ** add CONFIG_TARGET_{{HighlightParam|<VENDOR>}}_{{HighlightParam|<BOARD>}} ** change CONFIG_DEFAULT_DEVICE_TREE to the name of the board device tree: "{{HighlightParam|<board>}}" * save the updated defconfig: <code>make savedefconfig</code> * verify and copy the file "defconfig" in configs/{{HighlightParam|<vendor>}}_{{HighlightParam|<board>}}_defconfig For example see the file {{CodeSource | U-Boot |configs/stm32mp15_dhcom_basic_defconfig}}. == Configuration file == The configuration file is the include file in {{CodeSource | U-Boot | include/configs}} directory selected in Makefile.autoconf by {{Highlight|CONFIG_SYS_CONFIG_NAME}}. This file defines the CONFIG_ flags of the boards that are not defined with Kconfig. For example, in this configuration file, you can choose the initial U-Boot environment through CONFIG_EXTRA_ENV_SETTINGS, including the boot command. A generic configuration file is provided for each family: * {{MicroprocessorDevice | device=13}}: {{CodeSource | U-Boot | include/configs/stm32mp13_common.h}} * {{MicroprocessorDevice | device=15}}: {{CodeSource | U-Boot | include/configs/stm32mp15_common.h}} For STMicroelectronics boards in OpenSTLinux, some configuration (bootcmd) are modified with {{Highlight|CONFIG_SYS_CONFIG_NAME}} = * {{MicroprocessorDevice | device=13}}: {{HighlightParam|stm32mp13_st_common}} and the configuration file is {{CodeSource | U-Boot | include/configs/stm32mp13_st_common.h}} * {{MicroprocessorDevice | device=15}} : {{HighlightParam|stm32mp15_st_common}} and the configuration file is {{CodeSource | U-Boot | include/configs/stm32mp15_st_common.h}} These STMicroelectronics configuration files can be: * either used in your project without mofiication (through {{Highlight|CONFIG_SYS_CONFIG_NAME}}="{{HighlightParam|stm32mp13_common.h}}", "{{HighlightParam|stm32mp13_st_common.h}}", "{{HighlightParam|stm32mp15_common.h}}" or " {{HighlightParam|stm32mp15_st_common.h}}"), or * included in your board configuration file (e.g. #include "{{HighlightParam|stm32mp13_common.h}}") before to override them or * used a starting point for your configuration file (copy and update it). == Configuration example == === MTD partitions === In U-Boot, all the mtd partitions are managed in <code>mtdparts</code> and <code>mtdids</code> [[U-Boot_overview#U-Boot_environment_variables|U-Boot variables]]. U-Boot then dynamically updates the Linux<sup>®</sup> kernel device tree with these information under {{Highlight|CONFIG_OF_BOARD_SETUP}} in {{CodeSource |U-Boot|board/st/stm32mp1/stm32mp1.c}}::ft_board_setup(). This device tree update enables the alignment of MTD configuration between U-Boot and Linux, and avoids STM32CubeProgrammer support issues as the [[STM32CubeProgrammer_flashlayout#MTD_partition_sizes|MTD partition sizes]] has to be aligned with Flashlayout. To define the MTD partitions in Linux device tree, deactivate {{Highlight|CONFIG_OF_BOARD_SETUP}} in the customer defconfig. However this might result in misalignments with U-Boot. To simplify the STMicroelectronics board deployment (same software for boot with and without TEE and for all devices), the <code>mtdparts</code> and <code>mtdids</code> variables are dynamically built under {{Highlight|CONFIG_SYS_MTDPARTS_RUNTIME}} with : * several {{Highlight|CONFIG_MTDPARTS_XXX}} config defined in {{CodeSource |U-Boot|board/st/common/Kconfig}} * some hardcoded treatment in {{CodeSource |U-Boot|board/st/common/stm32mp_mtdparts.c}}::board_mtdparts_default() function. To check this U-Boot behavior and the generated value of theses variables, execute the <code>mtdparts</code> command via a U-Boot console. The default values of {{Highlight|CONFIG_MTDPARTS_XXX}} are used for STMicroelectronics boards (see values provided in {{CodeSource |U-Boot|board/st/common/Kconfig}}). However the customer can modify them in [[#Defconfig|her/his defconfig]] if the {{CodeSource |U-Boot|board/st/common/stm32mp_mtdparts.c|stm32mp_mtdparts.c}} file is also used in [[#Board subdirectory|board configuration file]]. For example {{Highlight|CONFIG_MTDPARTS_NAND0_BOOT}} = "{{HighlightParam|1m(u-boot),512k(params)}}" and the 'UBI' partition is automatically added at the end of the device. The MTD default configuration can also be directly hardcoded in the [[#Defconfig|customer defconfig]] ({{CodeSource |U-Boot|board/st/common/stm32mp_mtdparts.c|stm32mp_mtdparts.c}} is not used). To do this: * Deactivate {{Highlight|CONFIG_SYS_MTDPARTS_RUNTIME}} * Select your MTDPARTS default configuration with ** {{Highlight|CONFIG_MTDPARTS_DEFAULT}} ** {{Highlight|CONFIG_MTDIDS_DEFAULT}} For example: {{Highlight|CONFIG_MTDPARTS_DEFAULT}}="{{HighlightParam|mtdparts{{=}}nand0:1m(u-boot),512k(params),-(ubifs)}}" {{Highlight|CONFIG_MTDIDS_DEFAULT}}="{{HighlightParam|nand0{{=}}nand0}}" For information, only <code>mtdids_default</code> and <code>mtdparts_default</code> are generated in mtdparts_init() / board_mtdparts_default() and these defaults values are used only if <code>mtdpart</code>/<code>mtdids</code> variables are empty. As a result you can also define the MTD configuration directly through these U-Boot variables by setting {{Highlight|CONFIG_EXTRA_ENV_SETTINGS}} in your [[#Configuration file|board configuration file]]: * {{Highlight|mtdparts}}="{{HighlightParam|mtdparts{{=}}nand0:2m(fsbl),4m(fip1),4m(fip2),-(UBI)}}" * {{Highlight|mtdids}}="{{HighlightParam|nand0{{=}}nand0}}" This corresponds to a generic U-Boot configuration (see [[U-Boot overview|U-Boot documentation]] for additional details). {{Warning|Other U-Boot configurations depend on the offset of MTD partition.}} E.g for {{MicroprocessorDevice | device=1}}, the offset of U-Boot ENV in NOR is defined by * {{Highlight|CONFIG_ENV_SECT_SIZE}}={{HighlightParam|0x40000}}, aligned with the maximum supported erase block for NOR = 256 Kbytes * {{Highlight|CONFIG_ENV_OFFSET}}={{HighlightParam|0x900000}}, offset of ENV partition in NOR * {{Highlight|CONFIG_ENV_OFFSET_REDUND}}={{HighlightParam|0x940000}}, offset of the second 'sector' in the ENV partition == References ==<references/> <noinclude> {{PublicationRequestId |17913| 2020-10-27 | }} [[Category:How to customize software]] [[Category:U-Boot|U-Boot - 7]]</noinclude>
Line 125: | Line 125: | ||
=== USB OTG node === |
=== USB OTG node === |
||
− | The U-Boot driver for USB OTG, with the compatible {{HighlightParam|st, |
+ | The U-Boot driver for USB OTG, with the compatible {{HighlightParam|st,stm32mp15-hsotg}}, does not have a full OTG support, so only the gadget is used in STM32 MPU board with {{CodeSource | U-Boot |drivers/usb/host/dwc2.c }}. |
Two U-Boot specific properties are added to support the possible USB connection of ID pin and VBUS on the board: |
Two U-Boot specific properties are added to support the possible USB connection of ID pin and VBUS on the board: |