Difference between revisions of "How to configure TF-A BL2"
[quality revision] | [quality revision] |
m
|
m (Trusted board add info)
|
Contents
1 Article purpose[edit]
This section details the TF-A BL2 stage (Trusted Firmware-A Boot Loader stage 2) used as FSBL (First Stage Boot Loader). It explains how to configure and build BL2 in STM32 MPU context, describes the build process from sources, and shows how to deploy it on your target.
2 Source code access and build process[edit]
2.1 Cross compilation[edit]
Cross compilation of TF-A BL2 is only required if it needs to be modified.
Refer to Setup Cross compile environment.
The build process creates an STM32 image. This binary is built in a single step during the build process.
2.2 Install sources[edit]
2.2.1 From the Developer package[edit]
The Developer Package contains OpenSTLinux and TF-A sources: TF-A Installation
2.2.2 Official source tree[edit]
Download the source code from the official Trusted Firmware-A git repository.
PC $> git clone https://git.trustedfirmware.org/TF-A/trusted-firmware-a.git
![]() |
The STM32MP1 platform is not yet fully upstreamed. Depending on the version used, some features may not be available. |
For a full-featured software, go to STMicroelectronics github:
PC $> git clone https://github.com/STMicroelectronics/arm-trusted-firmware.git
2.2.3 Distribution Package[edit]
It is possible to use the distribution package to download and rebuid TF-A BL2
2.3 Build process[edit]
2.3.1 TF-A Build flags[edit]
Here is the list of the mandatory flags that need to be specified to complete the TF-A BL2 build:
- ARM_ARCH_MAJOR = 7: the major version of Arm architecture to target (STM32MP1 is based on an Arm v7 architecture)
- ARCH = aarch32: specifies aarch32 architecture to be built
- PLAT = stm32mp1: builds an STM32MP1 platform
- DTB_FILE_NAME = <fdt file name>.dtb: this flag must be defined to build the proper target and include the correct DTB file into the final file
- The boot device(s) you use, one (or several) of:
- STM32MP_EMMC = 1
- STM32MP_SDMMC = 1
- STM32MP_RAW_NAND = 1
- STM32MP_SPI_NAND = 1
- STM32MP_SPI_NOR = 1
- or a programming interface:
- STM32MP_UART_PROGRAMMER = 1
- STM32MP_USB_PROGRAMMER = 1
Optional flags:
- TRUSTED_BOARD_BOOT = 1: Enable Secure boot authentication
![]() |
TRUSTED_BOARD_BOOT requires to have first downloaded The MBEDLTS[1] source code aligned version as specify in TF-A prerequisites [2].
MBEDTLS_DIR=<path_to_mbedtls_directory> must be used to compile. |
- BUILD_PLAT = <folder>: custom output folder name (by default build/<debug/release>/)
- DEBUG = 1: adds debug information in all binaries
- V = 1: prints verbose compilation traces
- TRUSTED_BOARD_BOOT = 1: adds MBEDTLS build sources and authentication framework enabled
- DYN_DISABLE_AUTH = 1: enables/disables authentication using device tree
- STM32MP_FORCE_MTD_START_OFFSET = <value>: overrides the default start offset to read FIP on MTD devices (need to be aligned with FlashLayout).
![]() |
Default offsets are STM32MP_NOR_FIP_OFFSET = 0x00080000 and STM32MP_NAND_FIP_OFFSET = 0x00200000 |
- STM32MP_USE_EXTERNAL_HEAP = 1: can be enabled to define MBEDTLS heap out of BL2 sources (defined in device tree).
For ecosystem release ≤ v3.0.0 compatibility
It is still possible to generate the a single BL2/BL32 file without FIP support, an option flag is available:
2.4 Build command[edit]
The BL2 generation depends on the selected storage device. By default, only one storage device is supported.
![]() |
The DTB_FILE_NAME flag and the selected storage must be set to select the correct board configuration. The device tree file for the target must be located in fdts folder (<board>.dts) |
First add your own environment flags:
PC $> unset LDFLAGS; PC $> unset CFLAGS;
Then compile the TF-A BL2.
The default build command for STM32MP15 is
PC $> make ARM_ARCH_MAJOR=7 ARCH=aarch32 PLAT=stm32mp1 \ <Selected storage> DTB_FILE_NAME=<board_name>.dtb
Here are build commands for the stm32mp157c-ev1 board (which supports different storage devices):
- Flash programming support
PC $> make ARM_ARCH_MAJOR=7 ARCH=aarch32 PLAT=stm32mp1 STM32MP_USB_PROGRAMMER=1 \ DTB_FILE_NAME=stm32mp157c-ev1.dtb PC $> make ARM_ARCH_MAJOR=7 ARCH=aarch32 PLAT=stm32mp1 STM32MP_UART_PROGRAMMER=1 \ DTB_FILE_NAME=stm32mp157c-ev1.dtb
- Dedicated boot storage
PC $> make ARM_ARCH_MAJOR=7 ARCH=aarch32 PLAT=stm32mp1 STM32MP_SDMMC=1 \
DTB_FILE_NAME=stm32mp157c-ev1.dtb
PC $> make ARM_ARCH_MAJOR=7 ARCH=aarch32 PLAT=stm32mp1 STM32MP_EMMC=1 \
DTB_FILE_NAME=stm32mp157c-ev1.dtb
PC $> make ARM_ARCH_MAJOR=7 ARCH=aarch32 PLAT=stm32mp1 STM32MP_RAW_NAND=1 \
DTB_FILE_NAME=stm32mp157c-ev1.dtb
PC $> make ARM_ARCH_MAJOR=7 ARCH=aarch32 PLAT=stm32mp1 STM32MP_SPI_NOR=1 \
DTB_FILE_NAME=stm32mp157c-ev1.dtb
Not available on board
PC $> make ARM_ARCH_MAJOR=7 ARCH=aarch32 PLAT=stm32mp1 STM32MP_SPI_NAND=1 \
DTB_FILE_NAME=stm32mp157c-ev1.dtb
- Enable Secure boot on SDCard
PC $> MBEDTLS_DIR=<path_to_mbedtls_directory> make ARM_ARCH_MAJOR=7 \ ARCH=aarch32 PLAT=stm32mp1 TRUSTED_BOARD_BOOT=1 STM32MP_SDMMC=1 \ DTB_FILE_NAME=stm32mp157c-ev1.dtb
2.5 Final image[edit]
The final image is available for Flash memory or SDCard update in the corresponding folder:
<BUILD_PLAT>/tf-a-<board>.stm32 Ex: build/release/tf-a-stm32mp157c-ev1.stm32
3 Updating the software on board[edit]
3.1 Partitioning of binaries[edit]
The TF-A build provides a binary named tf-a-<board>.stm32 that MUST be copied to a dedicated partition named "fsblX" (X depends on the number of needed backups in the Flash).
![]() |
TF-A must be located in the first partition of your boot device. You can just update the first partition for a simple test, but all backup partitions must contain the same image at the end. |
3.2 Updating via SDCard[edit]
If you use an SDCard, simply update TF-A using the dd command on your host.
Plug your SDCard into the computer and copy the binary to the dedicated partition; on an SDCard/USB disk the "fsbl1" partition is partition 1:
- SDCard: /dev/mmcblkXp1 (where X is the instance number) - SDCard via USB reader: /dev/sdX1 (where X is the instance number)
- Under Linux®
PC $> dd if=<tf-a file>.stm32 of=/dev/<device partition> bs=1M conv=fdatasync
- Under Windows®
CoreUtils [13] that includes the dd command is available for Windows.
3.3 Updating via USB mass storage on U-boot[edit]
See How to use USB mass storage in U-Boot.
Refer to the previous section to put tf-a-<board>.stm32 into SDCard/USB disk.
3.4 Updating your boot device via STM32CubeProgrammer[edit]
Refer to the STM32CubeProgrammer documentation to update your target.
4 Secure secret provisioning (SSP)[edit]
A specific TF-A BL2 build is required to manage SSP.
![]() |
This STM32 output file must be signed to complete the SSP feature. |
Dedicated files are delivered in the platform folder that contains the specific Makefile and bl2_plat_setup for the TF-A SSP.
The TF-A SSP is a subset of the standard TF-A BL2 that includes only:
- BL2 device tree
- BL2 image with limited support to the serial link device.
4.1 Additional flags[edit]
The mandatory flags to build the TF-A SSP are:
- STM32MP_SSP = 1
For the serial link (exclusive):
- STM32MP_UART_PROGRAMMER = 1
- STM32MP_USB_PROGRAMMER = 1
4.2 Build command[edit]
PC $> make ARM_ARCH_MAJOR=7 ARCH=aarch32 PLAT=stm32mp1 \
STM32MP_SSP=1 STM32MP_USB_PROGRAMMER=1 \
DTB_FILE_NAME=<board>.dtb
or
PC $> make ARM_ARCH_MAJOR=7 ARCH=aarch32 PLAT=stm32mp1 \
STM32MP_SSP=1 STM32MP_UART_PROGRAMMER=1 \
DTB_FILE_NAME=<board>.dtb
4.3 Final image[edit]
The final image is available in the corresponding folder:
tf-a-ssp-<board>.stm32 For example: tf-a-ssp-stm32mp157c-ev1.stm32
== Article purpose == This section details the TF-A BL2 stage (Trusted Firmware-A Boot Loader stage 2) used as FSBL (First Stage Boot Loader). It explains how to configure and build BL2 in STM32 MPU context, describes the build process from sources, and shows how to deploy it on your target.<br> == Source code access and build process == === Cross compilation === Cross compilation of TF-A BL2 is only required if it needs to be modified.<br> Refer to [[Cross-compile with OpenSTLinux SDK|Setup Cross compile environment]]. The build process creates an STM32 image. This binary is built in a single step during the build process. === Install sources === ==== From the Developer package ==== The Developer Package contains OpenSTLinux and TF-A sources: [[STM32MP1_Developer_Package#Installing the TF-A|TF-A Installation]] ==== Official source tree ==== Download the source code from the official Trusted Firmware-A git repository. {{PC$}} git clone https://git.trustedfirmware.org/TF-A/trusted-firmware-a.git {{Warning|The STM32MP1 platform is not yet fully upstreamed. Depending on the version used, some features may not be available.}}<br> For a full-featured software, go to STMicroelectronics github: {{PC$}} git clone https://github.com/STMicroelectronics/arm-trusted-firmware.git {{InternalInfo | Development source tree: Download the source code from the internal git {{PC$}} git clone ssh://gerrit.st.com:29418/mpu/oe/st/tf-a.git }} ==== Distribution Package ==== It is possible to use the distribution package to download and rebuid [[How_to_cross-compile_with_the_Distribution_Package#Modifying_the_TF-A|TF-A BL2]] === Build process === ==== TF-A Build flags ==== Here is the list of the mandatory flags that need to be specified to complete the TF-A BL2 build: * ARM_ARCH_MAJOR = 7: the major version of Arm architecture to target (STM32MP1 is based on an Arm v7 architecture) * ARCH = aarch32: specifies aarch32 architecture to be built * PLAT = stm32mp1: builds an STM32MP1 platform * DTB_FILE_NAME = <fdt file name>.dtb: this flag must be defined to build the proper target and include the correct DTB file into the final file * The boot device(s) you use, one (or several) of: ** STM32MP_EMMC = 1 ** STM32MP_SDMMC = 1 ** STM32MP_RAW_NAND = 1 ** STM32MP_SPI_NAND = 1 ** STM32MP_SPI_NOR = 1 * or a programming interface: ** STM32MP_UART_PROGRAMMER = 1 ** STM32MP_USB_PROGRAMMER = 1 Optional flags: * TRUSTED_BOARD_BOOT {{=}} 1: Enable Secure boot authentication {{Warning| TRUSTED_BOARD_BOOT requires to have first downloaded The MBEDLTS<ref>https://github.com/ARMmbed/mbedtls</ref> source code aligned version as specify in TF-A prerequisites <ref>https://trustedfirmware-a.readthedocs.io/en/v2.4/getting_started/prerequisites.html</ref>.<br> MBEDTLS_DIR{{=}}<path_to_mbedtls_directory> must be used to compile.}} * BUILD_PLAT = <folder>: custom output folder name (by default build/<debug/release>/) * DEBUG {{=}} 1: adds debug information in all binaries * V {{=}} 1: prints verbose compilation traces * TRUSTED_BOARD_BOOT {{=}} 1: adds MBEDTLS build sources and authentication framework enabled * DYN_DISABLE_AUTH {{=}} 1: enables/disables authentication using device tree * STM32MP_FORCE_MTD_START_OFFSET {{=}} <value>: overrides the default start offset to read FIP on MTD devices (need to be aligned with FlashLayout). {{Info | Default offsets are STM32MP_NOR_FIP_OFFSET {{=}} 0x00080000 and STM32MP_NAND_FIP_OFFSET {{=}} 0x00200000}} * STM32MP_USE_EXTERNAL_HEAP {{=}} 1: can be enabled to define MBEDTLS heap out of BL2 sources (defined in device tree). For {{EcosystemRelease | revision=3.0.0 | range=and before}} compatibility<div class="mw-collapsible mw-collapsed"> It is still possible to generate the a single BL2/BL32 file without FIP support, an option flag is available:<br> * STM32MP_USE_STM32IMAGE=1: Disable the FIP load and authentication management. Use the STM32 binary load and authentication used in {{EcosystemRelease | revision=3.0.0 | range=and before}}.</div> <br> {{InternalInfo | * STM32MP_FPGA {{=}} 1: includes FPGA specific code (not compatible with board) * STM32MP1_TEST {{=}} 1: enable tests This STM32MP1_TEST flag allows: * overriding the boot device using the backup register (18). * overriding the NAND parameters in OTP fuses using a backup register (19) with the same OTP layout. Some SPI flags are available for specific test purposes (Required Storage extension board): ** STM32MP_SPI_NOR_CS0 {{=}} 1: selects NOR on CS0 (0 for CS1) ** STM32MP_SPI_NOR_QUAD {{=}} 1: configures Quad-SPI mode ** STM32MP_SPI_NOR_DUAL {{=}} 1: configures Dual-SPI mode ** STM32MP_SPI_NOR_INDIRECT {{=}} 1: configures Indirect mode ** STM32MP_SPI_NAND_CS0 {{=}} 1: selects SPI NAND on CS0 (0 for CS1) ** STM32MP_SPI_NAND_QUAD {{=}} 1: configures Quad-SPI mode ** STM32MP_SPI_NAND_DUAL {{=}} 1: configures Quad-SPI mode }} === Build command === The BL2 generation depends on the selected storage device. By default, only one storage device is supported. <br> {{Warning|The DTB_FILE_NAME flag and the selected storage must be set to select the correct board configuration.<br> The device tree file for the target must be located in {{CodeSource | TF-A | fdts}} folder (<board>.dts)}} First add your own environment flags: {{PC$}} unset LDFLAGS; {{PC$}} unset CFLAGS; Then compile the TF-A BL2.<br> The default build command for STM32MP15 is {{PC$}} make ARM_ARCH_MAJOR=7 ARCH=aarch32 PLAT=stm32mp1 \<Selected storage> DTB_FILE_NAME=<board_name>.dtb Here are build commands for the stm32mp157c-ev1 board (which supports different storage devices): * Flash programming support {{PC$}} make ARM_ARCH_MAJOR=7 ARCH=aarch32 PLAT=stm32mp1 {{Highlight|STM32MP_USB_PROGRAMMER{{=}}1}} \ DTB_FILE_NAME=stm32mp157c-ev1.dtb {{PC$}} make ARM_ARCH_MAJOR=7 ARCH=aarch32 PLAT=stm32mp1 {{Highlight|STM32MP_UART_PROGRAMMER{{=}}1}} \ DTB_FILE_NAME=stm32mp157c-ev1.dtb * Dedicated boot storage {{PC$}} make ARM_ARCH_MAJOR=7 ARCH=aarch32 PLAT=stm32mp1 {{Highlight|STM32MP_SDMMC{{=}}1}} \ DTB_FILE_NAME=stm32mp157c-ev1.dtb {{PC$}} make ARM_ARCH_MAJOR=7 ARCH=aarch32 PLAT=stm32mp1 {{Highlight|STM32MP_EMMC{{=}}1}} \ DTB_FILE_NAME=stm32mp157c-ev1.dtb {{PC$}} make ARM_ARCH_MAJOR=7 ARCH=aarch32 PLAT=stm32mp1 {{Highlight|STM32MP_RAW_NAND{{=}}1}} \ DTB_FILE_NAME=stm32mp157c-ev1.dtb {{PC$}} make ARM_ARCH_MAJOR=7 ARCH=aarch32 PLAT=stm32mp1 {{Highlight|STM32MP_SPI_NOR{{=}}1}} \ DTB_FILE_NAME=stm32mp157c-ev1.dtb Not available on board {{PC$}} make ARM_ARCH_MAJOR=7 ARCH=aarch32 PLAT=stm32mp1 {{Highlight|STM32MP_SPI_NAND{{=}}1}} \ DTB_FILE_NAME=stm32mp157c-ev1.dtb {{* Enable Secure boot on SDCard {{PC$}} {{Highlight|MBEDTLS_DIR{{=}}<path_to_mbedtls_directory>}} make ARM_ARCH_MAJOR=7 \ ARCH=aarch32 PLAT=stm32mp1 {{Highlight|TRUSTED_BOARD_BOOT{{=}}1 STM32MP_SDMMC{{=}}1}} \ DTB_FILE_NAME=stm32mp157c-ev1.dtb {{InternalInfo| Add the BUILD_PLAT flag for multiple storage purpose: * Flash programming support {{PC$}} make ARM_ARCH_MAJOR{{=}}7 ARCH{{=}}aarch32 PLAT{{=}}stm32mp1 STM32MP_USB_PROGRAMMER{{=}}1 \ DTB_FILE_NAME{{=}}stm32mp157c-ev1.dtb BUILD_PLAT{{=}}build/usb {{PC$}} make ARM_ARCH_MAJOR{{=}}7 ARCH{{=}}aarch32 PLAT{{=}}stm32mp1 STM32MP_UART_PROGRAMMER{{=}}1 \ DTB_FILE_NAME{{=}}stm32mp157c-ev1.dtb BUILD_PLAT{{=}}build/uart * Dedicated boot storage {{PC$}} make ARM_ARCH_MAJOR{{=}}7 ARCH{{=}}aarch32 PLAT{{=}}stm32mp1 STM32MP_SDMMC{{=}}1 \ DTB_FILE_NAME{{=}}stm32mp157c-ev1.dtb BUILD_PLAT{{=}}build/sdmmc {{PC$}} make ARM_ARCH_MAJOR{{=}}7 ARCH{{=}}aarch32 PLAT{{=}}stm32mp1 STM32MP_EMMC{{=}}1 \ DTB_FILE_NAME{{=}}stm32mp157c-ev1.dtb BUILD_PLAT{{=}}build/emmc {{PC$}} make ARM_ARCH_MAJOR{{=}}7 ARCH{{=}}aarch32 PLAT{{=}}stm32mp1 STM32MP_RAW_NAND{{=}}1 \ DTB_FILE_NAME{{=}}stm32mp157c-ev1.dtb BUILD_PLAT{{=}}build/raw_nand {{PC$}} make ARM_ARCH_MAJOR{{=}}7 ARCH{{=}}aarch32 PLAT{{=}}stm32mp1 STM32MP_SPI_NOR{{=}}1 \ DTB_FILE_NAME{{=}}stm32mp157c-ev1.dtb BUILD_PLAT{{=}}build/spi_nor Not available on board {{PC$}} make ARM_ARCH_MAJOR{{=}}7 ARCH{{=}}aarch32 PLAT{{=}}stm32mp1 STM32MP_SPI_NAND{{=}}1 \ DTB_FILE_NAME{{=}}stm32mp157c-ev1.dtb BUILD_PLAT{{=}}build/spi_nand }} === Final image === The final image is available for Flash memory or SDCard update in the corresponding folder:<pre> <BUILD_PLAT>/tf-a-<board>.stm32 Ex: build/release/tf-a-stm32mp157c-ev1.stm32</pre> == Updating the software on board == === Partitioning of binaries === The TF-A build provides a binary named tf-a-<board>.stm32 that MUST be copied to a dedicated partition named "fsblX" (X depends on the number of needed backups in the Flash). {{Warning|TF-A must be located in the first partition of your boot device.<br> You can just update the first partition for a simple test, but all backup partitions must contain the same image at the end. }} === Updating via SDCard === If you use an SDCard, simply update TF-A using the dd command on your host.<br> Plug your SDCard into the computer and copy the binary to the dedicated partition; on an SDCard/USB disk the "fsbl1" partition is partition 1: - SDCard: /dev/mmcblkXp1 (where X is the instance number) - SDCard via USB reader: /dev/sdX1 (where X is the instance number) * Under Linux<sup>®</sup> {{PC$}} dd if=<tf-a file>.stm32 of=/dev/<device partition> bs=1M conv=fdatasync {{Info| To find the partition associated to a specific label, just plug the SDCard/USB disk into your PC and call the following command: {{PC$}} ls -l /dev/disk/by-partlabel/ total 0 lrwxrwxrwx 1 root root 10 Jan 17 17:38 bootfs -> ../../mmcblk0p4 lrwxrwxrwx 1 root root 10 Jan 17 17:38 fip -> ../../mmcblk0p3 lrwxrwxrwx 1 root root 10 Jan 17 17:38 fsbl1 -> ../../mmcblk0p1 ? FSBL1 (TF-A) lrwxrwxrwx 1 root root 10 Jan 17 17:38 fsbl2 -> ../../mmcblk0p2 ? FSBL2 (TF-A backup ? same content as FSBL) lrwxrwxrwx 1 root root 10 Jan 17 17:38 rootfs -> ../../mmcblk0p5 lrwxrwxrwx 1 root root 10 Jan 17 17:38 userfs -> ../../mmcblk0p6 }}<br> * Under Windows<sup>®</sup> CoreUtils <ref>http://gnuwin32.sourceforge.net/packages/coreutils.htm</ref> that includes the dd command is available for Windows. === Updating via USB mass storage on U-boot === See [[How to use USB mass storage in U-Boot]]. Refer to the previous section to put tf-a-<board>.stm32 into SDCard/USB disk. === Updating your boot device via STM32CubeProgrammer === Refer to the [[STM32CubeProgrammer]] documentation to update your target. == Secure secret provisioning (SSP) == A specific TF-A BL2 build is required to manage SSP. {{Warning| This STM32 output file must be signed to complete the SSP feature.}} Dedicated files are delivered in the platform folder that contains the specific Makefile and bl2_plat_setup for the TF-A SSP.<br> The TF-A SSP is a subset of the standard TF-A BL2 that includes only: * BL2 device tree * BL2 image with limited support to the serial link device. ==== Additional flags ==== The mandatory flags to build the TF-A SSP are: * '''STM32MP_SSP = 1''' For the serial link (exclusive): * STM32MP_UART_PROGRAMMER = 1 * STM32MP_USB_PROGRAMMER = 1 ==== Build command ==== {{PC$}} make ARM_ARCH_MAJOR=7 ARCH=aarch32 PLAT=stm32mp1 \ {{Highlight|STM32MP_SSP{{=}}1 STM32MP_USB_PROGRAMMER{{=}}1}} \ DTB_FILE_NAME=<board>.dtb or {{PC$}} make ARM_ARCH_MAJOR=7 ARCH=aarch32 PLAT=stm32mp1 \ {{Highlight|STM32MP_SSP{{=}}1 STM32MP_UART_PROGRAMMER{{=}}1}} \ DTB_FILE_NAME=<board>.dtb ==== Final image ==== The final image is available in the corresponding folder:<pre> tf-a-ssp-<board>.stm32 For example: tf-a-ssp-stm32mp157c-ev1.stm32</pre> <noinclude> {{PublicationRequestId | 19288| 2021-03-10 | PhilipS}} [[Category:Trusted Firmware-A (BL2)| 03]]</noinclude>
Line 50: | Line 50: | ||
Optional flags: |
Optional flags: |
||
+ | * TRUSTED_BOARD_BOOT {{=}} 1: Enable Secure boot authentication |
||
+ | {{Warning| TRUSTED_BOARD_BOOT requires to have first downloaded The MBEDLTS<ref>https://github.com/ARMmbed/mbedtls</ref> source code aligned version as specify in TF-A prerequisites <ref>https://trustedfirmware-a.readthedocs.io/en/v2.4/getting_started/prerequisites.html</ref>.<br> MBEDTLS_DIR{{=}}<path_to_mbedtls_directory> must be used to compile.}} |
||
* BUILD_PLAT = <folder>: custom output folder name (by default build/<debug/release>/) |
* BUILD_PLAT = <folder>: custom output folder name (by default build/<debug/release>/) |
||
* DEBUG {{=}} 1: adds debug information in all binaries |
* DEBUG {{=}} 1: adds debug information in all binaries |
||
* V {{=}} 1: prints verbose compilation traces |
* V {{=}} 1: prints verbose compilation traces |
||
− | |||
* DYN_DISABLE_AUTH {{=}} 1: enables/disables authentication using device tree |
* DYN_DISABLE_AUTH {{=}} 1: enables/disables authentication using device tree |
||
* STM32MP_FORCE_MTD_START_OFFSET {{=}} <value>: overrides the default start offset to read FIP on MTD devices (need to be aligned with FlashLayout). |
* STM32MP_FORCE_MTD_START_OFFSET {{=}} <value>: overrides the default start offset to read FIP on MTD devices (need to be aligned with FlashLayout). |
||
Line 119: | Line 120: | ||
DTB_FILE_NAME=stm32mp157c-ev1.dtb |
DTB_FILE_NAME=stm32mp157c-ev1.dtb |
||
+ | * Enable Secure boot on SDCard |
||
+ | {{PC$}} {{Highlight|MBEDTLS_DIR{{=}}<path_to_mbedtls_directory>}} make ARM_ARCH_MAJOR=7 \ |
||
+ | ARCH=aarch32 PLAT=stm32mp1 {{Highlight|TRUSTED_BOARD_BOOT{{=}}1 STM32MP_SDMMC{{=}}1}} \ |
||
+ | DTB_FILE_NAME=stm32mp157c-ev1.dtb |
||
+ | |||
{{InternalInfo| Add the BUILD_PLAT flag for multiple storage purpose: |
{{InternalInfo| Add the BUILD_PLAT flag for multiple storage purpose: |
||
* Flash programming support |
* Flash programming support |