Difference between revisions of "How to compile the device tree with the Distribution Package"

[quality revision] [quality revision]
m
m
 

/tmp/bshtmldiff/sfr_62bab82960f9/91193.html (No such file or directory)

<noinclude>

{{ReviewsComments|-- [[User:Yves Coppeaux|Yves Coppeaux]] ([[User talk:Yves Coppeaux|talk]]) 16:56, 20 September 2022 (CEST)<br />bad title for this page but right category, it is not only DTS compile but a permanent distribution update, with a new machine definition via a customize meta-layer included DTS and if needed some recipes<br>

The update of DTS can be made with the update of the meta-st-stm32mp-addons, right ? so it is not mandatory to create a new layer.<br>

If we keep the option to create a new layer, I suggest to keep the name my-custo-layer instead of my-demo-layer created here  [[How to create a new open embedded layer]] }}
{{ReviewsComments | [[User:Romuald Jeanne|Romuald Jeanne]] ([[User talk:Romuald Jeanne|talk]]) 15:57, 21 November 2022 (CET) - This section deals with CubeMX DTS generated file that user want to build through our distribution package. It refers to [[How to create a new open embedded layer]] to initiate the needed layer, but then it explains how to configure the machine that will set-up use of CubeMX DTS files as source. We don't want user to directly modify our meta-st-stm32mp-addons layer, this layer is a sample one to help user to create its own layer and machine to compile the CubeMX DTS files.}}

{{ApplicableFor
|MPUs list=STM32MP13x, STM32MP15x
|MPUs checklist=STM32MP13x,STM32MP15x
}}</noinclude>

==Introduction==
This article is intended for Yocto experts, or people who have some practical experience of the Yocto environmment.<br><br>

This section describes the steps needed to create and configure a demo layer using DeviceTree files from the STM32CubeMX tool, and to add and configure a machine similar to those already supported by the OpenSTLinux Distribution Package (in particular the machine delivered inside the existing STM32MP BSP layer 'addons').<br>


Reminder: this addon-layer is deployed under the following path in the delivery : '''<path of OpenSTLinux distribution delivery>/layers/meta-st/meta-st-stm32mp-addons/'''

==Creating a new open embedded layer for your demo==
You first need to create a new layer. See the latest  [[How to create a new open embedded layer]]<br><br>

After creation, you have under '''<path of OpenSTLinux distribution delivery>/layers/meta-st/''':
<pre>

$ tree meta-my-demo-layer
meta-my-demo-layer
├── conf
│   └── layer.conf
├── recipes-example
│   └── example
│       └── example.bb
├── COPYING.MIT
└── README

3 directories, 4 files</pre>


===Update layer.conf file===
Open the layer.conf file and add the lines below for the licenses,  demo layer path, and dependency with the STM32MP BSP layer 'addons' :

 EULA_FILE_ST_:{{Highlight|stm32mpmydemo}} = "${LAYERDIR}/conf/eula/${MACHINE}"
 EULA_FILE_ST_MD5SUM_:{{Highlight|stm32mpmydemo}} = "8b505090fb679839cefbcc784afe8ce9"

 #Inform bitbake for adding another location to search for licenses
 LICENSE_PATH += "${LAYERDIR}/files/licenses"

 # Set a variable to get the STM32MP MX BSP location
 {{Highlight|STM32MP_MY_DEMO_BASE}} = "${LAYERDIR}"

 # This should only be incremented on significant changes that may
 # cause compatibility issues with other layers
 LAYERVERSION_meta-my-demo-layer = "1"

 LAYERDEPENDS_meta-my-demo-layer = "{{Highlight|stm-st-stm32mp-mx}}"

 # OpenEmbedded compatibility information
 # This should only be incremented on significant changes that will
 # cause compatibility issues with other layers
 LAYERVERSION_meta-my-demo-layer = "1"
 LAYERSERIES_COMPAT_meta-my-demo-layer = "dunfellkirkstone"

{{Info| LAYERSERIES_COMPAT must be aligned with the version of OpenEmbedded used.<br>Please refer to https://wiki.yoctoproject.org/wiki/Releases}}

===Create the machine for your demo===
====Prepare the machine configuration file====
* Copy the machine delivered inside the existing STM32MP BSP layer 'addons' into your demo layer

 $ cp <path of OpenSTLinux distribution delivery>/layers/meta-st/meta-st-stm32mp-addons/conf/machine/'''stm32mp1X-mx.conf''' <path of OpenSTLinux distribution delivery>/layers/meta-st/meta-my-demo-layer/conf/machine/'''stm32mp1-demo.conf'''

* Open stm32mp1-demo.conf and update the line below
 #@NEEDED_BSPLAYERS: layers/meta-openembedded/meta-oe layers/meta-openembedded/meta-python {{Highlight|layers/meta-st/meta-st-stm32mp-addons}}

* Replace STM32MP_MX_BASE by {{Highlight|STM32MP_MY_DEMO_BASE}}

* Add these lines after the series of includes: 

 # Define specific common machine name
 MACHINEOVERRIDES .= ":{{Highlight|stm32mpmydemo}}"

====Configure the machine configuration file for your demo====
{{:How to create your own machine}}

===Associate EULA with the new demo machine===
Copy the eula folder delivered inside the existing STM32MP BSP layer 'addons' into your demo layer 

 $ cp -Rf <path of OpenSTLinux distribution delivery>/layers/meta-st/meta-st-stm32mp-addons/conf/'''eula'''/ <path of OpenSTLinux distribution delivery>/layers/meta-st/meta-my-demo-layer/conf/.

Cleanup unexpected symbolic links from eula folder newly populated:

 $ find <path of OpenSTLinux distribution delivery>/layers/meta-st/meta-my-demo-layer/conf/eula -type l -exec rm -f {} \;

Then create the symbolic link with the machine used for your demo:

 $ cd <path of OpenSTLinux distribution delivery>/layers/meta-st/meta-my-demo-layer/conf/eula
 $ ln -sf ST_EULA_SLA stm32mp1-demo

===Move DeviceTree files and project coming from STM32CubeMX tool===
The principle is that the user generates devicetree files for the targeted demo from the STM32CubeMX tool.
{{Warning|'''Most of the time, generated devicetree files - mainly user sections - must be reworked by the end user for compilation and functional purposes. Each demo is delivered with an application note that describe changes applied on STM32CubeMX devicetree files'''}}.{{InternalInfo|For a motor control demo the application note is located [https://epm-st.st.com/ProjectServerST/Wildcat%20APPLI%20Introduction%20Package/Working%20Documents/Support%20and%20Application/Demonstrations/MotorControlAN_v1.01.docx here]}}
These files are then moved into the “mx” folder created into your demo layer  : '''<path of OpenSTLinux distribution delivery>/layers/meta-st/meta-my-demo-layer/mx/'''

Sub-folders are created and populated with the generated devicetree files:
 mx/${CUBEMX_PROJECT}/kernel
 mx/${CUBEMX_PROJECT}/u-boot
 mx/${CUBEMX_PROJECT}/tf-a
 mx/${CUBEMX_PROJECT}/optee-os

With {{Highlight|CUBEMX_PROJECT}} that is equal to the value defined inside the machine used for the demo.

===Update the README file===
Please update the README file with the information needed for building and executing the demo.

===Clean up useless content===
You can delete the content of the recipes-example folder created by the create-layer command.

After making all of the updates, your demo layer should be similar to:
<pre>

$ tree meta-my-demo-layer
meta-my-demo-layer
├── conf
│   ├── eula
│   │   ├── ST_EULA_SLA
│   │   ├── stm32mp1-demo -> ST_EULA_SLA
│   │   └──  ...
│   ├── machine
│   │   └── stm32mp1-demo.conf
│   └── layer.conf
├── mx
│   └── ${CUBEMX_PROJECT}
│            ├── kernel
│            │   └── stm32mp1XXx-my-demo-mx.dts
│            ├── optee-os
│            │   └── stm32mp1XXx-my-demo-mx.dts
│            ├── tf-a
│            │   ├── stm32mp1X-mx.dtsi
│            │   ├── stm32mp1XXx-my-demo-mx.dts
│            │   └── stm32mp1XXx-my-demo-mx-fw-config.dts
│            └── u-boot
│                ├── stm32mp1XXx-my-demo-mx.dts
│                └── stm32mp1XXx-my-demo-mx-u-boot.dtsi
├── COPYING.MIT
└── README</pre>


==Adding specific recipes and content necessary for your demo==

Examples of further add-on components: 
* Recipes for installing distro-specific configuration files
* Any image recipes specific to user distribution
* A ''psplash append file'' for a branded splash screen
* Any other append files to make custom changes

Some other added components (*bb) are more specific: images, system services, and so on (a non-exhaustive list is shown below):
* Recipes-core for ''psplash screen'', ''systemd services''
* Recipes-samples for example images
...<br>

<noinclude>

[[Category:How to customize software]]
{{PublicationRequestId | 12272| 2019-06-07}}</noinclude>
(5 intermediate revisions by 2 users not shown)
Line 1: Line 1:
 
<noinclude>
 
<noinclude>
  +
{{ReviewsComments|-- [[User:Yves Coppeaux|Yves Coppeaux]] ([[User talk:Yves Coppeaux|talk]]) 16:56, 20 September 2022 (CEST)<br />bad title for this page but right category, it is not only DTS compile but a permanent distribution update, with a new machine definition via a customize meta-layer included DTS and if needed some recipes<br>
  +
The update of DTS can be made with the update of the meta-st-stm32mp-addons, right ? so it is not mandatory to create a new layer.<br>
  +
If we keep the option to create a new layer, I suggest to keep the name my-custo-layer instead of my-demo-layer created here  [[How to create a new open embedded layer]] }}
  +
{{ReviewsComments | [[User:Romuald Jeanne|Romuald Jeanne]] ([[User talk:Romuald Jeanne|talk]]) 15:57, 21 November 2022 (CET) - This section deals with CubeMX DTS generated file that user want to build through our distribution package. It refers to [[How to create a new open embedded layer]] to initiate the needed layer, but then it explains how to configure the machine that will set-up use of CubeMX DTS files as source. We don't want user to directly modify our meta-st-stm32mp-addons layer, this layer is a sample one to help user to create its own layer and machine to compile the CubeMX DTS files.}}
  +
 
{{ApplicableFor
 
{{ApplicableFor
 
|MPUs list=STM32MP13x, STM32MP15x
 
|MPUs list=STM32MP13x, STM32MP15x
Line 32: Line 37:
 
Open the layer.conf file and add the lines below for the licenses,  demo layer path, and dependency with the STM32MP BSP layer 'addons' :
 
Open the layer.conf file and add the lines below for the licenses,  demo layer path, and dependency with the STM32MP BSP layer 'addons' :
   
  EULA_FILE_ST_{{Highlight|stm32mpmydemo}} = "${LAYERDIR}/conf/eula/${MACHINE}"
+
  EULA_FILE_ST:{{Highlight|stm32mpmydemo}} = "${LAYERDIR}/conf/eula/${MACHINE}"
  EULA_FILE_ST_MD5SUM_{{Highlight|stm32mpmydemo}} = "8b505090fb679839cefbcc784afe8ce9"
+
  EULA_FILE_ST_MD5SUM:{{Highlight|stm32mpmydemo}} = "8b505090fb679839cefbcc784afe8ce9"
 
   
 
   
 
  #Inform bitbake for adding another location to search for licenses
 
  #Inform bitbake for adding another location to search for licenses
Line 51: Line 56:
 
  # cause compatibility issues with other layers
 
  # cause compatibility issues with other layers
 
  LAYERVERSION_meta-my-demo-layer = "1"
 
  LAYERVERSION_meta-my-demo-layer = "1"
  LAYERSERIES_COMPAT_meta-my-demo-layer = "dunfell"
+
  LAYERSERIES_COMPAT_meta-my-demo-layer = "kirkstone"
   
 
{{Info| LAYERSERIES_COMPAT must be aligned with the version of OpenEmbedded used.<br>Please refer to https://wiki.yoctoproject.org/wiki/Releases}}
 
{{Info| LAYERSERIES_COMPAT must be aligned with the version of OpenEmbedded used.<br>Please refer to https://wiki.yoctoproject.org/wiki/Releases}}
Line 91: Line 96:
 
The principle is that the user generates devicetree files for the targeted demo from the STM32CubeMX tool.
 
The principle is that the user generates devicetree files for the targeted demo from the STM32CubeMX tool.
 
{{Warning|'''Most of the time, generated devicetree files - mainly user sections - must be reworked by the end user for compilation and functional purposes. Each demo is delivered with an application note that describe changes applied on STM32CubeMX devicetree files'''}}.
 
{{Warning|'''Most of the time, generated devicetree files - mainly user sections - must be reworked by the end user for compilation and functional purposes. Each demo is delivered with an application note that describe changes applied on STM32CubeMX devicetree files'''}}.
{{InternalInfo|For a motor control demo the application note is located [https://epm-st.st.com/ProjectServerST/Wildcat%20APPLI%20Introduction%20Package/Working%20Documents/Support%20and%20Application/Demonstrations/MotorControlAN_v1.01.docx here]}}
+
 
 
These files are then moved into the “mx” folder created into your demo layer  : '''<path of OpenSTLinux distribution delivery>/layers/meta-st/meta-my-demo-layer/mx/'''
 
These files are then moved into the “mx” folder created into your demo layer  : '''<path of OpenSTLinux distribution delivery>/layers/meta-st/meta-my-demo-layer/mx/'''