Difference between revisions of "How to compile the device tree with the Developer Package"

[quality revision] [quality revision]
(Kernel : copy the DTB into bootfs)
(Prerequisites)
 

1 Purpose[edit]

This article explains how to update the boot chain (trusted mode) for a "custom" device tree.
In particular, STM32CubeMX can generate a "custom" device tree.

This article describes how to update the device tree compiled (DTB) part of the boot binaries.

2 Rationale[edit]

There are various rationale for using a custom device tree, such as:

  • the description of a new and private board
  • the swapping of some internal peripherals from Cortex®-M side to Cortex-A side (or the opposite)

3 Prerequisites[edit]

Info.png Even if STMicroelectronics strongly recommends to use a Linux® environment, the steps described in this article can be executed in a WSL2 (Windows Sub-system Linux 2) environment.

Compiling a new device tree means updating three software components belonging to the complete boot chain (trusted mode), Trusted Firmware A (TF-A), u-boot, and Linux kernel.


The material required to update the above software components is the following:

  • Starter package:
    • the flashlayout as well as the images to flash, provided within the IMAGESen.FLASH-ststm32mp1-imageopenstlinux<YY>-weston-openstlinux-weston-stm32mp1<MM>-<DD>.tar.xz file (download it from st.com)
  • Developer package:
    • the component sources and patches, provided within the en.SOURCES-ststm32mp1-imageopenstlinux-weston<YY>-openstlinux<MM>-weston-stm32mp1<DD>.tar.xz file (download it from st.com)
    • the SDK toolchain, provided within the en.SDK-x86_64-ststm32mp1-imageopenstlinux-weston<YY>-openstlinux<MM>-weston-stm32mp1<DD>.tar.xz file (download it from st.com)
  • the STM32CubeProgrammer, which is the tool used to flash the images and binaries into the target.


  • Custom device tree sources:
    • In the rest of this document, we assume that the custom device tree is generated by STM32CubeMX and stored in a MyDeviceTree_fromCubeMX.tar.xz tarball with following file tree:
MyDeviceTree_fromCubeMX
|-- kernel
|   |-- stm32mp157c-mydevicetree-mx.dts
|-- tf-a
|  |-- stm32mp15-mx.h
|  |-- stm32mp157c-mydevicetree-mx.dts
|-- u-boot
|  |-- stm32mp15-mx.h
|  |-- stm32mp157c-mydevicetree-mx-u-boot.dtsi
|  |-- stm32mp157c-mydevicetree-mx.dts


4 Preparing your environment[edit]

It is recommended to organize the numerous inputs described in #Prerequisites in your environment.
First create a dedicated WORKDIR under your HOME folder and copy there all the inputs listed in #Prerequisites:

PC $> cd $HOME
PC $> mkdir WORKDIR
PC $> cd WORKDIR
PC $> export WORKDIR="$PWD"
PC $> tar --strip-components=1 -xf <IMAGES<FLASH-st-image-weston-openstlinux-weston-stm32mp1.tar.xz> -C $WORKDIR/
PC $> tar --strip-components=1 -xf <SOURCES-st-image-weston-openstlinux-weston-stm32mp1.tar.xz> -C $WORKDIR/
PC $> tar --strip-components=1 -xf <SDK-st-image-weston-openstlinux-weston-stm32mp1.tar.xz> -C $WORKDIR/
PC $> tar xf <MyDeviceTree_fromCubeMX.tar.xz> -C $WORKDIR/

Then proceed with the SDK installation.


The commands described in the rest of the document must be run in an SDK environment context: (Starting_up_the_SDK).

5 Updating the kernel device tree[edit]

Since 'extlinux.conf' explicitly points to the DTB, just update the kernel device tree by replacing the DTB file of the '/boot' partition. The path used must be something like '/boot/<devicetree>.dtb'.

The following chapters describe the procedure to generate and copy the new DTB into the target.

5.1 Kernel : unpack and patch sources[edit]

Info.png The procedure below is equivalent to chapter 3 of the README_HOWTO.txt file available in $WORKDIR/sources/arm-openstlinux_weston-linux-gnueabi/linux-stm32mp-*

Run the following command into a shell:

PC $> pushd $WORKDIR
PC $> mkdir -p kernel
PC $> tar xf sources/arm-openstlinux_weston-linux-gnueabi/linux-stm32mp-4.19-r0/linux-4.19.*.tar.xz -C kernel
PC $> mv kernel/linux-* kernel/kernel-sources/
PC $> pushd kernel/kernel-sources/
PC $> for p in $(ls -1 ../../sources/arm-openstlinux_weston-linux-gnueabi/linux-stm32mp-4.19-r0/*.patch); do patch -p1 < $p; done
PC $> popd
PC $> popd

5.2 Kernel : copy the DTS into the source code[edit]

PC $> pushd $WORKDIR
PC $> cp -r MyDeviceTree_fromCubeMX/kernel/* kernel/kernel-sources/arch/arm/boot/dts/
PC $> popd

5.3 Kernel : regenerate the kernel DTB[edit]

Info.png The procedure below is equivalent to chapter 5 of the README_HOWTO.txt file available in $WORKDIR/sources/arm-openstlinux_weston-linux-gnueabi/linux-stm32-*
PC $> pushd $WORKDIR/kernel/kernel-sources
PC $> make O="$PWD/../build" multi_v7_defconfig
PC $> for f in `ls -1 ../../sources/arm-openstlinux_weston-linux-gnueabi/linux-stm32mp-4.19-r0/fragment*.config`; do scripts/kconfig/merge_config.sh -m -r -O $PWD/../build $PWD/../build/.config $f; done
PC $> make oldconfig O="$PWD/../build"
PC $> make stm32mp157c-mydevicetree-mx.dtb LOADADDR=0xC2000040 O="$PWD/../build"
PC $> popd
PC $> ls -l $WORKDIR/kernel/build/arch/arm/boot/dts/stm32mp157c-mydevicetree-mx.dtb

5.4 Kernel : copy the DTB into bootfs[edit]

First of all #Updating bootfs with the new DTB so that it is taken it into account at the next boot of the target.

Then, if needed, #Updating extlinux for the target according to this new DTB filename. This is only required if the filename of the generated DTB is different from the one used by extlinux to boot.

6 Updating the u-boot device tree[edit]

To update the u-boot device tree, replace the DTB part of the u-boot binary.
Adding a new device tree to the u-boot source code forces the Makefile to regenerate a new u-boot.stm32 containing the new DTS.
The following chapters describe the procedure to update the u-boot device tree.

6.1 U-boot : unpack and patch sources[edit]

Info.png The procedure below is equivalent to chapter 3 of the README_HOWTO.txt file available in $WORKDIR/sources/arm-openstlinux_weston-linux-gnueabi//u-boot-stm32mp-*
PC $> pushd $WORKDIR
PC $> mkdir -p u-boot
PC $> tar xf sources/arm-openstlinux_weston-linux-gnueabi/u-boot-stm32mp-*/v*.tar.gz -C u-boot
PC $> mv u-boot/u-boot* u-boot/u-boot-sources/
PC $> pushd u-boot/u-boot-sources
PC $> for p in $(ls -1 ../../sources/arm-openstlinux_weston-linux-gnueabi/u-boot-stm32mp-*/*.patch); do patch -p1 < $p; done
PC $> popd

6.2 U-boot : copy the DTS in the u-boot source code[edit]

PC $> pushd $WORKDIR
PC $> cp MyDeviceTree_fromCubeMX/u-boot/* u-boot/u-boot-sources/arch/arm/dts/
PC $> popd

Starting from u-boot 2019.04 version the device tree to be compiled must be explicitly added to the dts Makefile, u-boot/u-boot-sources/arch/arm/dts/Makefile:

 dtb-y += stm32mp157c-mydevicetree-mx.dtb
 targets += $(dtb-y)

6.3 U-boot : regenerate u-boot.stm32[edit]

Info.png The procedure below is equivalent to chapter 5.1 of the README_HOWTO.txt file available in $WORKDIR/sources/arm-openstlinux_weston-linux-gnueabi//u-boot-stm32mp-*
PC $> pushd $WORKDIR/u-boot/u-boot-sources
PC $> make stm32mp15_<config>_defconfig
<config> : could be trusted or basic according the boot type
PC $> make DEVICE_TREE=<device tree> all
<device tree> : is the device tree just copied, i.e.: stm32mp157c-mydevicetree-mx
PC $> popd
PC $> ls -l $WORKDIR/u-boot/u-boot-sources/u-boot.stm32

6.4 U-boot : copy the u-boot into the target[edit]

  • Because of 'extlinux' and before flashing the new u-boot.stm32, make sure #Updating extlinux is compliant with the 'compatible' value in the DTS file.
  • Then flash the u-boot.stm32 into the 'ssbl' partition of the target using STM32CubeProgrammer.

7 Updating the TF-A device tree[edit]

To update the TF-A device tree, replace the DTB part of the TF-A binary.
The TF-A binary allocates a 'fixed' area for the DTB, just after the 'mkimage" headers. If the DTB is smaller than the reserved area, the remaining memory is padded with zero.

Below the procedure to generate TF-A with a new DTB and then flash it on the target:

7.1 TF-A : unpack and patch sources[edit]

Info.png The procedure below is equivalent to chapter 3 of the README_HOWTO.txt file available in $WORKDIR/sources/arm-openstlinux_weston-linux-gnueabi/tf-a-stm32mp-*
PC $> pushd $WORKDIR
PC $> mkdir -p tf-a
PC $> tar xf sources/arm-openstlinux_weston-linux-gnueabi/tf-a-stm32mp-*/v*.tar.gz -C tf-a
PC $> mv tf-a/arm-trusted-firmware-* tf-a/tf-a-sources
PC $> pushd tf-a/tf-a-sources
PC $> for p in $(ls -1 ../../sources/arm-openstlinux_weston-linux-gnueabi/tf-a-stm32mp-*/*.patch); do patch -p1 < $p; done
PC $> popd
PC $> popd

7.2 TF-A : copy the DTS into the source code[edit]

PC $> pushd $WORKDIR
PC $> cp -r tf-a/ MyDeviceTree_fromCubeMX/tf-a/* tf-a/tf-a-sources/fdts/
PC $> popd

7.3 TF-A : regenerate TF-A.stm32[edit]

Info.png The procedure below is equivalent to chapter 5 of the README_HOWTO.txt file available in $WORKDIR/st-image-weston-openstlinux-weston-stm32mp1/sources/arm-openstlinux_weston-linux-gnueabi/tf-a-stm32mp-*
PC $> pushd $WORKDIR/tf-a/tf-a-sources
PC $> make -f $PWD../../sources/arm-openstlinux_weston-linux-gnueabi/tf-a-stm32mp-2.0-r0/Makefile.sdk TFA_DEVICETREE=<device tree> TF_A_CONFIG=<config> all
<config> : could be trusted or basic according the boot type
<device tree> : is the device tree just copied, i.e.: stm32mp157c-mydevicetree-mx
PC $> popd
PC $> ls -l $WORKDIR/tf-a/build/<config>/tf-a-<device tree>-<config>.stm32

7.4 TF-A : copy the DTB in target/bootfs[edit]

Then flash the tf-a-*.stm32 into the 'fsbl1' and 'fsbl2' partitions of the target with STM32CubeProgrammer

Warning.png 'fsbl1' and 'fsbl2' are two redondant partitions and so, they should have same content

8 Update methods[edit]

8.1 Updating bootfs[edit]

There are two methods to update bootfs

  • On an up and running target
PC $> scp stm32mp157c-mydevicetree-mx.dtb root@<Target_IP>:/boot/
  • Directly into 'bootfs' image

You do not need to have a target up and running. Only the "st-image-bootfs-openstlinux-weston-stm32mp1.ext4" file is required. To modify an 'ext4' file, a loopback mount, avaible within any Linux Distribution (even through WSL2), is required:

PC $> mkdir -p $WORKING/bootfs
PC $> mount -o loop <st-image-bootfs-openstlinux-weston-stm32mp1.ext4> $WORKING/bootfs
##Then copy the new dtb file at the root of $WORKING/bootfs
PC $> umount $WORKING/bootfs
PC $> sync
PC $> dd if=<st-image-bootfs-openstlinux-weston-stm32mp1.ext4> of=/dev/mmblk0p4 conv=fdatasync
Info.png The '/dev/mmcblk0p4' is in case of the sdcard is inserted in dedicated drive of the PC, using an USB sdcard reader will probably create /dev/sdb4 entry.

8.2 Updating extlinux[edit]

8.2.1 extlinux basics[edit]

extlinux describes how u-boot boots. Updating extlinux consists in updating the extlinux.conf:

  • In case of an DK-2 board booting from the sdcard. The extlinux.conf file is located in /boot/mmc0_stm32mp157c-dk2_extlinux/,
  • otherwise if mmc0_<something>_extlinux directory is not available, extlinux.conf is located in /boot/extlinux/.

extlinux.conf is the description of a boot menu with one or several entries; 'DEFAULT' selects the default entry.
Below an example of extlinux.conf:

menu title Select the boot mode
MENU BACKGROUND ../splash.bmp
TIMEOUT 5
DEFAULT stm32mp157c-mydevicetree-mx
LABEL stm32mp157c-dk2-sdcard
        KERNEL /uImage
        FDT /stm32mp157c-dk2.dtb
        APPEND root=/dev/mmcblk0p6 rootwait rw console=ttySTM0,115200
LABEL stm32mp157c-dk2-a7-examples-sdcard
        KERNEL /uImage
        FDT /stm32mp157c-dk2-a7-examples.dtb
        APPEND root=/dev/mmcblk0p6 rootwait rw console=ttySTM0,115200
LABEL stm32mp157c-dk2-m4-examples-sdcard
        KERNEL /uImage
        FDT /stm32mp157c-dk2-m4-examples.dtb
        APPEND root=/dev/mmcblk0p6 rootwait rw console=ttySTM0,115200
LABEL stm32mp157c-mydevicetree-mx
       KERNEL /uImage
       FDT /stm32mp157c-mydevicetree-mx.dtb
       APPEND root=/dev/mmcblk0p6 rootwait rw console=ttySTM0,115200

Please update/add the highlighted lines according to what have been compiled in chapter 5, 6 and/or 7:

  • DEFAULT: This is the default 'LABEL' to boot
  • LABEL : The entry 'LABEL' is the value of 'compatible' of the DTS file compiled with u-boot.
    The 'compatible' value is at head of the DTS file and looks like : "st,stm32mp157c-mydevicetree-mx"
  • FDT : The path from /boot of the kernel DTB to use

8.2.2 Updating extlinux[edit]

Updating 'extlinux' consists in modifying the extlinux.conf. There are two ways to do this:

  • On an up and running target

Open an ssh connection to the target or use a direct connection with a tty terminal. Then use an vi editor to modify the extlinux.conf file.

Do not forget to synchronize the file system before rebooting the target:
Board $> sync
  • Into 'bootfs' image directly

You do not need to have a target up and running. Only the "st-image-bootfs-openstlinux-weston-stm32mp1.ext4" file is required. To modify an 'ext4' file, a loopback mount tool, avaible in any Linux Distribution (even through WSL2), is needed:

PC $> mkdir -p $WORKING/bootfs
PC $> mount -o loop <st-image-bootfs-openstlinux-weston-stm32mp1.ext4> $WORKING/bootfs
##Then edit the extlinux.conf file (for WSL2 use a 'Linux' type editor; vi, ...)
##Once extlinux.conf up-to-date, umount loopback and flash the bootfs into sdcard with STM32CubeProgrammer
==Purpose==
This article explains how to update the [[Boot_chains_overview|boot chain]] (trusted mode) for a "custom" device tree. <br/>

In particular, STM32CubeMX can generate a "custom" device tree.<br/>


This article describes how to update the device tree compiled (DTB) part of the boot binaries.

==Rationale==

There are various rationale for using a custom ''device tree'', such as:
* the description of a new and private board
* the swapping of some internal peripherals from Cortex<sup>&reg;</sup>-M side to Cortex-A side (or the opposite)

==Prerequisites==
{{Info|Even if STMicroelectronics strongly recommends to use a Linux<sup>&reg;</sup> environment, the steps described in this article can be executed in a [[PC_prerequisites#WSL2_-28experimental-29|WSL2]] (Windows Sub-system Linux 2) environment. }}

Compiling a new device tree means updating three software components belonging to the complete [[Boot_chains_overview|boot chain]] (trusted mode), Trusted Firmware A (TF-A), u-boot, and Linux kernel.<br/>


The material required to update the above software components is the following:
* '''[[Which STM32MPU Embedded Software Package better suits your needs#Starter_Package|Starter package]]''': 
** the flashlayout as well as the images to flash, provided within the '''IMAGES-st-image-weston-openstlinux-weston-stm32mp1.tar.xz''' fileen.FLASH-stm32mp1-openstlinux&lt;YY&gt;-&lt;MM&gt;-&lt;DD&gt;.tar.xz''' file (download it from [https://www.st.com/content/st_com/en/products/embedded-software/mcu-mpu-embedded-software/stm32-embedded-software/stm32-mpu-openstlinux-distribution/stm32mp1starter.html#get-software st.com])* '''[[Which STM32MPU Embedded Software Package better suits your needs#Developer_Package|Developer package]]''': 
** the component sources and patches, provided within the '''en.SOURCES-st-image-weston-openstlinux-weston-stm32mp1.tar.xz''' file stm32mp1-openstlinux-&lt;YY&gt;-&lt;MM&gt;-&lt;DD&gt;.tar.xz''' file (download it from [https://www.st.com/content/st_com/en/products/embedded-software/mcu-mpu-embedded-software/stm32-embedded-software/stm32-mpu-openstlinux-distribution/stm32mp1dev.html#get-software st.com])** the SDK toolchain, provided within the '''en.SDK-x86_64-st-image-weston-openstlinux-weston-stm32mp1.tar.xz''' filestm32mp1-openstlinux-&lt;YY&gt;-&lt;MM&gt;-&lt;DD&gt;.tar.xz''' file (download it from [https://www.st.com/content/st_com/en/products/embedded-software/mcu-mpu-embedded-software/stm32-embedded-software/stm32-mpu-openstlinux-distribution/stm32mp1dev.html#get-software st.com])* the '''[[STM32CubeProgrammer]]''', which is the tool used to flash the images and binaries into the target. <br/>

* '''Custom device tree sources''':
** In the rest of this document, we assume that the custom device tree is generated by [[STM32CubeMX]] and stored in a ''MyDeviceTree_fromCubeMX.tar.xz'' tarball with following file tree:<pre>MyDeviceTree_fromCubeMX
|-- kernel
|   |-- stm32mp157c-mydevicetree-mx.dts
|-- tf-a
|  |-- stm32mp15-mx.h
|  |-- stm32mp157c-mydevicetree-mx.dts
|-- u-boot
|  |-- stm32mp15-mx.h
|  |-- stm32mp157c-mydevicetree-mx-u-boot.dtsi
|  |-- stm32mp157c-mydevicetree-mx.dts</pre>
<br/>

* Make sure the hardware configuration described in '''[[PC_prerequisites#Linux PC]] has been executed''' (even with a  [[PC_prerequisites#WSL2_-28experimental-29|WSL2]] setup)

==Preparing your environment==
It is recommended to organize the numerous inputs described in [[#Prerequisites]] in your environment.<br/>

First create a dedicated ''WORKDIR'' under your ''HOME'' folder and copy there all the inputs listed in [[#Prerequisites]]:
:{{PC$}} cd $HOME:{{PC$}} mkdir WORKDIR
:{{PC$}} cd WORKDIR
:{{PC$}} export WORKDIR="$PWD"
:{{PC$}} tar --strip-components=1 -xf ''<IMAGES-st-image-weston-openstlinux-weston-stm32mp1.tar.xz><FLASH-st-image-weston-openstlinux-weston-stm32mp1.tar.xz>'' -C $WORKDIR/
:{{PC$}} tar --strip-components=1 -xf ''<SOURCES-st-image-weston-openstlinux-weston-stm32mp1.tar.xz>'' -C $WORKDIR/
:{{PC$}} tar --strip-components=1 -xf ''<SDK-st-image-weston-openstlinux-weston-stm32mp1.tar.xz>'' -C $WORKDIR/
:{{PC$}} tar xf ''<MyDeviceTree_fromCubeMX.tar.xz>'' -C $WORKDIR/

Then proceed with the [[Install_the_SDK#Run_the_SDK_installation_script|SDK installation]].

The commands described in the rest of the document must be run in an SDK environment context: ([[Install_the_SDK#Starting_up_the_SDK|Starting_up_the_SDK]]).

==Updating the kernel device tree ==
Since 'extlinux.conf' explicitly points to the DTB, just update the kernel device tree by replacing the DTB file of the '/boot' partition. The path used must be something like '/boot/<devicetree>.dtb'.

The  following chapters describe the procedure to generate and copy the new DTB into the target.
=== Kernel : unpack and patch sources ===
{{Info|The procedure below is equivalent to '''chapter 3 of the [https://github.com/STMicroelectronics/meta-st-stm32mp/blob/thud/recipes-kernel/linux/linux-stm32mp/README.HOW_TO.txt README_HOWTO.txt]''' file available in ''$WORKDIR/sources/arm-openstlinux_weston-linux-gnueabi/linux-stm32mp-*''}}

Run the following command into a shell:
:{{PC$}} pushd $WORKDIR
:{{PC$}} mkdir -p kernel
:{{PC$}} tar xf sources/arm-openstlinux_weston-linux-gnueabi/linux-stm32mp-4.19-r0/linux-4.19.*.tar.xz -C kernel
:{{PC$}} mv kernel/linux-* kernel/kernel-sources/
:{{PC$}} pushd kernel/kernel-sources/
:{{PC$}} for p in $(ls -1 ../../sources/arm-openstlinux_weston-linux-gnueabi/linux-stm32mp-4.19-r0/*.patch); do patch -p1 < $p; done
:{{PC$}} popd
:{{PC$}} popd

=== Kernel : copy the DTS into the source code ===
:{{PC$}} pushd $WORKDIR
:{{PC$}} cp -r MyDeviceTree_fromCubeMX/kernel/* kernel/kernel-sources/arch/arm/boot/dts/
:{{PC$}} popd

=== Kernel : regenerate the kernel DTB ===
{{Info|The procedure below is equivalent to '''chapter 5 of the [https://github.com/STMicroelectronics/meta-st-stm32mp/blob/thud/recipes-kernel/linux/linux-stm32mp/README.HOW_TO.txt README_HOWTO.txt]''' file available in $WORKDIR/sources/arm-openstlinux_weston-linux-gnueabi/linux-stm32-*}}

:{{PC$}} pushd $WORKDIR/kernel/kernel-sources
:{{PC$}} make O="$PWD/../build" multi_v7_defconfig
:{{PC$}} for f in `ls -1 ../../sources/arm-openstlinux_weston-linux-gnueabi/linux-stm32mp-4.19-r0/fragment*.config`; do scripts/kconfig/merge_config.sh -m -r -O $PWD/../build $PWD/../build/.config $f; done
:{{PC$}} make oldconfig O="$PWD/../build"
:{{PC$}} make stm32mp157c-mydevicetree-mx.dtb LOADADDR=0xC2000040 O="$PWD/../build"
:{{PC$}} popd
:{{PC$}} ls -l $WORKDIR/kernel/build/arch/arm/boot/dts/stm32mp157c-mydevicetree-mx.dtb

=== Kernel : copy the DTB into bootfs ===
First of all [[#Updating bootfs]] with the new DTB so that it is taken it into account at the next boot of the target.

Then, if needed, [[#Updating extlinux]] for the target according to this new DTB filename. This is only required if the filename of the generated DTB is different from the one used by extlinux to boot.

== Updating the u-boot device tree ==
To update the u-boot device tree, replace the DTB part of the u-boot binary.<br/>
Adding a new device tree to the u-boot source code forces the Makefile to regenerate a new u-boot.stm32 containing the new DTS. <br/>

The following chapters describe the procedure to update the u-boot device tree.
=== U-boot : unpack and patch sources ===
{{Info|The procedure below is equivalent to '''chapter 3 of the [https://github.com/STMicroelectronics/meta-st-stm32mp/blob/thud/recipes-bsp/u-boot/u-boot-stm32mp/README.HOW_TO.txt README_HOWTO.txt]''' file available in $WORKDIR/sources/arm-openstlinux_weston-linux-gnueabi//u-boot-stm32mp-*}}

:{{PC$}} pushd $WORKDIR
:{{PC$}} mkdir -p u-boot
:{{PC$}} tar xf sources/arm-openstlinux_weston-linux-gnueabi/u-boot-stm32mp-*/v*.tar.gz -C u-boot
:{{PC$}} mv u-boot/u-boot* u-boot/u-boot-sources/
:{{PC$}} pushd u-boot/u-boot-sources
:{{PC$}} for p in $(ls -1 ../../sources/arm-openstlinux_weston-linux-gnueabi/u-boot-stm32mp-*/*.patch); do patch -p1 < $p; done
:{{PC$}} popd

=== U-boot : copy the DTS in the u-boot source code ===
:{{PC$}} pushd $WORKDIR
:{{PC$}} cp MyDeviceTree_fromCubeMX/u-boot/* u-boot/u-boot-sources/arch/arm/dts/
:{{PC$}} popd

'''Starting from ''u-boot'' 2019.04 version the device tree to be compiled must be explicitly added to the ''dts Makefile''''', ''u-boot/u-boot-sources/arch/arm/dts/Makefile'':
  dtb-y += {{highlight|stm32mp157c-mydevicetree-mx.dtb}}
  targets += $(dtb-y)

=== U-boot : regenerate u-boot.stm32 ===
{{Info|The procedure below is equivalent to '''chapter 5.1 of the [https://github.com/STMicroelectronics/meta-st-stm32mp/blob/thud/recipes-bsp/u-boot/u-boot-stm32mp/README.HOW_TO.txt README_HOWTO.txt]''' file available in $WORKDIR/sources/arm-openstlinux_weston-linux-gnueabi//u-boot-stm32mp-*}} 

:{{PC$}} pushd $WORKDIR/u-boot/u-boot-sources
:{{PC$}} make stm32mp15_''<config>''_defconfig
: ''<config>'' : could be ''trusted'' or ''basic'' according the boot type
:{{PC$}} make DEVICE_TREE=''<device tree>'' all
: ''<device tree>'' : is the device tree just copied, i.e.: stm32mp157c-mydevicetree-mx
:{{PC$}} popd
:{{PC$}} ls -l $WORKDIR/u-boot/u-boot-sources/'''u-boot.stm32'''

=== U-boot : copy the u-boot into the target ===
* Because of 'extlinux' and before flashing the new u-boot.stm32, make sure [[#Updating extlinux]] is compliant with the 'compatible' value in the DTS file.<br/>


* Then flash the u-boot.stm32 into the 'ssbl' partition of the target using [[STM32CubeProgrammer]].

==Updating the TF-A device tree ==
To update the TF-A device tree, replace the DTB part of the TF-A binary.<br/>

The TF-A binary allocates a 'fixed' area for the DTB, just after the 'mkimage" headers. If the DTB is smaller than the reserved area, the remaining memory is padded with zero.

Below the procedure to generate TF-A with a new DTB and then flash it on the target:<br/>

=== TF-A : unpack and patch sources ===
{{Info|The procedure below is equivalent to '''chapter 3 of the [https://github.com/STMicroelectronics/meta-st-stm32mp/blob/thud/recipes-bsp/trusted-firmware-a/tf-a-stm32mp/README.HOW_TO.txt README_HOWTO.txt]''' file available in $WORKDIR/sources/arm-openstlinux_weston-linux-gnueabi/tf-a-stm32mp-*}}

:{{PC$}} pushd $WORKDIR
:{{PC$}}  mkdir -p tf-a
:{{PC$}}  tar xf sources/arm-openstlinux_weston-linux-gnueabi/tf-a-stm32mp-*/v*.tar.gz -C tf-a
:{{PC$}}  mv tf-a/arm-trusted-firmware-* tf-a/tf-a-sources
:{{PC$}}  pushd tf-a/tf-a-sources
:{{PC$}}  for p in $(ls -1 ../../sources/arm-openstlinux_weston-linux-gnueabi/tf-a-stm32mp-*/*.patch); do patch -p1 < $p; done
:{{PC$}}  popd
:{{PC$}}  popd

=== TF-A : copy the DTS into the source code ===
:{{PC$}}  pushd $WORKDIR
:{{PC$}}  cp -r tf-a/MyDeviceTree_fromCubeMX/tf-a/* tf-a/tf-a-sources/fdts/
:{{PC$}}  popd

=== TF-A : regenerate TF-A.stm32 ===
{{Info|The procedure below is equivalent to '''chapter 5 of the [https://github.com/STMicroelectronics/meta-st-stm32mp/blob/thud/recipes-bsp/trusted-firmware-a/tf-a-stm32mp/README.HOW_TO.txt README_HOWTO.txt]''' file available in $WORKDIR/st-image-weston-openstlinux-weston-stm32mp1/sources/arm-openstlinux_weston-linux-gnueabi/tf-a-stm32mp-* }}

:{{PC$}} pushd $WORKDIR/tf-a/tf-a-sources
:{{PC$}} make -f $PWD/../../../sources/arm-openstlinux_weston-linux-gnueabi/tf-a-stm32mp-2.0-r0/Makefile.sdk TFA_DEVICETREE=''<device tree>'' TF_A_CONFIG=''<config>'' all
::''<config>'' : could be '''''trusted''''' or ''basic'' according the boot type
::''<device tree>'' : is the device tree just copied, i.e.: '''''stm32mp157c-mydevicetree-mx'''''
:{{PC$}} popd
:{{PC$}} ls -l $WORKDIR/tf-a/build/''<config>''/tf-a-''<device tree>''-''<config>''.stm32

=== TF-A : copy the DTB in target/bootfs ===
Then flash the tf-a-*.stm32 into the 'fsbl1' and 'fsbl2' partitions of the target with [[STM32CubeProgrammer]]
{{warning|'fsbl1' and 'fsbl2' are two redondant partitions and so, they should have same content}}

= Update methods =
== Updating bootfs ==
There are two methods to update bootfs 
* <u>{{STDarkBlue|On an up and running target}}</u>

:{{PC$}} scp stm32mp157c-mydevicetree-mx.dtb root@<Target_IP>:/boot/
* <u>{{STDarkBlue|Directly into 'bootfs' image}}</u>

You do not need to have a target up and running. Only the "st-image-bootfs-openstlinux-weston-stm32mp1.ext4" file is required.
To modify an 'ext4' file, a loopback mount, avaible within any Linux Distribution (even through [[PC_prerequisites#WSL2_-28experimental-29|WSL2]]), is required:
:{{PC$}} mkdir -p $WORKING/bootfs
:{{PC$}} mount -o loop {{HighlightParam|&lt;st-image-bootfs-openstlinux-weston-stm32mp1.ext4&gt;}} $WORKING/bootfs
:{{grey|##Then copy the new dtb file at the root of $WORKING/bootfs}}
:{{PC$}} umount $WORKING/bootfs
:{{PC$}} sync
:{{PC$}} dd if={{HighlightParam|&lt;st-image-bootfs-openstlinux-weston-stm32mp1.ext4&gt;}} of={{HighlightParam|/dev/mmblk0p4}} conv=fdatasync
:{{info|The '/dev/mmcblk0p4' is in case of the sdcard is inserted in dedicated drive of the PC, using an USB sdcard reader will probably create /dev/sdb4 entry.}}

== Updating extlinux ==
=== extlinux basics ===
'''extlinux''' describes how u-boot boots. Updating '''extlinux''' consists in updating the extlinux.conf:
* In case of an DK-2 board booting from the sdcard. The '''extlinux.conf''' file is located in ''/boot/mmc0_stm32mp157c-dk2_extlinux/'',
* otherwise if ''mmc0_{{HighlightParam|&lt;something&gt;}}_extlinux'' directory is not available, '''extlinux.conf''' is located in  ''/boot/extlinux/''.

'''extlinux.conf''' is the description of a boot menu with one or several entries; 'DEFAULT' selects the default entry.<br/>

Below an example of '''extlinux.conf''':
 menu title Select the boot mode
 MENU BACKGROUND ../splash.bmp
 TIMEOUT 5
 {{red|{{highlight|DEFAULT}} stm32mp157c-mydevicetree-mx}}
 LABEL stm32mp157c-dk2-sdcard
         KERNEL /uImage
         FDT /stm32mp157c-dk2.dtb
         APPEND root=/dev/mmcblk0p6 rootwait rw console=ttySTM0,115200
 LABEL stm32mp157c-dk2-a7-examples-sdcard
         KERNEL /uImage
         FDT /stm32mp157c-dk2-a7-examples.dtb
         APPEND root=/dev/mmcblk0p6 rootwait rw console=ttySTM0,115200
 LABEL stm32mp157c-dk2-m4-examples-sdcard
         KERNEL /uImage
         FDT /stm32mp157c-dk2-m4-examples.dtb
         APPEND root=/dev/mmcblk0p6 rootwait rw console=ttySTM0,115200
 {{red|{{highlight|LABEL}} stm32mp157c-mydevicetree-mx
        KERNEL /uImage
        {{highlight|FDT}} /stm32mp157c-mydevicetree-mx.dtb
        APPEND root&#61;/dev/mmcblk0p6 rootwait rw console&#61;ttySTM0,115200}}

Please update/add the highlighted lines according to what have been compiled in chapter 5, 6 and/or 7:
* {{highlight|DEFAULT}}: This is the default 'LABEL' to boot
* {{highlight|LABEL}} : The entry 'LABEL' is the value of 'compatible' of the DTS file compiled with u-boot.
*: The 'compatible' value is at head of the DTS file and looks like : "st,stm32mp157c-mydevicetree-mx"
* {{highlight|FDT}} : The path from /boot of the kernel DTB to use

=== Updating extlinux ===
Updating 'extlinux' consists in modifying the extlinux.conf. There are two ways to do this:
* <u>{{STDarkBlue|On an up and running target}}</u>

Open an ssh connection to the target or use a direct connection with a tty terminal. Then use an vi editor to modify the extlinux.conf file.<br/>

:{{highlight| Do not forget to synchronize the file system before rebooting the target:}}
:{{Board$}} sync

* <u>{{STDarkBlue|Into 'bootfs' image directly}}</u>

You do not need to have a target up and running. Only the "st-image-bootfs-openstlinux-weston-stm32mp1.ext4" file is required.
To modify an 'ext4' file, a loopback mount tool, avaible in any Linux Distribution (even through [[PC_prerequisites#WSL2_-28experimental-29|WSL2]]), is needed:
:{{PC$}} mkdir -p $WORKING/bootfs
:{{PC$}} mount -o loop {{HighlightParam|&lt;st-image-bootfs-openstlinux-weston-stm32mp1.ext4&gt;}} $WORKING/bootfs
:{{grey|##Then edit the extlinux.conf file (for WSL2 use a 'Linux' type editor; vi, ...)}}
:{{grey|##Once extlinux.conf up-to-date, umount loopback and flash the bootfs into sdcard with [[STM32CubeProgrammer]]}}
<noinclude>

[[Category:How to build software]]</noinclude>
(17 intermediate revisions by the same user not shown)
Line 19: Line 19:
 
The material required to update the above software components is the following:
 
The material required to update the above software components is the following:
 
* '''[[Which STM32MPU Embedded Software Package better suits your needs#Starter_Package|Starter package]]''':  
 
* '''[[Which STM32MPU Embedded Software Package better suits your needs#Starter_Package|Starter package]]''':  
** the flashlayout as well as the images to flash, provided within the '''IMAGES-st-image-weston-openstlinux-weston-stm32mp1.tar.xz''' file
+
** the flashlayout as well as the images to flash, provided within the '''en.FLASH-stm32mp1-openstlinux&lt;YY&gt;-&lt;MM&gt;-&lt;DD&gt;.tar.xz''' file (download it from [https://www.st.com/content/st_com/en/products/embedded-software/mcu-mpu-embedded-software/stm32-embedded-software/stm32-mpu-openstlinux-distribution/stm32mp1starter.html#get-software st.com])
 
* '''[[Which STM32MPU Embedded Software Package better suits your needs#Developer_Package|Developer package]]''':  
 
* '''[[Which STM32MPU Embedded Software Package better suits your needs#Developer_Package|Developer package]]''':  
** the component sources and patches, provided within the '''SOURCES-st-image-weston-openstlinux-weston-stm32mp1.tar.xz''' file  
+
** the component sources and patches, provided within the '''en.SOURCES-stm32mp1-openstlinux-&lt;YY&gt;-&lt;MM&gt;-&lt;DD&gt;.tar.xz''' file (download it from [https://www.st.com/content/st_com/en/products/embedded-software/mcu-mpu-embedded-software/stm32-embedded-software/stm32-mpu-openstlinux-distribution/stm32mp1dev.html#get-software st.com])
** the SDK toolchain, provided within the '''SDK-x86_64-st-image-weston-openstlinux-weston-stm32mp1.tar.xz''' file
+
** the SDK toolchain, provided within the '''en.SDK-x86_64-stm32mp1-openstlinux-&lt;YY&gt;-&lt;MM&gt;-&lt;DD&gt;.tar.xz''' file (download it from [https://www.st.com/content/st_com/en/products/embedded-software/mcu-mpu-embedded-software/stm32-embedded-software/stm32-mpu-openstlinux-distribution/stm32mp1dev.html#get-software st.com])
 
* the '''[[STM32CubeProgrammer]]''', which is the tool used to flash the images and binaries into the target.  
 
* the '''[[STM32CubeProgrammer]]''', which is the tool used to flash the images and binaries into the target.  
 
<br/>
 
<br/>
Line 44: Line 44:
 
It is recommended to organize the numerous inputs described in [[#Prerequisites]] in your environment.<br/>
 
It is recommended to organize the numerous inputs described in [[#Prerequisites]] in your environment.<br/>
 
First create a dedicated ''WORKDIR'' under your ''HOME'' folder and copy there all the inputs listed in [[#Prerequisites]]:
 
First create a dedicated ''WORKDIR'' under your ''HOME'' folder and copy there all the inputs listed in [[#Prerequisites]]:
:{{PC$}} cd
+
:{{PC$}} cd $HOME
 
:{{PC$}} mkdir WORKDIR
 
:{{PC$}} mkdir WORKDIR
 
:{{PC$}} cd WORKDIR
 
:{{PC$}} cd WORKDIR
 
:{{PC$}} export WORKDIR="$PWD"
 
:{{PC$}} export WORKDIR="$PWD"
:{{PC$}} tar --strip-components=1 -xf ''<IMAGES-st-image-weston-openstlinux-weston-stm32mp1.tar.xz>'' -C $WORKDIR/
+
:{{PC$}} tar --strip-components=1 -xf ''<FLASH-st-image-weston-openstlinux-weston-stm32mp1.tar.xz>'' -C $WORKDIR/
 
:{{PC$}} tar --strip-components=1 -xf ''<SOURCES-st-image-weston-openstlinux-weston-stm32mp1.tar.xz>'' -C $WORKDIR/
 
:{{PC$}} tar --strip-components=1 -xf ''<SOURCES-st-image-weston-openstlinux-weston-stm32mp1.tar.xz>'' -C $WORKDIR/
 
:{{PC$}} tar --strip-components=1 -xf ''<SDK-st-image-weston-openstlinux-weston-stm32mp1.tar.xz>'' -C $WORKDIR/
 
:{{PC$}} tar --strip-components=1 -xf ''<SDK-st-image-weston-openstlinux-weston-stm32mp1.tar.xz>'' -C $WORKDIR/
Line 77: Line 77:
 
=== Kernel : copy the DTS into the source code ===
 
=== Kernel : copy the DTS into the source code ===
 
:{{PC$}} pushd $WORKDIR
 
:{{PC$}} pushd $WORKDIR
:{{PC$}} cp -r MyDeviceTree_fromCubeMX/kernel kernel/kernel-sources/arch/arm/boot/dts/
+
:{{PC$}} cp -r MyDeviceTree_fromCubeMX/kernel/* kernel/kernel-sources/arch/arm/boot/dts/
 
:{{PC$}} popd
 
:{{PC$}} popd
   
Line 85: Line 85:
 
:{{PC$}} pushd $WORKDIR/kernel/kernel-sources
 
:{{PC$}} pushd $WORKDIR/kernel/kernel-sources
 
:{{PC$}} make O="$PWD/../build" multi_v7_defconfig
 
:{{PC$}} make O="$PWD/../build" multi_v7_defconfig
:{{PC$}} for f in `ls -1 ../fragment*.config`; do scripts/kconfig/merge_config.sh -m -r -O $PWD/../build $PWD/../build/.config $f; done
+
:{{PC$}} for f in `ls -1 ../../sources/arm-openstlinux_weston-linux-gnueabi/linux-stm32mp-4.19-r0/fragment*.config`; do scripts/kconfig/merge_config.sh -m -r -O $PWD/../build $PWD/../build/.config $f; done
 
:{{PC$}} make oldconfig O="$PWD/../build"
 
:{{PC$}} make oldconfig O="$PWD/../build"
:{{PC$}} make stm32mp157c-mydevicetree-mx LOADADDR=0xC2000040 O="$PWD/../build"
+
:{{PC$}} make stm32mp157c-mydevicetree-mx.dtb LOADADDR=0xC2000040 O="$PWD/../build"
 
:{{PC$}} popd
 
:{{PC$}} popd
 
:{{PC$}} ls -l $WORKDIR/kernel/build/arch/arm/boot/dts/stm32mp157c-mydevicetree-mx.dtb
 
:{{PC$}} ls -l $WORKDIR/kernel/build/arch/arm/boot/dts/stm32mp157c-mydevicetree-mx.dtb
Line 108: Line 108:
 
:{{PC$}} mv u-boot/u-boot* u-boot/u-boot-sources/
 
:{{PC$}} mv u-boot/u-boot* u-boot/u-boot-sources/
 
:{{PC$}} pushd u-boot/u-boot-sources
 
:{{PC$}} pushd u-boot/u-boot-sources
:{{PC$}} for p in $(ls -1 ../../sources/arm-openstlinux_weston-linux-gnueabi/u-boot-stm32mp-*/*.patch); do patch -p1 < $p; done
+
:{{PC$}} for p in ../../sources/arm-openstlinux_weston-linux-gnueabi/u-boot-stm32mp-*/*.patch; do patch -p1 < $p; done
 
:{{PC$}} popd
 
:{{PC$}} popd
   
Line 125: Line 125:
 
:{{PC$}} pushd $WORKDIR/u-boot/u-boot-sources
 
:{{PC$}} pushd $WORKDIR/u-boot/u-boot-sources
 
:{{PC$}} make stm32mp15_''<config>''_defconfig
 
:{{PC$}} make stm32mp15_''<config>''_defconfig
: ''<config>'' : could be trusted or basic according the boot type
+
: ''<config>'' : could be ''trusted'' or ''basic'' according the boot type
 
:{{PC$}} make DEVICE_TREE=''<device tree>'' all
 
:{{PC$}} make DEVICE_TREE=''<device tree>'' all
 
: ''<device tree>'' : is the device tree just copied, i.e.: stm32mp157c-mydevicetree-mx
 
: ''<device tree>'' : is the device tree just copied, i.e.: stm32mp157c-mydevicetree-mx
Line 149: Line 149:
 
:{{PC$}}  mv tf-a/arm-trusted-firmware-* tf-a/tf-a-sources
 
:{{PC$}}  mv tf-a/arm-trusted-firmware-* tf-a/tf-a-sources
 
:{{PC$}}  pushd tf-a/tf-a-sources
 
:{{PC$}}  pushd tf-a/tf-a-sources
:{{PC$}}  for p in $(ls -1 ../../sources/arm-openstlinux_weston-linux-gnueabi/tf-a-stm32mp-*/*.patch); do patch -p1 < $p; done
+
:{{PC$}}  for p in ../../sources/arm-openstlinux_weston-linux-gnueabi/tf-a-stm32mp-*/*.patch; do patch -p1 < $p; done
 
:{{PC$}}  popd
 
:{{PC$}}  popd
 
:{{PC$}}  popd
 
:{{PC$}}  popd
Line 155: Line 155:
 
=== TF-A : copy the DTS into the source code ===
 
=== TF-A : copy the DTS into the source code ===
 
:{{PC$}}  pushd $WORKDIR
 
:{{PC$}}  pushd $WORKDIR
:{{PC$}}  cp -r tf-a/MyDeviceTree_fromCubeMX/tf-a tf-a/tf-a-sources/fdts/
+
:{{PC$}}  cp -r MyDeviceTree_fromCubeMX/tf-a/* tf-a/tf-a-sources/fdts/
 
:{{PC$}}  popd
 
:{{PC$}}  popd
   
Line 162: Line 162:
   
 
:{{PC$}} pushd $WORKDIR/tf-a/tf-a-sources
 
:{{PC$}} pushd $WORKDIR/tf-a/tf-a-sources
:{{PC$}} make -f $PWD/../Makefile.sdk TFA_DEVICETREE=''<device tree>'' TF_A_CONFIG=''<config>'' all
+
:{{PC$}} make -f ../../sources/arm-openstlinux_weston-linux-gnueabi/tf-a-stm32mp-2.0-r0/Makefile.sdk TFA_DEVICETREE=''<device tree>'' TF_A_CONFIG=''<config>'' all
 
::''<config>'' : could be '''''trusted''''' or ''basic'' according the boot type
 
::''<config>'' : could be '''''trusted''''' or ''basic'' according the boot type
 
::''<device tree>'' : is the device tree just copied, i.e.: '''''stm32mp157c-mydevicetree-mx'''''
 
::''<device tree>'' : is the device tree just copied, i.e.: '''''stm32mp157c-mydevicetree-mx'''''

Attachments

Discussions