- Last edited one year ago ago
Hardware random overview
Contents
1 Article Purpose[edit]
This article gives information about the hardware random (HWRNG) framework.
2 Framework purpose[edit]
The Hardware random framework is integrated in the kernel. It provides access to RNG peripherals and focuses on supporting the hardware number generator.
3 System overview[edit]
The HW random framework allows retrieving random numbers in userland.
3.1 Component description[edit]
- HW random core (Kernel space)
Generic interface in kernel space. This layer is in charge of creating the character device (char device) and sysfs to access hw_random.
- RNG (Kernel space)
Hardware random Linux® drivers handling the HW blocks.
- RNG (Hardware)
HW blocks handling the RNG peripheral.
3.2 API description[edit]
The Hardware random framework uses char device API[1] ioctl operations. For additional information, refer to:
- sysfs interface.
- Kernel Documentation directory[2]
4 Configuration[edit]
4.1 Kernel configuration[edit]
The Hardware random support is activated by default in ST deliveries. No specific configuration is required apart from enabling or disabling peripheral support using Linux® Menuconfig tool. Refer to Menuconfig or how to configure kernel and select:
[*] Device Drivers ---> [*] Character devices ---> [*] Hardware Random Number Generator Core support ---> [*] STMicroelectronics STM32 random number generator
4.2 Device tree configuration[edit]
DT configuration can be done thanks to the STM32CubeMX.
A detailed device tree configuration is described in RNG device tree configuration.
5 How to use the framework[edit]
The framework provides external interfaces from userland : How to control RNG.
5.1 How to use from char device[edit]
The community tool for using Hardware random framework is rng_tools[3] which provides a complete set of utilities related to random number generators:
- rngd: runs a background daemon that opens /dev/hwrng file (default) to connect and retrieve random numbers.
- rngtest: runs different tests that check the entropy and verify the compliance regarding FIPS 140-2 standard.
5.2 How to use from sysfs[edit]
Available devices compatible with Hardware framework can be listed using sysfs commands:
cat /sys/class/misc/hw_random/rng_available stm32-rng
The selected device is shown here:
cat /sys/class/misc/hw_random/rng_current stm32-rng
To select a different device:
echo "stm32-rng"> /sys/class/misc/hw_random/rng_current
6 How to trace and debug the framework[edit]
Light information on the framework can be accessed by using sysfs.
By default, the framework does not provide any specific debug output or dynamic debugging tool.
7 Source code location[edit]
Hardware random drivers and framework are available here[4].
8 To go further[edit]
Code examples are directly available from rng-tools[3] github.