Difference between revisions of "HDP internal peripheral"
[quality revision] | [quality revision] |
m
|
m
|
Contents
1 Article purpose[edit]
The purpose of this article is to
- briefly introduce the HDP peripheral (hardware debug port) and its main features
- indicate the level of security supported by this hardware block
- explain how each instance can be allocated to the three runtime contexts and linked to the corresponding software components
- explain, when needed, how to configure the HDP peripheral.
2 Peripheral overview[edit]
The HDP peripheral is used to output some internal signals on up to 8 GPIO pins.
Follow the sequence below to connect a GPIO to an internal signal via the HDP:
- First of all, look for the internal signal you want to monitor in the HDP signal multiplexing table of the STM32MP15 reference manuals:
- Search for the HDP signal on which you can get it among eight possible choices.
- Note the corresponding HDPx multiplexing value to select.
- Then, look for the most suitable GPIO pin on which you can output HDPx in the datasheet:
The GPIO bank, pin, alternate function and HDPx multiplexing value are the information required to configure each HDP signal.
2.1 Features[edit]
Refer to STM32MP15 reference manuals for the complete list of features, and to the software components, introduced below, to know which features are really implemented.
2.2 Security support[edit]
The HDP is a non-secure peripheral.
3 Peripheral usage and associated software[edit]
3.1 Boot time[edit]
The HDP is not used at boot time.
3.2 Runtime[edit]
3.2.1 Overview[edit]
The HDP can be allocated to the Arm® Cortex®-A7 non-secure core to be used under Linux®HDP driver.
3.2.2 Software frameworks[edit]
Domain | Peripheral | Software frameworks | Comment | ||
Cortex-A7 secure (OP-TEE) |
Cortex-A7 non-secure (Linux) |
Cortex-M4 (STM32Cube) |
|||
Trace & Debug | HDP | HDP Linux driver |
3.2.3 Peripheral configuration[edit]
The configuration is applied by the firmware running in the context to which the peripheral is assigned. The configuration by itself can be performed via the STM32CubeMX tool for all internal peripherals. It can then be manually completed (especially for external peripherals) according to the information given in the corresponding software framework article.
3.2.4 Peripheral assignment[edit]
Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:
- ☐ means that the peripheral can be assigned (☑) to the given runtime context.
- ✓ is used for system peripherals that cannot be unchecked because they are statically connected in the device.
Refer to How to assign an internal peripheral to a runtime context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possiblities might be described in STM32MP15 reference manuals.
Domain | Peripheral | Runtime allocation | Comment | |||
Instance |
Cortex-A7 secure (OP-TEE) |
Cortex-A7 non-secure (Linux) |
Cortex-M4 (STM32Cube) |
|||
Trace & Debug | HDP | HDP | ☐ |
<noinclude> {{ArticleBasedOnModel| [[Contributors:Internal peripheral article model]]}} {{ArticleMainWriter|GeraldB}} {{ ArticleApprovedVersion| GeraldB | GeraldB |4Sep'18 | AnneJ - 2Aug'18 - 8314 | 15Feb'19 }} [[Category:Trace and debug peripherals]] {{ReviewsComments|JCT 1840: alignment needed with the last version of the model [[Contributors:Internal peripheral article model]]<br> [[Category:ToBeAlignedWithModel]] }}</noinclude> ==Article purpose== The purpose of this article is to * briefly introduce the '''HDP''' peripheral (hardware debug port) and its main features * indicate the level of security supported by this hardware block * explain how each instance can be allocated to the three runtime contexts and linked to the corresponding software components * explain, when needed, how to configure the HDP peripheral. ==Peripheral overview== The '''HDP''' peripheral is used to output some internal signals on up to 8 [[GPIO internal peripheral|GPIO]] pins.<br /><br /> Follow the sequence below to connect a GPIO to an internal signal via the HDP: * First of all, look for the internal signal you want to monitor in the HDP signal multiplexing table of the [[STM32MP15 resources#Reference manuals|STM32MP15 reference manuals]]: ** Search for the HDP signal on which you can get it among eight possible choices. ** Note the corresponding '''HDPx multiplexing value''' to select. * Then, look for the most suitable [[GPIO internal peripheral|GPIO]] pin on which you can output HDPx in the [[STM32MP15 resources#DS12505resources#STM32MP157Cxx datasheet|datasheet]]: ** Note the [[GPIO internal peripheral|GPIO]] '''bank''' and '''pin'''. ** Note the corresponding [[GPIO internal peripheral|GPIO]] '''alternate function''' (AF) to select. The [[GPIO internal peripheral|GPIO]] '''bank''', '''pin''', '''alternate function''' and '''HDPx multiplexing value''' are the information required to configure each HDP signal.<br /> ===Features=== Refer to [[STM32MP15 resources#Reference manuals|STM32MP15 reference manuals]] for the complete list of features, and to the software components, introduced below, to know which features are really implemented.<br> {{ReviewsComments|NSA W829 : it should be good to add here with few words what are the main features provided by this internal peripheral}} ===Security support=== The HDP is a '''non-secure''' peripheral. ==Peripheral usage and associated software== ===Boot time=== The HDP is not used at boot time. ===Runtime=== ====Overview==== The HDP can be allocated to the Arm<sup>®</sup> Cortex<sup>®</sup>-A7 non-secure core to be used under Linux<sup>®</sup> [[HDP Linux driver|HDP driver]]. ====Software frameworks==== {{:Internal_peripherals_software_table_template}} | Trace & Debug | [[HDP internal peripheral|HDP]] | | [[HDP Linux driver|HDP Linux driver]] | | |- |} ====Peripheral configuration==== The configuration is applied by the firmware running in the context to which the peripheral is assigned. The configuration by itself can be performed via the [[STM32CubeMX]] tool for all internal peripherals. It can then be manually completed (especially for external peripherals) according to the information given in the corresponding software framework article. ====Peripheral assignment==== {{:Internal_peripherals_assignment_table_template}}<onlyinclude> | rowspan="1" | Trace & Debug | rowspan="1" | [[HDP internal peripheral|HDP]] | HDP | | <span title="assignable peripheral" style="font-size:21px">☐</span> | | |-</onlyinclude> |} <noinclude> {{ArticleBasedOnModel| Internal peripheral article model}} {{PublicationRequestId | 8314 | 2018-08-02 | AnneJ}} [[Category:Trace and debug peripherals]] {{ReviewsComments|JCT 1840: alignment needed with the last version of the model [[Contributors:Internal peripheral article model]]<br> [[Category:ToBeAlignedWithModel]] }}</noinclude>
Line 1: | Line 1: | ||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
==Article purpose== |
==Article purpose== |
||
The purpose of this article is to |
The purpose of this article is to |
||
Line 25: | Line 13: | ||
** Search for the HDP signal on which you can get it among eight possible choices. |
** Search for the HDP signal on which you can get it among eight possible choices. |
||
** Note the corresponding '''HDPx multiplexing value''' to select. |
** Note the corresponding '''HDPx multiplexing value''' to select. |
||
− | * Then, look for the most suitable [[GPIO internal peripheral|GPIO]] pin on which you can output HDPx in the [[STM32MP15 resources# |
+ | * Then, look for the most suitable [[GPIO internal peripheral|GPIO]] pin on which you can output HDPx in the [[STM32MP15 resources#DS12505|datasheet]]: |
** Note the [[GPIO internal peripheral|GPIO]] '''bank''' and '''pin'''. |
** Note the [[GPIO internal peripheral|GPIO]] '''bank''' and '''pin'''. |
||
** Note the corresponding [[GPIO internal peripheral|GPIO]] '''alternate function''' (AF) to select. |
** Note the corresponding [[GPIO internal peripheral|GPIO]] '''alternate function''' (AF) to select. |
||
Line 74: | Line 62: | ||
</onlyinclude> |
</onlyinclude> |
||
|} |
|} |
||
+ | |||
+ | <noinclude> |
||
+ | {{ArticleBasedOnModel| Internal peripheral article model}} |
||
+ | {{PublicationRequestId | 8314 | 2018-08-02 | AnneJ}} |
||
+ | [[Category:Trace and debug peripherals]] |
||
+ | |||
+ | {{ReviewsComments|JCT 1840: alignment needed with the last version of the model [[Contributors:Internal peripheral article model]]<br> |
||
+ | [[Category:ToBeAlignedWithModel]] |
||
+ | }} |
||
+ | </noinclude> |