Difference between revisions of "HDP device tree configuration"

[quality revision] [pending revision]
m
m
 

1 Article purpose[edit]

This article explains how to configure the HDP driver when the peripheral is assigned to the Linux® OS.

The configuration is performed using the device tree mechanism, which provides a hardware description of the Ethernet peripheral used by STM32 HDP driver

2 DT bindings documentation[edit]

The HDP tree bindings are composed of:

  • STM32 HDP device tree bindings [1]
Info.png Please note that the upstreaming of the HDP Linux driver source code is in progress


3 DT configuration[edit]

This hardware description is a combination of the STM32 microprocessor device tree files (.dtsi extension) and board device tree files (.dts extension). See the Device tree for an explanation of the device tree file split.

STM32CubeMX can be used to generate the board device tree. Refer to How to configure the DT using STM32CubeMX for more details.

3.1 DT configuration (STM32 level)[edit]

The HDP node is described in the stm32mp151.dtsi [2] file with disabled status and required properties such as:

  • The physical base address and size of the device register map
  • The HDP clock
hdp: hdp@5002a000 {
	compatible = "st,stm32mp1-hdp";
	reg = <0x5002a000 0x400>;
	clocks = <&rcc HDP>;
	clock-names = "hdp";
	status = "disabled";
};

The required and optional properties are fully described in the bindings files.

Warning.png This device tree part is related to STM32 microprocessors. It must be kept as-is, without being modified by the end-user.

3.2 HDP DT configuration (board level)[edit]

Part of the device tree describes the HDP hardware used on a given board. The DT node ("hdp") must be filled in as follows:

  • Enable the HDP block by setting status = "okay".
  • Configure the pins in use via pinctrl, through pinctrl-0 (default pins), pinctrl-1 (sleep pins) and pinctrl-names.
  • Configure the HDP interface using muxing-hdp to indicate which one of the 16 possible output pins is assigned to each HDP output.
&hdp {
	pinctrl-names = "default", "sleep";
	pinctrl-0 = <&hdpx_pins_y>;
	pinctrl-1 = <&hdpx_pins_sleep_y>;
	status = "disabled";

	muxing-hdp = <(STM32_HDP(x, HDPx_value))>;
};

3.3 DT configuration examples[edit]

The example below shows how to configure and enable HDP instances at board level:

&hdp {
   pinctrl-names = "default", "sleep";                                    
   pinctrl-0 = <&hdp0_pins_a &hdp6_pins_a &hdp7_pins_a>;                  /* configure pinctrl for hdp pin 0, 6 and 7*/
   pinctrl-1 = <&hdp0_pins_sleep_a &hdp6_pins_sleep_a &hdp7_pins_sleep_a>;
   status = "okay";                                                       /* enable HDP */ 
   
   muxing-hdp = <(STM32_HDP(0, HDP0_GPOVAL_0) |                           /* For HDP pin 0, the signal HDP0_GPOVAL_0 is selected*/
                   STM32_HDP(6, HDP6_GPOVAL_6) |                          /* For HDP pin 6, the signal HDP0_GPOVAL_6 is selected*/
                   STM32_HDP(7, HDP7_GPOVAL_7))>;                         /* For HDP pin 7, the signal HDP0_GPOVAL_7 is selected*/
};

List of all possible HDP signals:


/* define HDP Pins number*/
HDP0_PWR_PWRWAKE_SYS
HDP0_CM4_SLEEPDEEP
HDP0_PWR_STDBY_WKUP
HDP0_PWR_ENCOMP_VDDCORE
HDP0_BSEC_OUT_SEC_NIDEN
HDP0_RCC_CM4_SLEEPDEEP
HDP0_GPU_DBG7
HDP0_DDRCTRL_LP_REQ
HDP0_PWR_DDR_RET_ENABLE_N
HDP0_GPOVAL_0

HDP1_PWR_PWRWAKE_MCU
HDP1_CM4_HALTED
HDP1_CA7_NAXIERRIRQ
HDP1_PWR_OKIN_MR
HDP1_BSEC_OUT_SEC_DBGEN
HDP1_EXTI_SYS_WAKEUP
HDP1_RCC_PWRDS_MPU
HDP1_GPU_DBG6
HDP1_DDRCTRL_DFI_CTRLUPD_REQ
HDP1_DDRCTRL_CACTIVE_DDRC_ASR
HDP1_GPOVAL_1

HDP2_PWR_PWRWAKE_MPU
HDP2_CM4_RXEV
HDP2_CA7_NPMUIRQ1
HDP2_CA7_NFIQOUT1
HDP2_BSEC_IN_RSTCORE_N
HDP2_EXTI_C2_WAKEUP
HDP2_RCC_PWRDS_MCU
HDP2_GPU_DBG5
HDP2_DDRCTRL_DFI_INIT_COMPLETE
HDP2_DDRCTRL_PERF_OP_IS_REFRESH
HDP2_DDRCTRL_GSKP_DFI_LP_REQ
HDP2_GPOVAL_2

HDP3_PWR_SEL_VTH_VDD_CORE
HDP3_CM4_TXEV
HDP3_CA7_NPMUIRQ0
HDP3_CA7_NFIQOUT0
HDP3_BSEC_OUT_SEC_DFTLOCK
HDP3_EXTI_C1_WAKEUP
HDP3_RCC_PWRDS_SYS
HDP3_GPU_DBG4
HDP3_DDRCTRL_STAT_DDRC_REG_SELREF_TYPE0
HDP3_DDRCTRL_CACTIVE_1
HDP3_GPOVAL_3

HDP4_PWR_PDDS
HDP4_CM4_SLEEPING
HDP4_CA7_NRESET1
HDP4_CA7_NIRQOUT1
HDP4_BSEC_OUT_SEC_DFTEN
HDP4_BSEC_OUT_SEC_DBGSWENABLE
HDP4_ETH_OUT_PMT_INTR_O
HDP4_GPU_DBG3
HDP4_DDRCTRL_STAT_DDRC_REG_SELREF_TYPE1
HDP4_DDRCTRL_CACTIVE_0
HDP4_GPOVAL_4

HDP5_CA7_STANDBYWFIL2
HDP5_PWR_VTH_VDDCORE_ACK
HDP5_CA7_NRESET0
HDP5_CA7_NIRQOUT0
HDP5_BSEC_IN_PWROK
HDP5_BSEC_OUT_SEC_DEVICEEN
HDP5_ETH_OUT_LPI_INTR_O
HDP5_GPU_DBG2
HDP5_DDRCTRL_CACTIVE_DDRC
HDP5_DDRCTRL_WR_CREDIT_CNT
HDP5_GPOVAL_5

HDP6_CA7_STANDBYWFI1
HDP6_CA7_STANDBYWFE1
HDP6_CA7_EVENT0
HDP6_CA7_DBGACK1
HDP6_BSEC_OUT_SEC_SPNIDEN
HDP6_ETH_OUT_MAC_SPEED_O1
HDP6_GPU_DBG1
HDP6_DDRCTRL_CSYSACK_DDRC
HDP6_DDRCTRL_LPR_CREDIT_CNT
HDP6_GPOVAL_6

HDP7_CA7_STANDBYWFI0
HDP7_CA7_STANDBYWFE0
HDP7_CA7_DBGACK0
HDP7_BSEC_OUT_FUSE_OK
HDP7_BSEC_OUT_SEC_SPIDEN
HDP7_ETH_OUT_MAC_SPEED_O0
HDP7_GPU_DBG0
HDP7_DDRCTRL_CSYSREQ_DDRC
HDP7_DDRCTRL_HPR_CREDIT_CNT
HDP7_GPOVAL_7

4 How to configure the DT using STM32CubeMX[edit]

The STM32CubeMX tool can be used to configure the STM32MPU device and get the corresponding platform configuration device tree files.
The STM32CubeMX may not support all the properties described in the above DT bindings documentation paragraph. If so, the tool inserts user sections in the generated device tree. These sections can then be edited to add some properties and they are preserved from one generation to another. Refer to STM32CubeMX user manual for further information.

5 References[edit]


== Article purpose ==
This article explains how to configure the [[HDP Linux driver|HDP driver]] when the peripheral is assigned to the Linux<sup>&reg;</sup> OS'''. 

The configuration is performed using the [[Device tree|device tree]] mechanism, which provides a hardware description of the Ethernet peripheral used by STM32 HDP driver

== DT bindings documentation ==
The ''HDP'' tree bindings are composed of:
* STM32 HDP device tree bindings <ref>{{CodeSource | Linux kernel | Documentation/devicetree/bindings/soc/stm32/stm32_hdp.txt | Documentation/devicetree/bindings/soc/stm32/stm32_hdp.txt}}</ref>

{{Info|Please note that the upstreaming of the HDP Linux driver source code is in progress}}
{{ReviewsComments|FDE W104 : remove that information}}
== DT configuration ==
This hardware description is a combination of the '''STM32 microprocessor''' device tree files (''.dtsi'' extension) and '''board''' device tree files (''.dts'' extension). See the [[Device tree]] for an explanation of the device tree file split.

'''STM32CubeMX''' can be used to generate the board device tree. Refer to [[#How_to_configure_the_DT_using_STM32CubeMX|How to configure the DT using STM32CubeMX]] for more details.

=== DT configuration (STM32 level) ===

The HDP node is described in the stm32mp151.dtsi <ref>{{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp151.dtsi | arch/arm/boot/dts/stm32mp151.dtsi}}, STM32MP151 device tree file</ref> file with disabled status and required properties such as:
* The physical base address and size of the device register map
* The HDP clock
<pre>

hdp: hdp@5002a000 {
	compatible = "st,stm32mp1-hdp";
	reg = <0x5002a000 0x400>;
	clocks = <&rcc HDP>;
	clock-names = "hdp";
	status = "disabled";
};</pre>


The required and optional properties are fully described in the [[HDP device tree configuration#DT bindings documentation|bindings files]].
{{Warning|This device tree part is related to STM32 microprocessors. It must be kept as-is, without being modified by the end-user.}}

=== HDP DT configuration (board level) ===

Part of the [[Device tree|device tree]] describes the HDP hardware used on a given board. The DT node ('''"hdp"''') must be filled in as follows:
* Enable the HDP block by setting '''status = "okay".'''
* Configure the pins in use via [[Pinctrl overview|pinctrl]], through '''pinctrl-0''' (default pins), '''pinctrl-1''' (sleep pins) and '''pinctrl-names'''.
* Configure the HDP interface using '''muxing-hdp''' to indicate which one of the 16 possible output pins is assigned to each HDP output.<pre>

&hdp {
	pinctrl-names = "default", "sleep";
	pinctrl-0 = <&hdpx_pins_y>;
	pinctrl-1 = <&hdpx_pins_sleep_y>;
	status = "disabled";

	muxing-hdp = <(STM32_HDP(x, HDPx_value))>;
};</pre>


=== DT configuration examples ===
The example below shows how to configure and enable HDP instances at board level:

 &hdp {
    pinctrl-names = "default", "sleep";                                    
    pinctrl-0 = <&hdp{{highlight|0}}_pins_a &hdp{{highlight|6}}_pins_a &hdp{{highlight|7}}_pins_a>;                  {{highlight|/* configure pinctrl for hdp pin 0, 6 and 7*/}}
    pinctrl-1 = <&hdp{{highlight|0}}_pins_sleep_a &hdp{{highlight|6}}_pins_sleep_a &hdp{{highlight|7}}_pins_sleep_a>;
    status = "okay";                                                       {{highlight|/* enable HDP */}} 

    muxing-hdp = <(STM32_HDP({{highlight|0}}, {{highlight|HDP0_GPOVAL_0}}) |                           {{highlight|/* For HDP pin 0, the signal HDP0_GPOVAL_0 is selected*/}}
                    STM32_HDP({{highlight|6}}, {{highlight|HDP6_GPOVAL_6}}) |                          {{highlight|/* For HDP pin 6, the signal HDP0_GPOVAL_6 is selected*/}}
                    STM32_HDP({{highlight|7}}, {{highlight|HDP7_GPOVAL_7}}))>;                         {{highlight|/* For HDP pin 7, the signal HDP0_GPOVAL_7 is selected*/}}
 };

List of all possible HDP signals:

 /{{ReviewsComments|FDE W104 : as the signals depend on the platform (eg diff between MP15 and MP13), it would be better to NOT list the signals but point to the file that define them (dt-bindings/soc/stm32-hdp.h)}}

 /* define HDP Pins number*/
 HDP0_PWR_PWRWAKE_SYS
 HDP0_CM4_SLEEPDEEP
 HDP0_PWR_STDBY_WKUP
 HDP0_PWR_ENCOMP_VDDCORE
 HDP0_BSEC_OUT_SEC_NIDEN
 HDP0_RCC_CM4_SLEEPDEEP
 HDP0_GPU_DBG7
 HDP0_DDRCTRL_LP_REQ
 HDP0_PWR_DDR_RET_ENABLE_N
 HDP0_GPOVAL_0

 HDP1_PWR_PWRWAKE_MCU
 HDP1_CM4_HALTED
 HDP1_CA7_NAXIERRIRQ
 HDP1_PWR_OKIN_MR
 HDP1_BSEC_OUT_SEC_DBGEN
 HDP1_EXTI_SYS_WAKEUP
 HDP1_RCC_PWRDS_MPU
 HDP1_GPU_DBG6
 HDP1_DDRCTRL_DFI_CTRLUPD_REQ
 HDP1_DDRCTRL_CACTIVE_DDRC_ASR
 HDP1_GPOVAL_1

 HDP2_PWR_PWRWAKE_MPU
 HDP2_CM4_RXEV
 HDP2_CA7_NPMUIRQ1
 HDP2_CA7_NFIQOUT1
 HDP2_BSEC_IN_RSTCORE_N
 HDP2_EXTI_C2_WAKEUP
 HDP2_RCC_PWRDS_MCU
 HDP2_GPU_DBG5
 HDP2_DDRCTRL_DFI_INIT_COMPLETE
 HDP2_DDRCTRL_PERF_OP_IS_REFRESH
 HDP2_DDRCTRL_GSKP_DFI_LP_REQ
 HDP2_GPOVAL_2

 HDP3_PWR_SEL_VTH_VDD_CORE
 HDP3_CM4_TXEV
 HDP3_CA7_NPMUIRQ0
 HDP3_CA7_NFIQOUT0
 HDP3_BSEC_OUT_SEC_DFTLOCK
 HDP3_EXTI_C1_WAKEUP
 HDP3_RCC_PWRDS_SYS
 HDP3_GPU_DBG4
 HDP3_DDRCTRL_STAT_DDRC_REG_SELREF_TYPE0
 HDP3_DDRCTRL_CACTIVE_1
 HDP3_GPOVAL_3

 HDP4_PWR_PDDS
 HDP4_CM4_SLEEPING
 HDP4_CA7_NRESET1
 HDP4_CA7_NIRQOUT1
 HDP4_BSEC_OUT_SEC_DFTEN
 HDP4_BSEC_OUT_SEC_DBGSWENABLE
 HDP4_ETH_OUT_PMT_INTR_O
 HDP4_GPU_DBG3
 HDP4_DDRCTRL_STAT_DDRC_REG_SELREF_TYPE1
 HDP4_DDRCTRL_CACTIVE_0
 HDP4_GPOVAL_4

 HDP5_CA7_STANDBYWFIL2
 HDP5_PWR_VTH_VDDCORE_ACK
 HDP5_CA7_NRESET0
 HDP5_CA7_NIRQOUT0
 HDP5_BSEC_IN_PWROK
 HDP5_BSEC_OUT_SEC_DEVICEEN
 HDP5_ETH_OUT_LPI_INTR_O
 HDP5_GPU_DBG2
 HDP5_DDRCTRL_CACTIVE_DDRC
 HDP5_DDRCTRL_WR_CREDIT_CNT
 HDP5_GPOVAL_5

 HDP6_CA7_STANDBYWFI1
 HDP6_CA7_STANDBYWFE1
 HDP6_CA7_EVENT0
 HDP6_CA7_DBGACK1
 HDP6_BSEC_OUT_SEC_SPNIDEN
 HDP6_ETH_OUT_MAC_SPEED_O1
 HDP6_GPU_DBG1
 HDP6_DDRCTRL_CSYSACK_DDRC
 HDP6_DDRCTRL_LPR_CREDIT_CNT
 HDP6_GPOVAL_6

 HDP7_CA7_STANDBYWFI0
 HDP7_CA7_STANDBYWFE0
 HDP7_CA7_DBGACK0
 HDP7_BSEC_OUT_FUSE_OK
 HDP7_BSEC_OUT_SEC_SPIDEN
 HDP7_ETH_OUT_MAC_SPEED_O0
 HDP7_GPU_DBG0
 HDP7_DDRCTRL_CSYSREQ_DDRC
 HDP7_DDRCTRL_HPR_CREDIT_CNT
 HDP7_GPOVAL_7

== How to configure the DT using STM32CubeMX ==
The [[STM32CubeMX]] tool can be used to configure the STM32MPU device and get the corresponding [[Device_tree#STM32|platform configuration device tree]] files.<br />

The STM32CubeMX may not support all the properties described in the above [[#DT bindings documentation|DT bindings documentation]] paragraph. If so, the tool inserts '''user sections''' in the generated device tree. These sections can then be edited to add some properties and they are preserved from one generation to another. Refer to [[STM32CubeMX]] user manual for further information.

==References==<references />

<noinclude>

[[Category:Device tree configuration]]
[[Category:Embedded trace and debug]]
{{PublicationRequestId | 10413 | 2019-01-24 | PhilipS}}
{{ArticleBasedOnModel |Peripheral or framework device tree configuration model}}</noinclude>
Line 8: Line 8:
 
* STM32 HDP device tree bindings <ref>{{CodeSource | Linux kernel | Documentation/devicetree/bindings/soc/stm32/stm32_hdp.txt | Documentation/devicetree/bindings/soc/stm32/stm32_hdp.txt}}</ref>
 
* STM32 HDP device tree bindings <ref>{{CodeSource | Linux kernel | Documentation/devicetree/bindings/soc/stm32/stm32_hdp.txt | Documentation/devicetree/bindings/soc/stm32/stm32_hdp.txt}}</ref>
 
{{Info|Please note that the upstreaming of the HDP Linux driver source code is in progress}}
 
{{Info|Please note that the upstreaming of the HDP Linux driver source code is in progress}}
  +
{{ReviewsComments|FDE W104 : remove that information}}
   
 
== DT configuration ==
 
== DT configuration ==
Line 65: Line 66:
   
 
List of all possible HDP signals:
 
List of all possible HDP signals:
  +
{{ReviewsComments|FDE W104 : as the signals depend on the platform (eg diff between MP15 and MP13), it would be better to NOT list the signals but point to the file that define them (dt-bindings/soc/stm32-hdp.h)}}
   
 
  /* define HDP Pins number*/
 
  /* define HDP Pins number*/