Difference between revisions of "HASH device tree configuration"

[quality revision] [quality revision]
m (Cleanup)
m
 

1 Article purpose[edit]

This article explains how to configure the HASH internal peripheral when it is assigned to the Linux® OS. In that case, it is controlled by the Crypto framework.

The configuration is performed using the device tree mechanism that provides a hardware description of the HASH peripheral, used by the STM32 HASH Linux driver.

If the peripheral is assigned to another execution context, refer to How to assign an internal peripheral to a runtime context article for guidelines on peripheral assignment and configuration.

2 DT bindings documentation[edit]

The HASH is represented by the STM32 HASH device tree bindings[1]

3 DT configuration[edit]

This hardware description is a combination of the STM32 microprocessor device tree files (.dtsi extension) and board device tree files (.dts extension). See the Device tree for an explanation of the device tree file split.

STM32CubeMX can be used to generate the board device tree. Refer to How to configure the DT using STM32CubeMX for more details.

3.1 DT configuration (STM32 level)[edit]

The HASH node is declared in stm32mp157cstm32mp151.dtsi[2]. It describes the hardware register address, clock, interrupt, reset and dma.

 hash1: hash@54002000 {                                                         Comments
 	compatible = "st,stm32f756-hash";
 	reg = <0x54002000 0x400>;                                               --> Register location and length
 	interrupts = <GIC_SPI 80 IRQ_TYPE_LEVEL_HIGH>;                          --> The interrupt number used
 	clocks = <&rcc scmi0_clk CK_SCMI0_HASH1>;
 	resets = <&rccscmi0_reset HASH1RST_R>SCMI0_HASH1>;
 	dmas = <&mdma1 31 0x10 0x1000A02 0x0 0x0 0x0>;                          --> DMA specifiers[3]
 	dma-names = "in";
 	dma-maxburst = <2>;
 	status = "disabled";
 };
Warning.png This device tree part is related to STM32 microprocessors. It must be kept as is, without being modified by the end-user.

3.2 DT configuration (board level)[edit]

This part is used to enable the HASH used on a board which is done by setting the status property to okay.

3.3 DT configuration examples[edit]

&hash1 {
	status = "okay";
};

4 How to configure the DT using STM32CubeMX[edit]

The STM32CubeMX tool can be used to configure the STM32MPU device and get the corresponding platform configuration device tree files.
The STM32CubeMX may not support all the properties described in the above DT bindings documentation paragraph. If so, the tool inserts user sections in the generated device tree. These sections can then be edited to add some properties and they are preserved from one generation to another. Refer to STM32CubeMX user manual for further information.

5 References[edit]

Please refer to the following links for additional information:



== Article purpose ==
This article explains how to configure the [[HASH internal peripheral|'''HASH''' internal peripheral]] when it is assigned to the Linux<sup>&reg;</sup> OS. In that case, it is controlled by the [[Crypto API overview|Crypto framework]].

The configuration is performed using the [[Device tree|device tree]] mechanism that provides a hardware description of the HASH peripheral, used by the STM32 HASH Linux driver.
If the peripheral is assigned to another execution context, refer to [[How to assign an internal peripheral to a runtime context]] article for guidelines on peripheral assignment and configuration.
== DT bindings documentation ==
The [[HASH internal peripheral|HASH]] is represented by the STM32 HASH device tree bindings<ref>{{CodeSource | Linux kernel | Documentation/devicetree/bindings/crypto/st,stm32-hash.txt | Device tree bindings}}</ref>


== DT configuration ==
This hardware description is a combination of the '''STM32 microprocessor''' device tree files (''.dtsi'' extension) and '''board''' device tree files (''.dts'' extension). See the [[Device tree]] for an explanation of the device tree file split.

'''STM32CubeMX''' can be used to generate the board device tree. Refer to [[#How_to_configure_the_DT_using_STM32CubeMX|How to configure the DT using STM32CubeMX]] for more details.

===DT configuration (STM32 level) ===
The HASH node is declared in stm32mp157cstm32mp151.dtsi<ref name="stm32mp157cstm32mp151_dtsi">{{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp157cstm32mp151.dtsi | STM32MP157CSTM32MP151 device tree file}}</ref>. It describes the hardware register address, clock, interrupt, reset and dma.

  hash1: hash@54002000 {                                                        {{highlight| Comments}}
  	compatible = "st,stm32f756-hash";
  	reg = <0x54002000 0x400>;                                               {{highlight|--> Register location and length}}
  	interrupts = <GIC_SPI 80 IRQ_TYPE_LEVEL_HIGH>;                          {{highlight|--> The interrupt number used}}
  	clocks = <&rcc HASH1><&scmi0_clk CK_SCMI0_HASH1>;
  	resets = <&rcc HASH1_R><&scmi0_reset RST_SCMI0_HASH1>;
  	dmas = <&mdma1 31 0x10 0x1000A02 0x0 0x0 0x0>;                          {{highlight|--> DMA specifiers<ref>{{CodeSource | Linux kernel | Documentation/devicetree/bindings/dma/stm32-mdma.txt | Documentation/devicetree/bindings/dma/stm32-mdma.txt}}, STM32 MDMA controller</ref>}}
  	dma-names = "in";
  	dma-maxburst = <2>;
  	status = "disabled";
  };
{{Warning|This device tree part is related to STM32 microprocessors. It must be kept as is, without being modified by the end-user.}}

=== DT configuration (board level) ===
This part is used to enable the HASH used on a board which is done by setting the '''status''' property to '''okay'''.

=== DT configuration examples ===
 &hash1 {
 	status = "okay";
 };

==How to configure the DT using STM32CubeMX==
The [[STM32CubeMX]] tool can be used to configure the STM32MPU device and get the corresponding [[Device_tree#STM32|platform configuration device tree]] files.<br />

The STM32CubeMX may not support all the properties described in the above [[#DT bindings documentation|DT bindings documentation]] paragraph. If so, the tool inserts '''user sections''' in the generated device tree. These sections can then be edited to add some properties and they are preserved from one generation to another. Refer to [[STM32CubeMX]] user manual for further information.

==References==
Please refer to the following links for additional information:
<references />

<noinclude>

{{ArticleBasedOnModel|[[Peripheral or framework device tree configuration model]]}}
{{PublicationRequestId | 8898 | 2018-10-08 | AlainF}}
[[Category:Device tree configuration]]
[[Category:Crypto]]</noinclude>
(2 intermediate revisions by 2 users not shown)
Line 3: Line 3:
   
 
The configuration is performed using the [[Device tree|device tree]] mechanism that provides a hardware description of the HASH peripheral, used by the STM32 HASH Linux driver.
 
The configuration is performed using the [[Device tree|device tree]] mechanism that provides a hardware description of the HASH peripheral, used by the STM32 HASH Linux driver.
  +
  +
If the peripheral is assigned to another execution context, refer to [[How to assign an internal peripheral to a runtime context]] article for guidelines on peripheral assignment and configuration.
   
 
== DT bindings documentation ==
 
== DT bindings documentation ==
Line 13: Line 15:
   
 
===DT configuration (STM32 level) ===
 
===DT configuration (STM32 level) ===
The HASH node is declared in stm32mp157c.dtsi<ref name="stm32mp157c_dtsi">{{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp157c.dtsi | STM32MP157C device tree file}}</ref>. It describes the hardware register address, clock, interrupt, reset and dma.
+
The HASH node is declared in stm32mp151.dtsi<ref name="stm32mp151_dtsi">{{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp151.dtsi | STM32MP151 device tree file}}</ref>. It describes the hardware register address, clock, interrupt, reset and dma.
   
 
   hash1: hash@54002000 {                                                        {{highlight| Comments}}
 
   hash1: hash@54002000 {                                                        {{highlight| Comments}}
Line 19: Line 21:
 
   reg = <0x54002000 0x400>;                                              {{highlight|--> Register location and length}}
 
   reg = <0x54002000 0x400>;                                              {{highlight|--> Register location and length}}
 
   interrupts = <GIC_SPI 80 IRQ_TYPE_LEVEL_HIGH>;                          {{highlight|--> The interrupt number used}}
 
   interrupts = <GIC_SPI 80 IRQ_TYPE_LEVEL_HIGH>;                          {{highlight|--> The interrupt number used}}
   clocks = <&rcc HASH1>;
+
   clocks = <&scmi0_clk CK_SCMI0_HASH1>;
   resets = <&rcc HASH1_R>;
+
   resets = <&scmi0_reset RST_SCMI0_HASH1>;
 
   dmas = <&mdma1 31 0x10 0x1000A02 0x0 0x0 0x0>;                          {{highlight|--> DMA specifiers<ref>{{CodeSource | Linux kernel | Documentation/devicetree/bindings/dma/stm32-mdma.txt | Documentation/devicetree/bindings/dma/stm32-mdma.txt}}, STM32 MDMA controller</ref>}}
 
   dmas = <&mdma1 31 0x10 0x1000A02 0x0 0x0 0x0>;                          {{highlight|--> DMA specifiers<ref>{{CodeSource | Linux kernel | Documentation/devicetree/bindings/dma/stm32-mdma.txt | Documentation/devicetree/bindings/dma/stm32-mdma.txt}}, STM32 MDMA controller</ref>}}
 
   dma-names = "in";
 
   dma-names = "in";
Line 42: Line 44:
 
==References==
 
==References==
 
Please refer to the following links for additional information:
 
Please refer to the following links for additional information:
 
 
<references />
 
<references />
   
 
<noinclude>
 
<noinclude>
{{ArticleBasedOnModel|[[Peripheral or framework device tree configuration model]]}}
+
{{ArticleBasedOnModel|Peripheral or framework device tree configuration model}}
 
{{PublicationRequestId | 8898 | 2018-10-08 | AlainF}}
 
{{PublicationRequestId | 8898 | 2018-10-08 | AlainF}}
 
[[Category:Device tree configuration]]
 
[[Category:Device tree configuration]]
 
[[Category:Crypto]]
 
[[Category:Crypto]]
 
</noinclude>
 
</noinclude>