Difference between revisions of "Gst-play"
[unchecked revision] | [quality revision] |
m (→Usage)
|
m (→Usage)
|
Applicable for | STM32MP13x lines, STM32MP15x lines |
Contents
1 Overview[edit]
gst-play (gst-play-1.0) is a GStreamer command line utility available with GStreamer-1.X.
This utility plays multimedia content using the Playbin element as a basic player. It takes as an input either individual files, URLs or a whole directories (in this case it will recurse into sub-directories as well).
2 Usage[edit]
gst-play accepts the following options:
gst-play-1.0 --help
Usage: gst-play-1.0 [OPTION?] FILE1|URI1 [FILE2|URI2] [FILE3|URI3] ... Help Options: -h, --help Show help options --help-all Show all help options --help-gst Show GStreamer Options Application Options: -v, --verbose Output status information and property notifications --flags Control playback behaviour setting playbin 'flags' property --version Print version information and exit --videosink Video sink to use (default is autovideosink) --audiosink Audio sink to use (default is autoaudiosink) --gapless Enable gapless playback --shuffle Shuffle playlist --no-interactive Disable interactive control via the keyboard --volume Volume --playlist Playlist file containing input media files -q, --quiet Do not print any output (apart from errors)
The user can control the playback through the host terminal keyboard. Press k to list the available keyboard shortcuts once the content is playing:
<space> Pause/Resume playback <up/down arrows> Volume up/down <left/right arrows> Seek back/forward +/- Increase/decrease playback rate d Reverse playback direction t Cycle through trick modes a Switch audio track s Switch subtitle track v Switch video track > Skip to next item in playlist < Go back to previous item in playlist q, ESC Quit
Information provided by gst-play Ubuntu manual
3 Examples[edit]
![]() |
Don't have /usr/local/demo/media/ST2297_visionv3.webm ? Follow instructions in this article. |
![]() |
To hear audio track, depending on the considered board, an audio headset must be plugged on |
3.1 Basic audio/video playback[edit]
gst-play-1.0 /usr/local/demo/media/ST2297_visionv3.webm
3.2 Video only playback[edit]
gst-play-1.0 /usr/local/demo/media/ST2297_visionv3.webm --audiosink=fakesink
Audio rendering is disabled, but audio decoding continues.
3.3 Playlist playback[edit]
gst-play-1.0 /usr/local/demo/media/ST2297_visionv3.webm /usr/local/demo/media/ST2297_visionv3.webm /usr/local/demo/media/ST2297_visionv3.webm /usr/local/demo/media/ST2297_visionv3.webm
Press ">" key to play the next file, "<" key to play the previous one.
3.4 Loop or repeat the same video[edit]
This option is not currently available within gst-play but here are some alternatives:
- Playlist with the same video over and over. In the example below, the same video file is played 3 times. The video file can be added as many times as needed:
gst-play-1.0 /usr/local/demo/media/ST2297_visionv3.webm /usr/local/demo/media/ST2297_visionv3.webm /usr/local/demo/media/ST2297_visionv3.webm
- For loop (here 1000 times):
for i in `seq 1 1000`;do gst-play-1.0 /usr/local/demo/media/ST2297_visionv3.webm; done
3.5 Seek while playing[edit]
gst-play-1.0 /usr/local/demo/media/ST2297_visionv3.webm /usr/local/demo/media/ST2297_visionv3.webm /usr/local/demo/media/ST2297_visionv3.webm /usr/local/demo/media/ST2297_visionv3.webm
Press "right arrow key" to seek forward, "left arrow key" to seek backward.
3.6 Change playback speed[edit]
gst-play-1.0 /usr/local/demo/media/ST2297_visionv3.webm
Press "+" key to increase rate and "-" key to decreased it.
3.7 HTTP streaming[edit]
![]() |
An internet connection is required, for example by plugging an Ethernet cable on |
gst-play-1.0 https://github.com/STMicroelectronics/meta-st-openstlinux/blob/thud/recipes-samples/demo/demo-launcher/media/ST2297_visionv3.webm?raw=true
3.8 Audio/video playback on HDMI TV[edit]
![]() |
Plug first HDMI TV cable as described in How to display on HDMI article |
Switch audio output on HDMI:
pacmd set-card-profile 0 output:hdmi-stereo
Than play the video:
gst-play-1.0 /usr/local/demo/media/ST2297_visionv3.webm
3.9 Audio/video playback in background[edit]
Option --no-interactive must be set in order to be able to play in background:
gst-play-1.0 /usr/local/demo/media/ST2297_visionv3.webm --no-interactive &
[1] 14998
root@stm32mp1:~# Now playing /av_h264_main_640x480_30fps_1000kbps_aac-lc_192kbps.mp4
Then to stop playback:
killall gst-play-1.0
or
fg <CTRL+C>
<noinclude>{{ApplicableFor |MPUs list=STM32MP13x, STM32MP15x |MPUs checklist=STM32MP13x,STM32MP15x }}</noinclude> == Overview == {{highlight|'''gst-play'''}} (gst-play-1.0) is a GStreamer command line utility available with GStreamer-1.X. This utility plays multimedia content using the Playbin element as a basic player. It takes as an input either individual files, URLs or a whole directories (in this case it will recurse into sub-directories as well). == Usage == gst-play accepts the following options: {{Board$}} gst-play-1.0 --help<pre> Usage: gst-play-1.0 [OPTION?] FILE1|URI1 [FILE2|URI2] [FILE3|URI3] ... Help Options: -h, --help Show help options --help-all Show all help options --help-gst Show GStreamer Options Application Options: -v, --verbose Output status information and property notifications --flags Control playback behaviour setting playbin 'flags' property --version Print version information and exit --videosink Video sink to use (default is autovideosink) --audiosink Audio sink to use (default is autoaudiosink) --gapless Enable gapless playback --shuffle Shuffle playlist --no-interactive Disable interactive control via the keyboard --volume Volume --playlist Playlist file containing input media files -q, --quiet Do not print any output (apart from errors)</pre> The user can control the playback through the host terminal keyboard. Press {{highlight|'''k'''}} to list the available keyboard shortcuts once the content is playing:<pre> <space> Pause/Resume playback <up/down arrows> Volume up/down <left/right arrows> Seek back/forward +/- Increase/decrease playback rate d Reverse playback direction t Cycle through trick modes a Switch audio track s Switch subtitle track v Switch video track > Skip to next item in playlist < Go back to previous item in playlist q, ESC Quit</pre> Information provided by [http://manpages.ubuntu.com/manpages/latest/man1/gst-play-1.0.1.html gst-play Ubuntu manual] {{Warning | If Weston is configured with a "weston" user instead of a "root" user, please use the following commands: {{Board$}} su -l "weston" -c "your_weston_command" {{Board$}} su -l "weston" -c "gst-play-1.0 --help"..." {{Board$}} su -l "weston" -c "pacmd ..."}} == Examples == {{Info|Don't have ''{{av_ref_file}}'' ? Follow instructions in [[Template:Av_ref_file#Download_this_file|this article]].}} {{Info|To hear audio track, depending on the considered board, an audio headset must be plugged on * the [[STM32MP157x-EV1 - hardware description#MB1262-CN5|STM32MP157x-EV1 Evaluation board CN5 jack connector]] * the [[STM32MP157x-DKx - hardware description#MB1272-CN10|STM32MP157x-DKx Discovery kit CN10 jack connector]] }}{{UpdateNeededForNewBoard|Point to the jack connector (if any) of the new board}} === Basic audio/video playback === {{Board$}} gst-play-1.0 {{av_ref_file}} === Video only playback === {{Board$}} gst-play-1.0 {{av_ref_file}} --audiosink=fakesink Audio rendering is disabled, but audio decoding continues. === Playlist playback === {{Board$}} gst-play-1.0 {{av_ref_file}} {{av_ref_file}} {{av_ref_file}} {{av_ref_file}} Press {{highlight|'''">" key'''}} to play the next file, {{highlight|'''"<" key'''}} to play the previous one. === Loop or repeat the same video === This option is not currently available within gst-play but here are some alternatives: * Playlist with the same video over and over. In the example below, the same video file is played 3 times. The video file can be added as many times as needed: {{Board$}} gst-play-1.0 {{av_ref_file}} {{av_ref_file}} {{av_ref_file}} * For loop (here 1000 times): {{Board$}} for i in `seq 1 1000`;do gst-play-1.0 {{av_ref_file}}; done === Seek while playing === {{Board$}} gst-play-1.0 {{av_ref_file}} {{av_ref_file}} {{av_ref_file}} {{av_ref_file}} Press {{highlight|'''"right arrow key"'''}} to seek forward, {{highlight|'''"left arrow key"'''}} to seek backward. === Change playback speed === {{Board$}} gst-play-1.0 {{av_ref_file}} Press {{highlight|'''"+" key'''}} to increase rate and {{highlight|'''"-" key'''}} to decreased it. === HTTP streaming === {{Info|An internet connection is required, for example by plugging an Ethernet cable on * the [[STM32MP157x-EV1 - hardware description#MB1262-CN3|STM32MP157x-EV1 Evaluation board CN3 Ethernet connector]] * the [[STM32MP157x-DKx - hardware_description#MB1272-CN8|STM32MP157x-DKx Discovery kit CN8 Ethernet connector]] }}{{UpdateNeededForNewBoard|Point to the Ethernet connector (if any) of the new board}} {{InternalInfo| When connected on ST internal network, http requests must be redirected to appgw.gnb.st.com ST proxy using command: {{Board$}} export http_proxy{{=}}<nowiki>http://</nowiki><login>:<pwd>@10.129.92.5:8080 See [[How to avoid proxy issues]] article for more details. Then you can play the video: }} {{Board$}} gst-play-1.0 {{av_ref_http}} === Audio/video playback on HDMI TV === {{Info|Plug first HDMI TV cable as described in [[How to display on HDMI]] article}} {{UpdateNeededForNewBoard|Point to the HDMI connector (if any) of the new board}} Switch audio output on HDMI: {{Board$}} pacmd set-card-profile 0 output:hdmi-stereo Than play the video: {{Board$}} gst-play-1.0 {{av_ref_file}} === Audio/video playback in background === Option {{highlight|'''--no-interactive'''}} must be set in order to be able to play in background: {{Board$}} gst-play-1.0 {{av_ref_file}} {{highlight|'''--no-interactive'''}} & [1] 14998 root@stm32mp1:~# Now playing /av_h264_main_640x480_30fps_1000kbps_aac-lc_192kbps.mp4 Then to stop playback: {{Board$}} killall gst-play-1.0 or {{Board$}} fg<CTRL+C> <noinclude> {{PublicationRequestId| 7660 | 2018-06-11 | BrunoB}} [[Category:GStreamer]]</noinclude>
Line 66: | Line 66: | ||
{{Warning | If Weston is configured with a "weston" user instead of a "root" user, please use the following commands: |
{{Warning | If Weston is configured with a "weston" user instead of a "root" user, please use the following commands: |
||
{{Board$}} su -l "weston" -c "your_weston_command" |
{{Board$}} su -l "weston" -c "your_weston_command" |
||
− | {{Board$}} su -l "weston" -c "gst-play-1.0 -- |
+ | {{Board$}} su -l "weston" -c "gst-play-1.0 ..."
|
+ |
{{Board$}} su -l "weston" -c "pacmd ..." |
||
}} |
}} |
||