Difference between revisions of "Glossary"

[quality revision] [quality revision]
m
m (M)
 




Jump to letter: A B C D E F G H I J K L M N O P Q R S T U V W X Y Z 0-9 See Also


Note: The glossary content is automatically used in all wiki pages.


1 A[edit]

A2DP
Advanced audio distribution profile
ABI
Application binary interface. ( In computer software, an application binary interface (ABI) describes the low-level interface between a computer program and the operating system or another program.)
ACL
Automatic current limit (LCD power improvement solution)
ADB
Android debug bridge (Android specific)
ADBD
Android debug bridge daemon (Android specific)
ADC
Analog-to-digital converter. The process of converting a sampled analog signal to a digital code that represents the amplitude of the original signal sample.
AES
Advanced encryption standard
AF
GPIO alternate function
AHB
Advanced high-performance bus
AI
Artificial intelligence
AIDL
Android interface definition language (see https://developer.android.com/guide/components/aidl)
aka
also known as
ALSA
Advanced Linux sound architecture
AOSP
Android open source project
APB
Advanced peripheral bus
API
Application programming interface
APT
Advanced package tool (see https://wiki.debian.org/Apt)
Arm® 
Arm® is a registered trademark of Arm Limited (or its subsidiaries) in the US and/or elsewhere. Arm logo.png
Arm
Arm® is a registered trademark of Arm Limited (or its subsidiaries) in the US and/or elsewhere. Arm logo.png
ARP
Protocol used by the internet protocol, specifically IPv4, to map IP network addresses to the hardware addresses used by a data link protocol (https://en.wikipedia.org/wiki/Address_Resolution_Protocol)
ART
Android runtime (see https://source.android.com/devices/tech/dalvik)
ASoC
ALSA system on chip
AVB
Audio video bridging over Ethernet (set of IEEE standards for transporting audio and other real-time content over Ethernet)
AVD
Analog voltage detector

2 B[edit]

BCC
BPF compiler collection
BL1
Boot loader stage 1
BL2
Boot loader stage 2
BL32
Boot loader stage 3-2
BL33
Boot loader stage 3-3
BLE
Bluetooth low energy. Bluetooth LE, marketed as Bluetooth Smart is a wireless personal area network technology designed and marketed by the Bluetooth Special Interest Group aimed at novel applications in the healthcare, fitness, beacons, security, and home entertainment industries.
Compared to Classic Bluetooth, Bluetooth Smart is intended to provide considerably reduced power consumption and cost while maintaining a similar communication range. (sourcehttps://en.wikipedia.org/wiki/Bluetooth_Low_Energy)
BoardId
eval, disco (Generic term used, to complete configuration modules paths depending on used board)
BOR
Brownout reset
BSP
Board support package
BSEC
Boot and Security and OTP control
BT
BlueTooth

3 C[edit]

CABC
Content-adaptative backlight control (LCD power improvement solution)
CAB
Content-adaptative backlight (LCD power improvement solution)
CAN
Controller area network (robust bus mainly used for automotive applications)
CEC
Consumer electronics control (HDMI standard)
CLUT
Colour look-up table
CMSIS
Cortex microcontroller software interface standard
CNN
Convolutional neural network
configfs
Configuration file system (see https://en.wikipedia.org/wiki/Configfs for more details)
Cortex
Cortex®
CoT
Chain of trust
CPL
Common public license
CPU
Central processing unit
CRC
Cyclic redundancy check calculation unit
CRYP
Cryptographic processor
CSG
Constructive solid geometry
CSI
Multi Speed Internal oscillator (STM32 clock source)
CSS
Cascading style sheets (web standard)
CTS
Compatibility test suite (Android specific) or clear to send (in UART context)
CV
Computer vision

4 D[edit]

DAC
Digital-to-analog converter (Electronic circuit that converts a binary number into a continuously varying value.)
DAI
Digital audio interface
DAPM
Dynamic audio power management
DBI
Display bus interface (MIPI® Alliance standard)
DCMI
Digital Camera memory interface
DCMIPP
Digital Camera memory interface pixel processor
DDB
Device descriptor block (MIPI® Alliance standard)
DDC
Display data channel (VESA standard)
DDR
Doubledata rate (memory domain)
debugfs
Debug file system (see https://en.wikipedia.org/wiki/Debugfs for more details)
devfs
Device file system (see https://en.wikipedia.org/wiki/Device_file#DEVFS for more details)
DES
Data encryption standard
DFSDM
Digital filter for sigma-delta modulator
DFT
Techniques implemented during semiconductor development to improve device testability (Scan, BIST…).
DFU
Device firmware upgrade
DHCP
Dynamic host configuration pProtocol (see https://en.wikipedia.org/wiki/Dynamic_Host_Configuration_Protocol for more details)
DISCO
Discovery kit
DMA
Direct memory access
DMA2D
Chrom-art accelerator™ controller (STM32 specific)
DMIC
Digital microphone
DPA
Differential power analysis
DPI
Display pixel interface (MIPI® Alliance standard)
DRD
Dual-role device (USB standard defines host and device roles. OTG controllers support both roles and can be called Dual-role devices controllers.)
DRI
Direct rendering infrastructure (Linux® framework for allowing direct access to graphics hardware... find more information on official DRI web site http://dri.freedesktop.org/wiki/FrontPage)
DRM
Direct rendering manager (kernel module that gives direct hardware access to DRI clients, find more information on official DRI web site http://dri.freedesktop.org/wiki/DRM)
DRP
Dual role port, an USB port that can operate in host or device mode
DSI
Display serial interface (MIPI® Alliance standard)
DT
Device tree
DTB
Device tree binary (or Blob)
DTS
Device tree source (in software context) or digital temperature sensor (in peripheral context)
DVI
Digital visual interface (digital display working group)
DVFS
Dynamic voltage and frequency scaling

5 E[edit]

EAL
Evaluation assurance level
ECC
Error correction capability
ECC
Elliptic curve cryptography
ECDSA
Elliptic curve digital signature algorithm
EDID
Extended Display identification data (HDMI standard)
EDMK
Encryption Decryption master key, used for secure boot - NEW
EDP
Embedded Display port (VESA standard). See http://www.displayport.org/ for more details
EEPROM
Electrically-erasable programmable read-only memory
EGL
Khronos native platform graphics interface (See http://www.khronos.org/egl/ for more details)
EHCI
Enhanced host controller interface
ELF
Executable and linkable file
EMI
External memory interface
eMMC
Former spelling for e•MMC ('e' in italic)
e•MMC
Embedded uulti-media card
EOT
End of transmission (MIPI® Alliance DSI standard)
eSDK
Extensible software development kit
ETH
Ethernet
ETM
Embedded trace macrocell
ETZPC
Extended trustzone protection controller
EVAL
Evaluation board
EXTI
External interrupt

6 F[edit]

FB
Frame buffer (could be the Kernel framebuffer linked to the display, a GPU framebuffer, an imaging framebuffer...)
FCONF
Firmware configuration framework used by TF-A - NEW
FHS
File hierarchy standard defines by Linux® Foundation
FIP
Firmware image package is a packaging format used by TF-A
FIT
Flattened image tree is a packaging format used by U-Boot
Flash
Flash memory shortened to gain space in titles, tables and block diagrams
Flash memory 
Flash memories combine high density and cost effectiveness of EPROMs with the electrical erasability of EEPROMs. For this reason, the Flash memory market is one of the most exciting areas of the semiconductor industry today and new applications requiring in system reprogramming, such as cellular telephones, automotive engine management systems, hard disk drives, PC BIOS software for Plug & Play, digital TV, set top boxes, fax and other modems, PC cards and multimedia CD-ROMs, offer the prospect of very high volume demand.
foo_driver
foo_driver could be any driver that needs to control a GPIO
FPS
Frames per second
fs
File system or filesystem, method and data structure that the operating system uses to control how data is stored and retrieved - NEW
FS
File system or filesystem, method and data structure that the operating system uses to control how data is stored and retrieved -NEW
FSBL
First stage boot loader
FTR
First time right

7 G[edit]

GDB
GNU dedugger, a portable debugger that runs on many Unix-like systems
GIC
Generic interrupt controller
GP
Geometry processor, used to execute Vertex Shaders (3D IP/IC specific).
GPIO
General-purpose input/output (A realization of open ended transmission between devices on an embedded level. These pins available on a processor can be programmed to be used to either accept input or provide output to external devices depending on user desires and applications requirements.)
GPGPU
General-purpose computation on graphics processing units
GPT
GUID partition table
GPU
Graphics processing units
GRALLOC
Graphic allocation HAL or library (Android specific)
GUI
Graphical user interface

8 H[edit]

HAL
Hardware abstraction layer
HDCP
High-bandwidth digital content protection (HDMI standard)
HDMI
High-definition multimedia interface (HDMI standard)
HDP
Hardware debug port
HDR
High dynamic range (HDMI standard)
HID
Human interface device (for USB, Bluetooth...)
HIDL
HAL interface definition language (see https://source.android.com/devices/architecture/hidl)
HMAC
Hash-based Message authentication code
HPD
Hot plug detect
HS
High speed (MIPI® alliance DSI standard)
HSEM 
Hardware semaphore
HSE
High speed external oscillator (STM32 clock source)
HSI
High speed internal oscillator (STM32 clock source) or High speed synchronous serial interface (MIPI® Alliance standard)
HSLV
High speed low voltage pin mode
HSM
Hardware security module

9 I[edit]

I2C
Inter-integrated circuit (Bi-directional 2-wire bus standard for efficient inter-IC control.)
I2S
Integrated interchip sound

I2S (without the 2 in superscript) refers to the STMicroelectronics integrated interchip sound IP.

I420
fourcc of YUV420 planar pixel format
IDE
(Software)Integrated development/design/debugging environment
IFP
Image formatting pipeline
IIC
Inter-integrated circuit (Bi-directional 2-wire bus standard for efficient inter-IC control.)
IIO
Industrial I/O Linux® subsystem
initramfs
Initial ramdisk (https://en.wikipedia.org/wiki/Initial_ramdisk)
initrd
Initial ramdisk (https://en.wikipedia.org/wiki/Initial_ramdisk)
IMU
Inertial measurement unit
IO
input/output
IoT
Internet of things
IPC
Inter-processor communication
IPCC
Inter-processor communication controller
IPP
Image preprocessor pipeline
ITM
Instruction trace Macrocell
IWDG 
Independent watchdog

10 J[edit]

JIT
Just-In-Time (Way of working for a given Virtual Machine)
JNI
Java Native Interface (for Android)
JTAG
debug and test protocol, named from the Joint Test Action Group that developed it

11 K[edit]

KMS
Kernel Mode Setting


12 L[edit]

LBA
Logical block addressing
LDISC
Line discipline
LED
Light-emitting diode
LIN
Local interconnect network
Linux
Linux® is a registered trademark of Linus Torvalds.
LDO
Low-dropout regulator
LL
Low layer of STM32Cube
LP
Low power (MIPI® Alliance DSI standard)
LTDC
LCD TFT display controller (STM32 specific)
LPTIM 
Low-power timer (STM32 specific)
LSE
Low speed external oscillator (STM32 clock source)
LSI
Low speed internal oscillator (STM32 clock source)

13 M[edit]

MAC address
media access control address (https://en.wikipedia.org/wiki/MAC_address)
MCU
Microcontroller unit (MCUs have internal flash memory and are intended to operate with a minimum amount of external support ICs. They commonly are a self-contained, system-on-chip (SoC) designs.)
MD5
Message digest 5
MDK
Microcontroller Development Kit from Keil® (see https://www2.keil.com/mdk5)
MFD
Multifunction device
microSDTM;
eg microSD card ('m' in lowcase whatever its position)
Micro-AB
Micro-AB connector/port ('M' in uppercase whatever its position)
Micro-USB
eg Micro-USB connector ('M' in uppercase whatever its position)
MIPI
Mobile Industry Processor Interface, open membership organization that includes leading companies in the mobile industry that share the objective of defining and promoting open specifications for interfaces inside mobile terminals, see MIPI® Alliance standard web site https://www.mipi.org
MMC
Multimedia card
MMU
Memory management unit. (A hardware device or circuit that supports virtual memory and paging by translating virtual addresses into physical addresses.)
MPU 
Microprocessor unit
MQTT
Message queuing telemetry transport
MTD
Memory technology device

14 N[edit]

NA
Non applicable
NDA
Non-disclosure agreement
NFC
Near field communication ( is a short-range wireless standard for communication over distances up to around 10cm that will enable enhanced services for users of NFC-enabled smart phones. These could include receiving coupons from retailers upon entering a store, or sharing contacts or photos, in addition to making mobile payments and collecting data from medical monitors, smart meters or other equipment containing ST’s dual-interface EEPROM. We produce a wireless memory that can transmit and receive information from the heart of an application to a smart phone containing NFC technology. NFC is expected to become a widely used system for making payments by smart phone in the United States and it is estimated that by 2015, 30.5% (iSupply) of all handsets shipped will contain NFC technology.)
NFS
Network file system (https://en.wikipedia.org/wiki/Network_File_System)
NN
Neural network
NV12
fourcc of YUV420 semi-planar pixel format
NVIC
Nested vectored interrupt controller
NVM
Non volatile memory, like a flash memory

15 O[edit]

OEM
Original equipment manufacturer
OGL
Open graphics library (see http://www.opengl.org/ for more details)
OHCI
Open host controller interface
ONFI
Open NAND flash interface (The ONFI working group, acronym for Open NAND flash interface, was founded in 2005. The group’s mission consists in creating a common industry standard for NAND Flash interfaces, to simplify integration of NAND Flash memory into consumer electronics (CE) devices and computing platforms. ST is one of the co-founder companies together with Hynix, Intel, Micron, Phison and Sony.)
OOM
Out of memory
OPC UA
Open platform communications unified architecture
OpenAMP
Open Asymmetric Multi-Processing (See https://www.openampproject.org/)
OpenCL
Open computing language (See http://www.opencl.org/ for more details)
OpenGL
Open graphics library (see http://www.opengl.org/ for more details)
OpenGLES
Open graphics library for embedded system (See http://www.khronos.org/opengles/ for more details)
OpenVG
Open vector gGraphics (see http://www.khronos.org/openvg/ for more details)
OPP
Operating performance point (link to voltage and frequency scaling)
OP-TEE
Open portable trusted execution environment
OS
Operating system
OSS
Open source software
OST
Open system trace
OTG
USB on-the-go (Capability/type of USB port, acting primarily as USB device, to also act as USB host. Also known as USB OTG.)
OTP
One time programmed

16 P[edit]

PCB
Printed circuit board
PEM
Privacy enhanced mail (File format for storing and sending cryptographic keys, certificates, and other data)
PIE
Position-independent executable - NEW
PKH
Public key hash, used for secure boot - NEW
PKHTH
Public key hash table hash, used for secure boot - NEW
PLB
Polygon list builder (3D IP/IC specific)
PMIC
Power management integrated circuit
PMU
Power management unit (in STPMIC context) or performance monitoring unit (in Arm® Cortex®-A context)
POSIX
Portable operating system interface based on uniX (https://en.wikipedia.org/wiki/POSIX_terminal_interface for more details)
POT
Power of two (could be linked to graphics, like in OpenGL textures)
PP
Pixel processor, used to execute fragment shaders (3D IP/IC specific)
procfs
Process file system (see https://en.wikipedia.org/wiki/Procfs for more details)
PSCI 
Power state coordination interface
PTA
Pseudo Trusted Application
PVD
Programmable voltage detector
PWM
Pulse width modulation

17 Q[edit]

18 R[edit]

RAM
Random access memory (Early computer memories generally hadserial access. Memories where any given address can be accessed when desired were then called "random access" to distinguish them from the memories where contents can only be accessed in a fixed order. The term is used today for volatile random-acces ssemiconductor memories.)
RCC
Reset and clock control
REGMAP
Register map (Linux® registers map abstraction API)
RMA
Return materials authorization
RNG
Random number generator
ro
Read only
ROM
Read only memory
RPMsg
Remote processor messaging
RSE
Remote system explorer (Eclipse Perceptive)
RTC
Real time clock
RTOS
Real time operating system
RX
Receive

19 S[edit]

SAI
Serial audio interface (Mechanism used to transfer non-buffered audio data between processors and/or audio converters.)
SCL
Serial clock line
SCMI
System control and management interface
SCP
Secure coprocessor
SD
Secure digital
SDA
Serial data line
SD card
SD memory card (https://www.sdcard.org)
SDIO
Secure digital input/output
SDIO card 
SDIO is an SD-size card with extended input/output functions
SDK
Software development kit (A programming package that enables a programmer to develop applications for a specific platform.)
Serdev
Serial device bus
SFI
Secure firmware install
SFR
Special function registers
SGI
Software generated interrupt
SHA
Secure hash algorithm
SiP
Silicon provider
SLC
Single-level cell is a kind of NAND flash
SMC
Secure monitor call
SMCCC
Secure monitor call (SMC) calling convention
SMBus
System management bus
SMP
Symetric multiprocessing
SOM
System-on-module
SOT
Start of transmission (MIPI® Alliance DSI standard)
S/PDIF
Sony/Philips digital interface format (Protocol (IEC-60958))
SP-MIN
Secure payload minimal
SP_min
Secure payload minimal
SP_min
Secure payload minimal
SPI
Serial peripheral interface
SPL
Secondary program loader, Also known as U-Boot SPL
SSBL
Second stage boot loader
SSP
Secure secrets secret provisioning
STGEN
System time generator
ST-Link
spelling for older versions of STLink, ST in-circuit debugger and programmer for the STM8 and STM32 microcontroller families
STLink
ST in-circuit debugger and programmer for the STM8 and STM32 microcontroller families (See ST-LINK for more details)
STM
System trace module
STM32Series
stm32mp1
STP
System trace protocol (MIPI® Alliance standard specifying the protocol to carry above system traces)
SSP
Secure secret provisioning
SYSCFG
System configuration
sysfs
System file system (see https://en.wikipedia.org/wiki/Sysfs for more details)
SYSTICK
System tick
SWD
Serial wire debug
SWIM
Single wire interface module (debug protocol for STM8 microcontrollers)

20 T[edit]

TA
Trusted application
TAF
Trusted application function
TAMP
Tamper
TBG
Test byte generator, part of DSI, used to generate - on CPU demand - a stream of byte to the DSI D-PHY. The goal is to perform basic DSI D-PHY lane check
TCG
Trusted computing group
TCM
Tightly coupled memory
TDES
Triple data encryption standard
TEE
Trusted execution environment
termios
Terminal input output structure
TF-A
Trusted firmware for Arm® Cortex®-A
TFTP
Trivial file transfer protocol (https://en.wikipedia.org/wiki/Trivial_File_Transfer_Protocol)
TPM
Trusted platform module
TrEQ
Transducer equalizer
TSS
TPM Software Stack
TTY
TeleTYpewriter
TVG
Test video generator, part of DSI, used to generate a video stream automatically (for verification and validation task)
TX
Transmit
TrustZone
TrustZone®
Arm® and TrustZone® are registered trademarks of Arm Limited (or its subsidiaries) in the US and/or elsewhere.
TZ
TrustZone®
Arm® and TrustZone® are registered trademarks of Arm Limited (or its subsidiaries) in the US and/or elsewhere.
TZC
TrustZone® address space Controller for DDR
Arm® and TrustZone® are registered trademarks of Arm Limited (or its subsidiaries) in the US and/or elsewhere.

21 U[edit]

UART
Universal asynchronous receiver/transmitter
UBI
Unsorted block images
UDC
USB device controller
UI
User interface
UMS
User-space mode setting
µClinux
The letters "μC" are for "microcontroller", the name is pronounced "you-see-Linux" (httphttps://wwwen.uclinuxwikipedia.org/wiki/%CE%9CClinux)
UP
uniprocessor
U-Boot
Das U-Boot -- the universal boot loader (see U-Boot)
USART
Universal synchronous/asynchronous receiver/transmitter
USBH
USB Host (STM32 specific)
USB Type-A
USB port or connector
USB Type-C
USB port or connector
UTMI
USB 2.0 Transceiver Macrocell Interface
USB On-The-Go
Capability/type of USB port, acting primarily as USB device, to also act as USB host. Also known as USB OTG.
UUID
universally unique identifier (https://en.wikipedia.org/wiki/Universally_unique_identifier)
UVC
USB vdeo class

22 V[edit]

V4L2
Video 4 Linux® version 2
VCP
Virtual COM Port. ST-Link console support
VESA
Video electronics standards association
VFS
Virtual file system
VLAN
Virtual LAN. Network of computers that behave as if they are connected to the same wire even though they may actually be physically located on different segments of a LAN
VREFBUF
Voltage reference buffer (STM32 specific)
VTS
Vendor test suite (Android specific)

23 W[edit]

Wi-Fi
Technology for wireless local area networking with devices based on the IEEE 802.11 standards

24 X[edit]

XIP
Execute in place. Method of executing programs directly from long term storage rather than copying it into RAM (linked to NOR Flash).
XTI
Protocol specifying a way to define OST frame boundary and to support trace activation using uart channel.

25 Y[edit]

YAVTA
Yet Another V4L2 Test Application (V4L2 standard)
Yocto Project® 
The Linux Foundation® and Yocto Project® are registered trademarks of the Linux Foundation. Linux® is a registered trademark of Linux Torvalds
Yocto Project 
The Linux Foundation® and Yocto Project® are registered trademarks of the Linux Foundation. Linux® is a registered trademark of Linux Torvalds

26 Z[edit]

27 0-9[edit]

28 See Also[edit]

<noinclude>

{{InternalInfo|Before entering a new term , please refer [http://best.st.com/ResourceCenter/glossary/Glossary/home.aspxhttps://stmicroelectronics.sharepoint.com/sites/Glossary ST internal corporation Glossary ] }} 
{{InternalInfo| New terms and abbreviations should be added in Glossary article, with defintion post fixed by "- NEW", like this  : <nowiki>;API: Application Programming Interface - NEW  </nowiki> <br>

Before creating a new definition, writer must check first if the wished term is already defined inside ST '''internal''' glossary. ST glossary is  available at this link http://best.st.com/ResourceCenter/glossary/Glossary/home.aspx.https://stmicroelectronics.sharepoint.com/sites/Glossary. If the term exists then the definiton given in the ST glossary must be copied in wiki glossary.<br>

If term does not exist in ST glossary, then you can make a proposal in the wiki glossary with the postfix "NEW" as explained above.
Every 2 months, all terms prefixed by NEW in wiki glossary are proposed to be integrated into ST internal glossary, by  wiki administrators.<br> Terminologys /concepts related to stm32mpu wiki  are defined in [[stcontributormanual:Contributors:Wiki_internal_glossary]] }}
{{ReviewsComments|W908.1 : NSA : Glossary must be largely reviewed byST glossary team. For the MML the current version is approved}}</noinclude>

__NOTOC__
Jump to letter: [[#A|A]] [[#B|B]] [[#C|C]] [[#D|D]] [[#E|E]] [[#F|F]] [[#G|G]] [[#H|H]] [[#I|I]] [[#J|J]] [[#K|K]] [[#L|L]] [[#M|M]] [[#N|N]] [[#O|O]] [[#P|P]] [[#Q|Q]] [[#R|R]] [[#S|S]] [[#T|T]] [[#U|U]] [[#V|V]] [[#W|W]] [[#X|X]] [[#Y|Y]] [[#Z|Z]] [[#0-9|0-9]] [[#See Also|See Also]]

Note: The glossary content is '''automatically''' used in all wiki pages.

==A==
;A2DP: Advanced audio distribution profile
;ABI: Application binary interface. ( In computer software, an application binary interface (ABI) describes the low-level interface between a computer program and the operating system or another program.)
;ACL: Automatic current limit (LCD power improvement solution)
;ADB: Android debug bridge (Android specific)
;ADBD: Android debug bridge daemon (Android specific)
;ADC: Analog-to-digital converter. The process of converting a sampled analog signal to a digital code that represents the amplitude of the original signal sample.
;AES: Advanced encryption standard
;AF:GPIO alternate function 
;AHB: Advanced high-performance bus
;AI: Artificial intelligence
;AIDL: Android interface definition language (see https://developer.android.com/guide/components/aidl)
;aka: also known as 
;ALSA: Advanced Linux sound architecture 
;AOSP: Android open source project
;APB: Advanced peripheral bus 
;API: Application programming interface
;APT: Advanced package tool (see https://wiki.debian.org/Apt)
;Arm<sup>&reg;</sup> : ''Arm<sup>&reg;</sup> is a registered trademark of Arm Limited (or its subsidiaries) in the US and/or elsewhere.'' [[File:Arm logo.png|72px|link=]] 
;Arm: ''Arm<sup>&reg;</sup> is a registered trademark of Arm Limited (or its subsidiaries) in the US and/or elsewhere.'' [[File:Arm logo.png|72px|link=]] 
;ARP:Protocol used by the internet protocol, specifically IPv4, to map IP network addresses to the hardware addresses used by a data link protocol (https://en.wikipedia.org/wiki/Address_Resolution_Protocol)
;ART: Android runtime (see https://source.android.com/devices/tech/dalvik)
;ASoC: ALSA system on chip
;AVB: Audio video bridging over Ethernet (set of IEEE standards for transporting audio and other real-time content over Ethernet)
;AVD: Analog voltage detector

==B==
;BCC: BPF compiler collection
;BL1: Boot loader stage 1
;BL2: Boot loader stage 2
;BL32: Boot loader stage 3-2
;BL33: Boot loader stage 3-3
;BLE: Bluetooth low energy. Bluetooth LE, marketed as Bluetooth Smart is a wireless personal area network technology designed and marketed by the Bluetooth Special Interest Group aimed at novel applications in the healthcare, fitness, beacons, security, and home entertainment industries. <br>Compared to Classic Bluetooth, Bluetooth Smart is intended to provide considerably reduced power consumption and cost while maintaining a similar communication range. (sourcehttps://en.wikipedia.org/wiki/Bluetooth_Low_Energy)
;BoardId: eval, disco (Generic term used, to complete configuration modules paths depending on used board)
;BOR: Brownout reset
;BSP: Board support package
;BSEC: Boot and Security and OTP control 
;BT: BlueTooth

==C==
;CABC: Content-adaptative backlight control (LCD power improvement solution)
;CAB: Content-adaptative backlight (LCD power improvement solution)
;CAN: Controller area network (robust bus mainly used for automotive applications)
;CEC: Consumer electronics control (HDMI standard)
;CLUT: Colour look-up table
;CMSIS: Cortex microcontroller software interface standard
;CNN: Convolutional neural network
;configfs: Configuration file system (see https://en.wikipedia.org/wiki/Configfs for more details)
;Cortex: Cortex<sup>&reg;</sup>

;CoT: Chain of trust
;CPL: Common public license 
;CPU: Central processing unit
;CRC: Cyclic redundancy check calculation unit
;CRYP: Cryptographic processor
;CSG: Constructive solid geometry
;CSI: Multi Speed Internal oscillator (STM32 clock source) 
;CSS: Cascading style sheets (web standard)
;CTS: Compatibility test suite (Android specific) or clear to send (in UART context)
;CV: Computer vision

==D==
;DAC: Digital-to-analog converter (Electronic circuit that converts a binary number into a continuously varying value.)
;DAI: Digital audio interface
;DAPM: Dynamic audio power management
;DBI: Display bus interface (MIPI<sup>&reg;</sup> Alliance standard)
;DCMI:Digital Camera memory interface 
;DCMIPP:Digital Camera memory interface pixel processor
;DDB: Device descriptor block (MIPI<sup>&reg;</sup> Alliance standard)
;DDC: Display data channel (VESA standard)
;DDR: Doubledata rate (memory domain)
;debugfs: Debug file system (see https://en.wikipedia.org/wiki/Debugfs for more details)  
;devfs: Device file system (see https://en.wikipedia.org/wiki/Device_file#DEVFS for more details)
;DES: Data encryption standard
;DFSDM: Digital filter for sigma-delta modulator
;DFT: Techniques implemented during semiconductor development to improve device testability (Scan, BIST…).
;DFU: Device firmware upgrade
;DHCP: Dynamic host configuration pProtocol (see https://en.wikipedia.org/wiki/Dynamic_Host_Configuration_Protocol for more details)
;DISCO: Discovery kit
;DMA: Direct memory access
;DMA2D:Chrom-art accelerator™ controller (STM32 specific)
;DMIC: Digital microphone
;DPA: Differential power analysis
;DPI: Display pixel interface (MIPI<sup>&reg;</sup> Alliance standard)
;DRD: Dual-role device (USB standard defines host and device roles. OTG controllers support both roles and can be called Dual-role devices controllers.)
;DRI: Direct rendering infrastructure (Linux<sup>&reg;</sup> framework for allowing direct access to graphics hardware... find more information on official DRI web site http://dri.freedesktop.org/wiki/FrontPage)
;DRM: Direct rendering manager (kernel module that gives direct hardware access to DRI clients, find more information on official DRI web site http://dri.freedesktop.org/wiki/DRM)
;DRP: Dual role port, an USB port that can operate in host or device mode
;DSI: Display serial interface (MIPI<sup>&reg;</sup> Alliance standard)
;DT: Device tree
;DTB: Device tree binary (or Blob)
;DTS:Device tree source (in software context) or digital temperature sensor (in peripheral context) 
;DVI: Digital visual interface (digital display working group)
;DVFS: Dynamic voltage and frequency scaling

==E==
;EAL: Evaluation assurance level 
;ECC: Error correction capability 
;ECC: Elliptic curve cryptography
;ECDSA: Elliptic curve digital signature algorithm
;EDID: Extended Display identification data (HDMI standard)
;EDMK: Encryption Decryption master key, used for secure boot - NEW
;EDP: Embedded Display port (VESA standard). See http://www.displayport.org/ for more details
;EEPROM: Electrically-erasable programmable read-only memory 
;EGL: Khronos native platform graphics interface (See http://www.khronos.org/egl/ for more details)
;EHCI: Enhanced host controller interface
;ELF: Executable and linkable file
;EMI: External memory interface
;eMMC: Former spelling for e•MMC ('e' in italic) 
;''e''•MMC: Embedded uulti-media card 
;EOT: End of transmission (MIPI<sup>&reg;</sup> Alliance DSI standard)
;eSDK: Extensible software development kit
;ETH: Ethernet
;ETM: Embedded trace macrocell
;ETZPC: Extended trustzone protection controller 
;EVAL: Evaluation board 
;EXTI: External interrupt

==F==
;FB: Frame buffer (could be the Kernel framebuffer linked to the display, a GPU framebuffer, an imaging framebuffer...)
;FCONF: Firmware configuration framework used by TF-A - NEW
;FHS: File hierarchy standard defines by Linux<sup>&reg;</sup> Foundation
;FIP: Firmware image package is a packaging format used by TF-A 
;FIT: Flattened image tree is a packaging format used by U-Boot
;Flash: Flash memory shortened to gain space in titles, tables and block diagrams
;Flash memory : Flash memories combine high density and cost effectiveness of EPROMs with the electrical erasability of EEPROMs. For this reason, the Flash memory market is one of the most exciting areas of the semiconductor industry today and new applications requiring in system reprogramming, such as cellular telephones, automotive engine management systems, hard disk drives, PC BIOS software for Plug & Play, digital TV, set top boxes, fax and other modems, PC cards and multimedia CD-ROMs, offer the prospect of very high volume demand.
;foo_driver: foo_driver could be any driver that needs to control a GPIO
;FPS: Frames per second
;fs: File system or filesystem,  method and data structure that the operating system uses to control how data is stored and retrieved - NEW
;FS: File system or filesystem,  method and data structure that the operating system uses to control how data is stored and retrieved -NEW
;FSBL: First stage boot loader
;FTR: First time right

==G==

;GDB: GNU dedugger, a portable debugger that runs on many Unix-like systems
;GIC: Generic interrupt controller
;GP: Geometry processor, used to execute Vertex Shaders (3D IP/IC specific).
;GPIO: General-purpose input/output (A realization of open ended transmission between devices on an embedded level. These pins available on a processor can be programmed to be used to either accept input or provide output to external devices depending on user desires and applications requirements.)
;GPGPU: General-purpose computation on graphics processing units
;GPT: GUID partition table
;GPU: Graphics processing units
;GRALLOC: Graphic allocation HAL or library (Android specific)
;GUI: Graphical user interface

==H==

;HAL: Hardware abstraction layer
;HDCP: High-bandwidth digital content protection (HDMI standard)
;HDMI: High-definition multimedia interface (HDMI standard)
;HDP: Hardware debug port
;HDR: High dynamic range (HDMI standard)
;HID: Human interface device (for USB, Bluetooth...)
;HIDL: HAL interface definition language (see https://source.android.com/devices/architecture/hidl)
;HMAC: Hash-based Message authentication code
;HPD: Hot plug detect
;HS: High speed (MIPI<sup>&reg;</sup> alliance DSI standard)
;HSEM : Hardware semaphore
;HSE: High speed external oscillator (STM32 clock source)
;HSI: High speed internal oscillator (STM32 clock source) or High speed synchronous serial interface (MIPI<sup>&reg;</sup> Alliance standard)
;HSLV: High speed low voltage pin mode
;HSM: Hardware security module

==I==
;I2C: Inter-integrated circuit (Bi-directional 2-wire bus standard for efficient inter-IC control.)
;I2S: Integrated interchip sound
I2S (without the 2 in superscript) refers to the STMicroelectronics integrated interchip sound IP.
;I420: fourcc of YUV420 planar pixel format
;IDE: (Software)Integrated development/design/debugging environment
;IFP: Image formatting pipeline
;IIC: Inter-integrated circuit (Bi-directional 2-wire bus standard for efficient inter-IC control.)
;IIO: Industrial I/O Linux<sup>&reg;</sup> subsystem 
;initramfs: Initial ramdisk (https://en.wikipedia.org/wiki/Initial_ramdisk)
;initrd: Initial ramdisk (https://en.wikipedia.org/wiki/Initial_ramdisk)
;IMU: Inertial measurement unit
;IO: input/output 
;IoT: Internet of things 
;IPC: Inter-processor communication
;IPCC: Inter-processor communication controller
;IPP: Image preprocessor pipeline
;ITM: Instruction trace Macrocell 
;IWDG :Independent watchdog

==J==

;JIT:Just-In-Time (Way of working for a given Virtual Machine)
;JNI: Java Native Interface (for Android)
;JTAG: debug and test protocol, named from the Joint Test Action Group that developed it

==K==

;KMS:Kernel Mode Setting

==L==
;LBA: Logical block addressing
;LDISC: Line discipline
;LED: Light-emitting diode
;LIN: Local interconnect network
;Linux: Linux<sup>&reg;</sup> is a registered trademark of Linus Torvalds.
;LDO: Low-dropout regulator
;LL: Low layer of STM32Cube 
;LP: Low power (MIPI<sup>&reg;</sup> Alliance DSI standard)
;LTDC: LCD TFT display controller (STM32 specific)
;LPTIM : Low-power timer (STM32 specific)
;LSE: Low speed external oscillator (STM32 clock source) 
;LSI: Low speed internal oscillator (STM32 clock source)

==M==
;MAC address: media access control address (https://en.wikipedia.org/wiki/MAC_address) 
;MCU: Microcontroller unit (MCUs have internal flash memory and are intended to operate with a minimum amount of external support ICs.  They commonly are a self-contained, system-on-chip (SoC) designs.)
;MD5: Message digest 5
;MDK: Microcontroller Development Kit from Keil® (see https://www2.keil.com/mdk5) 
;MFD: Multifunction device 
;microSD<sup>TM;</sup>: eg microSD card ('m' in lowcase whatever its position)
;Micro-AB: Micro-AB connector/port ('M' in uppercase whatever its position)
;Micro-USB: eg Micro-USB connector ('M' in uppercase whatever its position)
;MIPI: Mobile Industry Processor Interface, open membership organization that includes leading companies in the mobile industry that share the objective of defining and promoting open specifications for interfaces inside mobile terminals, see MIPI<sup>&reg;</sup> Alliance standard web site https://www.mipi.org
;MMC: Multimedia card 
;MMU: Memory management unit. (A hardware device or circuit that supports virtual memory and paging by translating virtual addresses into physical addresses.)
;MPU :Microprocessor unit
;MQTT: Message queuing telemetry transport 
{{ReviewsComments|-- [[User:Nathalie Sangouard|Nathalie Sangouard]] ([[User talk:Nathalie Sangouard|talk]]) 18:18, 18 March 2021 (CET)<br /> MQTT not in ST glossary}}
;MTD: Memory technology device

==N==
;NA:Non applicable
;NDA: Non-disclosure agreement
;NFC: Near field communication ( is a short-range wireless standard for communication over distances up to around 10cm that will enable enhanced services for users of NFC-enabled smart phones. These could include receiving coupons from retailers upon entering a store, or sharing contacts or photos, in addition to making mobile payments and collecting data from medical monitors, smart meters or other equipment containing ST’s dual-interface EEPROM. We produce a wireless memory that can transmit and receive information from the heart of an application to a smart phone containing NFC technology. NFC is expected to become a widely used system for making payments by smart phone in the United States and it is estimated that by 2015, 30.5% (iSupply) of all handsets shipped will contain NFC technology.)
;NFS: Network file system (https://en.wikipedia.org/wiki/Network_File_System)
;NN: Neural network
;NV12: fourcc of YUV420 semi-planar pixel format
;NVIC: Nested vectored interrupt controller 
;NVM: Non volatile memory, like a flash memory

==O==
;OEM: Original equipment manufacturer
;OGL: Open graphics library (see http://www.opengl.org/ for more details)
;OHCI: Open host controller interface
;ONFI: Open NAND flash interface (The ONFI working group, acronym for Open NAND flash interface, was founded in 2005. The group’s mission consists in creating a common industry standard for NAND Flash interfaces, to simplify integration of NAND Flash memory into consumer electronics (CE) devices and computing platforms. ST is one of the co-founder companies together with Hynix, Intel, Micron, Phison and Sony.)
;OOM: Out of memory
;OPC UA: Open platform communications unified architecture 
{{ReviewsComments|-- [[User:Nathalie Sangouard|Nathalie Sangouard]] ([[User talk:Nathalie Sangouard|talk]]) 18:18, 18 March 2021 (CET)<br />OPC UA not in ST glossary}}
;OpenAMP: Open Asymmetric Multi-Processing (See https://www.openampproject.org/)
;OpenCL: Open computing language (See http://www.opencl.org/ for more details)
;OpenGL:Open graphics library (see http://www.opengl.org/ for more details)
;OpenGLES: Open graphics library for embedded system (See http://www.khronos.org/opengles/ for more details)
;OpenVG: Open vector gGraphics (see http://www.khronos.org/openvg/ for more details)
;OPP: Operating performance point (link to voltage and frequency scaling)
;OP-TEE: Open portable trusted execution environment
;OS: Operating system
;OSS: Open source software
;OST: Open system trace
;OTG: USB on-the-go (Capability/type of USB port, acting primarily as USB device, to also act as USB host. Also known as USB OTG.)
;OTP: One time programmed

==P==

;PCB: Printed circuit board 
;PEM: Privacy enhanced mail  (File format for storing and sending cryptographic keys, certificates, and other data)
;PIE: Position-independent executable - NEW
;PKH: Public key hash, used for secure boot - NEW
;PKHTH: Public key hash table hash, used for secure boot - NEW
;PLB: Polygon list builder (3D IP/IC specific)
;PMIC: Power management integrated circuit
;PMU: Power management unit (in STPMIC context) or performance monitoring unit (in Arm<sup>&reg;</sup> Cortex<sup>&reg;</sup>-A context) 
;POSIX: Portable operating system interface based on uniX (https://en.wikipedia.org/wiki/POSIX_terminal_interface for more details)
;POT: Power of two (could be linked to graphics, like in OpenGL textures)
;PP: Pixel processor, used to execute fragment shaders (3D IP/IC specific)
;procfs: Process file system (see https://en.wikipedia.org/wiki/Procfs for more details) 
;PSCI : Power state coordination interface 
;PTA: Pseudo Trusted Application
;PVD: Programmable voltage detector
;PWM: Pulse width modulation

==Q==

==R==
;RAM: Random access memory (Early computer memories generally hadserial access. Memories where any given address can be accessed when desired were then called "random access" to distinguish them from the memories where contents can only be accessed in a fixed order. The term is used today for volatile random-acces ssemiconductor memories.)

;RCC: Reset and clock control
;REGMAP: Register map (Linux<sup>&reg;</sup> registers map abstraction API) 
;RMA: Return materials authorization 
;RNG: Random number generator
;ro: Read only
;ROM:Read only memory 
;RPMsg: Remote processor messaging
;RSE: Remote system explorer (Eclipse Perceptive)
;RTC: Real time clock  
;RTOS: Real time operating system
;RX: Receive

==S==
;SAI: Serial audio interface (Mechanism used to transfer non-buffered audio data between processors and/or audio converters.)
;SCL: Serial clock line 
;SCMI: System control and management interface 
;SCP: Secure coprocessor
{{ReviewsComments|-- [[User:Nathalie Sangouard|Nathalie Sangouard]] ([[User talk:Nathalie Sangouard|talk]]) 09:59, 2 June 2021 (CEST)<br />In ST glossary : not the same definition : Secure Channel Protocol }}
;SD: Secure digital 
;SDA: Serial data line 
;SD card: SD memory card (https://www.sdcard.org)
;SDIO: Secure digital input/output
;SDIO card : SDIO is an SD-size card with extended input/output functions
;SDK: Software development kit (A programming package that enables a programmer to develop applications for a specific platform.)
;Serdev: Serial device bus 
;SFI: Secure firmware install
{{ReviewsComments|-- [[User:Nathalie Sangouard|Nathalie Sangouard]] ([[User talk:Nathalie Sangouard|talk]]) 18:34, 22 November 2022 (CET)<br />SFI is not in ST glossary}}
;SFR:  Special function registers
;SGI: Software generated interrupt
;SHA: Secure hash algorithm
;SiP: Silicon provider
;SLC:Single-level cell is a kind of NAND flash  
;SMC: Secure monitor call
;SMCCC: Secure monitor call (SMC) calling convention
{{ReviewsComments|-- [[User:Nathalie Sangouard|Nathalie Sangouard]] ([[User talk:Nathalie Sangouard|talk]]) 18:18, 18 March 2021 (CET)<br />SMCCC not in ST glossary}}
;SMBus: System management bus 
;SMP: Symetric multiprocessing 
;SOM: System-on-module
;SOT: Start of transmission (MIPI<sup>&reg;</sup> Alliance DSI standard)
;S/PDIF: Sony/Philips digital interface format (Protocol (IEC-60958))
;SP-MIN: Secure payload minimal
;SP_min: Secure payload minimal;SP_min: Secure payload minimal{{ReviewsComments|-- [[User:Nathalie Sangouard|Nathalie Sangouard]] ([[User talk:Nathalie Sangouard|talk]]) 18:36, 22 November 2022 (CET)<br />SP_ min or SP-Min are not in ST glossary}};SPI: Serial peripheral interface
;SPL: Secondary program loader, ''Also known as '''U-Boot SPL''''' 
;SSBL: Second stage boot loader
;SSP: Secure secretssecret provisioning {{ReviewsComments|-- [[User:Nathalie Sangouard|Nathalie Sangouard]] ([[User talk:Nathalie Sangouard|talk]]) 18:18, 18 March 2021 (CET)<br />SSP not in ST glossary with this meaning}};STGEN: System time generator
;ST-Link: spelling for older versions of STLink, ST in-circuit debugger and programmer for the STM8 and STM32 microcontroller families
;STLink: ST in-circuit debugger and programmer for the STM8 and STM32 microcontroller families (See [[ST-LINK]] for more details)
;STM: System trace module
;STM32Series: stm32mp1
;STP: System trace protocol (MIPI<sup>&reg;</sup> Alliance standard specifying the protocol to carry above system traces)
;SSP: Secure secret provisioning
;SYSCFG: System configuration
;sysfs: System file system (see https://en.wikipedia.org/wiki/Sysfs for more details)
;SYSTICK: System tick
;SWD: Serial wire debug 
;SWIM: Single wire interface module (debug protocol for STM8 microcontrollers)

==T==
;TA: Trusted application
;TAF: Trusted application function
;TAMP: Tamper
;TBG: Test byte generator, part of DSI, used to generate - on CPU demand - a stream of byte to the DSI D-PHY. The goal is to perform basic DSI D-PHY lane check
;TCG: Trusted computing group
;TCM: Tightly coupled memory
;TDES: Triple data encryption standard
;TEE: Trusted execution environment
;termios: Terminal input output structure
;TF-A: Trusted firmware for Arm<sup>&reg;</sup> Cortex<sup>&reg;</sup>-A
;TFTP: Trivial file transfer protocol (https://en.wikipedia.org/wiki/Trivial_File_Transfer_Protocol)
;TPM: Trusted platform module
;TrEQ: Transducer equalizer 
;TSS: TPM Software Stack
;TTY: TeleTYpewriter
;TVG: Test video generator, part of DSI, used to generate a video stream automatically (for verification and validation task)
;TX: Transmit 
;TrustZone: TrustZone<sup>&reg;</sup> <br> ''Arm<sup>&reg;</sup> and TrustZone<sup>&reg;</sup> are registered trademarks of Arm Limited (or its subsidiaries) in the US and/or elsewhere.''
;TZ: TrustZone<sup>&reg;</sup> <br>''Arm<sup>&reg;</sup> and TrustZone<sup>&reg;</sup> are registered trademarks of Arm Limited (or its subsidiaries) in the US and/or elsewhere.''
;TZC: TrustZone<sup>&reg;</sup> address space Controller for DDR <br> ''Arm<sup>&reg;</sup> and TrustZone<sup>&reg;</sup> are registered trademarks of Arm Limited (or its subsidiaries) in the US and/or elsewhere.''

==U==
;UART: Universal asynchronous receiver/transmitter
;UBI: Unsorted block images
;UDC: USB device controller
;UI: User interface
;UMS: User-space mode setting
;µClinux: The letters "μC" are for "microcontroller", the name is pronounced "you-see-Linux" (http://www.uclinux.org/https://en.wikipedia.org/wiki/%CE%9CClinux)
;UP: uniprocessor
;U-Boot: Das U-Boot -- the universal boot loader (see [[U-Boot]])
;USART: Universal synchronous/asynchronous receiver/transmitter
;USBH: USB Host (STM32 specific) 
;USB Type-A: USB port or connector  
;USB Type-C: USB port or connector
;UTMI: USB 2.0 Transceiver Macrocell Interface
;USB On-The-Go: Capability/type of USB port, acting primarily as USB device, to also act as USB host. Also known as USB OTG.
;UUID: universally unique identifier (https://en.wikipedia.org/wiki/Universally_unique_identifier)
;UVC: USB vdeo class

==V==
;V4L2: Video 4 Linux<sup>&reg;</sup> version 2
;VCP: Virtual COM Port. ST-Link console support
;VESA: Video electronics standards association
;VFS: Virtual file system
;VLAN: Virtual LAN. Network of computers that behave as if they are connected to the same wire even though they may actually be physically located on different segments of a LAN
;VREFBUF: Voltage reference buffer (STM32 specific)
;VTS: Vendor test suite (Android specific)

==W==
;Wi-Fi: Technology for wireless local area networking with devices based on the IEEE 802.11 standards

==X==
;XIP: Execute in place. Method of executing programs directly from long term storage rather than copying it into RAM (linked to NOR Flash).
;XTI: Protocol specifying a way to define OST frame boundary and to support trace activation using uart channel.

==Y==
;YAVTA: Yet Another V4L2 Test Application (V4L2 standard)
;Yocto Project<sup>®</sup> :The Linux Foundation® and Yocto Project® are registered trademarks of the Linux Foundation. Linux® is a registered trademark of Linux Torvalds
;Yocto Project :The Linux Foundation® and Yocto Project® are registered trademarks of the Linux Foundation. Linux® is a registered trademark of Linux Torvalds

==Z==

==0-9==

==See Also==
<noinclude>

[[Category:Sub-articles]]</noinclude>
(10 intermediate revisions by 3 users not shown)
Line 1: Line 1:
 
<noinclude>
 
<noinclude>
{{InternalInfo|Before entering a new term , please refer [http://best.st.com/ResourceCenter/glossary/Glossary/home.aspx ST internal corporation Glossary ] }}  
+
{{InternalInfo|Before entering a new term , please refer [https://stmicroelectronics.sharepoint.com/sites/Glossary ST internal corporation Glossary ] }}  
 
{{InternalInfo| New terms and abbreviations should be added in Glossary article, with defintion post fixed by "- NEW", like this  :  
 
{{InternalInfo| New terms and abbreviations should be added in Glossary article, with defintion post fixed by "- NEW", like this  :  
 
<nowiki>;API: Application Programming Interface - NEW  </nowiki> <br>
 
<nowiki>;API: Application Programming Interface - NEW  </nowiki> <br>
Before creating a new definition, writer must check first if the wished term is already defined inside ST '''internal''' glossary. ST glossary is  available at this link http://best.st.com/ResourceCenter/glossary/Glossary/home.aspx. If the term exists then the definiton given in the ST glossary must be copied in wiki glossary.<br>
+
Before creating a new definition, writer must check first if the wished term is already defined inside ST '''internal''' glossary. ST glossary is  available at this link https://stmicroelectronics.sharepoint.com/sites/Glossary. If the term exists then the definiton given in the ST glossary must be copied in wiki glossary.<br>
 
If term does not exist in ST glossary, then you can make a proposal in the wiki glossary with the postfix "NEW" as explained above.
 
If term does not exist in ST glossary, then you can make a proposal in the wiki glossary with the postfix "NEW" as explained above.
Every 2 months, all terms prefixed by NEW in wiki glossary are proposed to be integrated into ST internal glossary, by  wiki administrators.<br> Terminologys /concepts related to stm32mpu wiki  are defined in [[Contributors:Wiki_internal_glossary]] }}
+
Every 2 months, all terms prefixed by NEW in wiki glossary are proposed to be integrated into ST internal glossary, by  wiki administrators.<br> Terminologys /concepts related to stm32mpu wiki  are defined in [[stcontributormanual:Contributors:Wiki_internal_glossary]] }}
 
{{ReviewsComments|W908.1 : NSA : Glossary must be largely reviewed byST glossary team. For the MML the current version is approved}}
 
{{ReviewsComments|W908.1 : NSA : Glossary must be largely reviewed byST glossary team. For the MML the current version is approved}}
 
</noinclude>
 
</noinclude>
Line 99: Line 99:
 
;DPI: Display pixel interface (MIPI<sup>&reg;</sup> Alliance standard)
 
;DPI: Display pixel interface (MIPI<sup>&reg;</sup> Alliance standard)
 
;DRD: Dual-role device (USB standard defines host and device roles. OTG controllers support both roles and can be called Dual-role devices controllers.)
 
;DRD: Dual-role device (USB standard defines host and device roles. OTG controllers support both roles and can be called Dual-role devices controllers.)
;DRI: Direct rendering infrastructure (Linux<sup>&reg;</sup> framework for allowing direct access to graphics hardware... find more information on official DRI web site http://dri.freedesktop.org/wiki/FrontPage)
+
;DRI: Direct rendering infrastructure (Linux<sup>&reg;</sup> framework for allowing direct access to graphics hardware... find more information on official DRI web site http://dri.freedesktop.org/)
 
;DRM: Direct rendering manager (kernel module that gives direct hardware access to DRI clients, find more information on official DRI web site http://dri.freedesktop.org/wiki/DRM)
 
;DRM: Direct rendering manager (kernel module that gives direct hardware access to DRI clients, find more information on official DRI web site http://dri.freedesktop.org/wiki/DRM)
 
;DRP: Dual role port, an USB port that can operate in host or device mode
 
;DRP: Dual role port, an USB port that can operate in host or device mode
Line 226: Line 226:
 
;MCU: Microcontroller unit (MCUs have internal flash memory and are intended to operate with a minimum amount of external support ICs.  They commonly are a self-contained, system-on-chip (SoC) designs.)
 
;MCU: Microcontroller unit (MCUs have internal flash memory and are intended to operate with a minimum amount of external support ICs.  They commonly are a self-contained, system-on-chip (SoC) designs.)
 
;MD5: Message digest 5
 
;MD5: Message digest 5
  +
;MDK: Microcontroller Development Kit from Keil® (see https://www2.keil.com/mdk5)
 
;MFD: Multifunction device  
 
;MFD: Multifunction device  
 
;microSD<sup>TM;</sup>: eg microSD card ('m' in lowcase whatever its position)
 
;microSD<sup>TM;</sup>: eg microSD card ('m' in lowcase whatever its position)
Line 256: Line 257:
 
;OPC UA: Open platform communications unified architecture  
 
;OPC UA: Open platform communications unified architecture  
 
{{ReviewsComments|-- [[User:Nathalie Sangouard|Nathalie Sangouard]] ([[User talk:Nathalie Sangouard|talk]]) 18:18, 18 March 2021 (CET)<br />OPC UA not in ST glossary}}
 
{{ReviewsComments|-- [[User:Nathalie Sangouard|Nathalie Sangouard]] ([[User talk:Nathalie Sangouard|talk]]) 18:18, 18 March 2021 (CET)<br />OPC UA not in ST glossary}}
  +
;OpenAMP: Open Asymmetric Multi-Processing (See https://www.openampproject.org/)
 
;OpenCL: Open computing language (See http://www.opencl.org/ for more details)
 
;OpenCL: Open computing language (See http://www.opencl.org/ for more details)
 
;OpenGL:Open graphics library (see http://www.opengl.org/ for more details)
 
;OpenGL:Open graphics library (see http://www.opengl.org/ for more details)
Line 318: Line 320:
 
;SDK: Software development kit (A programming package that enables a programmer to develop applications for a specific platform.)
 
;SDK: Software development kit (A programming package that enables a programmer to develop applications for a specific platform.)
 
;Serdev: Serial device bus  
 
;Serdev: Serial device bus  
  +
;SFI: Secure firmware install
  +
{{ReviewsComments|-- [[User:Nathalie Sangouard|Nathalie Sangouard]] ([[User talk:Nathalie Sangouard|talk]]) 18:34, 22 November 2022 (CET)<br />SFI is not in ST glossary}}
 
;SFR:  Special function registers
 
;SFR:  Special function registers
 
;SGI: Software generated interrupt
 
;SGI: Software generated interrupt
Line 333: Line 337:
 
;SP-MIN: Secure payload minimal
 
;SP-MIN: Secure payload minimal
 
;SP_min: Secure payload minimal
 
;SP_min: Secure payload minimal
;SP_min: Secure payload minimal
+
{{ReviewsComments|-- [[User:Nathalie Sangouard|Nathalie Sangouard]] ([[User talk:Nathalie Sangouard|talk]]) 18:36, 22 November 2022 (CET)<br />SP_ min or SP-Min are not in ST glossary}}
 
;SPI: Serial peripheral interface
 
;SPI: Serial peripheral interface
 
;SPL: Secondary program loader, ''Also known as '''U-Boot SPL'''''  
 
;SPL: Secondary program loader, ''Also known as '''U-Boot SPL'''''  
 
;SSBL: Second stage boot loader
 
;SSBL: Second stage boot loader
;SSP: Secure secrets provisioning  
+
;SSP: Secure secret provisioning  
{{ReviewsComments|-- [[User:Nathalie Sangouard|Nathalie Sangouard]] ([[User talk:Nathalie Sangouard|talk]]) 18:18, 18 March 2021 (CET)<br />SSP not in ST glossary with this meaning}}
 
 
;STGEN: System time generator
 
;STGEN: System time generator
 
;ST-Link: spelling for older versions of STLink, ST in-circuit debugger and programmer for the STM8 and STM32 microcontroller families
 
;ST-Link: spelling for older versions of STLink, ST in-circuit debugger and programmer for the STM8 and STM32 microcontroller families
Line 345: Line 348:
 
;STM32Series: stm32mp1
 
;STM32Series: stm32mp1
 
;STP: System trace protocol (MIPI<sup>&reg;</sup> Alliance standard specifying the protocol to carry above system traces)
 
;STP: System trace protocol (MIPI<sup>&reg;</sup> Alliance standard specifying the protocol to carry above system traces)
;SSP: Secure secret provisioning
 
 
;SYSCFG: System configuration
 
;SYSCFG: System configuration
 
;sysfs: System file system (see https://en.wikipedia.org/wiki/Sysfs for more details)
 
;sysfs: System file system (see https://en.wikipedia.org/wiki/Sysfs for more details)
Line 380: Line 382:
 
;UI: User interface
 
;UI: User interface
 
;UMS: User-space mode setting
 
;UMS: User-space mode setting
;µClinux: The letters "μC" are for "microcontroller", the name is pronounced "you-see-Linux" (http://www.uclinux.org/)
+
;µClinux: The letters "μC" are for "microcontroller", the name is pronounced "you-see-Linux" (https://en.wikipedia.org/wiki/%CE%9CClinux)
 
;UP: uniprocessor
 
;UP: uniprocessor
 
;U-Boot: Das U-Boot -- the universal boot loader (see [[U-Boot]])
 
;U-Boot: Das U-Boot -- the universal boot loader (see [[U-Boot]])