Difference between revisions of "Getting started/STM32MP1 boards/STM32MP157x-EV1/Let's start/Use the demo launcher"

[quality revision] [quality revision]
m
m

Template:ArticleMainWriter

STM32MP157C-EV1.png
Let's start Develop on Arm® Cortex®-A7
Step category in.png Unpack the board Step.png Populate the target and boot the image Step.png Execute basic commands Step.png Use the demo launcher Step category out.png


1 Overview[edit]

This article gives information about the Demo Launcher application. The Demo Launcher starts by default in the Starter Package. This application is written in python3 and uses GTK to display the user interface. A touchscreen is required to control the application.


2 STM32MP13x lines Warning.png main menu[edit]

The main menu is composed of three demonstrations:

Main menu
Netdata perf monitor Gives information in how to connect to the board through Ethernet or Wi-Fi® (if available) in order to connect to netdata
Camera preview Displays the preview camera
Bluetooth® speaker Allows the connection to a Bluetooth®headset


To exit from this window, tap on the cross in the top-right corner. To launch it again, tap or click on the Weston icon launcher with nine blue squares.

2.1 Netdata perf monitor[edit]

Netdata perf monitor

Netdata is a tool which starts on boot and provides all monitoring information on a web page accessible using the board IP address. This window helps with the network connection and gets the board netdata information.

If an Ethernet network is available, the URL to connect to netdata is displayed.
If wireless network is available, a cursor button is displayed to enable hotspot Wi-Fi®.
If Wi-Fi® hotspot is enabled with default configuration, two QR-codes are displayed on screen:

  • The first one gives the Wi-Fi® hotspot connection parameters
  • The second one provides the URL to connect to netdata

To exit from this window, double tap anywhere on the screen.

2.2 Camera preview[edit]

This application displays the preview from /dev/video0:
A USB webcam can be used.

Make sure the webcam is compatible with Linux®.

The available actions to control the camera preview are:

  • First tap: as preview is composed by Wayland, the first tap has to be done outside the camera preview window to recover the GTK focus.
  • Simple tap: pause/resume the camera preview.
  • Double tap: double tap anywhere on the screen to exit from this window.

More information on V4L2 and how to manage the display are available in V4L2 camera overview and Wayland_Weston_overview, respectively.

2.3 Bluetooth® speaker[edit]

Bluetooth speaker

This application is able to discover Bluetooth® devices, and pair/connect to them. If an audio-capable device is connected, the message The audio BT device <your device> is connected is displayed.

First use:
1) Tap on start scan button: a scan of discoverable devices is performed during 15 seconds and a progress bar is displayed.
2) Select a device from the list and tap on connect.

If the device is already connected, the disconnect button is displayed instead.

To exit from this window, double tap anywhere on the screen.
More information on Bluetooth® are available in Bluetooth_overview.

2.4 Info menu[edit]

Info menu

Click the "i" icon on the right of the screen. It displays the menu describing how to use the demos. To exit from this window, double tap anywhere on the screen.


3 STM32MP15x lines More info.png main menu[edit]

The main menu is composed of six demonstrations:

Main menu
Netdata perf monitor Gives information in how to connect to the board through Ethernet or Wi-Fi® (if available) in order to connect to netdata
Camera preview Displays the preview camera
Video playback Displays the video playback
Artificial intelligence Handwriting character recognition (using Arm® Cortex®-M4 firmware)
3D GPU Displays a rotating 3D cube
Bluetooth® speaker Allows the connection to a Bluetooth®headset


To exit from this window, tap on the cross in the top-right corner. To launch it again, tap or click on the Weston icon launcher with nine blue squares.

3.1 Netdata perf monitor[edit]

Netdata perf monitor

Netdata is a tool which starts on boot and provides all monitoring information on a web page accessible using the board IP address. This window helps with the network connection and gets the board netdata information.

If an Ethernet network is available, the URL to connect to netdata is displayed.
If wireless network is available, a cursor button is displayed to enable hotspot Wi-Fi®.
If Wi-Fi® hotspot is enabled with default configuration, two QR-codes are displayed on screen:

  • The first one gives the Wi-Fi® hotspot connection parameters
  • The second one provides the URL to connect to netdata

To exit from this window, double tap anywhere on the screen.

3.2 Camera preview[edit]

This application displays the preview from /dev/video0:

  • On STM32MP157C-DK2 More info green.png boards, a USB webcam can be used.
  • On STM32MP157C-EV1 More info green.png and STM32MP135x-DK Warning.png boards, either a MB1379 camera daughter board or a USB webcam can be used.

Make sure the webcam is compatible with Linux®.

The available actions to control the camera preview are:

  • First tap: as preview is composed by Wayland, the first tap has to be done outside the camera preview window to recover the GTK focus.
  • Simple tap: pause/resume the camera preview.
  • Double tap: double tap anywhere on the screen to exit from this window.

More information on V4L2 and how to manage the display are available in V4L2 camera overview and Wayland_Weston_overview, respectively.

3.3 Video playback[edit]

Video Playback

Here are the available actions to control the video playback:

  • First tap: as video is composed by Wayland, the first tap has to be done outside the video playback window to recover the GTK focus.
  • Double tap: double tap anywhere on the screen to exit from this window.

More information on Gstreamer and how to manage the display are available in GStreamer_overview and Wayland_Weston_overview, respectively.

3.4 Artificial intelligence[edit]

Artificial Intelligence

This is a handwriting character recognition application:
1) It draws a character on the screen. The character is then analyzed by the firmware running on Arm® Cortex®-M4 side.
2) If the character is recognized, it is displayed on the left. Otherwise, a question mark is displayed.
3) When the recognized character is associated with an application, the application is launched:

  • A: launches audio playback
  • C: launches camera preview
  • P: displays a picture
  • V: launches a video playback
  • S: stops the launched application
  • Q: exits from the Artificial Intelligence demo.
Warning white.png Warning
It is possible to start several instances of the same application (for example three audio playbacks at the same time). However this is not recommended.

3.5 3D GPU[edit]

3D GPU

A cube rotates on the screen to demonstrate streaming video.

The available actions to control the video playback are:

  • Continuous tap: a continuous press on screen drags the cube.
  • Double tap: to exit from this window, double tap anywhere on the screen.

More information on how to manage the display are available in Wayland_Weston_overview.

3.6 Bluetooth® speaker[edit]

Bluetooth speaker

This application is able to discover Bluetooth® devices, and pair/connect to them. If an audio-capable device is connected, the message The audio BT device <your device> is connected is displayed.

First use:
1) Tap on start scan button: a scan of discoverable devices is performed during 15 seconds and a progress bar is displayed.
2) Select a device from the list and tap on connect.

If the device is already connected, the disconnect button is displayed instead.

To exit from this window, double tap anywhere on the screen.
More information on Bluetooth® are available in Bluetooth_overview.

3.7 Info menu[edit]

Info menu

Click the "i" icon on the right of the screen. It displays the menu describing how to use the demos. To exit from this window, double tap anywhere on the screen.




Back button.png Overview button.png Next button.png




<bookshelf src="Book:Getting started" />
<noinclude>

{{ArticleMainWriter | VincentA}}
{{DISPLAYTITLE:{{SUBPAGENAME}}}}
__NOTOC__
[[Category: STM32MP157x-EV1 - Let's start | 04]]</noinclude>


{| {| class="contenttable" style="margin: auto"
| colspan="9" style="text-align:center; border-color: white; background-color: white" | [[Image:STM32MP157C-EV1.png‎ | 65px | link=]]
|-
| colspan="4" style="text-align:left; border-color: white; background-color: white" | [[Getting started/STM32MP1 boards/STM32MP157x-EV1/Let's start | {{GSModuleCurrent|Let's start}}]]
| colspan="5" style="text-align:right; border-color: white; background-color: white" | [[Getting started/STM32MP1 boards/STM32MP157x-EV1/Develop on Arm® Cortex®-A7 | {{GSModuleNext|Develop on Arm® Cortex®-A7}}]]
|-
| style="border-color: white; background-color: white" | [[Image:step_category_in.png|link=]]
| style="width:110px; text-align:center; border-color: white; background-color: white" | [[Getting started/STM32MP1 boards/STM32MP157x-EV1/Let's start/Unpack the STM32MP157x-EV1 board | {{GSStepNext|Unpack the board}}]]
| style="border-color: white; background-color: white" | [[Image:step.png|link=]]
| style="width:110px; margin-top:0px; text-align:center; border-color: white; background-color: white" | [[Getting started/STM32MP1 boards/STM32MP157x-EV1/Let's start/Populate the target and boot the image | {{GSStepNext|Populate the target and boot the image}}]]
| style="border-color: white; background-color: white" | [[Image:step.png|link=]]
| style="width:110px; text-align:center; border-color: white; background-color: white" | [[Getting started/STM32MP1 boards/STM32MP157x-EV1/Let's start/Execute basic commands |{{GSStepNext|Execute basic commands}}]]
| style="border-color: white; background-color: white" | [[Image:step.png|link=]]
| style="width:110px; text-align:center; border-color: white; background-color: white" | [[Getting started/STM32MP1 boards/STM32MP157x-EV1/Let's start/Use the demo launcher | {{GSStepCurrent|Use the demo launcher}}]]
| style="border-color: white; background-color: white" | [[Image:step_category_out.png|link=]]
|}<br>

==Overview==
This article gives information about the Demo Launcher application. The Demo Launcher starts by default in the Starter Package. This application is written in python3 and uses GTK to display the user interface. A touchscreen is required to control the application.

{{:GTK_demo_launcher}}
<br>

{| class="contenttable" style="margin: auto"
| style="border-color: white; background-color: white; width:120px; text-align:left" | [[Image:back_button.png|link=Getting started/STM32MP1 boards/STM32MP157x-EV1/Let's start/Execute basic commands]]
| style="border-color: white; background-color: white; width:360px; text-align:center" | [[Image:overview_button.png|link=Getting started/STM32MP1 boards/STM32MP157x-EV1]]
| style="border-color: white; background-color: white; width:120px; text-align:right" | [[Image:next_button.png|link=Getting started/STM32MP1 boards/STM32MP157x-EV1/Develop on Arm® Cortex®-A7]]
|}

<noinclude>

{{DISPLAYTITLE:{{SUBPAGENAME}}}}
__NOTOC__
{{PublicationRequestId | Auto}}
[[Category:STM32MP157x-EV1 - Let's start | 04]]</noinclude>
Line 1: Line 1:
 
<bookshelf src="Book:Getting started" />
 
<bookshelf src="Book:Getting started" />
<noinclude>
 
{{ArticleMainWriter | VincentA}}
 
{{DISPLAYTITLE:{{SUBPAGENAME}}}}
 
__NOTOC__
 
[[Category: STM32MP157x-EV1 - Let's start | 04]]
 
</noinclude>
 
 
 
{| class="contenttable" style="margin: auto"
 
{| class="contenttable" style="margin: auto"
 
| colspan="9" style="text-align:center; border-color: white; background-color: white" | [[Image:STM32MP157C-EV1.png‎ | 65px | link=]]
 
| colspan="9" style="text-align:center; border-color: white; background-color: white" | [[Image:STM32MP157C-EV1.png‎ | 65px | link=]]
Line 35: Line 28:
 
| style="border-color: white; background-color: white; width:120px; text-align:right" | [[Image:next_button.png|link=Getting started/STM32MP1 boards/STM32MP157x-EV1/Develop on Arm® Cortex®-A7]]
 
| style="border-color: white; background-color: white; width:120px; text-align:right" | [[Image:next_button.png|link=Getting started/STM32MP1 boards/STM32MP157x-EV1/Develop on Arm® Cortex®-A7]]
 
|}
 
|}
  +
  +
<noinclude>
  +
{{DISPLAYTITLE:{{SUBPAGENAME}}}}
  +
__NOTOC__
  +
{{PublicationRequestId | Auto}}
  +
[[Category:STM32MP157x-EV1 - Let's start | 04]]
  +
</noinclude>