This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Overview[edit source]
This first step explains how to unpack the STM32MP157x-EV1 Evaluation board and the additional equipment you need.
The following block diagram provides high-level information on how to connect them together.
Out-of-the-box board[edit source]
Required equipment[edit source]
The following table lists the equipment required to start playing with your STM32MP157x-EV1 board.
Some of them are delivered within the STM32MP157x-EV1 Evaluation board. The others need to be purchased separately.
STM32MP157x-EV1 Evaluation board | Full-featured board for STM32MP15 microprocessor devices | Delivered |
MicroSD card | To be populated with the OpenSTLinux Distribution (Linux software) and providing extra storage capacity. A 2-Gbyte minimum microSD card is needed |
Delivered |
5V/3A power supply | The power supply should be able to output 5V / 3A (15W) | Delivered |
Micro USB Type-B to USB Type-A cable | Used to connect the STM32MP157x-EV1 Evaluation board to the PC through the USB micro-B (ST-LINK/V2-1) |
Not delivered |
Micro USB Type-B to USB Type-A cable | Used to connect the STM32MP157x-EV1 Evautation board to an USB OTG device. | Not delivered |
Laptop | A Linux PC running Ubuntu 16.04 is required. | Not delivered |
Ethernet cable (optional) | Used to connect the STM32MP157x-EV1 Evaluation board through ssh | Not delivered |
Connection[edit source]
- Connect your laptop to the board ST-LINK/V2-1 port through the micro USB Type-B to USB Type-A cable.
- Connect the power supply.
- Connect your laptop to the board USB Type-C™ OTG port through the micro USB Type-B to USB Type-A.
- Optionally connect your Ethernet network to the board Ethernet port through the Ethernet cable.
- Remove JP1 jumper and place JP4 and JP5 jumpers as shown below to enable debugging through ST-LINK/V2-1.