Difference between revisions of "Getting started/STM32MP1 boards/STM32MP157x-EV1/Let's start/Populate the target and boot the image"

[quality revision] [quality revision]
m
m (Boot the board)
 
STM32MP157C-EV1.png
Let's start Develop on Arm® Cortex®-A7
Step category in.png Unpack the board Step.png Populate the target and boot the image Step.png Execute basic commands Step.png Use the demo launcher Step category out.png


1 Overview[edit]

This stage step explains how to get the Starter Package, then install and boot the STM32MP15 Evaluation boards with the Starter Package.

2 Open a terminal[edit]

Open a terminal on the host computer.

Ubuntu terminal

All the commands preceded by PC $> have to be executed from the host computer terminal.

  • Create your STM32MPU workspace directory on your host computer
PC $> mkdir $HOME/STM32MPU_workspace
PC $> cd $HOME/STM32MPU_workspace

3 Check the host computer Internet access[edit]

  • An Internet access through http and https protocols must be provided.

The command below allows to check for Internet access through http/https protocols:

PC $> wget -q www.google.com && echo "Internet access over HTTP/HTTPS is OK !" || echo "No internet access over HTTP/HTTPS ! You may need to set up a proxy."

If an 'OK' message is returned, the network is well configured.
In such case, skip the rest of this section.

Any other likely situation indicates the need for a proxy for http/https protocols.
The best solution to set a proxy for http/https protocols is via the shell variables http_proxy and https_proxy:

PC $> export http_proxy=http://<MyProxyLogin>:<MyProxyPassword>@<MyProxyServerUrl>:<MyProxyPort>
PC $> export https_proxy=http://<MyProxyLogin>:<MyProxyPassword>@<MyProxyServerUrl>:<MyProxyPort>

Check again the Internet access with command:

PC $> wget -q www.google.com && echo "Internet access over HTTP/HTTPS is OK !" || echo "No internet access over HTTP/HTTPS ! You may need to set up a proxy."

4 Install the tools[edit]

4.1 STM32CubeProgrammer[edit]

  • Create your STM32MPU tools directory on your host computer
PC $> mkdir $HOME/STM32MPU_workspace/STM32MPU-Tools
PC $> mkdir $HOME/STM32MPU_workspace/STM32MPU-Tools/STM32CubeProgrammer-x.y.z
  • Create a temporary directory in your STM32MPU workspace
PC $> mkdir $HOME/STM32MPU_workspace/tmp
Warning.png ecosystem release ≥ v3.0.0 More info.png requires STM32CubeProgrammer V2.7 or upper
  • Uncompress the archive file to get the STM32CubeProgrammer installers
PC $> cd $HOME/STM32MPU_workspace/tmp
PC $> unzip SetupSTM32CubeProgrammer.zip
  • Execute the Linux® installer, which guides you through the installation process. Select "$HOME/STM32MPU-Tools/STM32CubeProgrammer-x.y.z" as the installation directory, when it's requested by the installer
PC $> ./SetupSTM32CubeProgrammer-x.y.z.linux

Screenshots, done with STM32CubeProgrammer V2.7.0, are given as examples below:

Splash screen
Welcome page
Installation path
  • Add the STM32CubeProgrammer binary path to your PATH environment variable
export PATH=$HOME/STM32MPU_workspace/STM32MPU-Tools/STM32CubeProgrammer-x.y.z/bin:$PATH
  • Check that the STM32CubeProgrammer tool is properly installed and accessible
PC $> STM32_Programmer_CLI --h
     -------------------------------------------------------------------
                       STM32CubeProgrammer vx.y.z                  
     -------------------------------------------------------------------

4.2 USB serial link[edit]

  • Install the libusb on your host computer
PC $> sudo apt-get install libusb-1.0-0
  • To allow STM32CubeProgrammer to access the USB port through low-level commands, proceed as follows
PC $> cd $HOME/STM32MPU_workspace/STM32MPU-Tools/STM32CubeProgrammer-x.y.z/Drivers/rules
PC $> sudo cp *.* /etc/udev/rules.d/

5 Download the image[edit]

The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA). The detailed content licenses can be found here.

Warning.png To download a package, it is recommended to be logged in to your "myst" account [1]. If, trying to download, you encounter a “403 error”, you could try to empty your browser cache to workaround the problem. We are working on the resolution of this problem.
We apologize for this inconvenience
Warning.png Only microSD card SanDisk Class 10 and UHS Speed Class 1 are verified. Others are not recommended.
  • Create your STM32MP15 Starter Package directory on your host computer
PC $> mkdir $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0
PC $> mkdir $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Starter-Package
PC $> cd $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Starter-Package
  • Download the STM32MP15-Ecosystem-v3.0.0 Starter Package to the following directory:
    $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Starter-Package
  • Uncompress the tarball file to get the binaries for the different partitions of the image, and the Flash layout files
PC $> tar xvf en.FLASH-stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31.tar.xz


6 Populate the SDCard[edit]

  • Set the boot switches (located at the back of the board) to the off position OFF position:
boot switches position to flash the board
  • Connect USB Type A to Type C cable between PC and the PC to CN16/USB_OTG port of the STM32MP157x-EV1 mother board through the USB Type A to Type C cable.
  • Power up the board.
  • Press the reset button to reset the board.
  • Launch STM32CubeProgrammer to get the GUI :
STM32CubeProgrammer GUI


  • On the right of the window, select USB (not instead of STLINK, set by default) in from the connexion connection picklist, and click on refresh the "Refresh" button. Serial Number The serial number is displayed if the USB is has been detected.
Select USB for connection with board
  • Click on "Connect"
  • Select the "Open File" tab and select choose the "FlashLayout_sdcard_stm32mp157c-ev1-trusted.tsv" file or the "FlashLayout_sdcard_stm32mp157f-ev1-trusted.tsv"" file (depending on the board) in the Starter Package installation folder ("$HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Starter-Package/stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31/images/stm32mp1/flashlayout_st-image-weston/trusted")
  • Fill the "Binaries Path" by browsing up to folder the $[Starter_Pack_Path]/images/stm32mp1 folder.
open .tsv and fill Binaries Path
  • Click on "Download" to start launch the flashing process.
  • Progress is displayed with A progress bar till indicates the process progress until a completion pop-up message is displayed.

7 Boot the board[edit]

  • Set the boot switches (located at the back of the board) to the ON position.
boot switches position to boot the board
  • Power up on the board.
  • Press the "Reset" button to reset the board.
  • After few seconds, the board starts and automatically goes through the following screens:
Warning.png Be patient for The very first boot after flash which flashing takes about 2 minminutes so be patient. It 's takes less than 20s afterward 20 seconds afterwards.
UBoot splash screen
Linux splash screen
Weston desktop
GTK demo launcher


Back button.png Overview button.png Next button.png



<bookshelf src="Book:Getting started" />

{|class="st-table"  style="text-align:center; margin: auto"
| colspan="9" style="border-style: hidden;" | [[Image:STM32MP157C-EV1.png‎ | 65px | link=]]
|-
| colspan="4" style="border-style: hidden; text-align:left;" | [[Getting started/STM32MP1 boards/STM32MP157x-EV1/Let's start | {{GSModuleCurrent|Let's start}}]]
| colspan="5" style="border-style: hidden; text-align:right;" | [[Getting started/STM32MP1 boards/STM32MP157x-EV1/Develop on Arm® Cortex®-A7 |{{GSModuleNext|Develop on Arm® Cortex®-A7}}]]
|-
| style="border-style: hidden;" | [[Image:step_category_in.png|link=]]
| style="border-style: hidden; width:110px;" | [[Getting started/STM32MP1 boards/STM32MP157x-EV1/Let's start/Unpack the STM32MP157x-EV1 board | {{GSStepNext|Unpack the board}}]]
| style="border-style: hidden;" | [[Image:step.png|link=]]
| style="border-style: hidden; width:110px;" | [[Getting started/STM32MP1 boards/STM32MP157x-EV1/Let's start/Populate the target and boot the image | {{GSStepCurrent|Populate the target and boot the image}}]]
| style="border-style: hidden;" | [[Image:step.png|link=]]
| style="border-style: hidden; width:110px;" | [[Getting started/STM32MP1 boards/STM32MP157x-EV1/Let's start/Execute basic commands |{{GSStepNext|Execute basic commands}}]]
| style="border-style: hidden;" | [[Image:step.png|link=]]
| style="border-style: hidden; width:110px;" | [[Getting started/STM32MP1 boards/STM32MP157x-EV1/Let's start/Use the demo launcher | {{GSStepNext|Use the demo launcher}}]]
| style="border-style: hidden;" | [[Image:step_category_out.png|link=]]
|}<br>

==Overview==
This stagestep explains how to get,  the Starter Package, then install and boot the STM32MP15 Evaluation boards with the Starter Package.

{{:Populate the target and boot the image}}

==Populate the SDCard==

* Set the boot switches (located at the back of the board) to the offOFF position :
[[File: STM32MP157x-EVx_jumper_flash.jpg|frame|center|link=|boot switches position to flash the board]]

* Connect USB Type A to Type C cable between PC and the PC to CN16/USB_OTG port of the STM32MP157x-EV1 mother board through the USB Type A to Type C cable.* Power up the board.

* Press the reset button to reset the board.

* Launch '''STM32CubeProgrammer''' to get the GUI : 
[[File: STM32CubePro GUI_27.png|800px|center|STM32CubeProgrammer GUI]]

* On the right, '''select USB''' (not  of the window, '''select USB''' (instead of STLINK, set by default)  in from the connexionconnection picklist, and click on refreshthe "Refresh" button. Serial Number The serial number is displayed if the USB is has been detected. 

[[File: STM32CubePro SelectUSB_27.png|800px|center|Select USB for connection with board]]

*Click on "Connect"

* Select the "Open File" tab and selectchoose the "FlashLayout_sdcard_stm32mp157{{highlight|c}}-ev1-trusted.tsv" file or the "FlashLayout_sdcard_stm32mp157{{Highlight|f}}-ev1-trusted.tsv"" file (depending on the board) in the Starter Package installation folder ("$HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Starter-Package/{{EcosystemRelease/Package | revision=latest | package=Images package | request=path}}/flashlayout_st-image-weston/trusted")

* Fill the "Binaries Path" by browsing up to folderthe $[Starter_Pack_Path]/images/stm32mp1 
folder.
[[File: STM32CubePro EV1 TSV and Binary_27.png|800px|center|open .tsv and fill Binaries Path]]

* Click on "Download" to startlaunch the flashing process. 
* Progress is displayed with progress bar tillA progress bar indicates the process progress until a completion pop-up message is displayed.

==Boot the board==
* Set the boot switches (located at the back of the board) to the ON position.

[[File: STM32MP157x-EVx_jumper_boot.jpg|frame|center|link=|boot switches position to boot the board]]
* Power upon the board.

* Press the "Reset"  button to reset the board.

* After few seconds, the board starts and automatically goes through the following screens:

{{Warning | Be patient for The very first boot after flash which flashing takes about 2 min. It's less than 20s afterward }}
minutes so be patient. It takes less than 20 seconds afterwards. }}
[[File: STM32MP1_uboot_splashscreen.png|thumb|upright=2|center|link=|UBoot splash screen]]
[[File: STM32MP1_psplash.png|thumb|upright=2|center|link=|Linux splash screen]]
[[File: STM32MP1_weston_desktop.png|thumb|upright=2|center|link=|Weston desktop]]
[[File: STM32MP1_gtk_demo_launcher.png|thumb|upright=2|center|link=|GTK demo launcher]]
<br>

{| class="st-table" style="margin: auto"
| style="border-style: hidden; width:120px; text-align:left" | [[Image:back_button.png|link=Getting started/STM32MP1 boards/STM32MP157x-EV1/Let's start/Unpack the STM32MP157x-EV1 board]]
| style="border-style: hidden; width:360px; text-align:center" | [[Image:overview_button.png|link=Getting started/STM32MP1 boards/STM32MP157x-EV1]]
| style="border-style: hidden; width:120px; text-align:right" | [[Image:next_button.png|link=Getting started/STM32MP1 boards/STM32MP157x-EV1/Let's start/Execute basic commands]]
|}
<noinclude>

[[Category:STM32MP157x-EV1 - Let's start | 02]]
{{DISPLAYTITLE:{{SUBPAGENAME}}}}
__NOTOC__
{{PublicationRequestId | Auto19647 | 2021-04-19}}</noinclude>
(12 intermediate revisions by 2 users not shown)
Line 18: Line 18:
 
<br>
 
<br>
 
==Overview==
 
==Overview==
This stage explains how to get, install and boot the STM32MP15 Evaluation boards with the Starter Package.
+
This step explains how to get the Starter Package, then install and boot the STM32MP15 Evaluation boards with the Starter Package.
 
   
 
   
 
{{:Populate the target and boot the image}}
 
{{:Populate the target and boot the image}}
Line 24: Line 24:
 
==Populate the SDCard==
 
==Populate the SDCard==
   
* Set the boot switches (located at the back of the board) to the off position :
+
* Set the boot switches (located at the back of the board) to the OFF position:
 
[[File: STM32MP157x-EVx_jumper_flash.jpg|frame|center|link=|boot switches position to flash the board]]
 
[[File: STM32MP157x-EVx_jumper_flash.jpg|frame|center|link=|boot switches position to flash the board]]
   
* Connect USB Type A to Type C cable between PC and CN16/USB_OTG port of the STM32MP157x-EV1 mother board
+
* Connect the PC to CN16/USB_OTG port of the STM32MP157x-EV1 mother board through the USB Type A to Type C cable.
* Power up the board
+
* Power up the board.
* Press the reset button to reset the board
+
* Press the reset button to reset the board.
 
* Launch '''STM32CubeProgrammer''' to get the GUI :  
 
* Launch '''STM32CubeProgrammer''' to get the GUI :  
 
[[File: STM32CubePro GUI_27.png|800px|center|STM32CubeProgrammer GUI]]
 
[[File: STM32CubePro GUI_27.png|800px|center|STM32CubeProgrammer GUI]]
   
   
* On the right, '''select USB''' (not STLINK, set by default) in the connexion picklist and click on refresh button. Serial Number is displayed if USB is detected.  
+
* On the right of the window, '''select USB''' (instead of STLINK, set by default) from the connection picklist, and click the "Refresh" button. The serial number is displayed if the USB has been detected.  
   
 
[[File: STM32CubePro SelectUSB_27.png|800px|center|Select USB for connection with board]]
 
[[File: STM32CubePro SelectUSB_27.png|800px|center|Select USB for connection with board]]
   
*Click on "Connect"
+
*Click "Connect"
   
* Select "Open File" tab and select the "FlashLayout_sdcard_stm32mp157{{highlight|c}}-ev1-trusted.tsv" file or the "FlashLayout_sdcard_stm32mp157{{Highlight|f}}-ev1-trusted.tsv"" file (depending on the board) in the Starter Package installation folder ("$HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Starter-Package/{{EcosystemRelease/Package | revision=latest | package=Images package | request=path}}/flashlayout_st-image-weston/trusted")
+
* Select the "Open File" tab and choose the "FlashLayout_sdcard_stm32mp157{{highlight|c}}-ev1-trusted.tsv" file or the "FlashLayout_sdcard_stm32mp157{{Highlight|f}}-ev1-trusted.tsv"" file (depending on the board) in the Starter Package installation folder ("$HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Starter-Package/{{EcosystemRelease/Package | revision=latest | package=Images package | request=path}}/flashlayout_st-image-weston/trusted")
   
* Fill the "Binaries Path" by browsing up to folder $[Starter_Pack_Path]/images/stm32mp1
+
* Fill the "Binaries Path" by browsing to the $[Starter_Pack_Path]/images/stm32mp1 folder.
   
 
[[File: STM32CubePro EV1 TSV and Binary_27.png|800px|center|open .tsv and fill Binaries Path]]
 
[[File: STM32CubePro EV1 TSV and Binary_27.png|800px|center|open .tsv and fill Binaries Path]]
   
* Click on "Download" to start the flashing process.  
+
* Click "Download" to launch the flashing process.  
* Progress is displayed with progress bar till completion pop-up message.
+
* A progress bar indicates the process progress until a completion pop-up message is displayed.
   
 
==Boot the board==
 
==Boot the board==
* Set the boot switches (located at the back of the board) to the ON position
+
* Set the boot switches (located at the back of the board) to the ON position.
 
[[File: STM32MP157x-EVx_jumper_boot.jpg|frame|center|link=|boot switches position to boot the board]]
 
[[File: STM32MP157x-EVx_jumper_boot.jpg|frame|center|link=|boot switches position to boot the board]]
* Power up the board
+
* Power on the board.
* Press the "Reset"  button to reset the board
+
* Press the "Reset"  button to reset the board.
* After few seconds, the board starts and automatically goes through the following screens
+
* After few seconds, the board starts and automatically goes through the following screens:
{{Warning | Be patient for very first boot after flash which takes about 2 min. It's less than 20s afterward }}
+
{{Warning | The very first boot after flashing takes about 2 minutes so be patient. It takes less than 20 seconds afterwards. }}
 
+
 
[[File: STM32MP1_uboot_splashscreen.png|thumb|upright=2|center|link=|UBoot splash screen]]
 
[[File: STM32MP1_uboot_splashscreen.png|thumb|upright=2|center|link=|UBoot splash screen]]
 
[[File: STM32MP1_psplash.png|thumb|upright=2|center|link=|Linux splash screen]]
 
[[File: STM32MP1_psplash.png|thumb|upright=2|center|link=|Linux splash screen]]
Line 73: Line 73:
 
{{DISPLAYTITLE:{{SUBPAGENAME}}}}
 
{{DISPLAYTITLE:{{SUBPAGENAME}}}}
 
__NOTOC__
 
__NOTOC__
{{PublicationRequestId | Auto}}
+
{{PublicationRequestId | 19647 | 2021-04-19}}
 
</noinclude>
 
</noinclude>