Populate the target and boot the image

< Getting started‎ | STM32MP1 boards‎ | STM32MP157x-DK2‎ | Let's start
STM32MP157X-DK2.png
Let's start Develop on Arm® Cortex®-A7
Step category in.png Unpack the board Step.png Populate the target and boot the image Step.png Execute basic commands Step.png Use the demo launcher Step category out.png


1 Overview

This step explains how to get the Starter Package, then install and boot the STM32MP15 Discovery kit with the Starter Package.


2 Open a terminal

Open a terminal on the host computer.

Ubuntu terminal

All the commands preceded by PC $> have to be executed from the host computer terminal.

  • Create your STM32MPU workspace directory on the host computer:
PC $> mkdir $HOME/STM32MPU_workspace
PC $> cd $HOME/STM32MPU_workspace

3 Check the host computer Internet access

  • An Internet access through http and https protocols must be provided.

The command below enables checking for Internet access through http/https protocols:

PC $> wget -q www.google.com && echo "Internet access over HTTP/HTTPS is OK !" || echo "No internet access over HTTP/HTTPS ! You may need to set up a proxy."

If an 'OK' message is returned, the network is correctly configured.
In this case, skip the rest of this section.

Otherwise, a proxy for http/https protocols is required.
The best solution is to set this proxy through the shell variables http_proxy and https_proxy:

PC $> export http_proxy=http://<MyProxyLogin>:<MyProxyPassword>@<MyProxyServerUrl>:<MyProxyPort>
PC $> export https_proxy=http://<MyProxyLogin>:<MyProxyPassword>@<MyProxyServerUrl>:<MyProxyPort>

Check again the Internet access using the command:

PC $> wget -q www.google.com && echo "Internet access over HTTP/HTTPS is OK !" || echo "No internet access over HTTP/HTTPS ! You may need to set up a proxy."

4 Install the tools

4.1 STM32CubeProgrammer

  • Create your STM32MPU tools directory on the host computer:
PC $> mkdir $HOME/STM32MPU_workspace/STM32MPU-Tools
PC $> mkdir $HOME/STM32MPU_workspace/STM32MPU-Tools/STM32CubeProgrammer-x.y.z
  • Create a temporary directory in your STM32MPU workspace:
PC $> mkdir $HOME/STM32MPU_workspace/tmp

STM32CubeProgrammer V2.9 recommended for ecosystem release v3.1.0 More info.png

STM32CubeProgrammer V2.8 recommended for ecosystem release v3.0.0 More info.png

  • Uncompress the archive file to get the STM32CubeProgrammer installers:
PC $> cd $HOME/STM32MPU_workspace/tmp
PC $> unzip SetupSTM32CubeProgrammer.zip
  • Execute the Linux® installer, which guides you through the installation process. Select "$HOME/STM32MPU-Tools/STM32CubeProgrammer-x.y.z" as installation directory when it is requested by the installer.
PC $> ./SetupSTM32CubeProgrammer-x.y.z.linux

The screenshots below have been obtained with old STM32CubeProgrammer V2.7.0. They are provided as examples still valid for higher version :

Splash screen
Welcome page
Installation path
  • Add the STM32CubeProgrammer binary path to your PATH environment variable:
export PATH=$HOME/STM32MPU_workspace/STM32MPU-Tools/STM32CubeProgrammer-x.y.z/bin:$PATH
  • Check that the STM32CubeProgrammer tool is properly installed and accessible:
PC $> STM32_Programmer_CLI --h
     -------------------------------------------------------------------
                       STM32CubeProgrammer vx.y.z                  
     -------------------------------------------------------------------

4.2 USB serial link

  • Install the libusb on your host computer:
PC $> sudo apt-get install libusb-1.0-0
  • To allow STM32CubeProgrammer to access the USB port through low-level commands, proceed as follows:
PC $> cd $HOME/STM32MPU_workspace/STM32MPU-Tools/STM32CubeProgrammer-x.y.z/Drivers/rules
PC $> sudo cp *.* /etc/udev/rules.d/

5 Download the image

The software package is provided AS IS, and by downloading it, you agree to be bound to the terms of the software license agreement (SLA). The detailed content licenses can be found here.

Warning white.png Warning
To download a package, it is recommended to be logged in to your "myst" account [1]. If, trying to download, you encounter a “403 error”, you could try to empty your browser cache to workaround the problem. We are working on the resolution of this problem.
We apologize for this inconvenience
Warning white.png Warning
Only microSD cards SanDisk Class 10 and UHS Speed Class 1 are verified. Others are not recommended.
5.1 For ecosystem release v3.1.0 More info.png
PC $> mkdir $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v3.1.0
PC $> mkdir $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v3.1.0/Starter-Package
PC $> cd $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v3.1.0/Starter-Package
  • Download the STM32MP15-Ecosystem-v3.1.0 Starter Package to the following directory:
    $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v3.1.0/Starter-Package
  • Uncompress the tarball file to get the binaries for the different partitions of the image, and the Flash layout files
PC $> tar xvf en.FLASH-stm32mp1-openstlinux-5-10-dunfell-mp1-21-11-17_tar.xz
5.2 For ecosystem release v3.0.0 More info.png
  • Create your STM32MP15 Starter Package directory on the host computer:
PC $> mkdir $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0
PC $> mkdir $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Starter-Package
PC $> cd $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Starter-Package
  • Download the STM32MP15-Ecosystem-v3.0.0 Starter Package to the following directory:
    $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Starter-Package
  • Uncompress the tarball file to get the binaries for the different partitions of the image, and the Flash layout files
PC $> tar xvf en.FLASH-stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31.tar.xz


6 Populate the SDCard

  • Set the boot switches (located at the back of the board) to the OFF position.
boot switches position to flash the board
  • Connect the PC to the CN7/USB_OTG port of the STM32MP157x-DK2 board through the USB Type A to Type C cable.
  • Power on the board.
  • Press the reset button to reset the board.
  • Launch STM32CubeProgrammer to get the GUI:
STM32CubeProgrammer GUI
  • On the right of the window, select USB (instead of STLINK, set by default) in the connection picklist and click the "Refresh" button. The serial number is displayed if the USB is detected. Then click "Connect".
Select USB for connection with board

For ecosystem release v3.1.0 More info.png :

  • Select the "Open File" tab and choose the "FlashLayout_sdcard_stm32mp157x-dk2-trusted.tsv" file in the Starter Package installation folder ("$HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v3.1.0/Starter-Package/stm32mp1-openstlinux-5.10-dunfell-mp1-21-11-17/images/stm32mp1/flashlayout_st-image-weston/trusted")

For ecosystem release v3.0.0 More info.png :

  • Select the "Open File" tab and choose the "FlashLayout_sdcard_stm32mp157x-dk2-trusted.tsv" file in the Starter Package installation folder ("$HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v3.0.0/Starter-Package/stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31/images/stm32mp1/flashlayout_st-image-weston/trusted")
  • Fill the "Binaries Path" by browsing to the $[Starter_Pack_Path]/images/stm32mp1 folder.
open .tsv and fill Binaries Path
  • Click "Download" to start the flashing process.
  • A progress bar indicates the process progress until a completion pop-up message is displayed.

7 Boot the board

  • Set the boot switches (located at the back of the board) to the ON position:
boot switches position to boot the board
  • Power on the board.
  • Press the "Reset "button to reset the board.
  • After few seconds, the board starts and automatically goes through the following screens
Warning white.png Warning
The very first boot after flashing takes about 2 minutes so be patient. It takes less than 20 seconds afterwards.
UBoot splash screen
Linux splash screen
Weston desktop
GTK demo launcher
  • If the board power supply does not supply enough current (3A), the red LED indicates the issue following the rules below:
LED blinking mode Console message Boot process
Twice WARNING 500mA power supply detected

Current too low, use a 3A power supply!

Continue and red LED stays ON
3 times WARNING 1500mA power supply detected

Current too low, use a 3A power supply!

Continue and red LED stays ON
forever ERROR USB TYPE-C connection in unattached mode

Check that USB TYPE-C cable is correctly plugged

stop
forever USB TYPE-C charger not compliant with USB specification stop


Back button.png Overview button.png Next button.png