Difference between revisions of "Getting started/STM32MP1 boards/STM32MP157x-DK2/Let's start/Populate the target and boot the image"
← Getting started/STM32MP1 boards/STM32MP157x-DK2/Let's start/Populate the target and boot the image
[unchecked revision] | [quality revision] |
m (Reverted edits by Olivier Gallien (talk) to last revision by Jean-Christophe Trotin)
(Tag: Rollback)
|
m (→Populate the SDCard)
|
![]() |
||||||||
Let's start | Develop on Arm® Cortex®-A7 | |||||||
![]() |
Unpack the board |
![]() |
Populate the target and boot the image |
![]() |
Execute basic commands |
![]() |
Use the demo launcher |
![]() |
1 Overview[edit]
This stage explains how to get, install and boot the STM32MP15 Discovery kit with the Starter Package.
2 Open a terminal[edit]
Open a terminal on the host computer.
All the commands preceded by have to be executed from the host computer terminal.
- Create your STM32MPU workspace directory on the host computer:
mkdir $HOME/STM32MPU_workspace cd $HOME/STM32MPU_workspace
3 Check the host computer Internet access[edit]
- An Internet access through http and https protocols must be provided.
The command below enables checking for Internet access through http/https protocols:
wget -q www.google.com && echo "Internet access over HTTP/HTTPS is OK !" || echo "No internet access over HTTP/HTTPS ! You may need to set up a proxy."
If an 'OK' message is returned, the network is correctly configured.
In this case, skip the rest of this section.
Otherwise, a proxy for http/https protocols is required.
The best solution is to set this proxy through the shell variables http_proxy and https_proxy:
export http_proxy=http://<MyProxyLogin>:<MyProxyPassword>@<MyProxyServerUrl>:<MyProxyPort> export https_proxy=http://<MyProxyLogin>:<MyProxyPassword>@<MyProxyServerUrl>:<MyProxyPort>
Check again the Internet access using the command:
wget -q www.google.com && echo "Internet access over HTTP/HTTPS is OK !" || echo "No internet access over HTTP/HTTPS ! You may need to set up a proxy."
4 Install the tools[edit]
4.1 STM32CubeProgrammer[edit]
- Create your STM32MPU tools directory on the host computer:
mkdir $HOME/STM32MPU_workspace/STM32MPU-Tools mkdir $HOME/STM32MPU_workspace/STM32MPU-Tools/STM32CubeProgrammer-x.y.z
- Create a temporary directory in your STM32MPU workspace:
mkdir $HOME/STM32MPU_workspace/tmp
- Download STM32CubeProgrammer in the following directory
$HOME/STM32MPU_workspace/tmp
STM32CubeProgrammer V2.11 is recommended for ecosystem release v4.0.0
- Uncompress the archive file to get the STM32CubeProgrammer installers:
cd $HOME/STM32MPU_workspace/tmp unzip SetupSTM32CubeProgrammer.zip
- Execute the Linux® installer, which guides you through the installation process. Select "$HOME/STM32MPU-Tools/STM32CubeProgrammer-x.y.z" as installation directory when it is requested by the installer.
./SetupSTM32CubeProgrammer-x.y.z.linux
The screenshots below have been obtained with old STM32CubeProgrammer V2.7.0. They are provided as examples still valid for higher version :
- Add the STM32CubeProgrammer binary path to your PATH environment variable:
export PATH=$HOME/STM32MPU_workspace/STM32MPU-Tools/STM32CubeProgrammer-x.y.z/bin:$PATH
- Go inside the binary folder:
cd $HOME/STM32MPU_workspace/STM32MPU-Tools/STM32CubeProgrammer-x.y.z/bin/
- Check that the STM32CubeProgrammer tool is properly installed and accessible:
STM32_Programmer_CLI --h ------------------------------------------------------------------- STM32CubeProgrammer vx.y.z -------------------------------------------------------------------
4.2 USB serial link[edit]
- Install the libusb on your host computer:
sudo apt-get install libusb-1.0-0
- To allow STM32CubeProgrammer to access the USB port through low-level commands, proceed as follows:
cd $HOME/STM32MPU_workspace/STM32MPU-Tools/STM32CubeProgrammer-x.y.z/Drivers/rules sudo cp *.* /etc/udev/rules.d/
5 Download the image[edit]
- Create your STM32MP1 Starter Package directory on the host computer:
mkdir $HOME/STM32MPU_workspace/STM32MP1-Ecosystem-v4.0.0 mkdir $HOME/STM32MPU_workspace/STM32MP1-Ecosystem-v4.0.0/Starter-Package cd $HOME/STM32MPU_workspace/STM32MP1-Ecosystem-v4.0.0/Starter-Package
- Download the STM32MP1-Ecosystem-v4.0.0 Starter Package to the following directory:
$HOME/STM32MPU_workspace/STM32MP1-Ecosystem-v4.0.0/Starter-Package - Uncompress the tarball file to get the binaries for the different partitions of the image, and the Flash layout files
tar xvf FLASH-stm32mp1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15.tar.xz
6 Populate the SDCard[edit]
- Set the boot switches (located at the back of the board) to the off position
- Connect USB Type A to Type C cable between PC and CN7/USB_OTG port of the STM32MP157x-DK2 board
- Power up the board
- Press the reset button to reset the board
- Launch STM32CubeProgrammer to get the GUI
- On the right, select USB (not STLINK, set by default) in the connection picklist and click on "Refresh" button. Serial Number is displayed if USB is detected. Click on "Connect"
- Select "Open File" tab and select the "FlashLayout_sdcard_stm32mp157c-dk2-trusted.tsv" file in the Starter Package installation folder ("$HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v2.y.z/Starter-Package/stm32mp1-openstlinux-5.15-yocto-kirkstone-mp1-v22.06.15/images/stm32mp1/flashlayout_st-image-weston/trusted")
- Fill the "Binaries Path" by browsing up to folder $[Starter_Pack_Path]/images/stm32mp1
- Click on "Download" to start the flashing process.
- Progress is displayed with progress bar till completion popup message.
7 Boot the board[edit]
- Set the boot switches (located at the back of the board) to the ON position
- Power up the board
- Press the "Reset "button to reset the board
- After few seconds, the board starts and automatically goes through the following screens
-
- If the board power supply doesn't supply enough current (3A), the red LED indicates the issue following the rules below:
-
-
-
blink console message boot process 2 times WARNING 500mA power supply detected Current too low, use a 3A power supply!
Continue and red LED stays ON 3 times WARNING 1500mA power supply detected Current too low, use a 3A power supply!
Continue and red LED stays ON forever ERROR USB TYPE-C connection in unattached mode Check that USB TYPE-C cable is correctly plugged
stop forever USB TYPE-C charger not compliant with USB specification stop
-
-
![]() |
![]() |
![]() |
<bookshelf src="Book:Getting started" /> {| class="st-table" style="text-align:center; margin: auto" | colspan="9" style="border-style: hidden;" | [[Image:STM32MP157X-DK2.png | 80px | link=]] |- | colspan="4" style="border-style: hidden; text-align:left;" | [[Getting started/STM32MP1 boards/STM32MP157x-DK2/Let's start | {{GSModuleCurrent|Let's start}}]] | colspan="5" style="border-style: hidden; text-align:right;" | [[Getting started/STM32MP1 boards/STM32MP157x-DK2/Develop on Arm® Cortex®-A7 | {{GSModuleNext|Develop on Arm® Cortex®-A7}}]] |- | style="border-style: hidden;" | [[Image:step_category_in.png|link=]] | style="border-style: hidden; width:110px;" | [[Getting started/STM32MP1 boards/STM32MP157x-DK2/Let's start/Unpack the STM32MP157x-DK2 board | {{GSStepNext|Unpack the board}}]] | style="border-style: hidden;" | [[Image:step.png|link=]] | style="border-style: hidden; width:110px;" | [[Getting started/STM32MP1 boards/STM32MP157x-DK2/Let's start/Populate the target and boot the image | {{GSStepCurrent|Populate the target and boot the image}}]] | style="border-style: hidden;" | [[Image:step.png|link=]] | style="border-style: hidden; width:110px;" | [[Getting started/STM32MP1 boards/STM32MP157x-DK2/Let's start/Execute basic commands | {{GSStepNext|Execute basic commands}}]] | style="border-style: hidden;" | [[Image:step.png|link=]] | style="border-style: hidden; width:110px;" | [[Getting started/STM32MP1 boards/STM32MP157x-DK2/Let's start/Use the demo launcher | {{GSStepNext|Use the demo launcher}}]] | style="border-style: hidden;" | [[Image:step_category_out.png|link=]] |}<br> ==Overview== This stage explains how to get, install and boot the STM32MP15 Discovery kit with the Starter Package. {{:Populate the target and boot the image}} ==Populate the SDCard== * Set the boot switches (located at the back of the board) to the off position [[File: STM32MP157C-DK2_jumper_flash.jpg|frame|center|link=|boot switches position to flash the board]] * Connect USB Type A to Type C cable between PC and CN7/USB_OTG port of the STM32MP157x-DK2 board * Power up the board * Press the reset button to reset the board * Launch '''STM32CubeProgrammer''' to get the GUI [[File: STM32CubePro GUI_25.png|800px|center|STM32CubeProgrammer GUI]] * On the right, select USB (not STLINK, set by default) in the connection picklist and click on "Refresh" button. Serial Number is displayed if USB is detected. Click on "Connect" [[File: STM32CubePro SelectUSB_25.png|800px|center|Select USB for connection with board]] * Select "Open File" tab and select the "FlashLayout_sdcard_stm32mp157{{Highlight|c}}-dk2-trusted.tsv" file in the Starter Package installation folder ("$HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v2.y.z/Starter-Package/{{EcosystemRelease/Package | revision=latest | package=Images package | request=path}}/flashlayout_st-image-weston/trusted") * Fill the "Binaries Path" by browsing up to folder $[Starter_Pack_Path]/images/stm32mp1 [[File: STM32CubePro TSandBinaryDK2 TSV and Binary_25.png|800px|center|open .tsv and fill Binaries Path]] * Click on "Download" to start the flashing process. * Progress is displayed with progress bar till completion popup message. ==Boot the board== * Set the boot switches (located at the back of the board) to the ON position [[File: STM32MP157C-DK2_jumper_boot.jpg|frame|center|link=|boot switches position to boot the board]] * Power up the board * Press the "Reset "button to reset the board * After few seconds, the board starts and automatically goes through the following screens [[File: STM32MP1_uboot_splashscreen.png|thumb|upright=2|center|link=|UBoot splash screen]] [[File: STM32MP1_psplash.png|thumb|upright=2|center|link=|Linux splash screen]] [[File: STM32MP1_weston_desktop.png|thumb|upright=2|center|link=|Weston desktop]] [[File: STM32MP1_gtk_demo_launcher.png|thumb|upright=2|center|link=|GTK demo launcher]] :* If the board power supply doesn't supply enough current (3A), the red LED indicates the issue following the rules below: :::{| ! blink ! console message ! boot process |- | 2 times | WARNING 500mA power supply detected Current too low, use a 3A power supply! | Continue and red LED stays ON |- | 3 times | WARNING 1500mA power supply detected Current too low, use a 3A power supply! | Continue and red LED stays ON |- | forever | ERROR USB TYPE-C connection in unattached mode Check that USB TYPE-C cable is correctly plugged | stop |- | forever | USB TYPE-C charger not compliant with USB specification | stop |} <br> {| class="st-table" style="margin: auto" | style="border-style: hidden; width:120px; text-align:left" | [[Image:back_button.png|link=Getting started/STM32MP1 boards/STM32MP157x-DK2/Let's start/Unpack the STM32MP157x-DK2 board]] | style="border-style: hidden; width:360px; text-align:center" | [[Image:overview_button.png|link=Getting started/STM32MP1 boards/STM32MP157x-DK2]] | style="border-style: hidden; width:120px; text-align:right" | [[Image:next_button.png|link=Getting started/STM32MP1 boards/STM32MP157x-DK2/Let's start/Execute basic commands]] |} <noinclude> {{DISPLAYTITLE:{{SUBPAGENAME}}}} __NOTOC__ [[Category:STM32MP157x-DK2 - let's start | 02]] {{PublicationRequestId | Auto}}</noinclude>
Line 30: | Line 30: | ||
* Launch '''STM32CubeProgrammer''' to get the GUI |
* Launch '''STM32CubeProgrammer''' to get the GUI |
||
− | [[File: STM32CubePro |
+ | [[File: STM32CubePro GUI_25.png|800px|center|STM32CubeProgrammer GUI]] |
* On the right, select USB (not STLINK, set by default) in the connection picklist and click on "Refresh" button. Serial Number is displayed if USB is detected. Click on "Connect" |
* On the right, select USB (not STLINK, set by default) in the connection picklist and click on "Refresh" button. Serial Number is displayed if USB is detected. Click on "Connect" |
||
− | [[File: STM32CubePro |
+ | [[File: STM32CubePro SelectUSB_25.png|800px|center|Select USB for connection with board]] |
* Select "Open File" tab and select the "FlashLayout_sdcard_stm32mp157{{Highlight|c}}-dk2-trusted.tsv" file in the Starter Package installation folder ("$HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v2.y.z/Starter-Package/{{EcosystemRelease/Package | revision=latest | package=Images package | request=path}}/flashlayout_st-image-weston/trusted") |
* Select "Open File" tab and select the "FlashLayout_sdcard_stm32mp157{{Highlight|c}}-dk2-trusted.tsv" file in the Starter Package installation folder ("$HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v2.y.z/Starter-Package/{{EcosystemRelease/Package | revision=latest | package=Images package | request=path}}/flashlayout_st-image-weston/trusted") |
||
Line 40: | Line 40: | ||
* Fill the "Binaries Path" by browsing up to folder $[Starter_Pack_Path]/images/stm32mp1 |
* Fill the "Binaries Path" by browsing up to folder $[Starter_Pack_Path]/images/stm32mp1 |
||
− | [[File: STM32CubePro |
+ | [[File: STM32CubePro DK2 TSV and Binary_25.png|800px|center|open .tsv and fill Binaries Path]] |
* Click on "Download" to start the flashing process. |
* Click on "Download" to start the flashing process. |