Approved version. Approved on: 15:29, 7 March 2023
- Last edited one year ago ago
Unpack the STM32MP135x-DK board
< Getting started | STM32MP1 boards | STM32MP135x-DK | Let's start
1 Overview[edit]
This first step explains how to unpack the STM32MP135x-DK Discovery kit and the additional equipment you need.
The following block diagram provides high-level information on how to connect them together.
2 Out-of-the-box kit[edit]
3 Required equipment[edit]
The following table lists the equipment required to start playing with your STM32MP135x-DK board.
Some of them are delivered within the STM32MP135x-DK Discovery kit . The others need to be purchased separately.
4 Connection[edit]
- Connect your laptop to the board ST-LINK/V3E port through the micro USB Type-B to USB Type-A cable.
- Connect the USB Type-C™ to USB Type-C™ cable to the 5V/3A power supply.
- Connect your laptop to the board USB Type-C™ OTG port through the USB Type-C™ to USB Type-A cable.
- Optionally connect your Ethernet network to the board Ethernet port through the Ethernet cable.