Difference between revisions of "Gdbgui"
[unchecked revision] | [quality revision] |
m
|
m
|
Contents
1 Article purpose[edit]
This article provides the basic information needed to start using the gdbgui[1] host PC tool.
2 Introduction[edit]
The following table provides a brief description of the tool, as well as its availability depending on the software packages:
: this tool is either present (ready to use or to be activated), or can be integrated and activated on the software package.
: this tool is not present and cannot be integrated, or it is present but cannot be activated on the software package.
Tool | STM32MPU Embedded Software distribution | STM32MPU Embedded Software distribution for Android™ | ||||||
---|---|---|---|---|---|---|---|---|
Name | Category | Purpose | Starter Package | Developer Package | Distribution Package | Starter Package | Developer Package | Distribution Package |
gdbgui | Debugging tools |
gdbgui[1] runs GDB in the background to build an easy-to-use graphical user interface. It is a browser-based debugger that operates through a web browser page. Since it is based on GDB, it can be used through a JTAG or an ethernet link with gdbserver. |
![]() |
![]() |
![]() |
![]() |
![]() |
![]() |
*: The Developer Package is required to run a GDB debug session that includes all dependencies. |
3 Installing the trace and debug tool on your host PC (Ubuntu Linux distribution)[edit]
![]() |
To avoid variable conflicts, the following steps must not be executed from a console where the SDK environment is set. |
If it is not present on your Ubuntu Linux® machine, install gdbgui via the Python package installer (pip):
PC $> pip install --trusted-host pypi.python.org --cert /etc/ssl/certs/ --proxy $https_proxy --upgrade gdbgui
Note1: If pip is not already installed, install it as follows:
PC $> sudo apt-get install python-pip
Note2: Depending on your environment, the --proxy option is not mandatory; if required, please check that $https_proxy is well defined, or replace it by your environment variable in the command line.
The gdbgui binary is then installed under $HOME/.local/bin/gdbgui. You can check it by using ths following command:
PC $> which gdbgui
4 Getting started with gdbgui[edit]
4.1 Running gdbgui using gdbserver[edit]
This environment is mainly used to debug applications. The Developer Package context (SDK) is used for setup.
- Start gdbserver on your target board for the userland program you want to debug:
Board $> gdbserver host:1234 hello_world_example
- Go to the source directory path:
PC $> cd <source_file_folder_path>
- Set the SDK environment and start gdbgui:
PC $> source <Your_SDK_path>/environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi PC $> gdbgui -g $OECORE_NATIVE_SYSROOT/usr/bin/arm-ostl-linux-gnueabi/arm-ostl-linux-gnueabi-gdb
Note: In case of issue when starting gdbgui, please refer to the Error cases chapter.
- Then:
-
- Select the "Connect to gdbserver" option from the top left menu.
- Fill in the ip address of the remote target including the port.
4.2 Running gdbgui using ST-LINK[edit]
In that case, GDB with openOCD environment is used in a Developer Package context (SDK). Please refer to Running OpenOCD and GDB.
Only GDB console command will be changed:
- OpenOCD console
- No change for OpenOCD. Please refer to the command described in the above link.
- GDB console
- gdbgui must be started with an argument providing the path to the GDB version available on your target board, as well as the config setup file:
PC $> source <Your_SDK_path>/environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi PC $> gdbgui -g $OECORE_NATIVE_SYSROOT/usr/bin/arm-ostl-linux-gnueabi/arm-ostl-linux-gnueabi-gdb --gdb-args="-x <Your_full_path_to>/Setup.gdb"
Note: Please refer to GDB page for information on Setup.gdb file and how to configure it: Attach on running target or Attach on boot.
5 To go further[edit]
5.1 Execution and debug[edit]
A button to program the execution (continue, step, next), and a panel showing all debug information (signals, thread, variables, memory) can be found on the top right of the gdbgui web page.
Please refer to the gdbgui[1] web page for details.
5.2 Error cases[edit]
- socket.error: [Errno 98] Address already in use: ('127.0.0.1', 5000)
- This error occurs when an instance of gdbgui is already running in background.
- In that case, the connection to the gdbserver fails in gdbgui, and the message "remote 'g' packet reply is too long" is displayed.
- Just kill the gdbgui instance running in background to solve the issue.
6 References[edit]
== Article purpose == This article provides the basic information needed to start using the '''gdbgui'''<ref name=gdbguidotcom/> host PC tool. == Introduction == {{:Trace_and_debug_tools_assignment_table_template}}<onlyinclude> | rowspan="2" | [[Gdbgui|gdbgui]] | rowspan="2" | [[:Category:Debugging tools|Debugging tools]] | rowspan="2" style="text-align:left;" | '''gdbgui'''<ref name=gdbguidotcom>https://gdbgui.com/</ref> runs [[GDB]] in the background to build an easy-to-use graphical user interface. It is a browser-based debugger that operates through a web browser page. Since it is based on [[GDB]], it can be used through a JTAG or an ethernet link with gdbserver.<br> | style="height:240px;" | {{N}} | style="height:240px;" | {{Y}} | style="height:240px;" | {{N}}* | rowspan="2" | {{N}} | rowspan="2" | {{N}} | rowspan="2" | {{N}} |- | colspan="3" style="text-align:left;font-size:70%;" | *: ''The Developer Package is required to run a GDB debug session that includes all dependencies.'' |-</onlyinclude> |} == Installing the trace and debug tool on your host PC (Ubuntu Linux distribution) == {{Warning|To avoid variable conflicts, the following steps must not be executed from a console where the SDK environment is set.}} If it is not present on your Ubuntu Linux<sup>®</sup> machine, install gdbgui via the Python package installer (pip): {{PC$}} pip install --trusted-host pypi.python.org --cert /etc/ssl/certs/ --proxy $https_proxy --upgrade gdbgui ''Note1: If pip is not already installed, install it as follows:'' {{PC$}} sudo apt-get install python-pip ''Note2: Depending on your environment, the --proxy option is not mandatory; if required, please check that $https_proxy is well defined, or replace it by your environment variable in the command line.'' The gdbgui binary is then installed under ''$HOME/.local/bin/gdbgui''. You can check it by using ths following command: {{PC$}} which gdbgui == Getting started with gdbgui == === Running gdbgui using gdbserver === This environment is mainly used to debug applications. The Developer Package context (SDK) is used for setup. * Start gdbserver on your target board for the userland program you want to debug: {{Board$}} gdbserver host:1234 hello_world_example * Go to the source directory path: {{PC$}} cd {{orange|<''source_file_folder_path''>}} * Set the SDK environment and start '''gdbgui''': {{PC$}} source {{orange|<''Your_SDK_path''>}}/{{EcosystemRelease/Package | revision=2.0.0 | package=SDK setup script | request=name}} {{PC$}} gdbgui -g $OECORE_NATIVE_SYSROOT/{{EcosystemRelease/Package | revision=2.0.0 | package=GDB | request=path}}/{{EcosystemRelease/Package | revision=2.0.0 | package=GDB | request=name}} ''Note: In case of issue when starting gdbgui, please refer to the [[#Error cases|Error cases]] chapter.'' * Then: :* Select the "Connect to gdbserver" option from the top left menu. :* Fill in the ip address of the remote target including the port. [[File:Screenshot gdbgui.png|1000px|link=]] === Running gdbgui using ST-LINK === In that case, GDB with openOCD environment is used in a Developer Package context (SDK). Please refer to [[GDB#Running_OpenOCD_and_GDB|Running OpenOCD and GDB]]. {{highlight|Only GDB console command will be changed:}} * OpenOCD console :No change for OpenOCD. Please refer to the command described in the above link. * GDB console :'''gdbgui''' must be started with an argument providing the path to the GDB version available on your target board, as well as the config setup file: {{PC$}} source {{orange|<''Your_SDK_path''>}}/{{EcosystemRelease/Package | revision=2.0.0 | package=SDK setup script | request=name}} {{PC$}} gdbgui -g $OECORE_NATIVE_SYSROOT/{{EcosystemRelease/Package | revision=2.0.0 | package=GDB | request=path}}/{{EcosystemRelease/Package | revision=2.0.0 | package=GDB | request=name}} --gdb-args="-x {{orange|<''Your_full_path_to''>}}/Setup.gdb" ''Note: Please refer to [[GDB]] page for information on Setup.gdb file and how to configure it: [[GDB#Configuring GDB and OpenOCD for attachment on a running target|Attach on running target]] or [[GDB#Configuring GDB and OpenOCD for attachment on boot|Attach on boot]]''. == To go further == === Execution and debug === A button to program the execution (continue, step, next), and a panel showing all debug information (signals, thread, variables, memory) can be found on the top right of the gdbgui web page. Please refer to the '''gdbgui'''<ref name=gdbguidotcom/> web page for details. === Error cases === * ''socket.error: [Errno 98] Address already in use: ('127.0.0.1', 5000)'' : This error occurs when an instance of gdbgui is already running in background.<br/> : In that case, the connection to the gdbserver fails in gdbgui, and the message "remote 'g' packet reply is too long" is displayed. : Just kill the gdbgui instance running in background to solve the issue. == References ==<references /> {{ArticleBasedOnModel | Trace and debug tools article model}} {{PublicationRequestId | 10163 | 07Jan'19}} [[Category:Debugging tools]]
Line 44: | Line 44: | ||
* Set the SDK environment and start '''gdbgui''': |
* Set the SDK environment and start '''gdbgui''': |
||
{{PC$}} source {{orange|<''Your_SDK_path''>}}/{{EcosystemRelease/Package | revision=2.0.0 | package=SDK setup script | request=name}} |
{{PC$}} source {{orange|<''Your_SDK_path''>}}/{{EcosystemRelease/Package | revision=2.0.0 | package=SDK setup script | request=name}} |
||
− | {{PC$}} gdbgui -g |
+ | {{PC$}} gdbgui -g {{EcosystemRelease/Package | revision=2.0.0 | package=GDB | request=name}} |
''Note: In case of issue when starting gdbgui, please refer to the [[#Error cases|Error cases]] chapter.'' |
''Note: In case of issue when starting gdbgui, please refer to the [[#Error cases|Error cases]] chapter.'' |
||
Line 63: | Line 63: | ||
:'''gdbgui''' must be started with an argument providing the path to the GDB version available on your target board, as well as the config setup file: |
:'''gdbgui''' must be started with an argument providing the path to the GDB version available on your target board, as well as the config setup file: |
||
{{PC$}} source {{orange|<''Your_SDK_path''>}}/{{EcosystemRelease/Package | revision=2.0.0 | package=SDK setup script | request=name}} |
{{PC$}} source {{orange|<''Your_SDK_path''>}}/{{EcosystemRelease/Package | revision=2.0.0 | package=SDK setup script | request=name}} |
||
− | {{PC$}} gdbgui -g |
+ | {{PC$}} gdbgui -g {{EcosystemRelease/Package | revision=2.0.0 | package=GDB | request=name}} |
--gdb-args="-x {{orange|<''Your_full_path_to''>}}/Setup.gdb" |
--gdb-args="-x {{orange|<''Your_full_path_to''>}}/Setup.gdb" |
||
''Note: Please refer to [[GDB]] page for information on Setup.gdb file and how to configure it: [[GDB#Configuring GDB and OpenOCD for attachment on a running target|Attach on running target]] or [[GDB#Configuring GDB and OpenOCD for attachment on boot|Attach on boot]]''. |
''Note: Please refer to [[GDB]] page for information on Setup.gdb file and how to configure it: [[GDB#Configuring GDB and OpenOCD for attachment on a running target|Attach on running target]] or [[GDB#Configuring GDB and OpenOCD for attachment on boot|Attach on boot]]''. |