Difference between revisions of "GPIO internal peripheral"
[unchecked revision] | [quality revision] |
(Merge articles)
|
m
|
Applicable for | STM32MP13x lines, STM32MP15x lines |
Contents
1 Article purpose[edit]
The purpose of this article is to
- briefly introduce the GPIO peripheral and its main features
- indicate the level of security supported by this hardware block
- explain how each instance can be allocated to the runtime contexts and linked to the corresponding software components
- explain how to configure the GPIO peripheral.
2 Peripheral overview[edit]
The GPIO peripheral is used to configure the device IO ports, also called pins or pads.
On STM32MP15x STM32MP13x lines , each GPIO instance controls 16 pins (for GPIOA to GPIOJ) GPIOG), 15 pins (for GPIOH) or 8 pins (for GPIOK and GPIOZGPIOI).
On STM32MP13x STM32MP15x lines , each GPIO instance controls 16 pins (for GPIOA to GPIOG), 15 pins (for GPIOH) GPIOJ) or 8 pins (for GPIOIGPIOK and GPIOZ).
Every IO port implements the logic shown in the image below, taken from STM32MP15 reference manuals (and the same exists in STM32MP13 reference manuals):
- The IO pin (on the right) is the physical connection to a chip external ball, soldered on the PCB. The link between each GPIO pin and each ball of the package is given in the datasheet (Datasheets for STM32MP13x lines
and Datasheets for STM32MP15x lines
).
- The Read and Write accesses allow the processor (Arm® Cortex®-A7 for for STM32MP1 Series or Arm® Cortex®-M4 for for STM32MP15x lines
) to configure the peripheral, control the IO pin and get its status.
- Alternate function (AF) links allow to connect the IO port to an internal peripheral digital line. In such a case, the IO direction is given by the line purpose: for instance, UART transmit line (TX) is an output.
-
Analog links allow to connect the IO port to an internal peripheral analog line. In such a case, the IO direction is given by the line purpose: for instance, ADC input line is an input.
- Note:
- the pull-up and pull-down resistors are disabled (by hardware) in analog mode.
- at reset, all pins are set in analog input mode to protect the device and minimize the power consumption. All unused pins should be kept in this state.
The pin configuration done by the software consists in:
- setting the pin mode in the GPIOx_MODER register:
- input or output if the pin is used as general purpose (GPIO), controlled by software.
- analog.
- alternate function (AF).
- selecting the alternate function in the GPIOx_AFRH/L register (only when the pin mode is AF):
- each IO port can support up to 16 alternate functions that are documented in the datasheet (Datasheets for STM32MP13x lines
and Datasheets for STM32MP15x lines
).
- each IO port can support up to 16 alternate functions that are documented in the datasheet (Datasheets for STM32MP13x lines
- setting the pin characteristics:
- no pull-up and no pull-down or pull-up or pull-down in the GPIOx_PUPDR register, needs to be selected to be coherent with the hardware schematics.
- push-pull or open-drain in the GPIOx_OTYPER register, needs to be selected to be coherent with the hardware schematics.
- output speed in the GPIOx_OSPEEDR register needs to be tuned to achieve the expected level of performance (rising and falling times) while limiting electromagnetic interferences (EMI) and overconsumption. As example, the table below summarizes the maximum achievable frequency for each supported IO voltage and a 30pF load:
-
GPIOx_OSPEEDR Meaning VDD=3v3 VDD=1v8
HSLV OFFVDD=1v8
HSLV ONb00 Low speed 24 MHz 11 MHz 22 MHz b01 Medium speed 83 MHz 28 MHz 79 MHz b10 High speed 125 MHz 66 MHz 101 MHz b11 Very high speed 150 MHz 70 MHz 111 MHz
- Note:
- More information is available in the IO speed settings chapter of the "Getting started with..." Application Note (AN for STM32MP13x lines
or AN5031 for STM32MP15x lines
.
- There are different IO types with different characteristics: for instance, all pads are not able to achieve 150 MHz while supplied at 3v3. Refer to the datasheet (Datasheets for STM32MP13x lines
and Datasheets for STM32MP15x lines
) to get the characteristics for each pin.
- When supplied with VDD=1v8, it is possible to enable the high speed low voltage (HSLV) pad mode for FTH (Five volt Tolerant High speed) and FTE (Five volt Tolerant Extended high speed) IO types on some peripherals via SYSCFG HSLVEN bits. Warning: As it could be destructive if used when VDD>2.7V, thanks to carefully read the HSLVEN bits documentation in STM32MP13 reference manuals or STM32MP15 reference manuals, especially the management of the OTP bit PRODUCT_BELOW_2V5 (for STM32MP1 Series) and lock mechanism (for STM32MP13x lines
only).
- More information is available in the IO speed settings chapter of the "Getting started with..." Application Note (AN for STM32MP13x lines
The table below shows all possible characteristics combinations for each pin mode:
-
pin mode GPIOx_PUPDR GPIOx_OTYPER GPIOx_OSPEEDR analog
Not applicable Not applicable Not applicable input (GPIO or AF)
no pull-up and no pull-down
or pull-down
or pull-upNot applicable Not applicable output (GPIO or AF)
or bi-directional (AF)push-pull
or open-draincf. the table above
- Note:
- 'Not applicable' means that setting this register has no effect but, in any case, there is no risk for the device.
- On the other hand, leaving a register not initialized whereas it should be, may lead to an unpredictable behavior!
2.1 Features[edit]
Refer to STM32MP13 reference manuals or STM32MP15 reference manuals for the complete features list, and to the software components, introduced below, to know which features are really implemented.
2.2 Security support[edit]
2.2.1 On STM32MP13x lines
[edit]
All banks, so GPIOA to GPIOI, are secure aware.
2.2.2 On STM32MP15x lines
[edit]
The GPIOA to GPIOK peripherals are non-secure.
The GPIOZ peripheral is secure aware.
3 Peripheral usage and associated software[edit]
3.1 Boot time[edit]
The STM32CubeMX tool allows to configure in one place the GPIO configuration that is applied at boot time and used at runtime, so it is highly recommended to use it to generate your device tree. Moreover, STM32CubeMX integrates all the information documented in the datasheet (Datasheets for STM32MP13x lines and Datasheets for STM32MP15x lines
), making this configuration step straightforward.
Since a GPIO configuration is done via atomic registers read and write, concurrent accesses from different cores must be avoided and that is why all GPIO configurations are done by the Arm® Cortex®-A7. The strategy is to progressively initialize the GPIO all along the boot chain, as soon as one boot component needs to use them:
- Most of the GPIOs used by the ROM code are directly defined in the ROM code but it is possible to change some pins muxing via dedicated words in BSEC.
- The other boot components are relying on a common binding[1] in the device tree to get the pins configuration:
- The SSBL and Linux pinctrl only configure non-secure pins.
- The FSBL configures both secure and non-secure pins.
- On STM32MP15x lines
, Linux also initializes the GPIO used by the coprocessor, via its resource manager.
- On STM32MP15x lines
3.2 Runtime[edit]
3.2.1 Overview[edit]
The GPIO configuration must not be done from different cores to avoid concurrent accesses, but this is not the case for the GPIO using: each core can manipulate IO on its own since dedicated set/clear registers are available for that.
Nevertheless, beyond the boot time, the GPIO configuration also evolves at runtime: while entering in low power mode, some GPIOs may be put back to analog input mode in order to reduce the power consumption. This is done in two times:
- the Arm® Cortex®-A7 non-secure takes care of the non-secure pins with Linux IOs pins frameworks.
- the Arm® Cortex®-A7 secure takes care of the secure pins behind PSCI secure services.
On wakeup, the boot chain restores the GPIO configuration similarly to what is done at boot time.
Let's come back to the runtime allocation...
The pins of the secure aware (see Security support) GPIO instance(s) can individually be:
- set secure and assigned to the Arm® Cortex®-A7 secure for using with OP-TEE
or
- set non-secure and assigned to the Arm® Cortex®-A7 non-secure for using in Linux® with the IOs pins frameworks
or
- set non-secure and assigned to the Arm® Cortex®-M4 for using in STM32Cube with GPIO HAL driver, on STM32MP15x lines
only
The pins of the non-secure (see Security support) GPIO instances can individually be:
- assigned to the Arm® Cortex®-A7 non-secure for using in Linux® with the IOs pins frameworks
or
- assigned to the Arm® Cortex®-M4 for using in STM32Cube with GPIO HAL driver, on STM32MP15x lines
only
3.2.2 Software frameworks[edit]
3.2.2.1 On STM32MP13x lines
[edit]
Domain | Peripheral | Software components | Comment | |
---|---|---|---|---|
OP-TEE | Linux | |||
Core/IOs | GPIO | OP-TEE GPIO driver | Linux IOs pins overview |
3.2.2.2 On STM32MP15x lines
[edit]
Internal peripherals software table template
| Core/IOs | GPIO | OP-TEE GPIO driver | Linux IOs pins overview | STM32Cube GPIO driver | |- |}
3.2.3 Peripheral configuration[edit]
The configuration is applied by the firmware running in the context to which the peripheral is assigned. The configuration by itself can be done via STM32CubeMX tool for all internal peripheral, then it can be manually completed (especially for external peripherals) according to the information given in the corresponding software framework article.
In Linux kernel, each GPIO bank is declared as a "gpio-controller" in the device tree and each pin can then be used via two different consumer frameworks:
- Pinctrl framework is used to control the alternate function (AF) selection for a given device driver, via the Pinctrl device tree configuration.
- Gpiolib framework is used to control a pin in GPIO mode from another device driver or a user space application: refer to GPIO device tree configuration for further details.
3.2.4 Peripheral assignment[edit]
3.2.4.1 On STM32MP13x lines
[edit]
Click on the right to expand the legend...
Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:
- ☐ means that the peripheral can be assigned (☑) to the given runtime context.
- ⬚ means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
- ✓ is used for system peripherals that cannot be unchecked because they are statically connected in the device.
Refer to How to assign an internal peripheral to a runtime context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possiblities might be described in STM32MP13 reference manuals.
Domain | Peripheral | Runtime allocation | Comment | ||
---|---|---|---|---|---|
Instance |
Cortex-A7 secure (OP-TEE) |
Cortex-A7 non-secure (Linux) |
|||
Core/IOs | GPIO | GPIOA-I | ✓ | ✓ | Shared (with pin granularity) |
3.2.4.2 On STM32MP15x lines
[edit]
Internal peripherals assignment table template
| rowspan="2" | Core/IOs | rowspan="2" | GPIO | GPIOA-K | | ☐ | ☐ | Shareable (with pin granularity) |- | GPIOZ | ☐ | ☐ | ☐ | Shareable (with pin granularity) |-
|}
4 How to go further[edit]
Not applicable.
5 References[edit]
<noinclude>{{ApplicableFor |MPUs list=STM32MP13x, STM32MP15x |MPUs checklist=STM32MP13x,STM32MP15x }}</noinclude> ==Article purpose== The purpose of this article is to * briefly introduce the GPIO peripheral and its main features * indicate the level of security supported by this hardware block * explain how each instance can be allocated to the runtime contexts and linked to the corresponding software components * explain how to configure the GPIO peripheral. ==Peripheral overview== The '''GPIO''' peripheral is used to configure the device IO ports, also called pins or pads. <br /><br /> On {{MicroprocessorDevice | device=1513}}, each GPIO instance controls 16 pins (for GPIOA to GPIOJ) GPIOG), 15 pins (for GPIOH) or 8 pins (for GPIOK and GPIOZGPIOI).<br /><br /> On {{MicroprocessorDevice | device=1315}}, each GPIO instance controls 16 pins (for GPIOA to GPIOG), 15 pins (for GPIOH) GPIOJ) or 8 pins (for GPIOIGPIOK and GPIOZ).<br /><br /> Every IO port implements the logic shown in the image below, taken from [[STM32MP15 resources#Reference manuals|STM32MP15 reference manuals]] (and the same exists in [[STM32MP13 resources#Reference manuals|STM32MP13 reference manuals]]): * The '''IO pin''' (on the right) is the physical connection to a chip external ball, soldered on the PCB. The link between each GPIO pin and each ball of the package is given in the datasheet ([[STM32MP13 resources#Datasheets|Datasheets]] for {{MicroprocessorDevice | device=13}} and [[STM32MP15 resources#Datasheets|Datasheets]] for {{MicroprocessorDevice | device=15}}). * The '''Read''' and '''Write''' accesses allow the processor (Arm<sup>®</sup> Cortex<sup>®</sup>-A7 for for {{MicroprocessorDevice | device=1}} or Arm<sup>®</sup> Cortex<sup>®</sup>-M4 for for {{MicroprocessorDevice | device=15}}) to configure the peripheral, control the IO pin and get its status. * '''Alternate function''' (AF) links allow to connect the IO port to an internal peripheral digital line. In such a case, the IO direction is given by the line purpose: for instance, [[USART internal peripheral|UART]] transmit line (TX) is an output. * '''Analog''' links allow to connect the IO port to an internal peripheral analog line. In such a case, the IO direction is given by the line purpose: for instance, [[ADC internal peripheral|ADC]] input line is an input.<br /><br /> [[File:IO_port.png|link=]] :Note: :* the pull-up and pull-down resistors are disabled (by hardware) in analog mode. :* at reset, all pins are set in analog input mode to protect the device and minimize the power consumption. All unused pins should be kept in this state.<br /> The pin configuration done by the software consists in: * setting the '''pin mode''' in the GPIOx_MODER register: ** '''input''' or '''output''' if the pin is used as general purpose (GPIO), controlled by software. ** '''analog'''. ** '''alternate function''' (AF). * selecting the '''alternate function''' in the GPIOx_AFRH/L register (only when the pin mode is AF): ** each IO port can support up to 16 alternate functions that are documented in the datasheet ([[STM32MP13 resources#Datasheets|Datasheets]] for {{MicroprocessorDevice | device=13}} and [[STM32MP15 resources#Datasheets|Datasheets]] for {{MicroprocessorDevice | device=15}}). * setting the '''pin characteristics''': ** '''no pull-up and no pull-down''' or '''pull-up''' or '''pull-down''' in the GPIOx_PUPDR register, needs to be selected to be coherent with the hardware schematics. ** '''push-pull''' or '''open-drain''' in the GPIOx_OTYPER register, needs to be selected to be coherent with the hardware schematics. ** '''output speed''' in the GPIOx_OSPEEDR register needs to be tuned to achieve the expected level of performance (rising and falling times) while limiting electromagnetic interferences (EMI) and overconsumption. As example, the table below summarizes the maximum achievable frequency for each supported IO voltage and a 30pF load: :{| class="st-table" width="60%" |- ! width="20%" | GPIOx_OSPEEDR !! width="20%" | Meaning !! width="20%" | VDD=3v3 !! width="20%" | VDD=1v8<br />HSLV OFF !! width="20%" | VDD=1v8<br />HSLV ON |- | align="center" | b00 || Low speed || 24 MHz || 11 MHz || 22 MHz |- | align="center" | b01 || Medium speed || 83 MHz || 28 MHz || 79 MHz |- | align="center" | b10 || High speed || 125 MHz || 66 MHz || 101 MHz |- | align="center" | b11 || Very high speed || 150 MHz || 70 MHz || 111 MHz |} :Note: :* More information is available in the '''IO speed settings''' chapter of the "''Getting started with...''" Application Note ([[STM32MP13 resources#Application notes|AN]] for {{MicroprocessorDevice | device=13}} or [[STM32MP15 resources#Application notes|AN5031]] for {{MicroprocessorDevice | device=15}}. :* There are different '''IO types''' with different characteristics: for instance, all pads are not able to achieve 150 MHz while supplied at 3v3. Refer to the datasheet ([[STM32MP13 resources#Datasheets|Datasheets]] for {{MicroprocessorDevice | device=13}} and [[STM32MP15 resources#Datasheets|Datasheets]] for {{MicroprocessorDevice | device=15}}) to get the characteristics for each pin. :* When supplied with VDD=1v8, it is possible to enable the '''high speed low voltage''' (HSLV) pad mode for FTH (Five volt Tolerant High speed) and FTE (Five volt Tolerant Extended high speed) IO types on some peripherals via [[SYSCFG internal peripheral|SYSCFG]] HSLVEN bits. '''Warning''': As it could be destructive if used when VDD>2.7V, thanks to carefully read the HSLVEN bits documentation in [[STM32MP13 resources#Reference manuals|STM32MP13 reference manuals]] or [[STM32MP15 resources#Reference manuals|STM32MP15 reference manuals]], especially the management of the OTP bit PRODUCT_BELOW_2V5 (for {{MicroprocessorDevice | device=1}}) and lock mechanism (for {{MicroprocessorDevice | device=13}} only). The table below shows all possible characteristics combinations for each '''pin mode''': :{| class="st-table" width="60%" valign="top" |- ! width="25%" | pin mode ! width="25%" | GPIOx_PUPDR ! width="25%" | GPIOx_OTYPER ! width="25%" | GPIOx_OSPEEDR |- | '''analog'''<br /> | Not applicable | Not applicable | Not applicable |- | '''input''' (GPIO or AF)<br /> | rowspan="2" | '''no pull-up and no pull-down''' <br />or '''pull-down''' <br />or '''pull-up''' | Not applicable | Not applicable |- | '''output''' (GPIO or AF) <br /> or '''bi-directional''' (AF) | '''push-pull''' <br />or '''open-drain''' | cf. the table above |- |} :Note: :* 'Not applicable' means that setting this register has no effect but, in any case, there is no risk for the device. :* On the other hand, leaving a register not initialized whereas it should be, may lead to an unpredictable behavior! ===Features=== Refer to [[STM32MP13 resources#Reference manuals|STM32MP13 reference manuals]] or [[STM32MP15 resources#Reference manuals|STM32MP15 reference manuals]] for the complete features list, and to the software components, introduced below, to know which features are really implemented.<br> ===Security support=== ==== On {{MicroprocessorDevice | device=13}} ==== All banks, so GPIOA to GPIOI, are '''secure aware'''. ==== On {{MicroprocessorDevice | device=15}} ==== The GPIOA to GPIOK peripherals are '''non-secure'''.<br /> The GPIOZ peripheral is '''secure aware'''. ==Peripheral usage and associated software== ===Boot time=== The [[STM32CubeMX]] tool allows to configure in one place the GPIO configuration that is applied at boot time and used at runtime, so it is highly recommended to use it to generate your [[Device tree|device tree]]. Moreover, [[STM32CubeMX]] integrates all the information documented in the datasheet ([[STM32MP13 resources#Datasheets|Datasheets]] for {{MicroprocessorDevice | device=13}} and [[STM32MP15 resources#Datasheets|Datasheets]] for {{MicroprocessorDevice | device=15}}), making this configuration step straightforward.<br /><br /> Since a GPIO configuration is done via atomic registers read and write, concurrent accesses from different cores must be avoided and that is why all GPIO configurations are done by the Arm<sup>®</sup> Cortex<sup>®</sup>-A7. The strategy is to progressively initialize the GPIO all along the [[Boot chain overview|boot chain]], as soon as one boot component needs to use them: * Most of the GPIOs used by the [[ROM code overview|ROM code]] are directly defined in the ROM code but it is possible to change some pins muxing via dedicated words in [[BSEC internal peripheral|BSEC]]. * The other boot components are relying on a common binding<ref>{{CodeSource | Linux kernel | Documentation/devicetree/bindings/pinctrl/st,stm32-pinctrl.yaml| Documentation/devicetree/bindings/pinctrl/st,stm32-pinctrl.yaml}}</ref> in the [[Device tree|device tree]] to get the pins configuration: ** The [[Boot chain overview|SSBL]] and Linux [[Pinctrl overview|pinctrl]] only configure non-secure pins. ** The [[Boot chain overview|FSBL]] configures both secure and non-secure pins. *** On {{MicroprocessorDevice | device=15}}, Linux also initializes the GPIO used by the coprocessor, via its [[Resource_manager_for_coprocessing#Resource_management_on_the_Cortex-M_firmware|resource manager]]. ===Runtime=== ====Overview==== The '''GPIO configuration''' must not be done from different cores to avoid concurrent accesses, but this is not the case for the '''GPIO using''': each core can manipulate IO on its own since dedicated set/clear registers are available for that.<br /> <br /> Nevertheless, beyond the boot time, the GPIO configuration also evolves at runtime: while entering in [[Power overview|low power mode]], some GPIOs may be put back to analog input mode in order to reduce the power consumption. This is done in two times: # the Arm<sup>®</sup> Cortex<sup>®</sup>-A7 non-secure takes care of the non-secure pins with Linux [[Overview of GPIO pins|IOs pins]] frameworks. # the Arm<sup>®</sup> Cortex<sup>®</sup>-A7 secure takes care of the secure pins behind [[TF-A overview#BL32|PSCI secure services]]. On wakeup, the [[Boot chain overview|boot chain]] restores the GPIO configuration similarly to what is done at boot time.<br /><br /> Let's come back to the runtime allocation...<br /><br /> The pins of the '''secure aware''' (see [[#Security support|Security support]]) GPIO instance(s) can individually be: * set secure and assigned to the Arm<sup>®</sup> Cortex<sup>®</sup>-A7 secure for using with [[OP-TEE overview|OP-TEE]] or * set non-secure and assigned to the Arm<sup>®</sup> Cortex<sup>®</sup>-A7 non-secure for using in Linux<sup>®</sup> with the [[Overview of GPIO pins|IOs pins]] frameworks or * set non-secure and assigned to the Arm<sup>®</sup> Cortex<sup>®</sup>-M4 for using in STM32Cube with [[STM32CubeMP1 architecture|GPIO HAL driver]], on {{MicroprocessorDevice | device=15}} only<br /> The pins of the '''non-secure''' (see [[#Security support|Security support]]) GPIO instances can individually be: * assigned to the Arm<sup>®</sup> Cortex<sup>®</sup>-A7 non-secure for using in Linux<sup>®</sup> with the [[Overview of GPIO pins|IOs pins]] frameworks or * assigned to the Arm<sup>®</sup> Cortex<sup>®</sup>-M4 for using in STM32Cube with [[STM32CubeMP1 architecture|GPIO HAL driver]], on {{MicroprocessorDevice | device=15}} only ====Software frameworks==== ===== On {{MicroprocessorDevice | device=13}} ===== {{:STM32MP13_internal_peripherals_software_table_template}} | Core/IOs | [[GPIO internal peripheral|GPIO]] | [[OP-TEE_overview|OP-TEE GPIO driver]] | [[Overview of GPIO pins|Linux IOs pins overview]] | |- |} ===== On {{MicroprocessorDevice | device=15}} ===== {{:Internal_peripherals_software_table_template}} | Core/IOs | [[GPIO internal peripheral|GPIO]] | [[OP-TEE_overview|OP-TEE GPIO driver]] | [[Overview of GPIO pins|Linux IOs pins overview]] | [[STM32CubeMP1 architecture|STM32Cube GPIO driver]] | |- |} ====Peripheral configuration==== The configuration is applied by the firmware running in the context to which the peripheral is assigned. The configuration by itself can be done via [[STM32CubeMX]] tool for all internal peripheral, then it can be manually completed (especially for external peripherals) according to the information given in the corresponding software framework article. In Linux kernel, each GPIO bank is declared as a "gpio-controller" in the device tree and each pin can then be used via two different consumer frameworks: * [[Pinctrl overview|Pinctrl]] framework is used to control the alternate function (AF) selection for a given device driver, via the [[Pinctrl device tree configuration]]. * [[GPIOLib overview|Gpiolib]] framework is used to control a pin in GPIO mode from another device driver or a user space application: refer to [[GPIO device tree configuration]] for further details. ====Peripheral assignment==== ===== On {{MicroprocessorDevice | device=13}} ===== {{:STM32MP13_internal_peripherals_assignment_table_template}}<section begin=stm32mp13 /> | rowspan="1" | Core/IOs | rowspan="1" | [[GPIO internal peripheral|GPIO]] | GPIOA-I | <span title="system peripheral" style="font-size:21px">✓</span> | <span title="system peripheral" style="font-size:21px">✓</span> | Shared (with pin granularity) |-<section end=stm32mp13 /> |} ===== On {{MicroprocessorDevice | device=15}} ===== {{:Internal_peripherals_assignment_table_template}}<section begin=stm32mp15 /> | rowspan="2" | Core/IOs | rowspan="2" | [[GPIO internal peripheral|GPIO]] | GPIOA-K | | <span title="assignable peripheral" style="font-size:21px">☐</span> | <span title="assignable peripheral" style="font-size:21px">☐</span> | Shareable (with pin granularity) |- | GPIOZ | <span title="assignable peripheral" style="font-size:21px">☐</span> | <span title="assignable peripheral" style="font-size:21px">☐</span> | <span title="assignable peripheral" style="font-size:21px">☐</span> | Shareable (with pin granularity) |-<section end=stm32mp15 /> |} ==How to go further== Not applicable. ==References==<references/> <noinclude> [[Category:IOs pins peripherals]] {{ArticleBasedOnModel | Internal peripheral article model}} {{PublicationRequestId | 8785 | 2018-09-18 | AlainF}} </noinclude>
Line 12: | Line 12: | ||
==Peripheral overview== |
==Peripheral overview== |
||
The '''GPIO''' peripheral is used to configure the device IO ports, also called pins or pads. <br /><br /> |
The '''GPIO''' peripheral is used to configure the device IO ports, also called pins or pads. <br /><br /> |
||
− | + | On {{MicroprocessorDevice | device=13}}, each GPIO instance controls 16 pins (for GPIOA to GPIOG), 15 pins (for GPIOH) or 8 pins (for GPIOI).<br /> |
|
On {{MicroprocessorDevice | device=15}}, each GPIO instance controls 16 pins (for GPIOA to GPIOJ) or 8 pins (for GPIOK and GPIOZ).<br /><br /> |
On {{MicroprocessorDevice | device=15}}, each GPIO instance controls 16 pins (for GPIOA to GPIOJ) or 8 pins (for GPIOK and GPIOZ).<br /><br /> |
||
− | |||
− | |||
Every IO port implements the logic shown in the image below, taken from [[STM32MP15 resources#Reference manuals|STM32MP15 reference manuals]] (and the same exists in [[STM32MP13 resources#Reference manuals|STM32MP13 reference manuals]]): |
Every IO port implements the logic shown in the image below, taken from [[STM32MP15 resources#Reference manuals|STM32MP15 reference manuals]] (and the same exists in [[STM32MP13 resources#Reference manuals|STM32MP13 reference manuals]]): |
||
* The '''IO pin''' (on the right) is the physical connection to a chip external ball, soldered on the PCB. The link between each GPIO pin and each ball of the package is given in the datasheet ([[STM32MP13 resources#Datasheets|Datasheets]] for {{MicroprocessorDevice | device=13}} and [[STM32MP15 resources#Datasheets|Datasheets]] for {{MicroprocessorDevice | device=15}}). |
* The '''IO pin''' (on the right) is the physical connection to a chip external ball, soldered on the PCB. The link between each GPIO pin and each ball of the package is given in the datasheet ([[STM32MP13 resources#Datasheets|Datasheets]] for {{MicroprocessorDevice | device=13}} and [[STM32MP15 resources#Datasheets|Datasheets]] for {{MicroprocessorDevice | device=15}}). |