- Last edited 9 months ago ago
FMC internal peripheral
Contents
1 Article purpose[edit]
The purpose of this article is to
- briefly introduce the FMC peripheral and its main features
- indicate the level of security supported by this hardware block
- explain how each instance can be allocated to the runtime contexts and linked to the corresponding software components
- explain, when needed, how to configure the FMC peripheral.
2 Peripheral overview[edit]
The FMC peripheral includes two memory controllers:
- The NOR/PSRAM memory controller
- The NAND memory controller
2.1 NOR/PSRAM memory controller (or external bus interface controller)[edit]
The FMC NOR/PSRAM memory controller is used to interface static memory devices, but it is also used to interface Ethernet devices, LCD devices, .... .
The FMC NOR/PSRAM controller generates the appropriate signal timings to drive the following types of memories:
- Asynchronous SRAM, FRAM and ROM
- 8 bits
- 16 bits
- PSRAM (CellularRAM™)
- Asynchronous mode
- Burst mode for synchronous accesses with configurable option to split burst access when crossing boundary page for CRAM 1.5.
- Multiplexed or non-multiplexed
- NOR Flash memory
- Asynchronous mode
- Burst mode for synchronous accesses
- Multiplexed or non-multiplexed
The FMC NOR/PSRAM controller supports a wide range of devices through programmable timings among which:
- Programmable wait states (up to 15)
- Programmable bus turnaround cycles (up to 15)
- Programmable output enable and write enable delays (up to 15)
- Independent read and write timings and protocol to support the widest variety of memories and timings
- Programmable continuous clock output.
The FMC NOR/PSRAM controller supports up to four external devices.
2.2 NAND Flash controller[edit]
The FMC NAND Flash controller is used to interface STM32 MPU with SLC 8-bit or 16-bit NAND Flash memory devices.
The FMC NAND Flash controller supports:
- Programmable error correction capability (ECC) using BCH8 code, BCH4 code or Hamming code
- Programmable page size of 2048, 4096 and 8192 bytes
- Programmable memory timings
- Multiple dice per package.
2.3 Features[edit]
Refer to STM32MP13 reference manuals or STM32MP15 reference manuals for the complete list of features, and to the software components, introduced below, to know which features are really implemented.
2.4 Security support[edit]
2.4.1 On STM32MP13x lines [edit]
The FMC is a secure peripheral (under ETZPC control).
2.4.2 On STM32MP15x lines [edit]
The FMC is a non-secure peripheral.
3 Peripheral usage and associated software[edit]
3.1 Boot time[edit]
The FMC NAND Flash controller is the boot device that supports serial boot for Flash programming with STM32CubeProgrammer.
3.2 Runtime[edit]
3.2.1 Overview[edit]
The FMC peripheral can be allocated to:
- the Arm® Cortex®-A7 secure context, on STM32MP13x lines only, but this is not supported in OpenSTLinux.
or
- the Arm® Cortex®-A7 non-secure core to be controlled in Linux® by the MTD framework
or
- the Arm® Cortex®-M4, on STM32MP15x lines only, to be controlled in STM32Cube MPU Package by FMC HAL driver
Chapter #Peripheral assignment describes which instance can be assigned to which context.
3.2.2 Software frameworks[edit]
3.2.2.1 On STM32MP13x lines [edit]
Domain | Peripheral | Software components | Comment | |
---|---|---|---|---|
OP-TEE | Linux | |||
Mass storage | FMC | Linux MTD Framework |
3.2.2.2 On STM32MP15x lines [edit]
Domain | Peripheral | Software components | Comment | ||
---|---|---|---|---|---|
OP-TEE | Linux | STM32Cube | |||
Mass storage | FMC | Linux MTD Framework | STM32Cube FMC driver |
3.2.3 Peripheral configuration[edit]
The configuration is applied by the firmware running in the context to which the peripheral is assigned. The configuration can be done alone via the STM32CubeMX tool for all internal peripherals, and then manually completed (particularly for external peripherals), according to the information given in the corresponding software framework article.
For Linux kernel configuration, please refer to FMC device tree configuration
3.2.4 Peripheral assignment[edit]
3.2.4.1 On STM32MP13x lines [edit]
Click on the right to expand the legend...
Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:
- ☐ means that the peripheral can be assigned (☑) to the given runtime context.
- ⬚ means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
- ✓ is used for system peripherals that cannot be unchecked because they are statically connected in the device.
Refer to How to assign an internal peripheral to an execution context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possiblities might be described in STM32MP13 reference manuals.
Domain | Peripheral | Runtime allocation | Comment | ||
---|---|---|---|---|---|
Instance | Cortex-A7 secure (OP-TEE) |
Cortex-A7 non-secure (Linux) | |||
Mass storage | FMC | FMC | ⬚ | ☐ | Assignment (single choice) |
3.2.4.2 On STM32MP15x lines [edit]
Click on the right to expand the legend...
Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:
- ☐ means that the peripheral can be assigned (☑) to the given runtime context.
- ⬚ means that the peripheral can be assigned to the given runtime context, but this configuration is not supported in STM32 MPU Embedded Software distribution.
- ✓ is used for system peripherals that cannot be unchecked because they are statically connected in the device.
Refer to How to assign an internal peripheral to an execution context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possiblities might be described in STM32MP15 reference manuals.
Domain | Peripheral | Runtime allocation | Comment | |||
---|---|---|---|---|---|---|
Instance | Cortex-A7 secure (OP-TEE) |
Cortex-A7 non-secure (Linux) |
Cortex-M4 (STM32Cube) | |||
Mass storage | FMC | FMC | ☐ | ☐ | Assignment (single choice) |