Difference between revisions of "EXTI internal peripheral"

[quality revision] [quality revision]
m
 
m


Template:ArticleMainWriter Template:ArticleApprovedVersion


1 Peripheral overview[edit]

The EXTI peripheral is used to get an interrupt when a GPIO is toggling. It can also wake up the system from Stop low power mode, by means of the PWR internal peripheral when a wake up event occurs, before (eventualy - see the note below) propagating an interrupt to the client processor (Cortex-A7 GIC or Cortex-M4 NVIC). The wake up events can be internal (from other IPs clocked by the LSE, LSI or HSI from RCC), or external (from GPIO).

Notice that:

  • Up to 16 GPIO pins can be configured as external interrupts: for each index between 0 and 15, one EXTI can be selected among all banks (EXTI<index> = GPIO<one_bank><index>).
  • The 16 GPIO and 4 internal peripheral events can generate interrupts connected to the GIC and NVIC. All the other internal peripheral events can wake up the system, but the EXTI does not generate any interrupt to the GIC or NVIC for them; in such cases, another peripheral interrupt has to be used as a trigger via the GIC or NVIC.

1.1 Features[edit]

Refer to STM32MP15 reference manuals for the complete feature list, and to the software components, introduced below, to see which features are implemented.

1.2 Security support[edit]

The EXTI is a secure peripheral. By default, at reset, all EXTI wake up events are non-secure.

2 Peripheral usage and associated software[edit]

2.1 Boot time[edit]

The EXTI is not used by the boot chain, but is configured during Linux initialization. Since wake-up event configuration is done via register bit-field reads and writes, concurrent accesses from Linux and the co-processor are not possible at boot time:

  • Linux configures all EXTI events during their respective consumer driver probing
  • The co-processor uses the resource management mechanisms to request and configure the EXTI events it needs.

The article STM32MP15 interrupts gives more information on the EXTI configuration strategy.

2.2 Runtime[edit]

2.2.1 Overview[edit]

The EXTI can be allocated to:

  • the Cortex-A7 non-secure for use in Linux with the interrupts framework

or


2.2.2 Software frameworks[edit]

Domain Peripheral Software frameworks Comment
Cortex-A7
secure
(OP-TEE)
Cortex-A7
non-secure
(Linux)
Cortex-M4

(STM32Cube)
Core/Interrupts EXTI Linux interrupt framework STM32Cube EXTI driver

2.2.3 Peripheral configuration[edit]

The configuration is applied by the firmware running in the context to which the peripheral is assigned. The configuration can be done alone via the STM32CubeMX tool for all internal peripherals. It can then be manually completed (particularly for external peripherals), according to the information given in the corresponding software framework article.

2.2.4 Peripheral assignment[edit]

Internal peripherals

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned () to the given runtime context.
  • is used for system peripherals that cannot be unchecked because they are statically connected in the device.

Refer to How to assign an internal peripheral to a runtime context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possiblities might be described in STM32MP15 reference manuals.

Domain Peripheral Runtime allocation Comment
Instance Cortex-A7
secure
(OP-TEE)
Cortex-A7
non-secure
(Linux)
Cortex-M4

(STM32Cube)
Core/Interrupts EXTI EXTI Shareable (multiple choices supported)

3 How to go further[edit]

4 References[edit]

<noinclude>

{{ArticleBasedOnModel | [[Internal peripheral article model]]}}
{{ArticleMainWriter | GeraldB}}
{{ArticleApprovedVersion | GeraldB | AlexandreT, LudovicB (12Jul'18) | No previous approved version | PhilipS - 18Sep'18 - 8793 | 25Sep'18}}

[[Category:Interrupts peripherals]]
{{ReviewsComments|JCT 1840: alignment needed with the last version of the model [[Internal peripheral article model]]<br>

[[Category:ToBeAlignedWithModel]]
}}</noinclude>


==Peripheral overview==
The '''EXTI''' peripheral is used to get an interrupt when a GPIO is toggling. It can also wake up the system from Stop [[Power overview|low power mode]], by means of the [[PWR internal peripheral]] when a wake up event occurs, before (eventualy - see the note below) propagating an interrupt to the client processor (Cortex-A7 [[GIC internal peripheral|GIC]] or Cortex-M4 [[NVIC internal peripheral|NVIC]]). The wake up events can be internal (from other IPs clocked by the LSE, LSI or HSI from [[RCC internal peripheral|RCC]]), or external (from [[GPIO internal peripheral|GPIO]]).<br /><br />

Notice that:
* Up to 16 GPIO pins can be configured as external interrupts: for each index between 0 and 15, one EXTI can be selected among all banks (EXTI<index> = GPIO<one_bank><index>).
* The 16 GPIO and 4 internal peripheral events can generate interrupts connected to the GIC and NVIC. All the other internal peripheral events can wake up the system, but the EXTI does not generate any interrupt to the GIC or NVIC for them; in such cases, another peripheral interrupt has to be used as a trigger via the GIC or NVIC.

===Features===
Refer to [[STM32MP15 resources#Reference manuals|STM32MP15 reference manuals]] for the complete feature list, and to the software components, introduced below, to see which features are implemented.<br>


===Security support===
The EXTI is a '''secure''' peripheral.
By default, at reset, all EXTI wake up events are non-secure.

==Peripheral usage and associated software==
===Boot time===
The EXTI is not used by the boot chain, but is configured during Linux initialization. Since wake-up event configuration is done via register bit-field reads and writes, concurrent accesses from Linux and the co-processor are not possible at boot time:
* Linux configures all EXTI events during their respective consumer driver probing
* The co-processor uses the [[Resource manager for coprocessing|resource management]] mechanisms to request and configure the EXTI events it needs.
The article [[STM32MP15 interrupts]] gives more information on the EXTI configuration strategy.

===Runtime===
====Overview====
The EXTI can be allocated to:
* the Cortex-A7 non-secure for use in Linux with the [[Interrupt overview|interrupts]] framework
or
* the Cortex-M4 for using in STM32Cube with the [[STM32CubeMP1 architecture|EXTI HAL driver]]

{{InternalInfo| OP-TEE may also need to use some EXTI wake-up events. To achieve this, Linux relies on a secure service for wake-up event control from its EXTI driver, instead of direct reliance on register accesses. Once the EXTI is configured, each core (Cortex-A7 Secure, Cortex-A7 Non-Secure and Cortex-M4) can operate concurrently on the EXTI -edge pending registers- because those registers are cleared writing a 1 on the concerned EXTI, with secure protection on the secured ones}}

====Software frameworks====
{{:Internal_peripherals_software_table_template}}
 | Core/Interrupts
 | [[EXTI internal peripheral|EXTI]]
 | 
 | [[Interrupt overview|Linux interrupt framework]]
 | [[STM32CubeMP1 architecture|STM32Cube EXTI driver]]
 |
 |-
 |}

====Peripheral configuration====
The configuration is applied by the firmware running in the context to which the peripheral is assigned. The configuration can be done alone via the [[STM32CubeMX]] tool for all internal peripherals. It can then be manually completed (particularly for external peripherals), according to the information given in the corresponding software framework article.

====Peripheral assignment====
{{:Internal_peripherals_assignment_table_template}}<onlyinclude>

 | rowspan="1" | Core/Interrupts
 | rowspan="1" | [[EXTI internal peripheral|EXTI]]
 | EXTI
 |
 | <span title="assignable peripheral" style="font-size:21px"></span>

 | <span title="assignable peripheral" style="font-size:21px"></span>

 | Shareable (multiple choices supported)
 |-</onlyinclude>

 |}


==How to go further==

==References==<references/>
Line 66: Line 66:
 
  </onlyinclude>
 
  </onlyinclude>
 
  |}
 
  |}
 
==How to go further==
 
 
==References==
 
<references/>
 

Attachments

Discussions