Difference between revisions of "DMAMUX internal peripheral"

[quality revision] [quality revision]
m
 
 
Template:ArticleMainWriter Template:ArticleApprovedVersion

1 Article purpose[edit]

The purpose of this article is to:

  • briefly introduce the DMAMUX peripheral and its main features
  • indicate the level of security supported by this hardware block
  • explain how each instance can be allocated to the three runtime contexts and linked to the corresponding software components
  • explain, when necessary, how to configure the DMAMUX peripheral.

2 Peripheral overview[edit]

The DMAMUX peripheral is used to perform requestor line (or device controller) selection for each channel from DMA instances: there is a single DMAMUX instance to cover both DMA1 and DMA2.

2.1 Features[edit]

Refer to the STM32MP15 reference manuals for the complete list of features, and to the software components, introduced below, to see which features are implemented.

2.2 Security support[edit]

The DMAMUX is a non secure peripheral.

3 Peripheral usage and associated software[edit]

3.1 Boot time[edit]

The DMAMUX is not used at boot time.

3.2 Runtime[edit]

3.2.1 Overview[edit]

The DMAMUX manages DMA1 and DMA2 requestor line selection via different registers so it is possible to concurrently access to DMAMUX from Cortex®-A7 non-secure and Cortex®-M4 contexts, as far as each core is only configuring the requestor lines for the DMA instances (DMA1 and/or DMA2) assigned to itself.

Finally, DMAMUX can be allocated to:

  • the Arm® Cortex®-A7 non-secure core to be controlled in Linux® by the dmaengine framework

or

  • the Arm® Cortex®-M4 to be controlled in STM32Cube MPU Package by the DMA HAL driver

3.2.2 Software frameworks[edit]

Domain Peripheral Software components Comment
OP-TEE Linux STM32Cube
Core/DMA DMAMUX Linux dmaengine framework STM32Cube DMAMUX driver

3.2.3 Peripheral configuration[edit]

The configuration is applied by the firmware running in the context to which the peripheral is assigned. The configuration can be done alone via the STM32CubeMX tool for all internal peripherals, and then manually completed (particularly for external peripherals), according to the information given in the corresponding software framework article.

3.2.4 Peripheral assignment[edit]

Internal peripherals

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned () to the given runtime context.
  • is used for system peripherals that cannot be unchecked because they are statically connected in the device.

Refer to How to assign an internal peripheral to a runtime context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possiblities might be described in STM32MP15 reference manuals.

Domain Peripheral Runtime allocation Comment
Instance Cortex-A7
secure
(OP-TEE)
Cortex-A7
non-secure
(Linux)
Cortex-M4

(STM32Cube)
Core/DMA DMAMUX DMAMUX Shareable (multiple choices supported)


<noinclude>

{{ArticleBasedOnModel| [[Internal peripheral article model]]}}
{{ArticleMainWriter|Pierre-YvesM}}
{{ ArticleApprovedVersion|Pierre-YvesM| Pierre-YvesM, GeraldB |No previous approved version| AlainF - 10Oct'18 - 9110 | 12Oct'18 }} 
[[Category:DMA peripherals]]</noinclude>

==Article purpose==
The purpose of this article is to:
* briefly introduce the DMAMUX peripheral and its main features
* indicate the level of security supported by this hardware block
* explain how each instance can be allocated to the three runtime contexts and linked to the corresponding software components
* explain, when necessary, how to configure the DMAMUX peripheral.

==Peripheral overview==
The '''DMAMUX''' peripheral is used to perform requestor line (or device controller) selection for each channel from [[DMA internal peripheral|DMA]] instances: there is a single DMAMUX instance to cover both DMA1 and DMA2.

===Features===
Refer to the [[STM32MP15 resources#Reference manuals|STM32MP15 reference manuals]] for the complete list of features, and to the software components, introduced below, to see which features are implemented.

===Security support===
The DMAMUX is a '''non secure''' peripheral.

==Peripheral usage and associated software==
===Boot time===
The DMAMUX is not used at boot time.

===Runtime===
====Overview====
The DMAMUX manages DMA1 and DMA2 requestor line selection via different registers so it is possible to concurrently access to DMAMUX from Cortex<sup>&reg;</sup>-A7 non-secure and Cortex<sup>&reg;</sup>-M4 contexts, as far as each core is only configuring the requestor lines for the [[DMA internal peripheral|DMA]] instances (DMA1 and/or DMA2) assigned to itself.<br />


Finally, DMAMUX can be allocated to:
* the Arm<sup>&reg;</sup> Cortex<sup>&reg;</sup>-A7 non-secure core to be controlled in Linux<sup>&reg;</sup> by the [[Dmaengine overview|dmaengine]] framework
or
* the Arm<sup>&reg;</sup> Cortex<sup>&reg;</sup>-M4 to be controlled in STM32Cube MPU Package by the [[STM32CubeMP1 architecture|DMA HAL driver]]

====Software frameworks====
{{:Internal_peripherals_software_table_template}}
 | Core/DMA
 | [[DMAMUX internal peripheral|DMAMUX]]
 | 
 | [[Dmaengine overview|Linux dmaengine framework]]
 | [[STM32CubeMP1 architecture|STM32Cube DMAMUX driver]]
 |
 |-
 |}

====Peripheral configuration====
The configuration is applied by the firmware running in the context to which the peripheral is assigned. The configuration can be done alone via the [[STM32CubeMX]] tool for all internal peripherals, and then manually completed (particularly for external peripherals), according to the information given in the corresponding software framework article.

====Peripheral assignment====
{{:Internal_peripherals_assignment_table_template}}<onlyinclude>

 | rowspan="1" | Core/DMA
 | rowspan="1" | [[DMAMUX internal peripheral|DMAMUX]]
 | DMAMUX
 |
 | <span title="assignable peripheral" style="font-size:21px"></span>

 | <span title="assignable peripheral" style="font-size:21px"></span>

 | Shareable (multiple choices supported)
 |-</onlyinclude>

 |}

<noinclude>

[[Category:DMA peripherals]]
{{PublicationRequestId | 9110 | 2018-10-10 | AlainF}}
{{ArticleBasedOnModel| Internal peripheral article model}}</noinclude>
Line 1: Line 1:
<noinclude>
 
{{ArticleBasedOnModel| [[Internal peripheral article model]]}}
 
{{ArticleMainWriter|Pierre-YvesM}}
 
{{ ArticleApprovedVersion|Pierre-YvesM| Pierre-YvesM, GeraldB |No previous approved version| AlainF - 10Oct'18 - 9110 | 12Oct'18 }}
 
[[Category:DMA peripherals]]
 
</noinclude>
 
 
 
==Article purpose==
 
==Article purpose==
 
The purpose of this article is to:
 
The purpose of this article is to:
Line 62: Line 55:
 
</onlyinclude>
 
</onlyinclude>
 
  |}
 
  |}
  +
  +
<noinclude>
  +
[[Category:DMA peripherals]]
  +
{{PublicationRequestId | 9110 | 2018-10-10 | AlainF}}
  +
{{ArticleBasedOnModel| Internal peripheral article model}}
  +
</noinclude>