Difference between revisions of "DFSDM Linux driver"

[quality revision] [quality revision]
 
m
 


Template:ArticleMainWriter Template:ArticleMainWriter Template:ReviewersList Template:ArticleApprovedVersion


1 Article purpose[edit]

The purpose of this article is to introduce the Linux® driver for the DFSDM internal peripheral:

  • Which DFSDM features are supported by the driver
  • How to configure, use and debug it
  • What is the driver structure, where to the find source code.

2 Short Description[edit]

The DFSDM Linux® driver (kernel space) is based on the IIO and ALSA frameworks. It offers various modes:

  1. IIO direct mode: single capture on a channel
  2. IIO software buffer: capture one or more channels
  3. IIO triggered buffer mode: capture on one or more channels using triggers
    It uses hardware triggers available in IIO. See TIM Linux driver and LPTIM Linux driver.

It offers an extended API[1] for audio usage which allows PDM microphones capture through a SPI interface.

3 Configuration[edit]

3.1 Kernel configuration[edit]

Activate the DFSDM Linux® driver in the kernel configuration by using the menuconfig tool.

3.1.1 IIO driver[edit]

Configuration flag: CONFIG_STM32_DFSDM_ADC

Device Drivers  --->
   <*> Industrial I/O support  --->
      Analog to digital converters  --->
         <*> STMicroelectronics STM32 dfsdm adc
         <*>   STMicroelectronics STM32 adc                        # DFSDM ADC IIO driver

When using the DFSDM ADC IIO driver (only), the user must also enable the driver for the external analog front-end (e.g. sigma delta modulator). The generic sigma delta modulators driver may be used for instance (CONFIG_SD_ADC_MODULATOR):

Device Drivers  --->
   <*> Industrial I/O support  --->
      Analog to digital converters  --->
         <*> Generic sigma delta modulator                         # sigma delta modulator driver

3.1.2 Audio driver[edit]

Configuration flag: CONFIG_SND_SOC_STM32_DFSDM (Note: This configuration depends on CONFIG_STM32_DFSDM_ADC)

Device Drivers  --->
   <*> Sound card support  --->
      <*>   Advanced Linux Sound Architecture  --->
         <*>   ALSA for SoC audio support  --->
            STMicroelectronics STM32 SOC audio support  --->
               <*> SoC Audio support for STM32 DFSDM               # DFSDM Audio driver for digital microphone capture

3.2 Device tree[edit]

Refer to the DFSDM device tree configuration article when configuring the DFSDM Linux kernel driver.

4 How to use[edit]

4.1 IIO driver[edit]

In "IIO direct mode", the conversion result can be read directly from sysfs, see: How to do a simple ADC conversion using the sysfs interface.

In "IIO triggered buffer mode", the configuration must be performed by using sysfs first. Then, character device (/dev/iio:deviceX) is used to read data, see Convert one or more channels using triggered buffer mode.

For information on the standard IIO consumer interface, please refer to How to use IIO kernel API which gives an example of the IIO consumer kernel API.

4.2 Audio driver[edit]

The DFSDM Linux driver can be accessed from userland through an ALSA device. Refer to ALSA overview for information on how to list and use ALSA devices.

5 How to trace and debug[edit]

5.1 How to monitor[edit]

The DFSDM driver uses resources such as clocks and GPIOs.

5.1.1 How to monitor with debugfs[edit]

The DFSDM registers are accessed using REGMAP by DFSDM Linux® driver.

It comes with debugfs entries to dump registers:

$ cd /sys/kernel/debug/regmap/4400d000.dfsdm/
$ cat registers
000: 00000000
004: 00000000
008: 00000000

5.1.2 Other ways to monitor[edit]

  • Man can check the DFSDM interrupts and/or the DFSDM DMA interrupts:
$ cat /proc/interrupts
           CPU0       CPU1
...
 99:          0          0     GIC-0 142 Level     4400d000.dfsdm:filter@0
100:          0          0     GIC-0 143 Level     4400d000.dfsdm:filter@1
101:          0          0     GIC-0 144 Level     4400d000.dfsdm:filter@2
...

5.2 How to trace[edit]

5.2.1 IIO driver[edit]

Refer to How to trace with dynamic debug for how to enable the debug logs in the driver and in the framework.

Board $> dmesg -n8
Board $> echo "file drivers/iio/adc/stm32-dfsdm* +p" > /sys/kernel/debug/dynamic_debug/control

To enable dynamic debug at boot time, append the following arguments on the kernel command line:

loglevel=8 dyndbg="file drivers/iio/adc/stm32-dfsdm* +p"

5.2.2 Audio driver[edit]

Refer to ALSA_overview#How_to_trace for details on trace tools.

5.3 How to debug[edit]

5.3.1 Audio driver[edit]

Refer to ALSA_overview#How_to_debug for details on debugging tools.

6 Source code location[edit]

It is composed of:

See also sigma delta modulator driver:

7 References[edit]

<noinclude>

{{ArticleBasedOnModel | [[Linux driver article model]]}}
{{ArticleMainWriter | FabriceG}}
{{ArticleMainWriter | OlivierM}}
{{ReviewersList | FabriceG, OlivierM, ArnaudP}}
{{ArticleApprovedVersion | FabriceG | OlivierM | No previous approved version | AlainF - 28Nov'18 - 9772 | 28Nov'18}}
[[Category:IIO]]
[[Category:ALSA]]</noinclude>

==  Article purpose ==
The purpose of this article is to introduce the Linux<sup>&reg;</sup> driver for the [[DFSDM internal peripheral]]:
* Which DFSDM features are supported by the driver
* How to configure, use and debug it
* What is the driver structure, where to the find source code.

== Short Description ==
The DFSDM Linux<sup>&reg;</sup> driver (kernel space) is based on the [[IIO overview|IIO]] and [[ALSA overview|ALSA]] frameworks.
It offers various modes:
# '''IIO direct mode''': single capture on a channel
# '''IIO software buffer''': capture one or more channels
# '''IIO triggered buffer mode''': capture on one or more channels using triggers<br/>It uses hardware triggers available in IIO. See [[TIM Linux driver]] and [[LPTIM Linux driver]].

It offers an extended API<ref name="stm32-dfsdm-adc-h">{{CodeSource | Linux kernel | include/linux/iio/adc/stm32-dfsdm-adc.h}}, DFSDM IIO custom API</ref> for audio usage which allows '''PDM microphones capture''' through a SPI interface.

== Configuration ==
=== Kernel configuration ===
Activate the DFSDM Linux<sup>&reg;</sup> driver in the kernel configuration by using the [[Menuconfig or how to configure kernel|menuconfig]] tool.

==== IIO driver ====
Configuration flag: CONFIG_STM32_DFSDM_ADC<pre>

Device Drivers  ---><*> Industrial I/O support  --->
      Analog to digital converters  ---><*> STMicroelectronics STM32 dfsdm adc<*>   STMicroelectronics STM32 adc                        # DFSDM ADC IIO driver</pre>


When using the DFSDM ADC IIO driver (only), the user must also enable the driver for the external analog front-end (e.g. sigma delta modulator).
The generic sigma delta modulators driver may be used for instance (CONFIG_SD_ADC_MODULATOR):<pre>

Device Drivers  ---><*> Industrial I/O support  --->
      Analog to digital converters  ---><*> Generic sigma delta modulator                         # sigma delta modulator driver</pre>


==== Audio driver ====
Configuration flag: CONFIG_SND_SOC_STM32_DFSDM (Note: This configuration depends on [[#IIO_driver|CONFIG_STM32_DFSDM_ADC]])<pre>

Device Drivers  ---><*> Sound card support  ---><*>   Advanced Linux Sound Architecture  ---><*>   ALSA for SoC audio support  --->
            STMicroelectronics STM32 SOC audio support  ---><*> SoC Audio support for STM32 DFSDM               # DFSDM Audio driver for digital microphone capture</pre>

=== Device tree ===
Refer to the [[DFSDM device tree configuration]] article when configuring the DFSDM Linux kernel driver.

== How to use ==
=== IIO driver ===
In "'''IIO direct mode'''", the conversion result can be read directly from '''sysfs''', see:
[[How to use the IIO user space interface#How to do a simple ADC conversion using the sysfs interface|How to do a simple ADC conversion using the sysfs interface]].

In "'''IIO triggered buffer mode'''", the configuration must be performed by using '''sysfs''' first. Then, '''character device''' (/dev/iio:deviceX) is used to read data, see [[How to use the IIO user space interface#Convert_one_or_more_channels_using_triggered_buffer_mode|Convert one or more channels using triggered buffer mode]].

For information on the standard IIO consumer interface, please refer to [[IIO_overview#How_to_use_IIO_kernel_API|How to use IIO kernel API]] which gives an example of the IIO consumer kernel API.

=== Audio driver ===
The DFSDM Linux driver can be accessed from userland through an ALSA device. Refer to [[ALSA_overview#How_to_use|ALSA overview]] for information on how to list and use ALSA devices. 

==How to trace and debug==
=== How to monitor ===
The DFSDM driver uses resources such as clocks and GPIOs.
* Refer to [[Pinctrl_overview#How_to_monitor]] to check DFSDM GPIOs.
* Refer to [[Clock_overview#How_to_monitor_with_debugfs]] to check DFSDM clocks.

==== How to monitor with debugfs ====
The DFSDM registers are accessed using REGMAP by ''DFSDM Linux<sup>&reg;</sup> driver''.

It comes with [[Debugfs|debugfs]] entries to dump registers:
 $ {{highlight|cd /sys/kernel/debug/regmap/4400d000.dfsdm/}}
 $ {{highlight|cat registers}}
 000: 00000000
 004: 00000000
 008: 00000000

==== Other ways to monitor ====
* Man can check the DFSDM '''interrupts''' and/or the DFSDM '''DMA''' interrupts:
 $ {{highlight|cat /proc/interrupts}}
            CPU0       CPU1
 ...
  99:          0          0     GIC-0 142 Level     4400d000.dfsdm:filter@0
 100:          0          0     GIC-0 143 Level     4400d000.dfsdm:filter@1
 101:          0          0     GIC-0 144 Level     4400d000.dfsdm:filter@2
 ...

=== How to trace ===
==== IIO driver ====
Refer to [[IIO_overview#How_to_trace_with_dynamic_debug|How to trace with dynamic debug]] for how to enable the debug logs in the driver and in the framework.
 {{Board$}} dmesg -n8
 {{Board$}} echo "file drivers/iio/adc/stm32-dfsdm* +p" > /sys/kernel/debug/dynamic_debug/control
To enable dynamic debug at boot time, append the following arguments on the kernel command line:
 loglevel=8 dyndbg="file drivers/iio/adc/stm32-dfsdm* +p"
==== Audio driver ====
Refer to [[ALSA_overview#How_to_trace]] for details on trace tools.

=== How to debug ===
==== Audio driver ====
Refer to [[ALSA_overview#How_to_debug]] for details on debugging tools.

== Source code location ==
It is composed of:
* {{CodeSource | Linux kernel | drivers/iio/adc/stm32-dfsdm-core.c | stm32-dfsdm-core.c}}, core part of DFSDM Linux driver to handle common resources: registers, clock
* {{CodeSource | Linux kernel | drivers/iio/adc/stm32-dfsdm-adc.c | stm32-dfsdm-adc.c}}, ADC part of DFSDM Linux driver to handle '''ADC''' operations
* {{CodeSource | Linux kernel | sound/soc/stm/stm32_adfsdm.c | stm32_adfsdm.c}}, ASoC DAI part of DFSDM Linux driver to handle '''audio''' operations
See also sigma delta modulator driver:
* {{CodeSource | Linux kernel | drivers/iio/adc/sd_adc_modulator.c | sd_adc_modulator.c}}, sigma delta modulator Linux driver to handle analog front-end
==References==<references />

<noinclude>

[[Category:IIO]]
[[Category:ALSA]]
{{PublicationRequestId | 9772 | 2018-11-28 | AlainF}}
{{ArticleBasedOnModel | Linux driver article model}}</noinclude>
Line 1: Line 1:
<noinclude>
 
{{ArticleBasedOnModel | [[Linux driver article model]]}}
 
{{ArticleMainWriter | FabriceG}}
 
{{ArticleMainWriter | OlivierM}}
 
{{ReviewersList | FabriceG, OlivierM, ArnaudP}}
 
{{ArticleApprovedVersion | FabriceG | OlivierM | No previous approved version | AlainF - 28Nov'18 - 9772 | 28Nov'18}}
 
[[Category:IIO]]
 
[[Category:ALSA]]
 
</noinclude>
 
 
 
==  Article purpose ==
 
==  Article purpose ==
 
The purpose of this article is to introduce the Linux<sup>&reg;</sup> driver for the [[DFSDM internal peripheral]]:
 
The purpose of this article is to introduce the Linux<sup>&reg;</sup> driver for the [[DFSDM internal peripheral]]:
Line 121: Line 111:
 
==References==
 
==References==
 
<references />
 
<references />
  +
  +
<noinclude>
  +
[[Category:IIO]]
  +
[[Category:ALSA]]
  +
{{PublicationRequestId | 9772 | 2018-11-28 | AlainF}}
  +
{{ArticleBasedOnModel | Linux driver article model}}
  +
</noinclude>

Attachments

Discussions