Difference between revisions of "DBGMCU internal peripheral"

[quality revision] [quality revision]
m
m

1 Article purpose[edit]

The purpose of this article is to:

  • briefly introduce the DBGMCU peripheral and its main features
  • indicate the level of security supported by this hardware block
  • explain how each instance can be allocated to the three runtime contexts and linked to the corresponding software components
  • explain, when necessary, how to configure the DBGMCU peripheral.

2 Peripheral overview[edit]

The DBGMCU peripheral is used to configure internal peripherals behavior when one of the cores (Cortex®-A7 or Cortex®-M4) enters in debug mode.
For instance, it allows to freeze a watchdog (IWDG) to avoid getting a watchdog reset when the Cortex®-A7 enters in debug mode (via a breakpoint or JTAG break).

2.1 Features[edit]

Refer to the STM32MP15 reference manuals for the complete list of features, and to the software components, introduced below, to see which features are implemented.

2.2 Security support[edit]

The DBGMCU is a non secure peripheral.

3 Peripheral usage and associated software[edit]

3.1 Boot time[edit]

DBGMCU is partly initialized by the FSBL at boot time in order to freeze IWDG2 when the Cortex®-A7 enters in debug mode.

3.2 Runtime[edit]

3.2.1 Overview[edit]

There is no real runtime support for DBGMCU. Instead, users who need to freeze some peripherals for a debug session should complete the minimal initialization done in the FSBL with their needs.

3.2.2 Software frameworks[edit]

Internal peripherals software table template

| Trace & Debug
| DBGMCU
| 
| 
| 
|
|-
|}

3.2.3 Peripheral configuration[edit]

The configuration is applied by the firmware running in the context to which the peripheral is assigned. The configuration can be done alone via the STM32CubeMX tool for all internal peripherals, and then manually completed (particularly for external peripherals), according to the information given in the corresponding software framework article.

3.2.4 Peripheral assignment[edit]

Internal peripherals assignment table template

| rowspan="1" | Trace & Debug
| rowspan="1" | DBGMCU
| DBGMCU
|
|
|
| No assignment
|-
|}



==Article purpose==
The purpose of this article is to:
* briefly introduce the DBGMCU peripheral and its main features
* indicate the level of security supported by this hardware block
* explain how each instance can be allocated to the three runtime contexts and linked to the corresponding software components
* explain, when necessary, how to configure the DBGMCU peripheral.

==Peripheral overview==
The '''DBGMCU''' peripheral is used to configure  internal peripherals behavior when one of the cores (Cortex<sup>&reg;</sup>-A7 or Cortex<sup>&reg;</sup>-M4) enters in debug mode.<br />

For instance, it allows to freeze a watchdog ([[IWDG internal peripheral|IWDG]]) to avoid getting a watchdog reset when the Cortex<sup>&reg;</sup>-A7 enters in debug mode (via a breakpoint or JTAG break).<br />


===Features===
Refer to the [[STM32MP15 resources#Reference manuals|STM32MP15 reference manuals]] for the complete list of features, and to the software components, introduced below, to see which features are implemented.

===Security support===
The DBGMCU is a '''non secure''' peripheral.

==Peripheral usage and associated software==
===Boot time===
DBGMCU is partly initialized  by the [[Boot chainschain overview|FSBL]] at boot time in order to freeze [[IWDG internal peripheral|IWDG2]] when the Cortex<sup>&reg;</sup>-A7 enters in debug mode.

===Runtime===
====Overview====
There is no real runtime support for DBGMCU. Instead, users who need to freeze some peripherals for a debug session should complete the minimal initialization done in the [[Boot chainschain overview|FSBL]] with their needs.

====Software frameworks====
{{:Internal_peripherals_software_table_template}}
 | Trace & Debug
 | [[DBGMCU internal peripheral|DBGMCU]]
 | 
 | 
 | 
 |
 |-
 |}

====Peripheral configuration====
The configuration is applied by the firmware running in the context to which the peripheral is assigned. The configuration can be done alone via the [[STM32CubeMX]] tool for all internal peripherals, and then manually completed (particularly for external peripherals), according to the information given in the corresponding software framework article.

====Peripheral assignment====
{{:Internal_peripherals_assignment_table_template}}<onlyinclude>

 | rowspan="1" | Trace & Debug
 | rowspan="1" | [[DBGMCU internal peripheral|DBGMCU]]
 | DBGMCU
 |
 |
 |
 | No assignment
 |-</onlyinclude>

 |}
<noinclude>

{{ArticleBasedOnModel| Internal peripheral article model}}
{{PublicationRequestId | 9107 | 2018-10-08 | BrunoB}}
[[Category:Trace and debug peripherals]]</noinclude>
Line 18: Line 18:
 
==Peripheral usage and associated software==
 
==Peripheral usage and associated software==
 
===Boot time===
 
===Boot time===
DBGMCU is partly initialized  by the [[Boot chains overview|FSBL]] at boot time in order to freeze [[IWDG internal peripheral|IWDG2]] when the Cortex<sup>&reg;</sup>-A7 enters in debug mode.
+
DBGMCU is partly initialized  by the [[Boot chain overview|FSBL]] at boot time in order to freeze [[IWDG internal peripheral|IWDG2]] when the Cortex<sup>&reg;</sup>-A7 enters in debug mode.
   
 
===Runtime===
 
===Runtime===
 
====Overview====
 
====Overview====
There is no real runtime support for DBGMCU. Instead, users who need to freeze some peripherals for a debug session should complete the minimal initialization done in the [[Boot chains overview|FSBL]] with their needs.
+
There is no real runtime support for DBGMCU. Instead, users who need to freeze some peripherals for a debug session should complete the minimal initialization done in the [[Boot chain overview|FSBL]] with their needs.
   
 
====Software frameworks====
 
====Software frameworks====