Difference between revisions of "Cross-compile with OpenSTLinux SDK"
[unchecked revision] | [quality revision] |
Lionel Vitte (talk | contribs)
m
|
m (→Modifying the TF-A)
|
Applicable for | STM32MP13x lines, STM32MP15x lines |
Contents
1 Article purpose[edit]
The pieces of software delivered as source code within the OpenSTLinux Developer Package (for example the Linux kernel) can be modified. External out-of-tree Linux kernel modules, and pieces of applicative software (for example Linux applications) can also be developed thanks to this Developer Package, and loaded onto the board.
The build of all these pieces of software by means of the SDK for OpenSTLinux distribution, and the deployment on-target of the resulting images is explained below.
![]() |
To use the cross-compilation efficiently with the OpenSTLinux SDK, it is recommended that you read the Developer Package article relative to the Series of your STM32 microprocessor: Category:Developer Package |
1.1 Modifying the Linux kernel[edit]
Prerequisites:
The <Linux kernel installation directory>/README.HOW_TO.txt helper file gives the commands to:
☐ configure the Linux kernel
☐ cross-compile the Linux kernel
☐ deploy the Linux kernel (that is, update the software on board)
You can refer to the following simple examples:
- Modification of the kernel configuration
- Modification of the device tree
- Modification of a built-in device driver
- Modification of an external in-tree module
1.2 Adding external out-of-tree Linux kernel modules[edit]
Prerequisites:
Most device drivers (or modules) in the Linux kernel can be compiled either into the kernel itself (built-in, or internal module) or as Loadable Kernel Modules (LKMs, or external modules) that need to be placed in the root file system under the /lib/modules directory. An external module can be in-tree (in the kernel tree structure), or out-of-tree (outside the kernel tree structure).
External Linux kernel modules are compiled taking reference to a Linux kernel source tree and a Linux kernel configuration file (.config).
Thus, a makefile for an external Linux kernel module points to the Linux kernel directory that contains the source code and the configuration file, with the "-C <Linux kernel path>" option.
This makefile also points to the directory that contains the source file(s) of the Linux kernel module to compile, with the "M=<Linux kernel module path>" option.
A generic makefile for an external out-of-tree Linux kernel module looks like the following:
# Makefile for external out-of-tree Linux kernel module # Object file(s) to be built obj-m := <module source file(s)>.o # Path to the directory that contains the Linux kernel source code # and the configuration file (.config) KERNEL_DIR ?= <Linux kernel path> # Path to the directory that contains the generated objects DESTDIR ?= <Linux kernel installation directory> # Path to the directory that contains the source file(s) to compile PWD := $(shell pwd) default: $(MAKE) -C $(KERNEL_DIR) M=$(PWD) modules install: $(MAKE) -C $(KERNEL_DIR) M=$(PWD) INSTALL_MOD_PATH=$(DESTDIR) modules_install clean: $(MAKE) -C $(KERNEL_DIR) M=$(PWD) clean
Such module is then cross-compiled with the following commands:
$ make clean $ make $ make install
You can refer to the following simple example:
1.3 Adding Linux user space applications[edit]
Prerequisites:
- the SDK is installed
- the SDK is started up
Once a suitable cross-toolchain (OpenSTLinux SDK) is installed, it is easy to develop a project outside of the OpenEmbedded build system.
There are different ways to use the SDK toolchain directly, among which Makefile and Autotools.
Whatever the method, it relies on:
- the sysroot that is associated with the cross-toolchain, and that contains the header files and libraries needed for generating binaries (see target sysroot)
- the environment variables created by the SDK environment setup script (see SDK startup)
You can refer to the following simple example:
1.4 Modifying the U-Boot[edit]
Prerequisites:
The <U-Boot installation directory>/README.HOW_TO.txt helper file gives the commands to:
☐ cross-compile the U-Boot
☐ deploy the U-Boot (that is, update the software on board)
You can refer to the following simple example:
1.5 Modifying the TF-A[edit]
Prerequisites:
- the SDK is installed
- the SDK is started up
- the [[STM32MP1 Developer Package#Installing the BSP packages|BSP package is installed]
The <TF-A installation directory>/README.HOW_TO.txt helper file gives the commands to:
☐ cross-compile the TF-A
☐ deploy the TF-A (that is, update the software on board)
You can refer to the following simple example:
1.6 Modifying the OP-TEE[edit]
Prerequisites:
The <OP-TEE installation directory>/README.HOW_TO.txt helper file gives the commands to:
☐ cross-compile the OP-TEE
☐ deploy the OP-TEE (that is, update the software on board)
You can refer to the following simple example:
<noinclude>{{ApplicableFor |MPUs list=STM32MP13x, STM32MP15x |MPUs checklist=STM32MP13x,STM32MP15x }}</noinclude> <noinclude> [[Category:SDK]] {{PublicationRequestId | 7646 | 2018-06-04 | PhilipS}} ==Article purpose== The pieces of software delivered as source code within the OpenSTLinux Developer Package (for example the Linux kernel) can be modified. External out-of-tree Linux kernel modules, and pieces of applicative software (for example Linux applications) can also be developed thanks to this Developer Package, and loaded onto the board. The build of all these pieces of software by means of the [[SDK for OpenSTLinux distribution]], and the deployment on-target of the resulting images is explained below. {{Warning|To use the cross-compilation efficiently with the OpenSTLinux SDK, it is recommended that you read the Developer Package article relative to the Series of your STM32 microprocessor: [[:Category:Developer Package]]}} </noinclude> ===Modifying the Linux kernel=== Prerequisites: * the [[STM32MP1 Developer Package#Installing the SDK|SDK is installed]] * the [[STM32MP1 Developer Package#Starting up the SDK|SDK is started up]] * the [[STM32MP1 Developer Package#Installing the BSP packages|BSP package is installed]] {{highlight|'''The ''<Linux kernel installation directory>/README.HOW_TO.txt'' helper file gives the commands to:'''}} <br> <span style="font-size:21px">☐</span> configure the Linux kernel <br> <span style="font-size:21px">☐</span> cross-compile the Linux kernel <br> <span style="font-size:21px">☐</span> deploy the Linux kernel (that is, update the software on board) <br> You can refer to the following simple examples: * [[How to cross-compile with the Developer Package#Modifying the Linux kernel configuration|Modification of the kernel configuration]] * [[How to cross-compile with the Developer Package#Modifying the Linux kernel device tree|Modification of the device tree]] * [[How to cross-compile with the Developer Package#Modifying a built-in Linux kernel device driver|Modification of a built-in device driver]] * [[How to cross-compile with the Developer Package#Modifying an external in-tree Linux kernel module|Modification of an external in-tree module]] ===Adding external out-of-tree Linux kernel modules=== Prerequisites: * the [[STM32MP1 Developer Package#Installing the SDK|SDK is installed]] * the [[STM32MP1 Developer Package#Starting up the SDK|SDK is started up]] * the [[STM32MP1 Developer Package#Installing the BSP packages|BSP package is installed]] Most device drivers (or modules) in the Linux kernel can be compiled either into the kernel itself (built-in, or internal module) or as Loadable Kernel Modules (LKMs, or external modules) that need to be placed in the root file system under the /lib/modules directory. An external module can be in-tree (in the kernel tree structure), or out-of-tree (outside the kernel tree structure). External Linux kernel modules are compiled taking reference to a Linux kernel source tree and a Linux kernel configuration file (''.config''). <br> Thus, a makefile for an external Linux kernel module points to the Linux kernel directory that contains the source code and the configuration file, with the '''"-C <Linux kernel path>"''' option. <br> This makefile also points to the directory that contains the source file(s) of the Linux kernel module to compile, with the '''"M=<Linux kernel module path>"''' option. <br> A generic makefile for an external out-of-tree Linux kernel module looks like the following: # Makefile for external out-of-tree Linux kernel module # Object file(s) to be built obj-m := {{HighlightParam|''<module source file(s)>''}}.o # Path to the directory that contains the Linux kernel source code # and the configuration file (.config) KERNEL_DIR ?= {{HighlightParam|''<Linux kernel path>''}} # Path to the directory that contains the generated objects DESTDIR ?= {{HighlightParam|''<Linux kernel installation directory>''}} # Path to the directory that contains the source file(s) to compile PWD := $(shell pwd) default: $(MAKE) -C $(KERNEL_DIR) M=$(PWD) modules install: $(MAKE) -C $(KERNEL_DIR) M=$(PWD) INSTALL_MOD_PATH=$(DESTDIR) modules_install clean: $(MAKE) -C $(KERNEL_DIR) M=$(PWD) clean Such module is then cross-compiled with the following commands: $ make clean $ make $ make install You can refer to the following simple example: * [[How to cross-compile with the Developer Package#Adding an external out-of-tree Linux kernel module|Addition of an external out-of-tree module]] ===Adding Linux user space applications=== Prerequisites: * the [[STM32MP1 Developer Package#Installing the SDK|SDK is installed]] * the [[STM32MP1 Developer Package#Starting up the SDK|SDK is started up]] Once a suitable cross-toolchain (OpenSTLinux SDK) is installed, it is easy to develop a project outside of the OpenEmbedded build system. <br> There are different ways to use the SDK toolchain directly, among which Makefile and Autotools. <br> Whatever the method, it relies on: * the sysroot that is associated with the cross-toolchain, and that contains the header files and libraries needed for generating binaries (see [[SDK for OpenSTLinux distribution#Native and target sysroots|target sysroot]]) * the environment variables created by the SDK environment setup script (see [[SDK for OpenSTLinux distribution#SDK startup|SDK startup]]) You can refer to the following simple example: * [[How to cross-compile with the Developer Package#Adding a "hello world" user space example|Addition of a "hello world" user space application]] ===Modifying the U-Boot=== Prerequisites: * the [[STM32MP1 Developer Package#Installing the SDK|SDK is installed]] * the [[STM32MP1 Developer Package#Starting up the SDK|SDK is started up]] * the [[STM32MP1 Developer Package#Installing the BSP packages|BSP package is installed]] {{highlight|'''The ''<U-Boot installation directory>/README.HOW_TO.txt'' helper file gives the commands to:'''}} <br> <span style="font-size:21px">☐</span> cross-compile the U-Boot <br> <span style="font-size:21px">☐</span> deploy the U-Boot (that is, update the software on board) <br> You can refer to the following simple example: * [[How to cross-compile with the Developer Package#Modifying the U-Boot|Modification of the U-Boot]] ===Modifying the TF-A=== Prerequisites: * the [[STM32MP1 Developer Package#Installing the SDK|SDK is installed]] * the [[STM32MP1 Developer Package#Starting up the SDK|SDK is started up]] * the [[STM32MP1 Developer Package#Installing the BSP packages|BSP package is installed]] {{highlight|'''The ''<TF-A installation directory>/README.HOW_TO.txt'' helper file gives the commands to:'''}} <br> <span style="font-size:21px">☐</span> cross-compile the TF-A <br> <span style="font-size:21px">☐</span> deploy the TF-A (that is, update the software on board) <br> You can refer to the following simple example: * [[How to cross-compile with the Developer Package#Modifying the TF-A|Modification of the TF-A]] ===Modifying the OP-TEE=== Prerequisites: * the [[STM32MP1 Developer Package#Installing the SDK|SDK is installed]] * the [[STM32MP1 Developer Package#Starting up the SDK|SDK is started up]] * the [[STM32MP1 Developer Package#Installing the BSP packages|BSP package is installed]] {{highlight|'''The ''<OP-TEE installation directory>/README.HOW_TO.txt'' helper file gives the commands to:'''}} <br> <span style="font-size:21px">☐</span> cross-compile the OP-TEE <br> <span style="font-size:21px">☐</span> deploy the OP-TEE (that is, update the software on board) <br> You can refer to the following simple example: * [[How to cross-compile with the Developer Package#Modifying the OP-TEE OS|Modification of the OP-TEE OS]]
Line 108: | Line 108: | ||
* the [[STM32MP1 Developer Package#Installing the SDK|SDK is installed]] |
* the [[STM32MP1 Developer Package#Installing the SDK|SDK is installed]] |
||
* the [[STM32MP1 Developer Package#Starting up the SDK|SDK is started up]] |
* the [[STM32MP1 Developer Package#Starting up the SDK|SDK is started up]] |
||
− | * the [[STM32MP1 Developer Package#Installing the BSP packages|BSP package is installed] |
+ | * the [[STM32MP1 Developer Package#Installing the BSP packages|BSP package is installed]] |
{{highlight|'''The ''<TF-A installation directory>/README.HOW_TO.txt'' helper file gives the commands to:'''}} <br> |
{{highlight|'''The ''<TF-A installation directory>/README.HOW_TO.txt'' helper file gives the commands to:'''}} <br> |