Difference between revisions of "Cross-compile with OpenSTLinux SDK"

[quality revision] [quality revision]
(Modifying the OP-TEE)
m (Adding external out-of-tree Linux kernel modules)
 


Template:ArticleMainWriter Template:ReviewersList Template:ArticleApprovedVersion

1 Article purpose[edit]

The pieces of software delivered as source code within the OpenSTLinux Developer Package (for example the Linux kernel) can be modified. External out-of-tree Linux kernel modules, and pieces of applicative software (for example Linux applications) can also be developed thanks to this Developer Package, and loaded onto the board.

The build of all these pieces of software by means of the SDK for OpenSTLinux distribution, and the deployment on-target of the resulting images is explained below.

Warning.png To use the cross-compilation efficiently with the OpenSTLinux SDK, it is recommended that you read the Developer Package article relative to the Series of your STM32 microprocessor: Category:Developer Package


1.1 Modifying the Linux kernel[edit]

Prerequisites:

The <Linux kernel installation directory>/README.HOW_TO.txt helper file gives the commands to:
configure the Linux kernel
cross-compile the Linux kernel
deploy the Linux kernel (that is, update the software on board)

You can refer to the following simple examples:

1.2 Adding external out-of-tree Linux kernel modules[edit]

Prerequisites:

Most device drivers (or modules) in the Linux kernel can be compiled either into the kernel itself (built-in, or internal module) or as Loadable Kernel Modules (LKMs, or external modules) that need to be placed in the root file system under the /lib/modules directory. An external module can be in-tree (in the kernel tree structure), or out-of-tree (outside the kernel tree structure).

External Linux kernel modules are compiled taking reference to a Linux kernel source tree and a Linux kernel configuration file (.config).
Thus, a makefile for an external Linux kernel module points to the Linux kernel directory that contains the source code and the configuration file, with the "-C <Linux kernel path>" option.
This makefile also points to the directory that contains the source file(s) of the Linux kernel module to compile, with the "M=<Linux kernel module path>" option.

A generic makefile for an external out-of-tree Linux kernel module looks like the following:


# Makefile for external out-of-tree Linux kernel module

# Object file(s) to be built
obj-m := <module source file(s)>.o

# Path to the directory that contains the Linux kernel source code
# and the configuration file (.config)
KERNEL_DIR ?= <Linux kernel path>

# Path to the directory that contains the generated objects
DESTDIR ?= <Linux kernel installation directory>

# Path to the directory that contains the source file(s) to compile
PWD := $(shell pwd) 
 

default:
 	$(MAKE) -C $(KERNEL_DIR) M=$(PWD) modules

install:
	$(MAKE) -C $(KERNEL_DIR) M=$(PWD) INSTALL_MOD_PATH=$(DESTDIR) modules_install

clean:  
	$(MAKE) -C $(KERNEL_DIR) M=$(PWD) clean

Such module is then cross-compiled with the following commands:

$ make clean
$ make
$ make install

You can refer to the following simple example:

1.3 Adding Linux user space applications[edit]

Prerequisites:

Once a suitable cross-toolchain (OpenSTLinux SDK) is installed, it is easy to develop a project outside of the OpenEmbedded build system.
There are different ways to use the SDK toolchain directly, among which Makefile and Autotools.
Whatever the method, it relies on:

  • the sysroot that is associated with the cross-toolchain, and that contains the header files and libraries needed for generating binaries (see SDK startup target sysroot)
  • the environment variables created by the SDK environment setup script (see target sysroot SDK startup)

You can refer to the following simple example:

1.4 Modifying the U-Boot[edit]

Prerequisites:

The <U-Boot installation directory>/README.HOW_TO.txt helper file gives the commands to:
cross-compile the U-Boot
deploy the U-Boot (that is, update the software on board)

You can refer to the following simple example:

1.5 Modifying the TF-A[edit]

Prerequisites:

The <TF-A installation directory>/README.HOW_TO.txt helper file gives the commands to:
cross-compile the TF-A
deploy the TF-A (that is, update the software on board)

You can refer to the following simple example:

1.6 Modifying the OP-TEE[edit]

Prerequisites:

The <OP-TEE installation directory>/README.HOW_TO.txt helper file gives the commands to:
cross-compile the OP-TEE
deploy the OP-TEE (that is, update the software on board)

<noinclude>
{{ArticleMainWriter | Jean-ChristopheT}}
{{ReviewersList | NathalieS, BernardP, RomualdJ , DenisH, Jean-PhilippeR}}
{{ArticleApprovedVersion | Jean-ChristopheT | NathalieS (Passed, 4Jun'18), BernardP (PASS, 28MAy'18), DenisH (Passed, 6Jun'18), Jean-PhilippeR (Passed, 23May'18) | No previous approved version | PhilipS  - 4Jun'18 - 7646 | 20Jun'18}}

[[Category:SDK]]</noinclude>

<noinclude>
[[Category:SDK]]
{{PublicationRequestId | 7646 | 2018-06-04 | PhilipS}}
==Article purpose==
The pieces of software delivered as source code within the OpenSTLinux Developer Package (for example the Linux kernel) can be modified. External out-of-tree Linux kernel modules, and pieces of applicative software (for example Linux applications) can also be developed thanks to this Developer Package, and loaded onto the board.

The build of all these pieces of software by means of the [[SDK for OpenSTLinux distribution]], and the deployment on-target of the resulting images is explained below.
{{Warning|To use the cross-compilation efficiently with the OpenSTLinux SDK, it is recommended that you read the Developer Package article relative to the Series of your STM32 microprocessor: [[:Category:Developer Package]]}}
</noinclude>

===Modifying the Linux kernel===
Prerequisites:
* the [[STM32MP1 Developer Package#Installing the SDK|SDK is installed]] 
* the [[STM32MP1 Developer Package#Starting up the SDK|SDK is started up]]
* the [[STM32MP1 Developer Package#Installing the Linux kernel|Linux kernel is installed]]

{{highlight|'''The ''<Linux kernel installation directory>/README.HOW_TO.txt'' helper file gives the commands to:'''}} <br>
<span style="font-size:21px"></span> configure the Linux kernel <br>
<span style="font-size:21px"></span> cross-compile the Linux kernel <br>
<span style="font-size:21px"></span> deploy the Linux kernel (that is, update the software on board) <br>


You can refer to the following simple examples:
* [[How to cross-compile with the Developer Package#Modifying the Linux kernel configuration|Modification of the kernel configuration]] 
* [[How to cross-compile with the Developer Package#Modifying the Linux kernel device tree|Modification of the device tree]]
* [[How to cross-compile with the Developer Package#Modifying a built-in Linux kernel device driver|Modification of a built-in device driver]]
* [[How to cross-compile with the Developer Package#Modifying an external in-tree Linux kernel module|Modification of an external in-tree module]]

===Adding external out-of-tree Linux kernel modules===
Prerequisites:
* the [[STM32MP1 Developer Package#Installing the SDK|SDK is installed]]
* the [[STM32MP1 Developer Package#Starting up the SDK|SDK is started up]]
* the [[STM32MP1 Developer Package#Installing the Linux kernel|Linux kernel is installed]]

Most device drivers (or modules) in the Linux kernel can be compiled either into the kernel itself (built-in, or internal module) or as Loadable Kernel Modules (LKMs, or external modules) that need to be placed in the root file system under the /lib/modules directory. An external module can be in-tree (in the kernel tree structure), or out-of-tree (outside the kernel tree structure).

External Linux kernel modules are compiled taking reference to a Linux kernel source tree and a Linux kernel configuration file (''.config''). <br>

Thus, a makefile for an external Linux kernel module points to the Linux kernel directory that contains the source code and the configuration file, with the '''"-C <Linux kernel path>"''' option. <br>

This makefile also points to the directory that contains the source file(s) of the Linux kernel module to compile, with the '''"M=<Linux kernel module path>"''' option. <br>


A generic makefile for an external out-of-tree Linux kernel module looks like the following:<pre>

# Makefile for external out-of-tree Linux kernel module
# Object file(s) to be built obj-m := <module source file(s)>.o
{{HighlightParam|''<module source file(s)>''}}.o
# Path to the directory that contains the Linux kernel source code # and the configuration file (.config) KERNEL_DIR ?= <Linux kernel path>

{{HighlightParam|''<Linux kernel path>''}}
# Path to the directory that contains the generated objects DESTDIR ?= <Linux kernel installation directory>

{{HighlightParam|''<Linux kernel installation directory>''}}
# Path to the directory that contains the source file(s) to compile PWD := $(shell pwd) 
 default:  	$(MAKE) -C $(KERNEL_DIR) M=$(PWD) modules
install: 	$(MAKE) -C $(KERNEL_DIR) M=$(PWD) INSTALL_MOD_PATH=$(DESTDIR) modules_install
clean:   	$(MAKE) -C $(KERNEL_DIR) M=$(PWD) clean</pre>


Such module is then cross-compiled with the following commands:
 $ make clean
 $ make
 $ make install

You can refer to the following simple example:
* [[How to cross-compile with the Developer Package#Adding an external out-of-tree Linux kernel module|Addition of an external out-of-tree module]]

===Adding Linux user space applications===
Prerequisites:
* the [[STM32MP1 Developer Package#Installing the SDK|SDK is installed]] 
* the [[STM32MP1 Developer Package#Starting up the SDK|SDK is started up]]

Once a suitable cross-toolchain (OpenSTLinux SDK) is installed, it is easy to develop a project outside of the OpenEmbedded build system. <br>

There are different ways to use the SDK toolchain directly, among which Makefile and Autotools. <br>

Whatever the method, it relies on:
* the sysroot that is associated with the cross-toolchain, and that contains the header files and libraries needed for generating binaries (see [[SDK for OpenSTLinux distribution#SDK startup|SDK startup]])
{{ReviewsComments|YCO 15-Feb-19: bad link , should be -> target sysroot}}distribution#Native and target sysroots|target sysroot]])

* the environment variables created by the SDK environment setup script (see [[SDK for OpenSTLinux distribution#Native and target sysroots|target sysroot]])
{{ReviewsComments|YCO 15-Feb-19: bad link , should be -> SDK startup}}
distribution#SDK startup|SDK startup]])
You can refer to the following simple example:
* [[How to cross-compile with the Developer Package#Adding a "hello world" user space example|Addition of a "hello world" user space application]]

===Modifying the U-Boot===
Prerequisites:
* the [[STM32MP1 Developer Package#Installing the SDK|SDK is installed]] 
* the [[STM32MP1 Developer Package#Starting up the SDK|SDK is started up]]
* the [[STM32MP1 Developer Package#Installing the U-Boot|U-Boot is installed]]

{{highlight|'''The ''&#60;U-Boot installation directory>/README.HOW_TO.txt'' helper file gives the commands to:'''}} <br>
<span style="font-size:21px"></span> cross-compile the U-Boot <br>
<span style="font-size:21px"></span> deploy the U-Boot (that is, update the software on board) <br>


You can refer to the following simple example:
* [[How to cross-compile with the Developer Package#Modifying the U-Boot|Modification of the U-Boot]]

===Modifying the TF-A===
Prerequisites:
* the [[STM32MP1 Developer Package#Installing the SDK|SDK is installed]]
* the [[STM32MP1 Developer Package#Starting up the SDK|SDK is started up]]
* the [[STM32MP1 Developer Package#Installing the TF-A|TF-A is installed]]

{{highlight|'''The ''<TF-A installation directory>/README.HOW_TO.txt'' helper file gives the commands to:'''}} <br>
<span style="font-size:21px"></span> cross-compile the TF-A <br>
<span style="font-size:21px"></span> deploy the TF-A (that is, update the software on board) <br>


You can refer to the following simple example:
* [[How to cross-compile with the Developer Package#Modifying the TF-A|Modification of the TF-A]]

===Modifying the OP-TEE===
Prerequisites:
* the [[STM32MP1 Developer Package#Installing the SDK|SDK is installed]]
* the [[STM32MP1 Developer Package#Starting up the SDK|SDK is started up]]
* the [[STM32MP1 Developer Package#Installing the OP-TEE|OP-TEE is installed]]

{{highlight|'''The ''<OP-TEE installation directory>/README.HOW_TO.txt'' helper file gives the commands to:'''}} <br>
<span style="font-size:21px"></span> cross-compile the OP-TEE <br>
<span style="font-size:21px"></span> deploy the OP-TEE (that is, update the software on board) <br>


 {{ReviewsComments|YCO 15-Feb-19 : link missing "Modification of the OP-TEE"<br>

There is no link because the page "How_to_cross-compile_with_the_Developer_Package" doesn't contain a paragraph for TEE, <br>

SO THIS PARAGRAH "Modifying the OP-TEE" is not useful, it gives no more informations.<br> 

The paragraph  "5.5 Installing the OP-TEE" is enough }}
(3 intermediate revisions by 3 users not shown)
Line 1: Line 1:
 
<noinclude>
 
<noinclude>
{{ArticleMainWriter | Jean-ChristopheT}}
 
{{ReviewersList | NathalieS, BernardP, RomualdJ , DenisH, Jean-PhilippeR}}
 
{{ArticleApprovedVersion | Jean-ChristopheT | NathalieS (Passed, 4Jun'18), BernardP (PASS, 28MAy'18), DenisH (Passed, 6Jun'18), Jean-PhilippeR (Passed, 23May'18) | No previous approved version | PhilipS  - 4Jun'18 - 7646 | 20Jun'18}}
 
 
 
[[Category:SDK]]
 
[[Category:SDK]]
</noinclude>
+
{{PublicationRequestId | 7646 | 2018-06-04 | PhilipS}}
   
<noinclude>
 
 
==Article purpose==
 
==Article purpose==
 
The pieces of software delivered as source code within the OpenSTLinux Developer Package (for example the Linux kernel) can be modified. External out-of-tree Linux kernel modules, and pieces of applicative software (for example Linux applications) can also be developed thanks to this Developer Package, and loaded onto the board.
 
The pieces of software delivered as source code within the OpenSTLinux Developer Package (for example the Linux kernel) can be modified. External out-of-tree Linux kernel modules, and pieces of applicative software (for example Linux applications) can also be developed thanks to this Developer Package, and loaded onto the board.
Line 45: Line 40:
   
 
A generic makefile for an external out-of-tree Linux kernel module looks like the following:
 
A generic makefile for an external out-of-tree Linux kernel module looks like the following:
<pre>
 
# Makefile for external out-of-tree Linux kernel module
 
 
# Object file(s) to be built
 
obj-m := <module source file(s)>.o
 
 
# Path to the directory that contains the Linux kernel source code
 
# and the configuration file (.config)
 
KERNEL_DIR ?= <Linux kernel path>
 
 
# Path to the directory that contains the generated objects
 
DESTDIR ?= <Linux kernel installation directory>
 
   
# Path to the directory that contains the source file(s) to compile
+
# Makefile for external out-of-tree Linux kernel module
PWD := $(shell pwd)  
+
  +
# Object file(s) to be built
  +
obj-m := {{HighlightParam|''<module source file(s)>''}}.o
  +
  +
# Path to the directory that contains the Linux kernel source code
  +
# and the configuration file (.config)
  +
KERNEL_DIR ?= {{HighlightParam|''<Linux kernel path>''}}
  +
  +
# Path to the directory that contains the generated objects
  +
DESTDIR ?= {{HighlightParam|''<Linux kernel installation directory>''}}
  +
  +
# Path to the directory that contains the source file(s) to compile
  +
PWD := $(shell pwd)  
 
    
 
    
default:
+
default:
$(MAKE) -C $(KERNEL_DIR) M=$(PWD) modules
+
  $(MAKE) -C $(KERNEL_DIR) M=$(PWD) modules
 
+
install:
+
install:
$(MAKE) -C $(KERNEL_DIR) M=$(PWD) INSTALL_MOD_PATH=$(DESTDIR) modules_install
+
$(MAKE) -C $(KERNEL_DIR) M=$(PWD) INSTALL_MOD_PATH=$(DESTDIR) modules_install
 
+
clean:   
+
clean:   
$(MAKE) -C $(KERNEL_DIR) M=$(PWD) clean
+
$(MAKE) -C $(KERNEL_DIR) M=$(PWD) clean
</pre>
 
   
 
Such module is then cross-compiled with the following commands:
 
Such module is then cross-compiled with the following commands:
Line 87: Line 81:
 
There are different ways to use the SDK toolchain directly, among which Makefile and Autotools. <br>
 
There are different ways to use the SDK toolchain directly, among which Makefile and Autotools. <br>
 
Whatever the method, it relies on:
 
Whatever the method, it relies on:
* the sysroot that is associated with the cross-toolchain, and that contains the header files and libraries needed for generating binaries (see [[SDK for OpenSTLinux distribution#SDK startup|SDK startup]])
+
* the sysroot that is associated with the cross-toolchain, and that contains the header files and libraries needed for generating binaries (see [[SDK for OpenSTLinux distribution#Native and target sysroots|target sysroot]])
{{ReviewsComments|YCO 15-Feb-19: bad link , should be -> target sysroot}}
+
* the environment variables created by the SDK environment setup script (see [[SDK for OpenSTLinux distribution#SDK startup|SDK startup]])
* the environment variables created by the SDK environment setup script (see [[SDK for OpenSTLinux distribution#Native and target sysroots|target sysroot]])
 
{{ReviewsComments|YCO 15-Feb-19: bad link , should be -> SDK startup}}
 
   
 
You can refer to the following simple example:
 
You can refer to the following simple example:
Line 130: Line 122:
 
<span style="font-size:21px">☐</span> cross-compile the OP-TEE <br>
 
<span style="font-size:21px">☐</span> cross-compile the OP-TEE <br>
 
<span style="font-size:21px">☐</span> deploy the OP-TEE (that is, update the software on board) <br>
 
<span style="font-size:21px">☐</span> deploy the OP-TEE (that is, update the software on board) <br>
 
{{ReviewsComments|YCO 15-Feb-19 : link missing "Modification of the OP-TEE"<br>
 
There is no link because the page "How_to_cross-compile_with_the_Developer_Package" doesn't contain a paragraph for TEE, <br>
 
SO THIS PARAGRAH "Modifying the OP-TEE" is not useful, it gives no more informations.<br>
 
The paragraph  "5.5 Installing the OP-TEE" is enough }}