Difference between revisions of "Coprocessor management troubleshooting grid"
[quality revision] | [quality revision] |
(→Coprocessor firmware loading and control)
|
Some typical issues related to the management of a coprocessor are listed below. Solutions or debugging methods are proposed for these issues.
If your issue is not listed, try looking in the articles in the Coprocessor management Linux, Coprocessor management STM32Cube or troubleshooting grids categories.
1 Coprocessor firmware loading and control[edit]
Symptom | Resolution |
---|---|
The coprocessor traces are not available on Linux® side cat /sys/kernel/debug/remoteproc/remoteproc0/trace0 No such file or directory |
This may happen for two reasons:
readelf -l <elf file> ... 02 .data .resource_table .bss ._user_heap_stack .... |
When starting the coprocessor from the bootloader (u-boot): "unsupported fw ver: 0 Remote Processor 0 resource table Not found : 0x00000000-0x0 " |
The firmware does not include any resource table. This is only a warning that does not prevent the firmware from starting properly. "rproc load_rsc" step can be bypassed. |
2 Inter processor communication[edit]
Symptom | Resolution |
---|---|
Frozen firmware as consequence of a deadlock in OpenAMP during IP communication with the the main processor. |
This Issue probably comes from rpmsg_virtio_rx_callback or rpmsg_virtio_send_offchannel_raw (rpmsg_virtio.c) functions that are called in interrupt context. These functions use a mutex lock in rpmsg_device struct when accessing the index of the virtio queue index. Rework your code so that these functions are not called in interrupt context. |
Linux kernel trace: stm32-ipcc 4c001000.mailbox: Try increasing MBOX_TX_QUEUE_LEN |
On each IPCC interrupt, the coprocessor treats all the buffered RPMsges RPMsgs (one IPCC event for several RPMsgesRPMsgs). On Linux side, one IPCC signal is programmed for each RPMsg sent. This can result is an overflow warning on Linux since too many IPCC events are queued. No RPMsges RPMsgs are dropped but this message could be interpreted as the coprocessor reaches its capacity to treat the received messages in time. |
Linux kernel trace ( example with rpmsg_tty driver): rpmsg_tty virtio0.rpmsg-tty-channel.-1.0: timeout waiting for a tx buffer |
This message means that there is no more TX buffer available to transmit messages to the remote processor. This may happen for two reasons:
|
Linux kernel trace: rpmsg_tty virtio0.rpmsg-tty-channel.-1.0: No memory for tty_prepare_flip_string |
There is no more space in the TTY temporary buffer on reception. The root cause is probably that the Linux application did not read the tty device on time to treat the incoming TTY stream. Consider reworking the Linux application so that it takes less time to process messages or decreasing the message exchange rate. |
Linux kernel trace: remoteproc remoteproc0: stm32_rproc_kick: failed (<mbx>, <error value>) |
The Linux remoteproc driver cannot use the IPCC mailbox. This may happen for two reasons:
|
<onlyinclude> Some typical issues related to the management of a coprocessor are listed below. Solutions or debugging methods are proposed for these issues. If your issue is not listed, try looking in the articles in the [[:Category:Coprocessor management Linux| Coprocessor management Linux]], [[:Category:Coprocessor management STM32Cube | Coprocessor management STM32Cube]] or [[:Category:Troubleshooting grids|troubleshooting grids]] categories. == Coprocessor firmware loading and control == {{:Troubleshooting grid table template}}<onlyinclude> <includeonly> ! colspan="2" | coprocessor firmware loading and control |-</includeonly> | The coprocessor traces are not available on Linux<sup>®</sup> side {{Board$}} cat /sys/kernel/debug/remoteproc/remoteproc0/trace0 No such file or directory || This may happen for two reasons: * The firmware does not include any [[Coprocessor_resource_table|resource table]] or the resource table does not define any [[Coprocessor_resource_table#How_to_add_trace_for_the_log_buffer|trace]]. : Update the firmware resource table and rebuild the firmware * The ".resource_table" section is empty or not defined in the elf file. :Use the following command to verify it in the generated elf file: {{PC$}} readelf -l <elf file> ... 02 .data .resource_table .bss ._user_heap_stack .... |- | When starting the coprocessor from the bootloader (u-boot): "unsupported fw ver: 0 Remote Processor 0 resource table Not found : 0x00000000-0x0 " || The firmware does not include any [[Coprocessor_resource_table|resource table]]. This is only a warning that does not prevent the firmware from starting properly. "rproc load_rsc" step can be bypassed.</onlyinclude> |} == Inter processor communication == {{:Troubleshooting grid table template}}<onlyinclude> <includeonly> ! colspan="2" | Inter processor communication |-</includeonly> | Frozen firmware as consequence of a deadlock in OpenAMP during IP communication with the the main processor. || This Issue probably comes from rpmsg_virtio_rx_callback or rpmsg_virtio_send_offchannel_raw (rpmsg_virtio.c) functions that are called in interrupt context. These functions use a mutex lock in rpmsg_device struct when accessing the index of the virtio queue index. Rework your code so that these functions are not called in interrupt context. |- | Linux kernel trace: stm32-ipcc 4c001000.mailbox: Try increasing MBOX_TX_QUEUE_LEN || On each IPCC interrupt, the coprocessor treats all the buffered RPMsgesRPMsgs (one IPCC event for several RPMsgesRPMsgs). On Linux side, one IPCC signal is programmed for each RPMsg sent. This can result is an overflow warning on Linux since too many IPCC events are queued. No RPMsgesRPMsgs are dropped but this message could be interpreted as the coprocessor reaches its capacity to treat the received messages in time.<br> Consider reworking the code so that the coprocessor processes messages more efficiently or decreasing the rate of messages sent by Linux. |- | Linux kernel trace ( example with rpmsg_tty driver): rpmsg_tty virtio0.rpmsg-tty-channel.-1.0: timeout waiting for a tx buffer || This message means that there is no more TX buffer available to transmit messages to the remote processor. This may happen for two reasons: * The firmware implementation is incomplete and the coprocessor does not process any IPCC interrupt (eg interrupt disabled or interrupt handler not defined). Fix the firmware code: refer to [[IPCC_internal_peripheral]] for details on the peripheral. * The coprocessor is busy, frozen or crashed. This can be confirmed by performing a debug tool analysis. |- | Linux kernel trace: rpmsg_tty virtio0.rpmsg-tty-channel.-1.0: No memory for tty_prepare_flip_string || There is no more space in the TTY temporary buffer on reception. The root cause is probably that the Linux application did not read the tty device on time to treat the incoming TTY stream. Consider reworking the Linux application so that it takes less time to process messages or decreasing the message exchange rate. |- | Linux kernel trace: remoteproc remoteproc0: stm32_rproc_kick: failed (<mbx>, <error value>) || The Linux remoteproc driver cannot use the [[IPCC_internal_peripheral | IPCC]] mailbox. This may happen for two reasons: * The Linux kernel is built without the support of the stm32 IPCC mailbox: to enable it, refer to [[Linux_Mailbox_framework_overview#Configuration|IPCC configuration]]. * The mailboxes are not or incorrectly defined in the Linux kernel DeviceTree: fix it as described in [[Linux_remoteproc_framework_overview#Device_tree_configuration|mailbox DeviceTree]].</onlyinclude> |} <noinclude> [[Category:Coprocessor management Linux]] [[Category:Coprocessor management STM32Cube]] [[Category:Troubleshooting grids]] {{PublicationRequestId | 14609 | 2020-01-15 |}}</noinclude>
Line 53: | Line 53: | ||
stm32-ipcc 4c001000.mailbox: Try increasing MBOX_TX_QUEUE_LEN |
stm32-ipcc 4c001000.mailbox: Try increasing MBOX_TX_QUEUE_LEN |
||
|| |
|| |
||
− | On each IPCC interrupt, the coprocessor treats all the buffered |
+ | On each IPCC interrupt, the coprocessor treats all the buffered RPMsgs (one IPCC event for several RPMsgs). On Linux side, one IPCC signal is programmed for each RPMsg sent. This can result is an overflow warning on Linux since too many IPCC events are queued. No RPMsgs are dropped but this message could be interpreted as the coprocessor reaches its capacity to treat the received messages in time.<br> |
Consider reworking the code so that the coprocessor processes messages more efficiently or decreasing the rate of messages sent by Linux. |
Consider reworking the code so that the coprocessor processes messages more efficiently or decreasing the rate of messages sent by Linux. |
||
|- |
|- |