Difference between revisions of "Clock device tree configuration"

[quality revision] [quality revision]
 
m
 
Template:ArticleMainWriter Template:ArticleApprovedVersion

1 Article purpose[edit]

This article explains how to configure the RCC internal peripheral when it is assigned to the Linux® OS. In that case, it is controlled by the Common Clock framework.

The configuration is performed using the device tree mechanism that provides a hardware description of the RCC peripheral, used by the clk-stm32mp1 Linux driver and by the Common Clock framework.

2 DT bindings documentation[edit]

The Clock device tree bindings are composed ofRCC is a multifunction device.

Each function is represented by a separate binding document:

  • generic DT bindings[1] used by the Common Clock framework.
  • vendor clock DT bindings[2] used by the clk-stm32mp1 driver: this binding document explains how to write device tree files for clocks.

3 DT configuration[edit]

3.1 DT configuration (STM32 level)[edit]

The STM32MP1 Clock node is located in the stm32mp157c.dtsi[3]. See Device tree for more explanations.

3.1.1 clocks node[edit]

These clocks have a fixed frequency (generally it's they are oscillators)


	clocks {
		clk_hse: clk-hse {
			#clock-cells = <0>;
			compatible = "fixed-clock";
			clock-frequency = <24000000>;
		};

		clk_hsi: clk-hsi {
			#clock-cells = <0>;
			compatible = "fixed-clock";
			clock-frequency = <64000000>;
		};

		clk_lse: clk-lse {
			#clock-cells = <0>;
			compatible = "fixed-clock";
			clock-frequency = <32768>;
		};

		clk_lsi: clk-lsi {
			#clock-cells = <0>;
			compatible = "fixed-clock";
			clock-frequency = <32000>;
		};

		clk_csi: clk-csi {
			#clock-cells = <0>;
			compatible = "fixed-clock";
			clock-frequency = <4000000>;
		};

		...
	};

3.1.2 STM32MP1 Clock node[edit]

We need to specify the number of cell cells in a clock specifier.
For the STM32MP1 this number shoud be 1 and is configured via 'clock-cells' property in rcc node.

rcc: rcc@50000000 {
 	compatible = "st,stm32mp1-rcc", "syscon";
	#clock-cells = <1>;
	#reset-cells = <1>;
	reg = <0x50000000 0x1000>;
	...
};
Warning.png This device tree part is related to STM32MP1 microprocessors. It must be kept as is, without being modified by the end-user.

3.2 DT configuration (board level)[edit]

If a Linux driver need needs a clock, it has to add be added in its DT node:
clocks = <phandle> : List of phandle and clock specifier pairs, one pair

for each clock input to the device. Note: if the
clock provider specifies '0' for #clock-cells, then
only the phandle portion of the pair will appear.
  • Example:
usart3: serial@4000f000 {
	compatible = "st,stm32h7-usart";
	reg = <0x4000f000 0x400>;
	interrupt-names = "event", "wakeup";
	interrupts-extended = <&intc GIC_SPI 39 IRQ_TYPE_LEVEL_HIGH>,
			      <&exti 28 1>;
	clocks = <&rcc USART3_K>;
	wakeup-source;
	power-domains = <&pd_core>;
	status = "disabled";
};

4 How to configure the DT using STM32CubeMX[edit]

The STM32CubeMX tool can be used to configure the STM32MPU device and get the corresponding platform configuration device tree files.
The STM32CubeMX may not support all the properties described in the above DT bindings documentation paragraph. If so, the tool inserts user sections in the generated device tree. These sections can then be edited to add some properties and they are preserved from one generation to another. Refer to STM32CubeMX user manual for further information.

5 References[edit]

Please refer to the following links for additional information:

  1. Documentation/devicetree/bindings/clock/clock-bindings.txt , Clock device tree bindings
  2. Documentation/devicetree/bindings/clock/st,stm32mp1-rcc.txt , STM32MP1 clock device tree bindings
  3. stm32mp157c.dtsi STM32MP157C device tree file



<noinclude>

{{ArticleBasedOnModel | [[Peripheral or framework device tree configuration model]]}}
{{ArticleMainWriter | OlivierB}}
{{ArticleApprovedVersion| GabrielF | OlivierB | No previous approved version | BrunoB - 21Jan-19 - 10339 | 21Jan'19}}

[[Category:Device tree configuration]]
[[Category:Clock]] </noinclude>

== Article purpose ==

This article explains how to configure the [[RCC internal peripheral|'''RCC''' internal peripheral]] when it is assigned to the Linux<sup>&reg;</sup> OS. In that case, it is controlled by the [[Clock_overview|Common Clock framework]].

The configuration is performed using the [[Device tree|device tree]] mechanism that provides a hardware description of the RCC peripheral, used by the clk-stm32mp1 Linux driver and by  the Common Clock framework.

== DT bindings documentation ==

The Clock device tree bindings are composed ofRCC is a multifunction device.

Each function is represented by a separate binding document:

*generic DT bindings<ref>{{CodeSource | Linux kernel | Documentation/devicetree/bindings/clock/clock-bindings.txt | Documentation/devicetree/bindings/clock/clock-bindings.txt}}, Clock device tree bindings</ref> used by the Common Clock framework.

*vendor clock DT bindings<ref>{{CodeSource | Linux kernel | Documentation/devicetree/bindings/clock/st,stm32mp1-rcc.txt | Documentation/devicetree/bindings/clock/st,stm32mp1-rcc.txt}}, STM32MP1 clock device tree bindings</ref> used by the clk-stm32mp1 driver: this binding document explains how to write device tree files for clocks.

== DT configuration ==

=== DT configuration (STM32 level) ===

The STM32MP1 Clock node is located in the ''stm32mp157c.dtsi''<ref name="stm32mp157_pin_dtsi">{{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp157c.dtsi | stm32mp157c.dtsi}} STM32MP157C device tree file</ref>. See [[Device tree]] for more explanations. 

==== clocks node ====

These clocks have a fixed frequency (generally it's they are oscillators)
<pre>

	clocks {
		clk_hse: clk-hse {
			#clock-cells = <0>;
			compatible = "fixed-clock";
			clock-frequency = <24000000>;
		};

		clk_hsi: clk-hsi {
			#clock-cells = <0>;
			compatible = "fixed-clock";
			clock-frequency = <64000000>;
		};

		clk_lse: clk-lse {
			#clock-cells = <0>;
			compatible = "fixed-clock";
			clock-frequency = <32768>;
		};

		clk_lsi: clk-lsi {
			#clock-cells = <0>;
			compatible = "fixed-clock";
			clock-frequency = <32000>;
		};

		clk_csi: clk-csi {
			#clock-cells = <0>;
			compatible = "fixed-clock";
			clock-frequency = <4000000>;
		};

		...
	};</pre>


==== STM32MP1 Clock node ====
We need to specify the number of cellcells in a clock specifier. <br/>

For the STM32MP1 this number shoud be 1 and is configured via 'clock-cells' property in rcc node.

 rcc: rcc@50000000 {
  	compatible = "st,stm32mp1-rcc", "syscon";
 	'''#clock-cells = <1>;'''
 	#reset-cells = <1>;
 	reg = <0x50000000 0x1000>;
 	...
 };

{{Warning|This device tree part is related to STM32MP1 microprocessors. It must be kept as is, without being modified by the end-user.}}

=== DT configuration (board level) ===

If a Linux driver needneeds a clock, it has to add be added in its DT node:<br/>

clocks = <phandle> :          List of phandle and clock specifier pairs, one pair
:::::for each clock input to the device.  Note: if the
:::::clock provider specifies '0' for #clock-cells, then
:::::only the phandle portion of the pair will appear.

*Example:

 usart3: serial@4000f000 {
 	compatible = "st,stm32h7-usart";
 	reg = <0x4000f000 0x400>;
 	interrupt-names = "event", "wakeup";
 	interrupts-extended = <&intc GIC_SPI 39 IRQ_TYPE_LEVEL_HIGH>,<&exti 28 1>;
 	'''clocks = <&rcc USART3_K>;'''
 	wakeup-source;
 	power-domains = <&pd_core>;
 	status = "disabled";
 };

==How to configure the DT using STM32CubeMX==
The [[STM32CubeMX]] tool can be used to configure the STM32MPU device and get the corresponding [[Device_tree#STM32|platform configuration device tree]] files.<br />

The STM32CubeMX may not support all the properties described in the above [[#DT bindings documentation|DT bindings documentation]] paragraph. If so, the tool inserts '''user sections''' in the generated device tree. These sections can then be edited to add some properties and they are preserved from one generation to another. Refer to [[STM32CubeMX]] user manual for further information.

==References==
Please refer to the following links for additional information:
<references />

<noinclude>

{{ArticleBasedOnModel | Peripheral or framework device tree configuration model}}
{{PublicationRequestId | 10339 | 2019-01-21 | BrunoB}}

[[Category:Device tree configuration]]
[[Category:Clock]] </noinclude>
(One intermediate revision by one other user not shown)
Line 1: Line 1:
<noinclude>
 
{{ArticleBasedOnModel | [[Peripheral or framework device tree configuration model]]}}
 
{{ArticleMainWriter | OlivierB}}
 
{{ArticleApprovedVersion| GabrielF | OlivierB | No previous approved version | BrunoB - 21Jan-19 - 10339 | 21Jan'19}}
 
 
[[Category:Device tree configuration]]
 
[[Category:Clock]]
 
</noinclude>
 
 
 
== Article purpose ==
 
== Article purpose ==
   
Line 16: Line 7:
 
== DT bindings documentation ==
 
== DT bindings documentation ==
   
The Clock device tree bindings are composed of:
+
The RCC is a multifunction device.
  +
 
  +
Each function is represented by a separate binding document:
   
 
*generic DT bindings<ref>{{CodeSource | Linux kernel | Documentation/devicetree/bindings/clock/clock-bindings.txt | Documentation/devicetree/bindings/clock/clock-bindings.txt}}, Clock device tree bindings</ref> used by the Common Clock framework.
 
*generic DT bindings<ref>{{CodeSource | Linux kernel | Documentation/devicetree/bindings/clock/clock-bindings.txt | Documentation/devicetree/bindings/clock/clock-bindings.txt}}, Clock device tree bindings</ref> used by the Common Clock framework.
Line 30: Line 23:
 
==== clocks node ====
 
==== clocks node ====
   
These clocks have a fixed frequency (generally it's oscillators)
+
These clocks have a fixed frequency (generally they are oscillators)
   
   
Line 70: Line 63:
   
 
==== STM32MP1 Clock node ====
 
==== STM32MP1 Clock node ====
We need to specify the number of cell in a clock specifier. <br/>
+
We need to specify the number of cells in a clock specifier. <br/>
 
For the STM32MP1 this number shoud be 1 and is configured via 'clock-cells' property in rcc node.
 
For the STM32MP1 this number shoud be 1 and is configured via 'clock-cells' property in rcc node.
   
Line 85: Line 78:
 
=== DT configuration (board level) ===
 
=== DT configuration (board level) ===
   
If a Linux driver need a clock, it has to add in its DT node:<br/>
+
If a Linux driver needs a clock, it has to be added in its DT node:<br/>
 
clocks = <phandle> :          List of phandle and clock specifier pairs, one pair
 
clocks = <phandle> :          List of phandle and clock specifier pairs, one pair
 
:::::for each clock input to the device.  Note: if the
 
:::::for each clock input to the device.  Note: if the
Line 113: Line 106:
   
 
<references />
 
<references />
  +
  +
<noinclude>
  +
{{ArticleBasedOnModel | Peripheral or framework device tree configuration model}}
  +
{{PublicationRequestId | 10339 | 2019-01-21 | BrunoB}}
  +
  +
[[Category:Device tree configuration]]
  +
[[Category:Clock]]
  +
</noinclude>

Attachments

Discussions