This category groups together all articles that are applicable for the STM32MP25x lines.
Subcategories
This category has the following 12 subcategories, out of 12 total.
A
I
M
O
S
T
X
Pages in category "STM32MP25x"
The following 200 pages are in this category, out of 706 total.
(previous page) (next page)H
- How to control a GPIO in kernel space
- How to control a GPIO in userspace
- How to control a RNG in userspace
- How to convert a Tensorflow Lite model to ONNX using tf2onnx
- How to create a bridge between ETH1, ETH2, ETH3
- How to create a new open embedded layer
- How to create an SDK for OpenSTLinux distribution
- How to create secure project on STM32MP25 co-processor in STM32CubeIDE
- How to create Signed FIT image from Distribution package
- How to create your board device tree
- How to create your own distribution
- How to create your own image
- How to create your own machine
- How to cross-compile with the Developer Package
- How to cross-compile with the Distribution Package
- How to customize Linux kernel for Android
- How to customize OpenSTDroid distribution
- How to customize the Linux kernel
- How to debug a user space application with STM32CubeIDE/User space CDT project
- How to debug a user space application with STM32CubeIDE/User space GTK library project
- How to debug a user space application with STM32CubeIDE/User space project
- How to debug a user space application with STM32CubeIDE/User space shared library project
- How to debug a user space application with STM32CubeIDE/User space static library project
- How to debug OP-TEE
- How to debug TF-A BL2
- How to debug Weston
- How to define your low-power strategy
- How to deploy SSP using a step-by-step approach
- How to deploy your NN model on STM32MPU
- How to detect memory leaks
- How to develop a Rust Application
- How to develop an OP-TEE Trusted Application
- How to develop an OP-TEE Trusted Application with STM32CubeIDE
- How to develop an X-Linux Expansion Package
- How to disable one CPU
- How to display an image using Weston
- How to display on HDMI
- How to enable earlycon for Linux kernel
- How to enable secure boot on STM32 MPU
- How to encode a video stream with the hardware video encoder
- How to encrypt a disk with dm-crypt
- How to exchange data buffers with the coprocessor
- How to find Linux kernel driver associated to a device
- How to find the description of a color format and check its support
- How to generate training artifacts for on-device learning feature
- How to get DRM KMS logs
- How to get name and current status of a DRM connector
- How to get Terminal
- How to get video details
- How to install JAVA JDK
- How to install the Yocto Project SDK in STM32CubeIDE
- How to integrate an external software package
- How to launch glmark2 benchmark
- How to launch Khronos OpenGLES conformance tests
- How to load U-Boot with dfu-util
- How to load U-Boot with STM32CubeProgrammer
- How to make a camera preview
- How to make a screen capture in Weston
- How to make a video capture of Weston desktop
- How to manage MP2 OpenSTLinux projects in STM32CubeIDE
- How to manage MP2 OpenSTLinux projects in STM32CubeIDE/SD card update with customized trusted image
- How to manually update bootloaders
- How to measure performance of your NN models using TensorFlow Lite runtime
- How to measure the DDR throughput
- How to measure the performance of NBG-based models
- How to measure the performance of your models using ONNX Runtime
- How to modify the panel backlight
- How to monitor the display framerate
- How to monitor the GCNANO GPU load
- How to optimize the boot time
- How to perform ping test
- How to perform Secure Boot from Distribution Package
- How to perform ssh connection
- How to play a video
- How to play a video with the hardware video decoder
- How to play audio
- How to populate boards for Android
- How to populate the SD card with dd command
- How to profile video framerate
- How to protect the coprocessor firmware
- How to record audio
- How to retrain a NN model using ONNXRuntime on STM32MP2x
- How to run inference using the STAI MPU Cpp API
- How to run inference using the STAI MPU Python API
- How to scan BLE devices
- How to scan Bluetooth devices
- How to Secure Firmware Update
- How to send or receive CAN data
- How to set up a Bluetooth connection
- How to set up a SocketCAN interface
- How to setup a WLAN connection
- How to setup the DDR configuration
- How to sign a software image using an external HSM
- How to start the coprocessor from the bootloader
- How to stop and start Weston
- How to stream RAW camera over network
- How to support EXT4 through MMC
- How to support UBIFS through MTD
- How to test and benchmark OpenGLES
- How to transcode a video
- How to transfer a file over network
- How to transfer a file over serial console
- How to tune ISP using the STM32 ISP IQTune
- How to tune RGMII GTX clock delay
- How to update OTP with U-Boot
- How to use hardware acceleration with TensorFlow Lite and ONNX Runtime frameworks
- How to use ISP features
- How to use libcamera
- How to use LTDC layers from CM33 and CA35 simultaneously
- How to use SPI from Linux userland with spidev
- How to use the Cortex-M0+
- How to use the DCMIPP ISP
- How to use the IIO user space interface
- How to use the kernel dynamic debug
- How to use the RTC
- How to use the secure display feature
- How to use TTY with User Terminal
- How to use U-Boot stm32key command
- How to use UART as serial boot device with STM32CubeProgrammer
- How to use USB mass storage in U-Boot
- How to verify the hardware video decoder and encoder activities
- How to write a display panel or bridge driver
- How to write a low resolution and slow interface display panel driver
- HPDMA device tree configuration
- HPDMA internal peripheral
I
- I2C device tree configuration
- I2C i2c-tools
- I2C internal peripheral
- I2C overview
- I2S device tree configuration
- I2S Linux driver
- I3C device tree configuration
- I3C internal peripheral
- I3C overview
- IAC internal peripheral
- Ifconfig
- IIO libiio
- IIO Linux kernel tools
- IIO overview
- Image classification
- Install STM32CubeMP2 package
- Install the IDE
- Install the SDK
- Interrupt overview
- IP Linux command line
- IPCC device tree configuration
- IPCC internal peripheral
- IWDG device tree configuration
- IWDG internal peripheral
L
- Latest wiki
- LEDs and buttons on STM32 MPU boards
- LegalInformation:Legal notice
- Linux application frameworks overview
- Linux Mailbox framework overview
- Linux remoteproc framework overview
- Linux RPMsg framework overview
- Linux tracing, monitoring and debugging
- LPDMA internal peripheral
- LPTIM device tree configuration
- LPTIM internal peripheral
- LPTIM Linux driver
- LPUART internal peripheral
- LTDC device tree configuration
- LTDC internal peripheral
- Ltrace
- LTTng
- LVDS device tree configuration
- LVDS internal peripheral