This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.The STM32Cube MPU Packages[1] are the embedded software bricks of the STM32Cube ecosystem[2], made to run on STM32 microprocessors.
The following STM32Cube MPU Packages are available:
- STM32CubeMP13 Package, running on the Arm® Cortex®-A7 processor, for the STM32MP13x lines
- STM32CubeMP15 Package, running on the Arm® Cortex®-M4 coprocessor, for the STM32MP15x lines
STM32Cube MPU packages offer for every STM32 MPU series all the required embedded software bricks to operate the available set of peripherals, including:
- The hardware abstraction layer (HAL) enabling portability between different STM32 devices via standardized API calls
- Low-layer (LL) APIs, and a lightweight, optimized, expert-oriented set of APIs designed for both performance and runtime efficiency
- A collection of examples, running on an MPU board and allowing demonstration of a basic implementation of features from a set of IPs
- A collection of middleware components including RTOS, USB library, file system, TCP/IP stack, OpenAMP and ResourceManage (depending on the lines)
- A collection of applications, running on an MPU board and allowing demonstration of a basic implementation of features from middleware
- The BSP drivers are based on HAL drivers and provide an API set for the evaluation board and third-party components.
Subcategories
This category has the following 3 subcategories, out of 3 total.