Difference between revisions of "Calibration device tree configuration"

[unchecked revision] [quality revision]
m
m
Applicable for STM32MP13x lines, STM32MP15x lines

1 Article purpose[edit]

The purpose of this article is to explain how to configure the OP-TEE Calibration service using the device tree mechanism, relying on the bindings documentation, that is the description of the required and optional device-tree properties.

2 DT bindings documentation[edit]

The device tree binding documents are stored in the given applicable components listed:

3 DT configuration[edit]

This hardware description is a combination of the STM32 microprocessor device tree files (.dtsi extension) and board device tree files (.dts extension). See the Device tree for an explanation of the device-tree file organization.

STM32CubeMX can be used to generate the board device tree. Refer to How to configure the DT using STM32CubeMX for more details.

3.1 DT configuration (STM32/SoC level)[edit]

The Calibration node is located in the device tree file for the software components, supporting the peripheral and listed in the above DT bindings documentation paragraph.

Warning white.png Warning
This device tree part is related to STM32 microprocessors. It must be kept as is, without being modified by the end-user.

3.1.1 STM32MP13x lines Warning.png[edit]

By default, Timer12 is the default counter used by both HSI/CSI calibration node at SoC level.

3.1.2 STM32MP15x lines More info.png[edit]

By default, Timer15 is the default counter used by both HSI/CSI calibration node at SoC level.

3.2 DT configuration (board level)[edit]

The objective of this chapter is to explain how to enable and configure the calibration DT nodes for a board.

Configuration should be done in specific board device tree files (board dts file).
By default, both HSI/CSI calibration are disabled. It must be explicitly enable at board level.

3.3 DT configuration examples[edit]

Here is an example for CSI calibration activation:

&csi-calibration {
	status = "okay";
};

Here is an example for HSI calibration activation with a counter update:

&hsi-calibration {
	counter = <&timers15 0 7>;
	status = "okay";
};
Warning white.png Warning
The timer channel entry is SoC specific for the internal signal calibration. Refer to How to configure the DT using STM32CubeMX for more details

4 How to configure the DT using STM32CubeMX[edit]

The STM32CubeMX tool can be used to configure the STM32MPU device and get the corresponding platform configuration device tree files.
STM32CubeMX may not support all the properties described in DT binding files listed in the above DT bindings documentation paragraph. If so, the tool inserts user sections in the generated device tree. These sections can then be edited to add some properties, and they are preserved from one generation to another. Refer to STM32CubeMX user manual for further information.

5 References[edit]

Refer to the following links for additional information:


<noinclude>{{ApplicableFor
|MPUs list=STM32MP13x, STM32MP15x
|MPUs checklist=STM32MP13x, STM32MP15x
}}</noinclude>

== Article purpose ==
The purpose of this article is to explain how to configure the [[OP-TEE_Calibration_PTA_overview|'''OP-TEE Calibration service''']] using the [[Device tree|device tree]] mechanism, relying on the bindings documentation, that is the description of the required and optional device-tree properties.

== DT bindings documentation ==
The device tree binding documents are stored in the given applicable components listed: <br>


* OP-TEE OS:
** Calibration device tree bindings: {{CodeSource | OP-TEE_OS | documentation/devicetree/bindings/clock/st,stm32-calibration.yaml}}

== DT configuration ==
This hardware description is a combination of the '''STM32 microprocessor''' device tree files (''.dtsi'' extension) and '''board''' device tree files (''.dts'' extension). See the [[Device tree]] for an explanation of the device-tree file organization.

'''STM32CubeMX''' can be used to generate the board device tree. Refer to [[#How_to_configure_the_DT_using_STM32CubeMX|How to configure the DT using STM32CubeMX]] for more details.

===DT configuration (STM32/SoC level) ===
The  '''Calibration''' node is located in the [[STM32 MPU device_tree#Device tree structure|device tree file]] for the software components, supporting the peripheral and listed in the above [[#DT bindings documentation|DT bindings documentation]] paragraph.

{{Warning|This device tree part is related to STM32 microprocessors. It must be kept as is, without being modified by the end-user.}}

==== {{MicroprocessorDevice | device=13}} ====
By default,  [[TIM_internal_peripheral|Timer12]] is the default counter used by both HSI/CSI calibration node at SoC level.

==== {{MicroprocessorDevice | device=15}} ====
By default,  [[TIM_internal_peripheral|Timer15]] is the default counter used by both HSI/CSI calibration node at SoC level.

=== DT configuration (board level) ===
The objective of this chapter is to explain how to enable and configure the '''calibration''' DT nodes for a board.<br>


Configuration should be done in specific board device tree files (board dts file).<br>

By default, both HSI/CSI calibration are disabled. It must be explicitly enable at board level.

=== DT configuration examples ===
Here is an example for CSI calibration activation:
<pre>

&csi-calibration {
	status = "okay";
};</pre>


Here is an example for HSI calibration activation with a counter update:<pre>

&hsi-calibration {
	counter = <&timers15 0 7>;
	status = "okay";
};</pre>


{{Warning| The timer channel entry is SoC specific for the internal signal calibration. Refer to [[#How_to_configure_the_DT_using_STM32CubeMX|How to configure the DT using STM32CubeMX]] for more details}}

==How to configure the DT using STM32CubeMX==
The [[STM32CubeMX]] tool can be used to configure the STM32MPU device and get the corresponding [[Device_tree#STM32|platform configuration device tree]] files.<br />

STM32CubeMX may not support all the properties described in DT binding files listed in the above [[#DT bindings documentation|DT bindings documentation]] paragraph. If so, the tool inserts '''user sections''' in the generated device tree. These sections can then be edited to add some properties, and they are preserved from one generation to another. Refer to [[STM32CubeMX]] user manual for further information.

==References==
Refer to the following links for additional information:<references />

<noinclude>

[[Category:Device tree configuration]]
[[Category:OP-TEE_Clock]]</noinclude>
Line 23: Line 23:
   
 
==== {{MicroprocessorDevice | device=13}} ====
 
==== {{MicroprocessorDevice | device=13}} ====
By default,  [[TIM_internal_peripheral|Timer12]] is the default counter used by both HSI/CSI calibration node at SoC level.
+
By default,  [[TIM_internal_peripheral|Timer12]] is the counter used by both HSI/CSI calibration node at SoC level.
   
 
==== {{MicroprocessorDevice | device=15}} ====
 
==== {{MicroprocessorDevice | device=15}} ====
By default,  [[TIM_internal_peripheral|Timer15]] is the default counter used by both HSI/CSI calibration node at SoC level.
+
By default,  [[TIM_internal_peripheral|Timer15]] is the counter used by both HSI/CSI calibration node at SoC level.
   
 
=== DT configuration (board level) ===
 
=== DT configuration (board level) ===