Difference between revisions of "CRYP device tree configuration"

[quality revision] [quality revision]
m
 

1 Article purpose[edit]

The purpose of this article is to explain how to configure the CRYP[1] when the peripheral is assigned to Linux® OS.

The configuration is performed using the device tree mechanism[2].

The Device tree provides a hardware description of the CRYP[1], used by STM32 CRYP Linux driver.

If the peripheral is assigned to another execution context, refer to How to assign an internal peripheral to a runtime context article for guidelines on peripheral assignment and configuration.

2 DT bindings documentation[edit]

The CRYP [1] is represented by the STM32 CRYP device tree bindings[3].

3 DT configuration[edit]

This hardware description is a combination of STM32 microprocessor and board device tree files. See Device tree for explanations on device tree file split.

The STM32CubeMX can be used to generate the board device tree. Refer to #How_to_configure_the_DT_using_STM32CubeMX for more details.

3.1 DT configuration (STM32 level)[edit]

The CRYP node is declared in stm32mp15xcstm32mp157c.dtsi[4] and stm32mp15xf. dtsi[5]. It provides the hardware registers base address, clock, interrupt and reset.

cryp1: cryp@54001000 {
	compatible = "st,stm32mp1-cryp";
	reg = <0x54001000 0x400>;
	interrupts = <GIC_SPI 79 IRQ_TYPE_LEVEL_HIGH>;
	clocks = <&scmi0_clk CK_SCMI0_rcc CRYP1>;
	resets = <&scmi0_resetrcc RSTCRYP1_SCMI0_CRYP1>R>;
	status = "disabled";
};
Warning.png This device tree part is related to STM32 microprocessors. It should be kept as is, without being modified by the end-user.

3.2 DT configuration (board level)[edit]

This part is used to enable the CRYP used on a board. This is done by setting the status property to okay.

3.3 DT configuration examples[edit]

&cryp1 {
	status = "okay";
};

4 How to configure the DT using STM32CubeMX[edit]

The STM32CubeMX tool can be used to configure the STM32MPU device and get the corresponding platform configuration device tree files.
The STM32CubeMX may not support all the properties described in the above DT bindings documentation paragraph. If so, the tool inserts user sections in the generated device tree. These sections can then be edited to add some properties and they are preserved from one generation to another. Refer to STM32CubeMX user manual for further information.

5 References[edit]

Please refer to the following links for additional information:



== Article purpose ==
The purpose of this article is to explain how to configure the ''CRYP''<ref name="CRYP internal peripheral"> [[CRYP internal peripheral]] </ref> ''' when the peripheral is assigned to Linux<sup>&reg;</sup> OS'''. 

The configuration is performed using the '''device tree mechanism'''<ref> [[Device tree]]</ref>.

The [[Device tree]] provides a hardware description of the ''CRYP''<ref name="CRYP internal peripheral"/>, used by STM32 ''CRYP Linux driver''.

If the peripheral is assigned to another execution context, refer to [[How to assign an internal peripheral to a runtime context]] article for guidelines on peripheral assignment and configuration.

== DT bindings documentation ==
The ''CRYP'' <ref name="CRYP internal peripheral"/> is represented by the ''STM32 CRYP device tree bindings''<ref>{{CodeSource | Linux kernel | Documentation/devicetree/bindings/crypto/st,stm32-cryp.txt | Documentation/devicetree/bindings/crypto/st,stm32-cryp.txt}}</ref>.

== DT configuration ==
This hardware description is a combination of STM32 microprocessor and board device tree files. See [[Device tree]] for explanations on device tree file split.

The '''STM32CubeMX''' can be used to generate the board device tree. Refer to [[#How_to_configure_the_DT_using_STM32CubeMX]] for more details.

===DT configuration (STM32 level) ===
The CRYP node is declared in stm32mp15xcstm32mp157c.dtsi<ref name="stm32mp15xcstm32mp157c_dtsi">{{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp15xcstm32mp157c.dtsi | STM32MP157C device tree file}}</ref> and stm32mp15xf.dtsi<ref name="stm32mp15xf_dtsi">{{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp15xf.dtsi | STM32MP157F device tree file}}</ref>. . It provides the hardware registers base address, clock, interrupt and reset.

 cryp1: cryp@54001000 {
 	compatible = "st,stm32mp1-cryp";
 	reg = <0x54001000 0x400>;
 	interrupts = <GIC_SPI 79 IRQ_TYPE_LEVEL_HIGH>;
 	clocks = <&scmi0_clk CK_SCMI0_CRYP1><&rcc CRYP1>;
 	resets = <&scmi0_reset RST_SCMI0_CRYP1><&rcc CRYP1_R>;
 	status = "disabled";
 };

{{Warning|This device tree part is related to STM32 microprocessors. It should be kept as is, without being modified by the end-user.}}

=== DT configuration (board level) ===
This part is used to enable the CRYP used on a board. This is done by setting the '''status''' property to '''okay'''.

=== DT configuration examples ===
 &cryp1 {
 	status = "okay";
 };

==How to configure the DT using STM32CubeMX==
The [[STM32CubeMX]] tool can be used to configure the STM32MPU device and get the corresponding [[Device_tree#STM32|platform configuration device tree]] files.<br />

The STM32CubeMX may not support all the properties described in the above [[#DT bindings documentation|DT bindings documentation]] paragraph. If so, the tool inserts '''user sections''' in the generated device tree. These sections can then be edited to add some properties and they are preserved from one generation to another. Refer to [[STM32CubeMX]] user manual for further information.

==References==
Please refer to the following links for additional information:<references />

<noinclude>

[[Category:Device tree configuration]]
[[Category:Crypto]]
{{PublicationRequestId | 8896 | 2018-09-21 | BrunoB}}
{{ArticleBasedOnModel|Peripheral or framework device tree configuration model}}
{{ReviewsComments|JCT 1840: alignment needed with the last version of the model<br>

[[Category:ToBeAlignedWithModel]]
}}</noinclude>
Line 17: Line 17:
   
 
===DT configuration (STM32 level) ===
 
===DT configuration (STM32 level) ===
The CRYP node is declared in stm32mp157c.dtsi<ref name="stm32mp157c_dtsi">{{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp157c.dtsi | STM32MP157C device tree file}}</ref>. It provides the hardware registers base address, clock, interrupt and reset.
+
The CRYP node is declared in stm32mp15xc.dtsi<ref name="stm32mp15xc_dtsi">{{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp15xc.dtsi | STM32MP157C device tree file}}</ref> and stm32mp15xf.dtsi<ref name="stm32mp15xf_dtsi">{{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp15xf.dtsi | STM32MP157F device tree file}}</ref>. It provides the hardware registers base address, clock, interrupt and reset.
   
 
  cryp1: cryp@54001000 {
 
  cryp1: cryp@54001000 {
Line 23: Line 23:
 
  reg = <0x54001000 0x400>;
 
  reg = <0x54001000 0x400>;
 
  interrupts = <GIC_SPI 79 IRQ_TYPE_LEVEL_HIGH>;
 
  interrupts = <GIC_SPI 79 IRQ_TYPE_LEVEL_HIGH>;
  clocks = <&rcc CRYP1>;
+
  clocks = <&scmi0_clk CK_SCMI0_CRYP1>;
  resets = <&rcc CRYP1_R>;
+
  resets = <&scmi0_reset RST_SCMI0_CRYP1>;
 
  status = "disabled";
 
  status = "disabled";
 
  };
 
  };