Difference between revisions of "CRC internal peripheral"

[quality revision] [quality revision]
m (Cleanup)
m (Software frameworks)

1 Article purpose[edit]

The purpose of this article is to

  • briefly introduce the CRC peripheral and its main features
  • indicate the level of security supported by this hardware block
  • explain how each instance can be allocated to the three runtime contexts and linked to the corresponding software components
  • explain how to configure the CRC peripheral.

2 Peripheral overview[edit]

The CRC peripheral is used to verify data transmission or storage integrity.

2.1 Features[edit]

Refer to the STM32MP15 reference manuals for the complete list of features, and to the software components, introduced below, to see which features are implemented.

2.2 Security support[edit]

CRC1 and CRC2 are non secure peripherals.

3 Peripheral usage and associated software[edit]

3.1 Boot time[edit]

CRC instances are not used at boot time.

3.2 Runtime[edit]

3.2.1 Overview[edit]

CRC instances can be allocated to:

or

Chapter Peripheral assignment describes which peripheral instance can be assigned to which context.

3.2.2 Software frameworks[edit]

Domain Peripheral Software components Comment
OP-TEE Linux STM32Cube
Security CRC Linux Crypto framework STM32Cube CRC driver

3.2.3 Peripheral configuration[edit]

The configuration is applied by the firmware running in the context to which the peripheral is assigned. The configuration can be done alone via the STM32CubeMX tool for all internal peripherals, and then manually completed (particularly for external peripherals), according to the information given in the corresponding software framework article.

3.2.4 Peripheral assignment[edit]

Internal peripherals

Check boxes illustrate the possible peripheral allocations supported by STM32 MPU Embedded Software:

  • means that the peripheral can be assigned () to the given runtime context.
  • is used for system peripherals that cannot be unchecked because they are statically connected in the device.

Refer to How to assign an internal peripheral to a runtime context for more information on how to assign peripherals manually or via STM32CubeMX.
The present chapter describes STMicroelectronics recommendations or choice of implementation. Additional possiblities might be described in STM32MP15 reference manuals.

Domain Peripheral Runtime allocation Comment
Instance Cortex-A7
secure
(OP-TEE)
Cortex-A7
non-secure
(Linux)
Cortex-M4

(STM32Cube)
Security CRC CRC1
CRC2

4 How to go further[edit]

Not applicable.

5 References[edit]




==Article purpose==
The purpose of this article is to
* briefly introduce the CRC  peripheral and its main features
* indicate the level of security supported by this hardware block
* explain how each instance can be allocated to the three runtime contexts and linked to the corresponding software components
* explain how to configure the CRC peripheral.
==Peripheral overview==
The '''CRC''' peripheral is used to verify data transmission or storage integrity.<br />


===Features===
Refer to the [[STM32MP15 resources#Reference manuals|STM32MP15 reference manuals]] for the complete list of features, and to the software components, introduced below, to see which features are implemented.

===Security support===
CRC1 and CRC2 are '''non secure''' peripherals.

==Peripheral usage and associated software==
===Boot time===
CRC instances are not used at boot time.

===Runtime===
====Overview====
CRC instances can be allocated to:
* the Arm<sup>&reg;</sup> Cortex<sup>&reg;</sup>-A7 non-secure for using in Linux<sup>&reg;</sup> with [[Crypto_API_overview|Linux Crypto framework]]
or
* the Arm<sup>&reg;</sup> Cortex<sup>&reg;</sup>-M4 for using in STM32Cube with [[STM32CubeMP1 architecture|STM32Cube CRC driver]]

Chapter [[#Peripheral assignment|Peripheral assignment]] describes which peripheral instance can be assigned to which context.

====Software frameworks====
{{:Internal_peripherals_software_table_template}}
 | rowspan="9" | Security
 | rowspan="9" | Security
 | [[CRC internal peripheral|CRC]]
 |-
 |
 | 

 | [[Crypto_API_overview|Linux Crypto framework]]
 | [[STM32CubeMP1 architecture|STM32Cube CRC driver]]
 |

 |-
 |}

====Peripheral configuration====
The configuration is applied by the firmware running in the context to which the peripheral is assigned. The configuration can be done alone via the [[STM32CubeMX]] tool for all internal peripherals, and then manually completed (particularly for external peripherals), according to the information given in the corresponding software framework article.

====Peripheral assignment====
{{:Internal_peripherals_assignment_table_template}}<onlyinclude>

 | rowspan="2" | Security
 | rowspan="2" | [[CRC internal peripheral|CRC]]
 | CRC1
 | 
 | <span title="assignable peripheral" style="font-size:21px"></span>

 |
 |
 |-
 | CRC2
 | 
 | 
 | <span title="assignable peripheral" style="font-size:21px"></span>

 |
 |-</onlyinclude>

 |}

==How to go further==
Not applicable.

==References==<references/>

<noinclude>

{{ArticleBasedOnModel| [[Internal peripheral article model]]}}
{{PublicationRequestId | 8786 | 2018-09-19 | AlainF}}
[[Category:Security peripherals]]</noinclude>
Line 29: Line 29:
 
====Software frameworks====
 
====Software frameworks====
 
{{:Internal_peripherals_software_table_template}}
 
{{:Internal_peripherals_software_table_template}}
  | rowspan="9" | Security
+
  | Security
  | rowspan="9" | [[CRC internal peripheral|CRC]]
+
  | [[CRC internal peripheral|CRC]]
|-
 
 
  |
 
  |
 
  | [[Crypto_API_overview|Linux Crypto framework]]
 
  | [[Crypto_API_overview|Linux Crypto framework]]
 
  | [[STM32CubeMP1 architecture|STM32Cube CRC driver]]
 
  | [[STM32CubeMP1 architecture|STM32Cube CRC driver]]
  +
|
 
  |-
 
  |-
 
  |}
 
  |}