Difference between revisions of "BSEC device tree configuration"
[checked revision] | [quality revision] |
(→DT configuration (board level): add nvmem_layout node description from v1.2.0)
|
m (Reverted edits by Nicolas Le Bayon (talk) to last revision by philip sage)
(Tag: Rollback)
|
Contents
- 1 Article purpose
- 2 DT bindings documentation
- 3 DT configuration 4
- 4 STM32MP1 nvmem_layout node (bootloader specific) for ecosystem release ≥ v1.2.0
- How to configure the DT using STM32CubeMX
- 5 References
1 Article purpose[edit]
![]() |
This article explains how to configure BSEC at boot time. |
This article describes the BSEC configuration performed using the device tree mechanism, which provides a hardware description of the BSEC peripheral.
2 DT bindings documentation[edit]
Generic information about NVMEM is available in NVMEM overview.
The following binding-related documentation explains how to write device tree files for BSEC:
- TF-A: tf-a/docs/devicetree/bindings/soc/st,stm32-romem.txt"[1]
- Linux® BSEC devicetree bindings: Documentation/devicetree/bindings/nvmem/st,stm32-romem.txt[2]
- Linux® generic NVMEM devicetree bindings: Documentation/devicetree/bindings/nvmem/nvmem.txt[3]
3 DT configuration[edit]
This hardware description is a combination of the STM32 microprocessor device tree files (.dtsi extension) and board device tree files (.dts extension). See the Device tree for an explanation of the device-tree file split.
STM32CubeMX can be used to generate the board device tree. Refer to How to configure the DT using STM32CubeMX for more details.
3.1 DT configuration (STM32 level)[edit]
The STM32MP1 BSEC node is located in stm32mp157c.dtsi[4] (see Device tree for further explanation).
/ {
...
soc {
...
bsec: nvmem@5c005000 {
compatible = "st,stm32mp15-bsec";
reg = <0x5c005000 0x400>;
#address-cells = <1>;
#size-cells = <1>;
ts_cal1: calib@5c {
reg = <0x5c 0x2>;
};
ts_cal2: calib@5e {
reg = <0x5e 0x2>;
};
};
...
};
...
};
Please refer to the NVMEM overview for the bindings common with Linux® kernel.
3.2 DT configuration (board level)[edit]
3.2.1 STM32MP1 BSEC node append[edit]
Board definition in the device tree may add some board-specific OTP declarations:
For ecosystem release ≥ v1.
&bsec {
board_id: board_id@ec {
reg = <0xec 0x4>;
st,non-secure-otp;
};
};
With only 32 lower NVMEM 32-bit data words, software needs to manage exceptions in order to allow some upper OTPs to be accessed by non-secure world, through secure world services for very specific needs. User can add OTP declaration in device tree, using "st,non-secure-otp" property, with a 32-bit length granularity (i.e. 4 bytes).
For ecosystem release ≥ v1.2.0
1.0
&bsec {
board_id: board_id@ec {
reg = <0xec 0x4>;
status = "okay";
};
};
The upper OTPs are intended to contain sensitive data such as keys or passwords. However, with only 32 lower NVMEM 32-bit data words, the software may need more. It is therefore possible, for very specific needs, to manage exceptions in order to allow some upper OTPs to be accessed by the non-secure world through secure-world services.
The user can add upper OTP declarations in the device tree by using the status property to define accessibility conditions, as described in the following table:
status | Upper OTP available from |
---|---|
disabled | secure only (normal behavior) |
okay | non-secure and secure (exception) |
![]() |
When status property is not filled, this is implicitly set as an "okay" status by default. |
![]() |
secure-status property can appear in some OTP declarations, please don't care. |
For ecosystem release v1.0.0
&bsec {
board_id: board_id@ec {
reg = <0xec 0x4>;
};
};
As in the previous section, exceptions are managed, but they are only checked in the case of closed_device BSEC mode. In open_device mode, all upper-OTP non-secure accesses are allowed. See STM32MP15 reference manuals for more information about these modes.
3.2.2 STM32MP1 BSEC node append (bootloader specific)[edit]
The bootloader-specific STM32MP1 BSEC node append data is located in stm32mp157c-security.dtsi[5] (see Device tree for further explanation).
&bsec {
mac_addr: mac_addr@e4 {
reg = <0xe4
Please find the "st,non-secure-otp" definition in the previous section above. No more spare field declaration here.
For ecosystem release ≤ v1.1.0
&bsec { mac_addr: mac_addr@e4 { reg = <0xe4
0x6>;
};
/* Spare field to align on 32-bit OTP granularity */
spare_ns_ea: spare_ns_ea@ea {
reg = <0xea 0x2>;
};
};
3.2.3 STM32MP1 driver node append[edit]
The driver can directly consume NVMEM data cells, as described in NVMEM overview.
The ADC_TEMP device is a good example, with a dedicated OTP containing calibration information.
The device node is located in the stm32mp157c.dtsi[6] file.
adc_temp: temp {
compatible = "st,stm32mp1-adc-temp";
io-channels = <&adc2 12>;
nvmem-cells = <&ts_cal1>, <&ts_cal2>;
nvmem-cell-names = "ts_cal1", "ts_cal2";
#io-channel-cells = <0>;
#thermal-sensor-cells = <0>;
status = "disabled";
};
With these nvmem-cells / nvmem-cell-names properties, the ADC_TEMP device can easily find the OTP number, in order to access calibration information.
4
The STM32MP1 nvmem_layout node gathers all NVMEM platform-dependent layout information, including OTP names and phandles, in order to allow easy access for data consumers, using pre-defined string in nvmem-cell-names property.
nvmem_layout: nvmem_layout@0 {
compatible = "st,stm32mp1-nvmem-layout";
nvmem-cells = <&cfg0_otp>,
<&part_number_otp>,
<&monotonic_otp>,
<&nand_otp>,
<&uid_otp>,
<&package_otp>,
<&hw2_otp>,
<&board_id>;
nvmem-cell-names = "cfg0_otp",
"part_number_otp",
"monotonic_otp",
"uid_otp",
"nand_otp",
"package_otp",
"hw2_otp",
"board_id";
};
With this new node, the platform can easily find the OTP numbers, in order to access all necessary information.
4How to configure the DT using STM32CubeMX[edit]
The STM32CubeMX tool can be used to configure the STM32MPU device and get the corresponding platform configuration device tree files.
STM32CubeMX may not support all the properties described in the documents listed in DT bindings documentation above. If so, the tool inserts user sections in the generated device tree. These sections can then be edited to add some properties that are preserved from one generation to another. Refer to the STM32CubeMX user manual for further information.
5 References[edit]
Please refer to the following links for additional information:
- ↑ docs/devicetree/bindings/soc/st,stm32-romem.txt TF-A BSEC binding information file
- ↑ Documentation/devicetree/bindings/nvmem/st,stm32-romem.txt
- ↑ Documentation/devicetree/bindings/nvmem/nvmem.txt
- ↑ fdts/stm32mp157c.dtsi (for TF-A): STM32MP157C device tree files
- ↑ fdts/stm32mp157c-security.dtsi (for TF-A): STM32MP157C device tree files
- ↑ arch/arm/boot/dts/stm32mp157c.dtsi
== Article purpose == {{Warning|This article explains how to configure [[BSEC_internal_peripheral|BSEC]] at boot time.}} This article describes the [[BSEC internal peripheral|BSEC]] configuration performed using the [[Device tree|device tree]] mechanism, which provides a hardware description of the [[BSEC_internal_peripheral|BSEC]] peripheral. == DT bindings documentation == Generic information about NVMEM is available in [[NVMEM_overview#Device_tree_configuration|NVMEM overview]]. The following binding-related documentation explains how to write device tree files for BSEC: * [[TF-A overview|TF-A]]: ''tf-a/docs/devicetree/bindings/soc/st,stm32-romem.txt"<ref name="st,stm32-romem.txt"> {{CodeSource | TF-A | docs/devicetree/bindings/soc/st,stm32-romem.txt}} [[TF-A overview|TF-A]] BSEC binding information file</ref> * Linux<sup>®</sup> BSEC devicetree bindings: Documentation/devicetree/bindings/nvmem/st,stm32-romem.txt<ref name="Linux,st,stm32-romem">{{CodeSource | Linux kernel | Documentation/devicetree/bindings/nvmem/st,stm32-romem.txt}}</ref> * Linux<sup>®</sup> generic NVMEM devicetree bindings: Documentation/devicetree/bindings/nvmem/nvmem.txt<ref name="nvmem.txt">{{CodeSource | Linux kernel | Documentation/devicetree/bindings/nvmem/nvmem.txt}}</ref> == DT configuration == This hardware description is a combination of the '''STM32 microprocessor''' device tree files (''.dtsi'' extension) and '''board''' device tree files (''.dts'' extension). See the [[Device tree]] for an explanation of the device-tree file split. '''STM32CubeMX''' can be used to generate the board device tree. Refer to [[#How_to_configure_the_DT_using_STM32CubeMX|How to configure the DT using STM32CubeMX]] for more details. === DT configuration (STM32 level) === The STM32MP1 [[BSEC_internal_peripheral|BSEC]] node is located in ''stm32mp157c.dtsi''<ref name="stm32mp157_pin_dtsi">{{CodeSource | TF-A | fdts/stm32mp157c.dtsi}} (for [[TF-A overview|TF-A]]): STM32MP157C device tree files</ref> (see [[Device tree]] for further explanation). / { ... soc { ... bsec: nvmem@5c005000 { compatible = "st,stm32mp15-bsec"; reg = <0x5c005000 0x400>; #address-cells = <1>; #size-cells = <1>; ts_cal1: calib@5c { reg = <0x5c 0x2>; }; ts_cal2: calib@5e { reg = <0x5e 0x2>; }; }; ... }; ... }; Please refer to the [[NVMEM_overview#Device_tree_configuration|NVMEM overview]] for the bindings common with Linux<sup>®</sup> kernel. === DT configuration (board level) === ==== STM32MP1 BSEC node append ====<div class="mw-collapsible-content"> Board definition in the device tree may add some board-specific OTP declarations: '''For {{EcosystemRelease | revision=1.21.0 | range=and after}}''' &bsec { board_id: board_id@ec { reg = <0xec 0x4>;st,non-secure-otp; }; }; With only 32 lower NVMEM 32-bit data words, software needs to manage exceptions in order to allow some upper OTPs to be accessed by non-secure world, through secure world services for very specific needs. User can add OTP declaration in device tree, using "st,non-secure-otp" property, with a 32-bit length granularity (i.e. 4 bytes).<br/> <div class="mw-collapsible mw-collapsed"> '''For {{EcosystemRelease | revision=1.1.0}}'''<div class="mw-collapsible-content"> &bsec { board_id: board_id@ec { reg = <0xec 0x4>;status = "okay"; }; }; The upper OTPs are intended to contain sensitive data such as keys or passwords. However, with only 32 lower NVMEM 32-bit data words, the software may need more. It is therefore possible, for very specific needs, to manage exceptions in order to allow some upper OTPs to be accessed by the non-secure world through secure-world services.<br/> The user can add upper OTP declarations in the device tree by using the status property to define accessibility conditions, as described in the following table:<br/> {| class="st-table" ! status !! Upper OTP available from |- | disabled || secure only (normal behavior) |- | okay || non-secure and secure (exception) |} {{Info|When status property is not filled, this is implicitly set as an "okay" status by default.}} {{Info|secure-status property can appear in some OTP declarations, please don't care.}}</div></div> <div class="mw-collapsible mw-collapsed"> '''For {{EcosystemRelease | revision=1.0.0}}'''<div class="mw-collapsible-content"> &bsec { board_id: board_id@ec { reg = <0xec 0x4>; }; }; As in the previous section, exceptions are managed, but they are only checked in the case of closed_device [[BSEC internal peripheral|BSEC]] mode. In open_device mode, all upper-OTP non-secure accesses are allowed. See [[STM32MP15 resources#Reference manuals|STM32MP15 reference manuals]] for more information about these modes. <br/> </div></div> ==== STM32MP1 BSEC node append (bootloader specific) ==== The bootloader-specific STM32MP1 [[BSEC_internal_peripheral|BSEC]] node append data is located in ''stm32mp157c-security.dtsi''<ref name="stm32mp157_security_dtsi">{{CodeSource | TF-A | fdts/stm32mp157c-security.dtsi}} (for [[TF-A overview|TF-A]]): STM32MP157C device tree files</ref> (see [[Device tree]] for further explanation).<br /> This completes NVMEM data providers, only for bootloader specific purpose, either for a driver, or the platform itself. '''For {{EcosystemRelease | revision=1.2.0 | range=and after}}''' &bsec { cfg0_otp: cfg0_otp@0 { reg = <0x0 0x1>; }; part_number_otp: part_number_otp@4 { reg = <0x4 0x1>; }; monotonic_otp: monotonic_otp@10 { reg = <0x10 0x4>; }; nand_otp: nand_otp@24 { reg = <0x24 0x4>; }; uid_otp: uid_otp@34 { reg = <0x34 0xc>; }; package_otp: package_otp@40 { reg = <0x40 0x4>; }; hw2_otp: hw2_otp@48 { reg = <0x48 0x4>; }; &bsec {mac_addr: mac_addr@e4 { reg = <0xe4 0x80x6>; st,non-secure-otp; }; }; Please find the "st,non-secure-otp" definition in the previous section above. No more spare field declaration here. <div class="mw-collapsible mw-collapsed"> '''For {{EcosystemRelease | revision=1.1.0 | range=and before}}'''<div class="mw-collapsible-content"> &bsec { mac_addr: mac_addr@e4 { reg = <0xe4 0x6>; };};/* Spare field to align on 32-bit OTP granularity */ spare_ns_ea: spare_ns_ea@ea { reg = <0xea 0x2>; }; };</div></div> ==== STM32MP1 driver node append ==== The driver can directly consume NVMEM data cells, as described in [[NVMEM_overview#Device_tree_configuration|NVMEM overview]].<br/> The ADC_TEMP device is a good example, with a dedicated OTP containing calibration information.<br/> The device node is located in the ''stm32mp157c.dtsi''<ref>{{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp157c.dtsi}}</ref> file. adc_temp: temp { compatible = "st,stm32mp1-adc-temp"; io-channels = <&adc2 12>; nvmem-cells = <&ts_cal1>, <&ts_cal2>; nvmem-cell-names = "ts_cal1", "ts_cal2"; #io-channel-cells = <0>; #thermal-sensor-cells = <0>; status = "disabled"; }; With these nvmem-cells / nvmem-cell-names properties, the ADC_TEMP device can easily find the OTP number, in order to access calibration information.<br/> ==== STM32MP1 nvmem_layout node (bootloader specific) for {{EcosystemRelease | revision=1.2.0 | range=and after}} ==== The STM32MP1 nvmem_layout node gathers all NVMEM platform-dependent layout information, including OTP names and phandles, in order to allow easy access for data consumers, using pre-defined string in nvmem-cell-names property. nvmem_layout: nvmem_layout@0 { compatible = "st,stm32mp1-nvmem-layout"; nvmem-cells = <&cfg0_otp>,<&part_number_otp>,<&monotonic_otp>,<&nand_otp>,<&uid_otp>,<&package_otp>,<&hw2_otp>,<&board_id>; nvmem-cell-names = "cfg0_otp", "part_number_otp", "monotonic_otp", "uid_otp", "nand_otp", "package_otp", "hw2_otp", "board_id"; }; With this new node, the platform can easily find the OTP numbers, in order to access all necessary information. ==How to configure the DT using STM32CubeMX== The [[STM32CubeMX]] tool can be used to configure the STM32MPU device and get the corresponding [[Device_tree#STM32|platform configuration device tree]] files.<br /> STM32CubeMX may not support all the properties described in the documents listed in [[#DT bindings documentation|DT bindings documentation]] above. If so, the tool inserts '''user sections''' in the generated device tree. These sections can then be edited to add some properties that are preserved from one generation to another. Refer to the [[STM32CubeMX]] user manual for further information. ==References== Please refer to the following links for additional information: <references /> <noinclude> [[Category:Device tree configuration]] [[Category:Trusted Firmware-A (TF-A)]] {{ArticleBasedOnModel | Peripheral or framework device tree configuration model}} {{PublicationRequestId | 13613 | 2019-10-09 | }}</noinclude>
Line 36: | Line 36: | ||
reg = <0x5e 0x2>; |
reg = <0x5e 0x2>; |
||
}; |
}; |
||
− | + |
}; |
|
... |
... |
||
}; |
}; |
||
Line 46: | Line 46: | ||
=== DT configuration (board level) === |
=== DT configuration (board level) === |
||
==== STM32MP1 BSEC node append ==== |
==== STM32MP1 BSEC node append ==== |
||
+ | <div class="mw-collapsible-content"> |
||
Board definition in the device tree may add some board-specific OTP declarations: |
Board definition in the device tree may add some board-specific OTP declarations: |
||
− | '''For {{EcosystemRelease | revision=1. |
+ | '''For {{EcosystemRelease | revision=1.1.0 | range=and after}}''' |
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
&bsec { |
&bsec { |
||
board_id: board_id@ec { |
board_id: board_id@ec { |
||
Line 79: | Line 69: | ||
{{Info|When status property is not filled, this is implicitly set as an "okay" status by default.}} |
{{Info|When status property is not filled, this is implicitly set as an "okay" status by default.}} |
||
{{Info|secure-status property can appear in some OTP declarations, please don't care.}} |
{{Info|secure-status property can appear in some OTP declarations, please don't care.}} |
||
− | |||
<div class="mw-collapsible mw-collapsed"> |
<div class="mw-collapsible mw-collapsed"> |
||
'''For {{EcosystemRelease | revision=1.0.0}}''' |
'''For {{EcosystemRelease | revision=1.0.0}}''' |
||
Line 93: | Line 82: | ||
==== STM32MP1 BSEC node append (bootloader specific) ==== |
==== STM32MP1 BSEC node append (bootloader specific) ==== |
||
− | The bootloader-specific STM32MP1 [[BSEC_internal_peripheral|BSEC]] node append data is located in ''stm32mp157c-security.dtsi''<ref name="stm32mp157_security_dtsi">{{CodeSource | TF-A | fdts/stm32mp157c-security.dtsi}} (for [[TF-A overview|TF-A]]): STM32MP157C device tree files</ref> (see [[Device tree]] for further explanation). |
+ | The bootloader-specific STM32MP1 [[BSEC_internal_peripheral|BSEC]] node append data is located in ''stm32mp157c-security.dtsi''<ref name="stm32mp157_security_dtsi">{{CodeSource | TF-A | fdts/stm32mp157c-security.dtsi}} (for [[TF-A overview|TF-A]]): STM32MP157C device tree files</ref> (see [[Device tree]] for further explanation). |
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
&bsec { |
&bsec { |
||
mac_addr: mac_addr@e4 { |
mac_addr: mac_addr@e4 { |
||
Line 139: | Line 93: | ||
}; |
}; |
||
}; |
}; |
||
− | |||
==== STM32MP1 driver node append ==== |
==== STM32MP1 driver node append ==== |
||
Line 157: | Line 110: | ||
With these nvmem-cells / nvmem-cell-names properties, the ADC_TEMP device can easily find the OTP number, in order to access calibration information.<br/> |
With these nvmem-cells / nvmem-cell-names properties, the ADC_TEMP device can easily find the OTP number, in order to access calibration information.<br/> |
||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
==How to configure the DT using STM32CubeMX== |
==How to configure the DT using STM32CubeMX== |