Difference between revisions of "BSEC device tree configuration"
[quality revision] | [quality revision] |
m (→STM32MP1 driver node append: reminder for later around example)
|
m (→BSEC node append)
|
Applicable for | STM32MP13x lines, STM32MP15x lines |
Contents
- 1 Article purpose
- 2 DT bindings documentation
- 3 DT configuration 4
- 4 STM32MP1 nvmem_layout node (bootloader specific) for ecosystem release ≥ v1.2.0
- How to configure the DT using STM32CubeMX
- 5 References
1 Article purpose[edit]

The purpose of this article is to explain how to configure
BSEC at boot time.This article describes the BSEC configuration performed using the device tree mechanism, which provides a hardware relying on the bindings documentation, that is the description of the BSEC peripheralrequired and optional device-tree properties.
2 DT bindings documentation[edit]
Generic information about NVMEM is available in the NVMEM overview.
The following binding-related documentation explains how to write device tree files binding documents for BSEC are stored either in the given applicable components listed below, or in the Linux kernel repository:
-
TF-A : tf-a/BL2:
- for example: docs/devicetree/bindings/soc/st,stm32-romem.txt
-
OP-TEE:
- for example: STM32 BSEC device tree bindings: documentation/devicetree/bindings/nvmem/st,stm32-romem.yaml
-
U-Boot, Linux® OS:
- for example: STM32 BSEC device tree bindings: Documentation/devicetree/bindings/nvmem/st,stm32-romem.
- yaml
- for example: generic NVMEM devicetree bindings: Documentation/devicetree/bindings/nvmem/nvmem.
3 DT configuration[edit]
This hardware description is a combination of the STM32 microprocessor device tree files (.dtsi extension) and board device tree files (.dts extension). See the Device tree for an explanation of the device-tree file splitorganization.
STM32CubeMX can be used to generate the board device tree. Refer to How to configure the DT using STM32CubeMX for more details.
3.1 DT configuration (STM32/SoC level)[edit]
The STM32MP1 BSEC node is located in stm32mp157c.dtsi[4] (see Device tree for further explanation).
/ {
...
soc {
...
bsec: nvmem@5c005000 {
compatible = "st,stm32mp15-bsec";
reg = <0x5c005000 0x400>;
#address-cells = <1>;
#size-cells = <1>;
ts_cal1: calib@5c {
reg = <0x5c 0x2>;
};
ts_cal2: calib@5e {
reg = <0x5e 0x2>;
};
};
...
};
...
};
Please refer to the NVMEM overview for the bindings common with Linux® kernel.
and NVMEM node are located in the device tree file for the software components, supporting the peripheral and listed in the above DT bindings documentation paragraph.
![]() |
This device tree part is related to STM32 microprocessors. It must be kept as is, without being modified by the end-user. |
3.2 DT configuration (board level)[edit]
The objective of this chapter is to explain how to enable and configure the BSEC DT nodes for a board.
Peripheral configuration should be done in specific board device tree files (board dts file).
3.2.1 STM32MP1 BSEC node append[edit]
Board The board definition in the device tree may add include some additional board-specific OTP declarations:
For ecosystem release ≥ v1.2.0
, for example to add a NVMEM data cell:
&bsec { calib@20 { reg = <0x20 0x2>; }; board_id: board_id@ec { reg = <0xec 0x4>; st,non-secure-otp; }; };
With only 32 lower NVMEM 32-bit data words, software needs to manage exceptions in order to allow some upper OTPs to be accessed by non-secure world, through secure world services for very specific needs. User can add OTP declaration in device tree, using "st,non-secure-otp" property, with a 32-bit length granularity (i.e. 4 bytes).
For ecosystem release v1.1.0
&bsec { board_id: board_id@ecoem_enc_key@170 { reg =<0xec
<0x1700x4>
0x10>;status = "okay"
st,non-secure-otp-provisioning; }; };The upper OTPs are intended to contain sensitive data such as keys or passwords. However, with only
Only the 32 lower NVMEM 32-bit data words
, the software may need more. It is therefore possible, for very specific needs, to manage exceptions in orderare accessible by the non-secure world by default; the secure world software (OP-TEE or SP-MIN) needs to manage exceptions to allow some upper OTPs to be accessed by the non-secure world, through secure
-world services.The user can add upper OTP declarations in the device tree by using the status property to define accessibility conditions, as described in the following table:
status | Upper OTP available from |
---|---|
disabled | secure only (normal behavior) |
okay | non-secure and secure (exception) |
![]() |
When status property is not filled, this is implicitly set as an "okay" status by default. |
![]() |
secure-status property can appear in some OTP declarations, please don't care. |
For ecosystem release v1.0.0
&bsec {
board_id: board_id@ec {
reg = <0xec 0x4>;
};
};
As in the previous section, exceptions are managed, but they are only checked in the case of closed_device BSEC mode. In open_device mode, all upper-OTP non-secure accesses are allowed. See STM32MP15 reference manuals for more information about these modes.
The bootloader-specific STM32MP1 BSEC node append data is located in stm32mp157c-security.dtsi[5] (see Device tree for further explanation).
This completes NVMEM data providers, only for bootloader specific purpose, either for a driver, or the platform itself.
For ecosystem release ≥ v1.2.0
&bsec {
cfg0_otp: cfg0_otp@0 {
reg = <0x0 0x1>;
};
part_number_otp: part_number_otp@4 {
reg = <0x4 0x1>;
};
monotonic_otp: monotonic_otp@10 {
reg = <0x10 0x4>;
};
nand_otp: nand_otp@24 {
reg = <0x24 0x4>;
};
uid_otp: uid_otp@34 {
reg = <0x34 0xc>;
};
package_otp: package_otp@40 {
reg = <0x40 0x4>;
};
hw2_otp: hw2_otp@48 {
reg = <0x48 0x4>;
};
mac_addr: mac_addr@e4 {
reg = <0xe4 0x8>;
st,non-secure-otp;
};
};
Please find the "st,non-secure-otp" definition in the previous section above. No more spare field declaration here.
For ecosystem release ≤ v1.1.0
&bsec {
mac_addr: mac_addr@e4 {
reg = <0xe4 0x6>;
};
/* Spare field to align on 32-bit OTP granularity */
spare_ns_ea: spare_ns_ea@ea {
reg = <0xea 0x2>;
};
};
3.2.3 STM32MP1 driver node append[edit]
The driver can directly consume NVMEM data cells, as described in NVMEM overview.The ADC_TEMP device is a good example, with a dedicated OTP containing calibration information.
The device node is located in the stm32mp157c.dtsi[6] file.
adc_temp: temp {
compatible = "st,stm32mp1-adc-temp";
io-channels = <&adc2 12>;
nvmem-cells = <&ts_cal1>, <&ts_cal2>;
nvmem-cell-names = "ts_cal1", "ts_cal2";
#io-channel-cells = <0>;
#thermal-sensor-cells = <0>;
status = "disabled";
};
With these nvmem-cells / nvmem-cell-names properties, the ADC_TEMP device can easily find the OTP number, in order to access calibration information.
The STM32MP1 nvmem_layout node gathers all NVMEM platform-dependent layout information, including OTP names and phandles, in order to allow easy access for data consumers, using pre-defined string in nvmem-cell-names property.
nvmem_layout: nvmem_layout@0 {
compatible = "st,stm32mp1-nvmem-layout";
nvmem-cells = <&cfg0_otp>,
<&part_number_otp>,
<&monotonic_otp>,
<&nand_otp>,
<&uid_otp>,
<&package_otp>,
<&hw2_otp>,
<&board_id>;
nvmem-cell-names = "cfg0_otp",
"part_number_otp",
"monotonic_otp",
"uid_otp",
"nand_otp",
"package_otp",
"hw2_otp",
"board_id";
};
With this new node, the platform can easily find the OTP numbers, in order to access all necessary information.
world services for very specific needs as described in documentation/devicetree/bindings/nvmem/st,stm32-romem.yaml .
This exceptions are defined by the OTP declaration in the secure world device tree with a 32-bit length granularity (that is, 4 bytes):
- using the st,non-secure-otp property to allow a read/write
- using the st,non-secure-otp-provisioning property to allow a write until the first programmed value or permanent lock; used for secrets used by secure world but provisioned by the non-secured world.
See example core/arch/arm/dts/stm32mp135f-dk.dts .
4 How to configure the DT using STM32CubeMX[edit]
The STM32CubeMX tool can be used to configure the STM32MPU device and get the corresponding platform configuration device tree files.
STM32CubeMX may not support all the properties described in the documents DT binding files listed in the above DT bindings documentation above paragraph. If so, the tool inserts user sections in the generated device tree. These sections can then be edited to add some properties that , and they are preserved from one generation to another. Refer to the STM32CubeMX user manual for further information.
5 References[edit]
Please refer to the following links for additional information:
- ↑ docs/devicetree/bindings/soc/st,stm32-romem.txt TF-A BSEC binding information file
- ↑ Documentation/devicetree/bindings/nvmem/st,stm32-romem.txt
- ↑ Documentation/devicetree/bindings/nvmem/nvmem.txt
- ↑ fdts/stm32mp157c.dtsi (for TF-A): STM32MP157C device tree files
- ↑ fdts/stm32mp157c-security.dtsi (for TF-A): STM32MP157C device tree files
- ↑ arch/arm/boot/dts/stm32mp157c.dtsi
== Article purpose == {{Warning|This article explains how to configure [[BSEC_internal_peripheral|BSEC]] at boot time.}} This article describes <noinclude>{{ApplicableFor |MPUs list=STM32MP13x, STM32MP15x |MPUs checklist=STM32MP13x,STM32MP15x }}</noinclude> == Article purpose == The purpose of this article is to explain how to configure the [[BSEC internal peripheral|BSEC]] configuration performed using the [[Device tree|device tree]] mechanism, which provides a hardware description of the [[BSEC_internal_peripheral|BSEC]] peripheralrelying on the bindings documentation, that is the description of the required and optional device-tree properties. == DT bindings documentation == Generic information about NVMEM is available in the [[NVMEM_overview#Device_tree_configuration|NVMEM overview]]. The following device tree binding-related documentation explains how to write device tree files for BSEC: * [[TF-A overview|TF-A]]: ''tf-a/ documents for [[BSEC internal peripheral|BSEC]] are stored either in the given applicable components listed below, or in the Linux kernel repository: * TF-A BL2: **for example: {{CodeSource | TF-A | docs/devicetree/bindings/soc/st,stm32-romem.txt"<ref name="st,stm32-romem.txt"> {{CodeSource | TF-A | docs/devicetree/bindings/soc/st,stm32-romem.txt}} [[TF-A overview|TF-A]] BSEC binding information file</ref> * }} * OP-TEE: ** for example: STM32 BSEC device tree bindings: {{CodeSource | OP-TEE_OS | documentation/devicetree/bindings/nvmem/st,stm32-romem.yaml}} * U-Boot, Linux<sup>®</sup> BSEC devicetree bindings: Documentation/devicetree/bindings/nvmem/st,stm32-romem.txt<ref name="Linux,st,stm32-romem">OS: ** for example: STM32 BSEC device tree bindings: {{CodeSource | Linux kernel | Documentation/devicetree/bindings/nvmem/st,stm32-romem.txt}}</ref> * Linux<sup>®</sup> yaml}} ** for example: generic NVMEM devicetree bindings: {{CodeSource | Linux kernel | Documentation/devicetree/bindings/nvmem/nvmem.txt<ref name="nvmem.txt">yaml}}, {{CodeSource | Linux kernel | Documentation/devicetree/bindings/nvmem/nvmem.txt}}</ref>-consumer.yaml}} == DT configuration == This hardware description is a combination of the '''STM32 microprocessor''' device tree files (''.dtsi'' extension) and '''board''' device tree files (''.dts'' extension). See the [[Device tree]] for an explanation of the device-tree file splitorganization. '''STM32CubeMX''' can be used to generate the board device tree. Refer to [[#How_to_configure_the_DT_using_STM32CubeMX|How to configure the DT using STM32CubeMX]] for more details. === DT configuration (STM32/SoC level) === The STM32MP1 [[BSEC_internal_peripheral|BSEC]] node is located in ''stm32mp157c.dtsi''<ref name="stm32mp157_pin_dtsi">{{CodeSource | TF-A | fdts/stm32mp157c.dtsi}} (for [[TF-A overview|TF-A]]): STM32MP157C device tree files</ref> (see [[Device tree]] for further explanation). / { ... soc { ... bsec: nvmem@5c005000 { compatible = "st,stm32mp15-bsec"; reg = <0x5c005000 0x400>; #address-cells = <1>; #size-cells = <1>; ts_cal1: calib@5c { reg = <0x5c 0x2>; }; ts_cal2: calib@5e { reg = <0x5e 0x2>; }; }; ... }; ... }; Please refer to the [[and [[NVMEM_overview#Device_tree_configuration|NVMEM overview]] for the bindings common with Linux<sup>®</sup> kernel. === DT configuration (board level) === ==== STM32MP1 BSEC node append ==== Board definition in the device tree may add some board-specific OTP declarations: '''For {{EcosystemRelease | revision=1.2.0 | range=and after}}''' &bsec { board_id: board_id@ec { reg = <0xec 0x4>; st,non-secure-otp; }; }; With only 32 lower NVMEM 32-bit data words, software needs to manage exceptions in order to allow some upper OTPs to be accessed by non-secure world, through secure world services for very specific needs. User can add OTP declaration in device tree, using "st,non-secure-otp" property, with a 32-bit length granularity (i.e. 4 bytes).<br/> <div class="mw-collapsible mw-collapsed"> '''For {{EcosystemRelease | revision=1.1.0}}'''<div class="mw-collapsible-content"> &bsec { board_id: board_id@ec { reg = <0xec 0x4>; status = "okay"; }; }; The upper OTPs are intended to contain sensitive data such as keys or passwords. However, with only 32 lower NVMEM 32-bit data words, the software may need more. It is therefore possible, for very specific needs, to manage exceptions in order to allow some upper OTPs to be accessed by the non-secure world through secure-world services.<br/> The user can add upper OTP declarations in the device tree by using the status property to define accessibility conditions, as described in the following table:<br/> {| class="st-table" ! status !! Upper OTP available from |- | disabled || secure only (normal behavior) |- | okay || non-secure and secure (exception) |} {{Info|When status property is not filled, this is implicitly set as an "okay" status by default.}} {{Info|secure-status property can appear in some OTP declarations, please don't care.}}</div></div> <div class="mw-collapsible mw-collapsed"> '''For {{EcosystemRelease | revision=1.0.0}}'''<div class="mw-collapsible-content"> &bsec { board_id: board_id@ec { reg = <0xec 0x4>; }; }; As in the previous section, exceptions are managed, but they are only checked in the case of closed_device [[BSEC internal peripheral|BSEC]] mode. In open_device mode, all upper-OTP non-secure accesses are allowed. See [[STM32MP15 resources#Reference manuals|STM32MP15 reference manuals]] for more information about these modes. <br/> </div></div> ==== STM32MP1 BSEC node append (bootloader specific) ==== The bootloader-specific STM32MP1 [[BSEC_internal_peripheral|BSEC]] node append data is located in ''stm32mp157c-security.dtsi''<ref name="stm32mp157_security_dtsi">{{CodeSource | TF-A | fdts/stm32mp157c-security.dtsi}} (for [[TF-A overview|TF-A]]): STM32MP157C device tree files</ref> (see [[Device tree]] for further explanation).<br /> This completes NVMEM data providers, only for bootloader specific purpose, either for a driver, or the platform itself. '''For {{EcosystemRelease | revision=1.2.0 | range=and after}}''' &bsec { cfg0_otp: cfg0_otp@0 { reg = <0x0 0x1>; }; part_number_otp: part_number_otp@4 { reg = <0x4 0x1>; }; monotonic_otp: monotonic_otp@10 { reg = <0x10 0x4>; }; nand_otp: nand_otp@24 { reg = <0x24 0x4>; }; uid_otp: uid_otp@34 { reg = <0x34 0xc>; }; package_otp: package_otp@40 { reg = <0x40 0x4>; }; hw2_otp: hw2_otp@48 { reg = <0x48 0x4>; }; mac_addr: mac_addr@e4 { reg = <0xe4 0x8>;]] node are located in the [[STM32 MPU device_tree#Device tree structure|device tree file]] for the software components, supporting the peripheral and listed in the above [[#DT bindings documentation|DT bindings documentation]] paragraph. {{Warning|This device tree part is related to STM32 microprocessors. It must be kept as is, without being modified by the end-user.}} === DT configuration (board level) === The objective of this chapter is to explain how to enable and configure the [[BSEC_internal_peripheral|BSEC]] DT nodes for a board. Peripheral configuration should be done in specific board device tree files (board dts file). ==== BSEC node append ==== The board definition in the device tree may include some additional board-specific OTP declarations, for example to add a NVMEM data cell: &bsec { calib@20 { reg = <0x20 0x2>; }; board_id: board_id@ec { reg = <0xec 0x4>; {{highlightParam|st,non-secure-otp}}; }; oem_enc_key@170 { reg = <0x170 0x10>; {{highlightParam|st,non-secure-otp; }; }; Please find the "st,non-secure-otp" definition in the previous section above. No more spare field declaration here. <div class="mw-collapsible mw-collapsed"> '''For {{EcosystemRelease | revision=1.1.0 | range=and before}}'''<div class="mw-collapsible-content"> &bsec { mac_addr: mac_addr@e4 { reg = <0xe4 0x6>; }; /* Spare field to align on 32-bit OTP granularity */ spare_ns_ea: spare_ns_ea@ea { reg = <0xea 0x2>; }; };</div></div> ==== STM32MP1 driver node append ==== {{ReviewsComments|FGA W2004: Just a reminder for later: the example bellow will require update/removal in V2.0.0, as the ADC temp sensor will be removed in V2.0.0 and later release}} {{ReviewsComments|NLB W2005: Let's keep this example for 1.2.0. If another example is possible for 2.0.0, an update will be done. If not, the ADC_TEMP example will stay in the 1.2.0 dedicated section, and a message in the 2.0.0 will indicate to refer to it as a template for specific implementation in 2.0.0.}} The driver can directly consume NVMEM data cells, as described in [[NVMEM_overview#Device_tree_configuration|NVMEM overview]].<br/> The ADC_TEMP device is a good example, with a dedicated OTP containing calibration information.<br/> The device node is located in the ''stm32mp157c.dtsi''<ref>{{CodeSource | Linux kernel | arch/arm/boot/dts/stm32mp157c.dtsi}}</ref> file. adc_temp: temp { compatible = "st,stm32mp1-adc-temp"; io-channels = <&adc2 12>; nvmem-cells = <&ts_cal1>, <&ts_cal2>; nvmem-cell-names = "ts_cal1", "ts_cal2"; #io-channel-cells = <0>; #thermal-sensor-cells = <0>; status = "disabled"; }; With these nvmem-cells / nvmem-cell-names properties, the ADC_TEMP device can easily find the OTP number, in order to access calibration information.<br/> ==== STM32MP1 nvmem_layout node (bootloader specific) for {{EcosystemRelease | revision=1.2.0 | range=and after}} ==== The STM32MP1 nvmem_layout node gathers all NVMEM platform-dependent layout information, including OTP names and phandles, in order to allow easy access for data consumers, using pre-defined string in nvmem-cell-names property. nvmem_layout: nvmem_layout@0 { compatible = "st,stm32mp1-nvmem-layout"; nvmem-cells = <&cfg0_otp>,<&part_number_otp>,<&monotonic_otp>,<&nand_otp>,<&uid_otp>,<&package_otp>,<&hw2_otp>,<&board_id>; nvmem-cell-names = "cfg0_otp", "part_number_otp", "monotonic_otp", "uid_otp", "nand_otp", "package_otp", "hw2_otp", "board_id"; }; With this new node, the platform can easily find the OTP numbers, in order to access all necessary information-provisioning}}; }; }; Only the 32 lower NVMEM 32-bit data words are accessible by the non-secure world by default; the '''secure world software''' (OP-TEE or SP-MIN) needs to manage exceptions to allow some upper OTPs to be accessed by the non-secure world, through secure world services for very specific needs as described in {{CodeSource | OP-TEE_OS | documentation/devicetree/bindings/nvmem/st,stm32-romem.yaml}}. {{Warning| These upper OTP 32-bit length words are ECC-protected. To avoid an invalid ECC, computed after a second write operation, these 64 upper OTPs should be be permanent write locked when they are programmed.}} This exceptions are defined by the OTP declaration in the secure world device tree with a 32-bit length granularity (that is, 4 bytes): * using the {{highlightParam|st,non-secure-otp}} property to allow a read/write * using the {{highlightParam|st,non-secure-otp-provisioning}} property to allow a write until the first programmed value or permanent lock; used for secrets used by secure world but provisioned by the non-secured world. See example {{CodeSource | OP-TEE_OS | core/arch/arm/dts/stm32mp135f-dk.dts}}. ==How to configure the DT using STM32CubeMX== The [[STM32CubeMX]] tool can be used to configure the STM32MPU device and get the corresponding [[Device_tree#STM32_MPU|platform configuration device tree]] files.<br /> STM32CubeMX may not support all the properties described in the documents listed in DT binding files listed in the above [[#DT bindings documentation|DT bindings documentation]] aboveparagraph. If so, the tool inserts '''user sections''' in the generated device tree. These sections can then be edited to add some properties that , and they are preserved from one generation to another. Refer to the [[STM32CubeMX]] user manual for further information. ==References== Please refer to the following links for additional information: <references /> <noinclude> [[Category:Device tree configuration]] [[Category:Trusted Firmware-A (TF-A)]]OP-TEE Persistent storage]] {{ArticleBasedOnModel | Peripheral or framework device tree configuration model}} {{PublicationRequestId | 13613 | 2019-10-09 | 15044 | 2020-02-21 | 13613 (PhilipS - 2019-10-09))}}</noinclude>
(55 intermediate revisions by 8 users not shown) | |||
Line 1: | Line 1: | ||
+ | <noinclude>{{ApplicableFor |
||
+ | |MPUs list=STM32MP13x, STM32MP15x |
||
+ | |MPUs checklist=STM32MP13x,STM32MP15x |
||
+ | }}</noinclude> |
||
== Article purpose == |
== Article purpose == |
||
− | + |
The purpose of this article is to explain how to configure the [[BSEC internal peripheral|BSEC]] using the [[Device tree|device tree]] mechanism, relying on the bindings documentation, that is the description of the required and optional device-tree properties. |
|
− | |||
− | |||
== DT bindings documentation == |
== DT bindings documentation == |
||
− | Generic information about NVMEM is available in [[NVMEM_overview#Device_tree_configuration|NVMEM overview]]. |
+ | Generic information about NVMEM is available in the [[NVMEM_overview#Device_tree_configuration|NVMEM overview]]. |
− | The |
+ | The device tree binding documents for [[BSEC internal peripheral|BSEC]] are stored either in the given applicable components listed below, or in the Linux kernel repository: |
− | * |
+ | * TF-A BL2:
|
− | * Linux<sup>®</sup> BSEC |
+ |
**for example: {{CodeSource | TF-A | docs/devicetree/bindings/soc/st,stm32-romem.txt}}
|
− | * |
+ |
* OP-TEE:
|
+ |
** for example: STM32 BSEC device tree bindings: {{CodeSource | OP-TEE_OS | documentation/devicetree/bindings/nvmem/st,stm32-romem.yaml}} |
||
+ | * U-Boot, Linux<sup>®</sup> OS:
|
||
+ |
** for example: STM32 BSEC device tree bindings: {{CodeSource | Linux kernel | Documentation/devicetree/bindings/nvmem/st,stm32-romem.yaml}} |
||
+ | ** for example: generic NVMEM devicetree bindings: {{CodeSource | Linux kernel | Documentation/devicetree/bindings/nvmem/nvmem.yaml}}, {{CodeSource | Linux kernel | Documentation/devicetree/bindings/nvmem/nvmem-consumer.yaml}} |
||
== DT configuration == |
== DT configuration == |
||
− | This hardware description is a combination of the '''STM32 microprocessor''' device tree files (''.dtsi'' extension) and '''board''' device tree files (''.dts'' extension). See the [[Device tree]] for an explanation of the device-tree file |
+ | This hardware description is a combination of the '''STM32 microprocessor''' device tree files (''.dtsi'' extension) and '''board''' device tree files (''.dts'' extension). See the [[Device tree]] for an explanation of the device-tree file organization. |
'''STM32CubeMX''' can be used to generate the board device tree. Refer to [[#How_to_configure_the_DT_using_STM32CubeMX|How to configure the DT using STM32CubeMX]] for more details. |
'''STM32CubeMX''' can be used to generate the board device tree. Refer to [[#How_to_configure_the_DT_using_STM32CubeMX|How to configure the DT using STM32CubeMX]] for more details. |
||
− | === DT configuration (STM32 level) === |
+ | === DT configuration (STM32/SoC level) === |
− | The |
+ | The [[BSEC_internal_peripheral|BSEC]] node and [[NVMEM_overview#Device_tree_configuration|NVMEM]] node are located in the [[STM32 MPU device_tree#Device tree structure|device tree file]] for the software components, supporting the peripheral and listed in the above [[#DT bindings documentation|DT bindings documentation]] paragraph. |
− | + | {{Warning|This device tree part is related to STM32 microprocessors. It must be kept as is, without being modified by the end-user.}} |
|
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
=== DT configuration (board level) === |
=== DT configuration (board level) === |
||
− | |||
− | |||
− | + |
The objective of this chapter is to explain how to enable and configure the [[BSEC_internal_peripheral|BSEC]] DT nodes for a board. |
|
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | + |
Peripheral configuration should be done in specific board device tree files (board dts file). |
|
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | The |
+ | ==== BSEC node append ==== |
− | + | The board definition in the device tree may include some additional board-specific OTP declarations, for example to add a NVMEM data cell: |
|
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
&bsec { |
&bsec { |
||
+ | calib@20 { |
||
+ | reg = <0x20 0x2>; |
||
+ | }; |
||
board_id: board_id@ec { |
board_id: board_id@ec { |
||
reg = <0xec 0x4>; |
reg = <0xec 0x4>; |
||
+ | {{highlightParam|st,non-secure-otp}}; |
||
}; |
}; |
||
− | + | oem_enc_key@170 { |
|
− | + | reg = <0x170 0x10>; |
|
− | + | {{highlightParam|st,non-secure-otp-provisioning}}; |
|
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | reg = <0x10 |
||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
}; |
}; |
||
}; |
}; |
||
− | |||
− | + |
Only the 32 lower NVMEM 32-bit data words are accessible by the non-secure world by default; the '''secure world software''' (OP-TEE or SP-MIN) needs to manage exceptions to allow some upper OTPs to be accessed by the non-secure world, through secure world services for very specific needs as described in {{CodeSource | OP-TEE_OS | documentation/devicetree/bindings/nvmem/st,stm32-romem.yaml}}. |
|
− | |||
− | |||
− | |||
− | |||
− | |||
− | + | {{Warning| These upper OTP 32-bit length words are ECC-protected. To avoid an invalid ECC, computed after a second write operation, these 64 upper OTPs should be be permanent write locked when they are programmed.}} |
|
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | + |
This exceptions are defined by the OTP declaration in the secure world device tree with a 32-bit length granularity (that is, 4 bytes): |
|
− | + |
* using the {{highlightParam|st,non-secure-otp}} property to allow a read/write
|
|
− | + |
* using the {{highlightParam|st,non-secure-otp-provisioning}} property to allow a write until the first programmed value or permanent lock; used for secrets used by secure world but provisioned by the non-secured world.
|
|
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | |||
− | + |
See example {{CodeSource | OP-TEE_OS | core/arch/arm/dts/stm32mp135f-dk.dts}}. |
|
==How to configure the DT using STM32CubeMX== |
==How to configure the DT using STM32CubeMX== |
||
− | The [[STM32CubeMX]] tool can be used to configure the STM32MPU device and get the corresponding [[Device_tree# |
+ | The [[STM32CubeMX]] tool can be used to configure the STM32MPU device and get the corresponding [[Device_tree#STM32_MPU|platform configuration device tree]] files.<br /> |
− | STM32CubeMX may not support all the properties described in |
+ | STM32CubeMX may not support all the properties described in DT binding files listed in the above [[#DT bindings documentation|DT bindings documentation]] paragraph. If so, the tool inserts '''user sections''' in the generated device tree. These sections can then be edited to add some properties, and they are preserved from one generation to another. Refer to [[STM32CubeMX]] user manual for further information. |
==References== |
==References== |
||
Line 195: | Line 72: | ||
<noinclude> |
<noinclude> |
||
[[Category:Device tree configuration]] |
[[Category:Device tree configuration]] |
||
− | [[Category: |
+ | [[Category:OP-TEE Persistent storage]] |
{{ArticleBasedOnModel | Peripheral or framework device tree configuration model}} |
{{ArticleBasedOnModel | Peripheral or framework device tree configuration model}} |
||
− | {{PublicationRequestId | 13613 |
+ | {{PublicationRequestId | 15044 | 2020-02-21 | 13613 (PhilipS - 2019-10-09))}} |
</noinclude> |
</noinclude> |