Approved version. Approved on: 15:07, 12 October 2021
- Last edited 5 months ago ago
Audio troubleshooting grid
Revision as of 14:36, 24 October 2022 by Jean Christophe Trotin (talk | contribs)
Some typical issues related to the audio domain are listed below. Solutions or debugging methods are proposed for these issues.
If your issue is not listed, try looking at in the articles in the Audio or troubleshooting grids categories.
Symptom | Resolution | |
---|---|---|
ALSA | ||
The sound card does not probe. | If one or more audio interfaces are missing, the sound card cannot probe:
| |
aplay: pcm_write:2030: write error: Input/output error |
This error occurs on an audio playback, when audio samples are not output. A possible cause is a wrong configuration of the audio interface:
Refer to Soundcard configuration | |
Error -16 setting sai_ck parent clock. Active stream rates conflict |
The two SAI sub blocks which are connected to the audio codec, share their master clock on Disco and Evaluation boards. When running both capture and playback on the codec, the chosen sampling rates must be multiple of each other, because of this dependency. If sampling rates are not compatible, an error is issued. | |
Miscellaneous | ||
Silence is recorded from headset microphone. | The following points have to be checked:
|
|
The capture level is too low at maximum volume. | The ALSA plugin softvol [1] can be used to boost the volume. However, this may lead to saturation. |