Difference between revisions of "Arm Cortex-M4"
[quality revision] | [quality revision] |
Gerald Baeza (talk | contribs)
m (→Boot time)
|
m
|
Applicable for | STM32MP15x lines |
Contents
1 Article purpose[edit]
The purpose of this article is to:
- briefly introduce the Arm® Cortex®-M4 core and its main features
- indicate the level of security supported by this processor
2 Peripheral overview[edit]
The Arm Cortex-M4 is seen as a coprocessor on STM32MP15, where the Arm Cortex-A7 is the main processor that controls it. The Cortex-M4 is present across all the STM32MP15x lines.
2.1 Features[edit]
The Cortex-M4 is a 32-bit processor that belongs to the Armv7E-M architecture family. Armv7E-M corresponds to the ARMv7-M architecture, with DSP extension. Among a wide range of features, it includes a memory protection unit (MPU) and a single-precision floating point unit (FPU).
Refer to the STM32MP15 reference manuals for the complete list of features.
2.2 Security support[edit]
The Cortex-M4 does not support secure mode: it only supports a non-secure mode that defines the Cortex-M4 non-secure hardware execution context.
3 Peripheral usage and associated software[edit]
3.1 Boot time[edit]
The STM32CubeMP1 package execution startup on the Cortex-M4 coprocessor is controlled by the Cortex-A7, that is running the OpenSTLinux distribution.
The coprocessor startup can be done at two different stages of the boot chain:
- by U-Boot SSBL, as explained in the How to start the coprocessor from the bootloader article
- by Linux remoteproc, by default
Thanks to a specific OP-TEE trusted application (TA) running on the Arm® TrustZone and to the ETZPC peripheral, it is possible to authenticate the Cortex®-M4 firmware and install it on isolated MCU RAM to ensure its integrity during the execution. For details, please refer to How_to_protect_the_coprocessor_firmware article.
3.2 Runtime[edit]
3.2.1 Overview[edit]
The Cortex-M4 runs the STM32CubeMP1 package.
The Cortex-M4 operates as a coprocessor, either autonomously as any external microcontroller (such as an STM32F4) could, or communicating with the main processor (Cortex-A7) via the RPMsg communication pipe.
3.2.2 Software frameworks[edit]
Domain | Peripheral | Software components | Comment | ||
---|---|---|---|---|---|
OP-TEE | Linux | STM32Cube | |||
Ecosystem | Cortex-M4 | STM32CubeMP1 package |
3.2.3 Peripheral configuration[edit]
The Cortex-M4 configuration is done in two steps:
- As the main processor of the system, the Cortex-A7 (running OpenSTLinux distribution) first takes care of the initialization of all system resources: supplies, clock tree, and so on.
- The STM32CubeMP1 package then takes care of all the Cortex-M4 local configuration (NVIC, MPU, and so on). It can rely on the resource manager to modify system resources without interfering with the Cortex-A7.
3.2.4 Peripheral assignment[edit]
The Cortex-M4 is the Cortex-A7's coprocessor, so it cannot assign peripheral to its usage but it manages all the peripherals assigned to its context.
4 How to go further[edit]
Refer to the Arm website[1] for more detailed information on this core.
5 References[edit]
==<noinclude>{{ApplicableFor |MPUs list=STM32MP15x |MPUs checklist=STM32MP13x, STM32MP15x }}</noinclude> ==Article purpose== The purpose of this article is to: * briefly introduce the Arm<sup>®</sup> Cortex<sup>®</sup>-M4 core and its main features * indicate the level of security supported by this processor ==Peripheral overview== The Arm Cortex-M4 is seen as a coprocessor on [[STM32MP15 microprocessor | STM32MP15]], where the [[Arm Cortex-A7]] is the main processor that controls it. The Cortex-M4 is present across all the [[STM32MP15_microprocessor#STM32MP15x_lines | STM32MP15x lines]]. <br /> ===Features=== The Cortex-M4 is a 32-bit processor that belongs to the Armv7E-M architecture family. Armv7E-M corresponds to the ARMv7-M architecture, with DSP extension. Among a wide range of features, it includes a memory protection unit (MPU) and a single-precision floating point unit (FPU). Refer to the [[STM32MP15 resources#Reference manuals|STM32MP15 reference manuals]] for the complete list of features. ===Security support=== The Cortex-M4 '''does not''' support secure mode: it only supports a non-secure mode that defines the Cortex-M4 non-secure [[:Category:STM32_MPU_microprocessor_devices#Hardware_execution_contexts | hardware execution context]]. ==Peripheral usage and associated software== ===Boot time=== The [[STM32CubeMP1 architecture | STM32CubeMP1]] package execution startup on the Cortex-M4 coprocessor is controlled by the Cortex-A7, that is running the [[OpenSTLinux architecture overview | OpenSTLinux]] distribution.<br><br> The coprocessor startup can be done at two different stages of the [[Boot chain overview | boot chain]]: * by U-Boot SSBL, as explained in the [[How to start the coprocessor from the bootloader]] article * by [[Linux remoteproc framework overview | Linux remoteproc]], by default Thanks to a specific [[OP-TEE_overview | OP-TEE trusted application (TA)]] running on the [[Security_overview | Arm<sup>®</sup> TrustZone]] and to the [[ETZPC_internal_peripheral | ETZPC peripheral]], it is possible to authenticate the Cortex<sup>®</sup>-M4 firmware and install it on isolated MCU RAM to ensure its integrity during the execution. For details, please refer to [[How_to_protect_the_coprocessor_firmware]] article. ===Runtime=== ====Overview==== The Cortex-M4 runs the [[STM32CubeMP1 architecture | STM32CubeMP1]] package. <br> <br> The Cortex-M4 operates as a coprocessor, either autonomously as any external microcontroller (such as an STM32F4) could, or communicating with the main processor (Cortex-A7) via the [[Linux RPMsg framework overview|RPMsg]] communication pipe. ====Software frameworks==== {{:STM32MP15_internal_peripherals_software_table_template}} | Ecosystem | [[Arm_Cortex-M4 | Cortex-M4]] | | | [[STM32CubeMP1 architecture | STM32CubeMP1]] package | |- |} ====Peripheral configuration==== The Cortex-M4 configuration is done in two steps: # As the main processor of the system, the Cortex-A7 (running [[OpenSTLinux architecture overview |OpenSTLinux]] distribution) first takes care of the initialization of all system resources: supplies, clock tree, and so on. # The [[STM32CubeMP1 architecture | STM32CubeMP1]] package then takes care of all the Cortex-M4 local configuration (NVIC, MPU, and so on). It can rely on the [[Resource_manager_for_coprocessing | resource manager]] to modify system resources without interfering with the Cortex-A7. ====Peripheral assignment==== The Cortex-M4 is the Cortex-A7's coprocessor, so it cannot assign peripheral to its usage but it manages all the peripherals assigned to its context. ==How to go further== Refer to the Arm website<ref>[https://developer.arm.com/ip-products/processors/cortex-m/cortex-m4 Cortex-M4 processor on Arm developer website]</ref> for more detailed information on this core. ==References==<references/> <noinclude> {{ArticleBasedOnModel | Internal peripheral article model}} [[Category:Arm processors]] {{PublicationRequestId | 19286 | 2021-03-10 | }}<noinclude>
Line 1: | Line 1: | ||
+ | <noinclude>{{ApplicableFor |
||
+ | |MPUs list=STM32MP15x |
||
+ | |MPUs checklist=STM32MP13x, STM32MP15x |
||
+ | }}</noinclude> |
||
==Article purpose== |
==Article purpose== |
||
The purpose of this article is to: |
The purpose of this article is to: |