Approved version. Approved on: 15:58, 16 March 2023
- Last edited one year ago ago
Board$
1 Usage
The Board$ template is used to prefix a command that must be executed on a board, with a board-specific prompt.
Thanks to the board-prompt
class defined in MediaWiki:Common.css, a double (or triple) click to select the command doesn't select the prompt.
Usage: {{Board$}}
2 Basic examples
You type | You get |
---|---|
ls test command executed on the board
{{Board$}}ls test<br> test1.txt test2.txt |
ls test |
3 More examples
You type | You get |
---|---|
2 commands executed on the board and preformatted text block (space at the beginning of each line)
{{Board$}}ls test test1.txt test2.txt {{Board$}}cat test/test1.txt This is a test |
ls test test1.txt test2.txt cat test/test1.txt This is a test |
Command executed on the board and preformatted text block (space at the beginning of each line)
{{Board$}}ls test test1.txt test2.txt |
ls test test1.txt test2.txt |
Long command executed on the board and preformatted text block (space at the beginning of each line)
{{Board$}}this is a so long command executed on the board that a horizontal scrolling bar is needed |
this is a so long command executed on the board that a horizontal scrolling bar is needed |
Template used within another public message box template
{{Info | Message before the command {{Board$}}ls test test1.txt test2.txt Message after the command }} |
|
Template used within another protected message box template
{{InternalInfo | Message before the command {{Board$}}ls test test1.txt test2.txt Message after the command }} |
4 Maintenance
This template is a template common to all ST wikis.
Modifications must be done into the WikiModel. They must be reviewed by all ST wikis maintainers.
When approved, the template can be pushed/merged towards all ST wikis.
5 Code