This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Libiio is a complete library which offers tools and an interface to develop an application using IIO subsystem.
1 Article purpose[edit source]
The purpose of this article is to:
- briefly introduce the libiio main features and API
- provide few examples, using libiio tools
2 Introduction[edit source]
- Libiio is a user space library that provides an interface for user space applications. It is basically a wrapper that resides above the following interfaces:
- /sys/bus/iio/devices sysfs interface (for configuration/setting)
- /dev/iio/deviceX device interface (for data)
- Libiio also provides tools that can be used for testing
- Libiio design goals:
- Interface with the kernel, to access IIO[1] devices
- Provide proper data structures and functions to the user application
- Support for local and remote backends allowing applications to access the devices when running on a local or a remote machine
The full description of the IIO library is provided by the author of the library, see below references:
3 API description[edit source]
The API description can be found here: https://analogdevicesinc.github.io/libiio
4 Tools[edit source]
Libiio offers tools such as:
- iiod server daemon
- iio_info to dump attributes
root@stm32mp1:~# iio_info Library version: 0.8 (git tag: v0.8) IIO context created with local backend. Backend version: 0.8 (git tag: v0.8) Backend description string: Linux stm32mp1 4.14.0-00004-gafe4a31 #778 SMP PREEMPT Tue Aug 28 14:02:25 CEST 2018 armv7l IIO context has 3 devices: trigger1: tim6_trgo 0 channels found: 3 device-specific attributes found: attr 0: sampling_frequency value: 100 attr 1: master_mode value: reset attr 2: master_mode_available value: reset enable update compare_pulse OC1REF OC2REF OC3REF OC4REF iio:device0: 48003000.adc:adc@0 (buffer capable) 2 channels found: voltage0: (input, index: 0, format: le:U16/16>>0) 3 channel-specific attributes found: attr 0: raw value: 72 attr 1: offset value: 0 attr 2: scale value: 0.044250488 voltage1: (input, index: 1, format: le:U16/16>>0) 3 channel-specific attributes found: attr 0: raw value: 1746 attr 1: offset value: 0 attr 2: scale value: 0.044250488 ...
- iio_readdev[4] (to read or scan from a device)
STM32AP [rc=0]# iio_readdev -t trigger1 -s 8 -b 8 iio:device0 voltage0 voltage1 | hexdump 0000000 0068 055a 0058 0520 00b4 03df 0070 055f 0000010 0096 03d6 0089 038f 0077 05c8 0096 03b3
See also: How to use the IIO user space interface
5 Source code[edit source]
Libiio can be downloaded on a public github[5]. It can be cloned using git command:
git clone https://github.com/analogdevicesinc/libiio.git
Tools source code can be found under libiio "tests" directory.
6 Installation on your target[edit source]
Libiio and the tools it provides are embedded by default in OpenSTLinux distribution.
7 References[edit source]
- ↑ IIO overview, IIO subsystem overview
- ↑ https://wiki.analog.com/resources/tools-software/linux-software/libiio, What is libiio
- ↑ https://wiki.analog.com/resources/tools-software/linux-software/libiio_internals, About libiio
- ↑ https://wiki.analog.com/resources/tools-software/linux-software/libiio/iio_readdev, iio_readdev
- ↑ https://github.com/analogdevicesinc/libiio, libiio download link