This page aims to provide links to archived wikis.
Each STM32 MPU ecosystem release flow has its corresponding wiki.
An ecosystem release flow designates all the ecosystem releases which are based on the same versions of the major software components (e.g. Linux® kernel) of the OpenSTLinux distribution (see details in the table).
Each vx flow groups together all the vx.y.z ecosystem releases, and has its own wiki.
The most recent flow is associated with the latest wiki also known as flagship wiki (whose URL is "https://wiki.st.com/stm32mpu"), while the previous flows are associated with archived wikis (whose URLs are "https://wiki.st.com/stm32mpu-ecosystem-vx").
The flagship wiki is for the v5 flow (v5.y.z ecosystem releases): if you discover the STM32 Arm® Cortex®-based MPUs, it is highly recommended to continue browsing the wiki that contains the latest major ecosystem release for STM32MP1 series.
However, if you need information about any previous ecosystem releases flow, browse the associated wiki thanks to the below table:
STM32 MP1 archived wiki for the v4.y.z ecosystem releases Not recommended for new design | |
STM32 MP15 archived wiki for the v3.y.z ecosystem releases Not recommended for new design | |
STM32 MP15 archived wiki for the v2.y.z ecosystem releases Not recommended for new design - Those releases are now deprecated | |
STM32 MP15 archived wiki for the v1.y.z ecosystem releases - Not recommended for new design - Those releases are now deprecated |
Wiki | Major ecosystem releases | Major software components (OpenSTLinux distribution) |
---|---|---|
This wiki dedicated to STM32MP1 v5 flow |
v5.0.0 |
Linux® kernel v6.1 (LTS) |
Archived wiki for the v4 flow |
v4.1.0 |
Linux® kernel v5.15 (LTS) |
Archived wiki for the v3 flow |
v3.1.0 |
Linux® kernel v5.10 (LTS) |
Archived wiki for the v2 flow |
Those releases are now deprecated |
Linux® kernel v5.4 (LTS) |
Archived wiki for the v1 flow |
Those releases are now deprecated |
Linux® kernel v4.19 (LTS) |